]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/shortlog
android-sdk/kernel-video.git
2016-03-03 Hannes Frederic... unix: correctly track in-flight fds in sending process...
2016-03-03 Manish Choprabnx2x: Don't notify about scratchpad parities
2016-03-03 Olga KornievskaiaFailing to send a CLOSE if file is opened WRONLY and...
2016-03-03 Christophe... splice: sendfile() at once fails for big files
2016-03-03 Sasha LevinRDS: verify the underlying transport exists before...
2016-03-03 Marcelo Leitneripv6: addrconf: validate new MTU before applying it
2016-03-03 James HoganMIPS: KVM: Uninit VCPU in vcpu_create error path
2016-03-03 James HoganMIPS: KVM: Fix CACHE immediate offset sign extension
2016-03-03 James HoganMIPS: KVM: Fix ASID restoration logic
2016-03-03 Al Virolock_parent: don't step on stale ->d_parent of all...
2016-03-03 Linus Torvaldsdcache: add missing lockdep annotation
2016-03-03 Al Virodentry_kill() doesn't need the second argument now
2016-03-03 Al Virodealing with the rest of shrink_dentry_list() livelock
2016-03-03 Al Viroshrink_dentry_list(): take parent's ->d_lock earlier
2016-03-03 Al Viroexpand dentry_kill(dentry, 0) in shrink_dentry_list()
2016-03-03 Al Virosplit dentry_kill()
2016-03-03 Al Virolift the "already marked killed" case into shrink_dentr...
2016-03-03 Hariprasad Siw_cxgb3: Fix incorrectly returning error on success
2016-03-03 Corey Wrightproc: Fix ptrace-based permission checks for accessing...
2016-03-03 Bjørn MorkUSB: option: add "4G LTE usb-modem U901"
2016-03-03 Andrey SkvortsovUSB: option: add support for SIM7100E
2016-03-03 Ken LinUSB: cp210x: add IDs for GE B650V3 and B850V3 boards
2016-03-03 Gerhard Uttenthalercan: ems_usb: Fix possible tx overflow
2016-03-03 Nikolay Borisovdm thin: fix race condition when destroying thin pool...
2016-03-03 Joe Thornberdm thin metadata: fix bug when taking a metadata snapshot
2016-03-03 Mike Snitzerdm thin: restore requested 'error_if_no_space' setting...
2016-03-03 Ingo Molnarefi: Disable interrupts around EFI calls, not in the...
2016-03-03 Dave Airliedrm/radeon: fix hotplug race at startup
2016-03-03 Kamal Mostafatools: Add a "make all" rule
2016-03-03 Kent Overstreetbcache: Change refill_dirty() to always scan entire...
2016-03-03 Stefan Baderbcache: prevent crash on changing writeback_running
2016-03-03 Zheng Liubcache: unregister reboot notifier if bcache fails...
2016-03-03 Al Virobcache: fix a leak in bch_cached_dev_run()
2016-03-03 Zheng Liubcache: clear BCACHE_DEV_UNLINK_DONE flag when attachin...
2016-03-03 Kent Overstreetbcache: Add a cond_resched() call to gc
2016-03-03 Zheng Liubcache: fix a livelock when we cause a huge number...
2016-03-03 Phil Sutternetfilter: ip6t_SYNPROXY: fix NULL pointer dereference
2016-03-03 luciennetfilter: ipt_rpfilter: remove the nh_scope test in...
2016-03-03 Mirek Kratochvilnetfilter: nf_tables: fix bogus warning in nft_data_uni...
2016-03-03 Egbert Eichdrm/ast: Initialized data needed to map fbdev memory
2016-03-03 Steven Rostedt... tracepoints: Do not trace when cpu is offline
2016-03-03 Praneeth BajjuriMerge branch 'ti-linux-3.14.y' of git://git.ti.com...
2016-03-03 Rob Clarkdrm/omap: EBUSY status handling in omap_gem_fault()
2016-03-03 Praneeth BajjuriMerge branch 'rpmsg-ti-linux-3.14.y' of git://git.ti...
2016-03-01 Suman AnnaMerge branch 'rpmsg-linux-3.14.y' of git://git.ti.com...
2016-03-01 Karthik Ramanannet/rpmsg: fix a use after free error
2016-03-01 Suman Annanet/rpmsg: fix autoloading of rpmsg-proto driver
2016-03-01 Angela Stegmaierrpmsg: fix a lockdep warning in virtio rpmsg driver
2016-02-27 Suman Annarpmsg: rpc: fix return values in rppc_local_to_remote_da
2016-02-27 Suman AnnaMerge branch 'rproc-linux-3.14.y' of git://git.ti.com...
2016-02-26 LCPD Auto MergerMerge tag 'v3.14.62' of http://git.kernel.org/pub/scm...
2016-02-26 Felipe Balbiremoteproc/pruss: fix couple of NULL pointer dereferences
2016-02-26 Suman Annaremoteproc/pruss: use %pa for printing phys_addr_t
2016-02-26 Suman Annaremoteproc/pruss: remove dead rproc_put() in pruss...
2016-02-26 Suman AnnaMerge branch 'iommu-linux-3.14.y' of git://git.ti.com...
2016-02-26 Suman AnnaARM: OMAP2+: iommu: fix sleeping lock usage in atomic...
2016-02-26 Joerg Roedeliommu/omap: Print phys_addr_t using %pa
2016-02-25 Praneeth BajjuriMerge branch 'p-ti-linux-3.14.y-common/audio-for-next...
2016-02-25 Greg Kroah... Linux 3.14.62
2016-02-25 Rusty Russellmodule: wrapper for symbol name.
2016-02-25 WANG Congip6mr: call del_timer_sync() in ip6mr_free_table()
2016-02-25 Thomas Gleixnerfutex: Drop refcount if requeue_pi() acquired the rtmutex
2016-02-25 Dan Carpenterintel_scu_ipcutil: underflow in scu_reg_access()
2016-02-25 Eric Dumazetdump_stack: avoid potential deadlocks
2016-02-25 Konstantin... radix-tree: fix oops after radix_tree_iter_retry
2016-02-25 Matthew Wilcoxradix-tree: fix race in gang lookup
2016-02-25 Martijn Coenenmemcg: only free spare array when readers are done
2016-02-25 Sergey Senozhatskyscripts/bloat-o-meter: fix python3 syntax error
2016-02-25 Laura Abbottdma-debug: switch check from _text to _stext
2016-02-25 Daniel Mentzdma-debug: Fix dma_debug_entry offset calculation
2016-02-25 Sudip Mukherjeem32r: fix m32104ut_defconfig build fail
2016-02-25 Mathias Nymanxhci: Fix list corruption in urb dequeue at host removal
2016-02-25 Andrew Banmanmm/memory_hotplug.c: check for missing sections in...
2016-02-25 CQ Tangiommu/vt-d: Fix 64-bit accesses to 32-bit DMAR_GSTS_REG
2016-02-25 Aurélien FrancillonInput: i8042 - add Fujitsu Lifebook U745 to the nomux...
2016-02-25 Benjamin TissoiresInput: elantech - mark protocols v2 and v3 as semi-mt
2016-02-25 Takashi IwaiInput: elantech - add Fujitsu Lifebook U745 to force...
2016-02-25 Naoya Horiguchimm: soft-offline: check return value in second __get_an...
2016-02-25 Roman Gushchinfuse: break infinite loop in fuse_fill_write_pages()
2016-02-25 Thomas HuthKVM: PPC: Fix emulation of H_SET_DABR/X on POWER8
2016-02-25 Linus WalleijARM: 8517/1: ICST: avoid arithmetic overflow in icst_hz()
2016-02-25 Linus WalleijARM: 8519/1: ICST: try other dividends than 1
2016-02-25 Anson HuangARM: 8471/1: need to save/restore arm register(r11...
2016-02-25 Helmut KleinARM: dts: Kirkwood: Fix QNAP TS219 power-off
2016-02-25 Andrew Gabbasovudf: Check output buffer length when converting name...
2016-02-25 Andrew Gabbasovudf: Prevent buffer overrun with multi-byte characters
2016-02-25 Vegard Nossumudf: limit the maximum number of indirect extents in...
2016-02-25 Andrew Elblenfs: Fix race in __update_open_stateid()
2016-02-25 Anton Protopopovcifs: fix erroneous return value
2016-02-25 Vasily Averincifs_dbg() outputs an uninitialized buffer in cifs_read...
2016-02-25 Yong Liiio: dac: mcp4725: set iio name property in sysfs
2016-02-25 Lars-Peter... iio: adis_buffer: Fix out-of-bounds memory access
2016-02-25 Dan Carpenteriio: fix some warning messages
2016-02-25 Lars-Peter... iio: ad5064: Fix ad5629/ad5669 shift
2016-02-25 Michael Hennerichiio:ad5064: Make sure ad5064_i2c_write() returns 0...
2016-02-25 Vladimir Zapolskiyiio: lpc32xx_adc: fix warnings caused by enabling unpre...
2016-02-25 Lars-Peter... iio:ad7793: Fix ad7785 product ID
2016-02-25 James Bottomleyscsi: fix soft lockup in scsi_remove_target() on module...
2016-02-25 Mika WesterbergSCSI: Add Marvell Console to VPD blacklist
2016-02-25 Hannes Reineckescsi_dh_rdac: always retry MODE SELECT on command lock...
next