1 /*
2 * Copyright (C) 2008 The Android Open Source Project
3 * All rights reserved.
4 *
5 * Redistribution and use in source and binary forms, with or without
6 * modification, are permitted provided that the following conditions
7 * are met:
8 * * Redistributions of source code must retain the above copyright
9 * notice, this list of conditions and the following disclaimer.
10 * * Redistributions in binary form must reproduce the above copyright
11 * notice, this list of conditions and the following disclaimer in
12 * the documentation and/or other materials provided with the
13 * distribution.
14 *
15 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
16 * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
17 * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS
18 * FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE
19 * COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT,
20 * INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING,
21 * BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS
22 * OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED
23 * AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
24 * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT
25 * OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF
26 * SUCH DAMAGE.
27 */
29 #include <machine/cpu-features.h>
31 #if defined(__ARM_NEON__)
33 .text
34 .fpu neon
36 .global memcpy
37 .type memcpy, %function
38 .align 4
40 /* a prefetch distance of 4 cache-lines works best experimentally */
41 #define CACHE_LINE_SIZE 64
42 #define PREFETCH_DISTANCE (CACHE_LINE_SIZE*4)
44 memcpy:
45 .fnstart
46 .save {r0, lr}
47 stmfd sp!, {r0, lr}
49 /* start preloading as early as possible */
50 pld [r1, #(CACHE_LINE_SIZE*0)]
51 pld [r1, #(CACHE_LINE_SIZE*1)]
53 /* do we have at least 16-bytes to copy (needed for alignment below) */
54 cmp r2, #16
55 blo 5f
57 /* align destination to half cache-line for the write-buffer */
58 rsb r3, r0, #0
59 ands r3, r3, #0xF
60 beq 0f
62 /* copy up to 15-bytes (count in r3) */
63 sub r2, r2, r3
64 movs ip, r3, lsl #31
65 ldrmib lr, [r1], #1
66 strmib lr, [r0], #1
67 ldrcsb ip, [r1], #1
68 ldrcsb lr, [r1], #1
69 strcsb ip, [r0], #1
70 strcsb lr, [r0], #1
71 movs ip, r3, lsl #29
72 bge 1f
73 // copies 4 bytes, destination 32-bits aligned
74 vld4.8 {d0[0], d1[0], d2[0], d3[0]}, [r1]!
75 vst4.8 {d0[0], d1[0], d2[0], d3[0]}, [r0, :32]!
76 1: bcc 2f
77 // copies 8 bytes, destination 64-bits aligned
78 vld1.8 {d0}, [r1]!
79 vst1.8 {d0}, [r0, :64]!
80 2:
82 0: /* preload immediately the next cache line, which we may need */
83 pld [r1, #(CACHE_LINE_SIZE*0)]
84 pld [r1, #(CACHE_LINE_SIZE*1)]
86 /* make sure we have at least 64 bytes to copy */
87 subs r2, r2, #64
88 blo 2f
90 /* preload all the cache lines we need.
91 * NOTE: the number of pld below depends on PREFETCH_DISTANCE,
92 * ideally would would increase the distance in the main loop to
93 * avoid the goofy code below. In practice this doesn't seem to make
94 * a big difference.
95 */
96 pld [r1, #(CACHE_LINE_SIZE*2)]
97 pld [r1, #(CACHE_LINE_SIZE*3)]
98 pld [r1, #(PREFETCH_DISTANCE)]
100 1: /* The main loop copies 64 bytes at a time */
101 vld1.8 {d0 - d3}, [r1]!
102 vld1.8 {d4 - d7}, [r1]!
103 pld [r1, #(PREFETCH_DISTANCE)]
104 subs r2, r2, #64
105 vst1.8 {d0 - d3}, [r0, :128]!
106 vst1.8 {d4 - d7}, [r0, :128]!
107 bhs 1b
109 2: /* fix-up the remaining count and make sure we have >= 32 bytes left */
110 add r2, r2, #64
111 subs r2, r2, #32
112 blo 4f
114 3: /* 32 bytes at a time. These cache lines were already preloaded */
115 vld1.8 {d0 - d3}, [r1]!
116 subs r2, r2, #32
117 vst1.8 {d0 - d3}, [r0, :128]!
118 bhs 3b
120 4: /* less than 32 left */
121 add r2, r2, #32
122 tst r2, #0x10
123 beq 5f
124 // copies 16 bytes, 128-bits aligned
125 vld1.8 {d0, d1}, [r1]!
126 vst1.8 {d0, d1}, [r0, :128]!
128 5: /* copy up to 15-bytes (count in r2) */
129 movs ip, r2, lsl #29
130 bcc 1f
131 vld1.8 {d0}, [r1]!
132 vst1.8 {d0}, [r0]!
133 1: bge 2f
134 vld4.8 {d0[0], d1[0], d2[0], d3[0]}, [r1]!
135 vst4.8 {d0[0], d1[0], d2[0], d3[0]}, [r0]!
136 2: movs ip, r2, lsl #31
137 ldrmib r3, [r1], #1
138 ldrcsb ip, [r1], #1
139 ldrcsb lr, [r1], #1
140 strmib r3, [r0], #1
141 strcsb ip, [r0], #1
142 strcsb lr, [r0], #1
144 ldmfd sp!, {r0, lr}
145 bx lr
146 .fnend
149 #else /* __ARM_ARCH__ < 7 */
152 .text
154 .global memcpy
155 .type memcpy, %function
156 .align 4
158 /*
159 * Optimized memcpy() for ARM.
160 *
161 * note that memcpy() always returns the destination pointer,
162 * so we have to preserve R0.
163 */
165 memcpy:
166 /* The stack must always be 64-bits aligned to be compliant with the
167 * ARM ABI. Since we have to save R0, we might as well save R4
168 * which we can use for better pipelining of the reads below
169 */
170 .fnstart
171 .save {r0, r4, lr}
172 stmfd sp!, {r0, r4, lr}
173 /* Making room for r5-r11 which will be spilled later */
174 .pad #28
175 sub sp, sp, #28
177 // preload the destination because we'll align it to a cache line
178 // with small writes. Also start the source "pump".
179 PLD (r0, #0)
180 PLD (r1, #0)
181 PLD (r1, #32)
183 /* it simplifies things to take care of len<4 early */
184 cmp r2, #4
185 blo copy_last_3_and_return
187 /* compute the offset to align the source
188 * offset = (4-(src&3))&3 = -src & 3
189 */
190 rsb r3, r1, #0
191 ands r3, r3, #3
192 beq src_aligned
194 /* align source to 32 bits. We need to insert 2 instructions between
195 * a ldr[b|h] and str[b|h] because byte and half-word instructions
196 * stall 2 cycles.
197 */
198 movs r12, r3, lsl #31
199 sub r2, r2, r3 /* we know that r3 <= r2 because r2 >= 4 */
200 ldrmib r3, [r1], #1
201 ldrcsb r4, [r1], #1
202 ldrcsb r12,[r1], #1
203 strmib r3, [r0], #1
204 strcsb r4, [r0], #1
205 strcsb r12,[r0], #1
207 src_aligned:
209 /* see if src and dst are aligned together (congruent) */
210 eor r12, r0, r1
211 tst r12, #3
212 bne non_congruent
214 /* Use post-incriment mode for stm to spill r5-r11 to reserved stack
215 * frame. Don't update sp.
216 */
217 stmea sp, {r5-r11}
219 /* align the destination to a cache-line */
220 rsb r3, r0, #0
221 ands r3, r3, #0x1C
222 beq congruent_aligned32
223 cmp r3, r2
224 andhi r3, r2, #0x1C
226 /* conditionnaly copies 0 to 7 words (length in r3) */
227 movs r12, r3, lsl #28
228 ldmcsia r1!, {r4, r5, r6, r7} /* 16 bytes */
229 ldmmiia r1!, {r8, r9} /* 8 bytes */
230 stmcsia r0!, {r4, r5, r6, r7}
231 stmmiia r0!, {r8, r9}
232 tst r3, #0x4
233 ldrne r10,[r1], #4 /* 4 bytes */
234 strne r10,[r0], #4
235 sub r2, r2, r3
237 congruent_aligned32:
238 /*
239 * here source is aligned to 32 bytes.
240 */
242 cached_aligned32:
243 subs r2, r2, #32
244 blo less_than_32_left
246 /*
247 * We preload a cache-line up to 64 bytes ahead. On the 926, this will
248 * stall only until the requested world is fetched, but the linefill
249 * continues in the the background.
250 * While the linefill is going, we write our previous cache-line
251 * into the write-buffer (which should have some free space).
252 * When the linefill is done, the writebuffer will
253 * start dumping its content into memory
254 *
255 * While all this is going, we then load a full cache line into
256 * 8 registers, this cache line should be in the cache by now
257 * (or partly in the cache).
258 *
259 * This code should work well regardless of the source/dest alignment.
260 *
261 */
263 // Align the preload register to a cache-line because the cpu does
264 // "critical word first" (the first word requested is loaded first).
265 bic r12, r1, #0x1F
266 add r12, r12, #64
268 1: ldmia r1!, { r4-r11 }
269 PLD (r12, #64)
270 subs r2, r2, #32
272 // NOTE: if r12 is more than 64 ahead of r1, the following ldrhi
273 // for ARM9 preload will not be safely guarded by the preceding subs.
274 // When it is safely guarded the only possibility to have SIGSEGV here
275 // is because the caller overstates the length.
276 ldrhi r3, [r12], #32 /* cheap ARM9 preload */
277 stmia r0!, { r4-r11 }
278 bhs 1b
280 add r2, r2, #32
285 less_than_32_left:
286 /*
287 * less than 32 bytes left at this point (length in r2)
288 */
290 /* skip all this if there is nothing to do, which should
291 * be a common case (if not executed the code below takes
292 * about 16 cycles)
293 */
294 tst r2, #0x1F
295 beq 1f
297 /* conditionnaly copies 0 to 31 bytes */
298 movs r12, r2, lsl #28
299 ldmcsia r1!, {r4, r5, r6, r7} /* 16 bytes */
300 ldmmiia r1!, {r8, r9} /* 8 bytes */
301 stmcsia r0!, {r4, r5, r6, r7}
302 stmmiia r0!, {r8, r9}
303 movs r12, r2, lsl #30
304 ldrcs r3, [r1], #4 /* 4 bytes */
305 ldrmih r4, [r1], #2 /* 2 bytes */
306 strcs r3, [r0], #4
307 strmih r4, [r0], #2
308 tst r2, #0x1
309 ldrneb r3, [r1] /* last byte */
310 strneb r3, [r0]
312 /* we're done! restore everything and return */
313 1: ldmfd sp!, {r5-r11}
314 ldmfd sp!, {r0, r4, lr}
315 bx lr
317 /********************************************************************/
319 non_congruent:
320 /*
321 * here source is aligned to 4 bytes
322 * but destination is not.
323 *
324 * in the code below r2 is the number of bytes read
325 * (the number of bytes written is always smaller, because we have
326 * partial words in the shift queue)
327 */
328 cmp r2, #4
329 blo copy_last_3_and_return
331 /* Use post-incriment mode for stm to spill r5-r11 to reserved stack
332 * frame. Don't update sp.
333 */
334 stmea sp, {r5-r11}
336 /* compute shifts needed to align src to dest */
337 rsb r5, r0, #0
338 and r5, r5, #3 /* r5 = # bytes in partial words */
339 mov r12, r5, lsl #3 /* r12 = right */
340 rsb lr, r12, #32 /* lr = left */
342 /* read the first word */
343 ldr r3, [r1], #4
344 sub r2, r2, #4
346 /* write a partial word (0 to 3 bytes), such that destination
347 * becomes aligned to 32 bits (r5 = nb of words to copy for alignment)
348 */
349 movs r5, r5, lsl #31
350 strmib r3, [r0], #1
351 movmi r3, r3, lsr #8
352 strcsb r3, [r0], #1
353 movcs r3, r3, lsr #8
354 strcsb r3, [r0], #1
355 movcs r3, r3, lsr #8
357 cmp r2, #4
358 blo partial_word_tail
360 /* Align destination to 32 bytes (cache line boundary) */
361 1: tst r0, #0x1c
362 beq 2f
363 ldr r5, [r1], #4
364 sub r2, r2, #4
365 orr r4, r3, r5, lsl lr
366 mov r3, r5, lsr r12
367 str r4, [r0], #4
368 cmp r2, #4
369 bhs 1b
370 blo partial_word_tail
372 /* copy 32 bytes at a time */
373 2: subs r2, r2, #32
374 blo less_than_thirtytwo
376 /* Use immediate mode for the shifts, because there is an extra cycle
377 * for register shifts, which could account for up to 50% of
378 * performance hit.
379 */
381 cmp r12, #24
382 beq loop24
383 cmp r12, #8
384 beq loop8
386 loop16:
387 ldr r12, [r1], #4
388 1: mov r4, r12
389 ldmia r1!, { r5,r6,r7, r8,r9,r10,r11}
390 PLD (r1, #64)
391 subs r2, r2, #32
392 ldrhs r12, [r1], #4
393 orr r3, r3, r4, lsl #16
394 mov r4, r4, lsr #16
395 orr r4, r4, r5, lsl #16
396 mov r5, r5, lsr #16
397 orr r5, r5, r6, lsl #16
398 mov r6, r6, lsr #16
399 orr r6, r6, r7, lsl #16
400 mov r7, r7, lsr #16
401 orr r7, r7, r8, lsl #16
402 mov r8, r8, lsr #16
403 orr r8, r8, r9, lsl #16
404 mov r9, r9, lsr #16
405 orr r9, r9, r10, lsl #16
406 mov r10, r10, lsr #16
407 orr r10, r10, r11, lsl #16
408 stmia r0!, {r3,r4,r5,r6, r7,r8,r9,r10}
409 mov r3, r11, lsr #16
410 bhs 1b
411 b less_than_thirtytwo
413 loop8:
414 ldr r12, [r1], #4
415 1: mov r4, r12
416 ldmia r1!, { r5,r6,r7, r8,r9,r10,r11}
417 PLD (r1, #64)
418 subs r2, r2, #32
419 ldrhs r12, [r1], #4
420 orr r3, r3, r4, lsl #24
421 mov r4, r4, lsr #8
422 orr r4, r4, r5, lsl #24
423 mov r5, r5, lsr #8
424 orr r5, r5, r6, lsl #24
425 mov r6, r6, lsr #8
426 orr r6, r6, r7, lsl #24
427 mov r7, r7, lsr #8
428 orr r7, r7, r8, lsl #24
429 mov r8, r8, lsr #8
430 orr r8, r8, r9, lsl #24
431 mov r9, r9, lsr #8
432 orr r9, r9, r10, lsl #24
433 mov r10, r10, lsr #8
434 orr r10, r10, r11, lsl #24
435 stmia r0!, {r3,r4,r5,r6, r7,r8,r9,r10}
436 mov r3, r11, lsr #8
437 bhs 1b
438 b less_than_thirtytwo
440 loop24:
441 ldr r12, [r1], #4
442 1: mov r4, r12
443 ldmia r1!, { r5,r6,r7, r8,r9,r10,r11}
444 PLD (r1, #64)
445 subs r2, r2, #32
446 ldrhs r12, [r1], #4
447 orr r3, r3, r4, lsl #8
448 mov r4, r4, lsr #24
449 orr r4, r4, r5, lsl #8
450 mov r5, r5, lsr #24
451 orr r5, r5, r6, lsl #8
452 mov r6, r6, lsr #24
453 orr r6, r6, r7, lsl #8
454 mov r7, r7, lsr #24
455 orr r7, r7, r8, lsl #8
456 mov r8, r8, lsr #24
457 orr r8, r8, r9, lsl #8
458 mov r9, r9, lsr #24
459 orr r9, r9, r10, lsl #8
460 mov r10, r10, lsr #24
461 orr r10, r10, r11, lsl #8
462 stmia r0!, {r3,r4,r5,r6, r7,r8,r9,r10}
463 mov r3, r11, lsr #24
464 bhs 1b
467 less_than_thirtytwo:
468 /* copy the last 0 to 31 bytes of the source */
469 rsb r12, lr, #32 /* we corrupted r12, recompute it */
470 add r2, r2, #32
471 cmp r2, #4
472 blo partial_word_tail
474 1: ldr r5, [r1], #4
475 sub r2, r2, #4
476 orr r4, r3, r5, lsl lr
477 mov r3, r5, lsr r12
478 str r4, [r0], #4
479 cmp r2, #4
480 bhs 1b
482 partial_word_tail:
483 /* we have a partial word in the input buffer */
484 movs r5, lr, lsl #(31-3)
485 strmib r3, [r0], #1
486 movmi r3, r3, lsr #8
487 strcsb r3, [r0], #1
488 movcs r3, r3, lsr #8
489 strcsb r3, [r0], #1
491 /* Refill spilled registers from the stack. Don't update sp. */
492 ldmfd sp, {r5-r11}
494 copy_last_3_and_return:
495 movs r2, r2, lsl #31 /* copy remaining 0, 1, 2 or 3 bytes */
496 ldrmib r2, [r1], #1
497 ldrcsb r3, [r1], #1
498 ldrcsb r12,[r1]
499 strmib r2, [r0], #1
500 strcsb r3, [r0], #1
501 strcsb r12,[r0]
503 /* we're done! restore sp and spilled registers and return */
504 add sp, sp, #28
505 ldmfd sp!, {r0, r4, lr}
506 bx lr
507 .fnend
510 #endif /* __ARM_ARCH__ < 7 */