1 /*
2 * Copyright (C) 2006 The Android Open Source Project
3 *
4 * Licensed under the Apache License, Version 2.0 (the "License");
5 * you may not use this file except in compliance with the License.
6 * You may obtain a copy of the License at
7 *
8 * http://www.apache.org/licenses/LICENSE-2.0
9 *
10 * Unless required by applicable law or agreed to in writing, software
11 * distributed under the License is distributed on an "AS IS" BASIS,
12 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13 * See the License for the specific language governing permissions and
14 * limitations under the License.
15 */
17 #include <stddef.h>
18 #include <endian.h>
20 #include "private/bionic_atomic_inline.h"
21 #include "private/bionic_futex.h"
23 // This file contains C++ ABI support functions for one time
24 // constructors as defined in the "Run-time ABI for the ARM Architecture"
25 // section 4.4.2
26 //
27 // ARM C++ ABI and Itanium/x86 C++ ABI has different definition for
28 // one time construction:
29 //
30 // ARM C++ ABI defines the LSB of guard variable should be tested
31 // by compiler-generated code before calling __cxa_guard_acquire et al.
32 //
33 // The Itanium/x86 C++ ABI defines the low-order _byte_ should be
34 // tested instead.
35 //
36 // Meanwhile, guard variable are 32bit aligned for ARM, and 64bit
37 // aligned for x86.
38 //
39 // Reference documentation:
40 //
41 // section 3.2.3 of ARM IHI 0041C (for ARM)
42 // section 3.3.2 of the Itanium C++ ABI specification v1.83 (for x86).
43 //
44 // There is no C++ ABI available for other ARCH. But the gcc source
45 // shows all other ARCH follow the definition of Itanium/x86 C++ ABI.
47 #if defined(__arm__)
48 // The ARM C++ ABI mandates that guard variables are 32-bit aligned, 32-bit
49 // values. The LSB is tested by the compiler-generated code before calling
50 // __cxa_guard_acquire.
51 union _guard_t {
52 int volatile state;
53 int32_t aligner;
54 };
56 const static int ready = 0x1;
57 const static int pending = 0x2;
58 const static int waiting = 0x6;
60 #else
61 // The Itanium/x86 C++ ABI (used by all other architectures) mandates that
62 // guard variables are 64-bit aligned, 64-bit values. The LSB is tested by
63 // the compiler-generated code before calling __cxa_guard_acquire.
64 union _guard_t {
65 int volatile state;
66 int64_t aligner;
67 };
69 const static int ready = letoh32(0x1);
70 const static int pending = letoh32(0x100);
71 const static int waiting = letoh32(0x10000);
72 #endif
74 extern "C" int __cxa_guard_acquire(_guard_t* gv) {
75 // 0 -> pending, return 1
76 // pending -> waiting, wait and return 0
77 // waiting: untouched, wait and return 0
78 // ready: untouched, return 0
80 retry:
81 if (__bionic_cmpxchg(0, pending, &gv->state) == 0) {
82 ANDROID_MEMBAR_FULL();
83 return 1;
84 }
85 __bionic_cmpxchg(pending, waiting, &gv->state); // Indicate there is a waiter
86 __futex_wait(&gv->state, waiting, NULL);
88 if (gv->state != ready) {
89 // __cxa_guard_abort was called, let every thread try since there is no return code for this condition
90 goto retry;
91 }
93 ANDROID_MEMBAR_FULL();
94 return 0;
95 }
97 extern "C" void __cxa_guard_release(_guard_t* gv) {
98 // pending -> ready
99 // waiting -> ready, and wake
101 ANDROID_MEMBAR_FULL();
102 if (__bionic_cmpxchg(pending, ready, &gv->state) == 0) {
103 return;
104 }
106 gv->state = ready;
107 __futex_wake(&gv->state, 0x7fffffff);
108 }
110 extern "C" void __cxa_guard_abort(_guard_t* gv) {
111 ANDROID_MEMBAR_FULL();
112 gv->state= 0;
113 __futex_wake(&gv->state, 0x7fffffff);
114 }