]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/platform-bionic.git/blob - libc/bionic/legacy_32_bit_support.cpp
Merge "Remove more BSD cruft from the public headers."
[android-sdk/platform-bionic.git] / libc / bionic / legacy_32_bit_support.cpp
1 /*
2  * Copyright (C) 2008 The Android Open Source Project
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *  * Redistributions of source code must retain the above copyright
9  *    notice, this list of conditions and the following disclaimer.
10  *  * Redistributions in binary form must reproduce the above copyright
11  *    notice, this list of conditions and the following disclaimer in
12  *    the documentation and/or other materials provided with the
13  *    distribution.
14  *
15  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
16  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
17  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS
18  * FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE
19  * COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT,
20  * INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING,
21  * BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS
22  * OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED
23  * AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
24  * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT
25  * OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF
26  * SUCH DAMAGE.
27  */
29 #include <errno.h>
30 #include <fcntl.h>
31 #include <stdarg.h>
32 #include <sys/resource.h>
33 #include <sys/types.h>
34 #include <sys/vfs.h>
35 #include <unistd.h>
37 #if __LP64__
38 #error This code is only needed on 32-bit systems!
39 #endif
41 // System calls we need.
42 extern "C" int __fcntl64(int, int, void*);
43 extern "C" int __fstatfs64(int, size_t, struct statfs*);
44 extern "C" int __llseek(int, unsigned long, unsigned long, off64_t*, int);
45 extern "C" int __statfs64(const char*, size_t, struct statfs*);
47 // For fcntl we use the fcntl64 system call to signal that we're using struct flock64.
48 int fcntl(int fd, int cmd, ...) {
49   va_list ap;
51   va_start(ap, cmd);
52   void* arg = va_arg(ap, void*);
53   va_end(ap);
55   return __fcntl64(fd, cmd, arg);
56 }
58 // For fstatfs we need to add the extra argument giving the kernel the size of the buffer.
59 int fstatfs(int fd, struct statfs* stat) {
60   return __fstatfs64(fd, sizeof(*stat), stat);
61 }
62 __strong_alias(fstatfs64, fstatfs);
64 // For statfs we need to add the extra argument giving the kernel the size of the buffer.
65 int statfs(const char* path, struct statfs* stat) {
66   return __statfs64(path, sizeof(*stat), stat);
67 }
68 __strong_alias(statfs64, statfs);
70 // For lseek64 we need to use the llseek system call which splits the off64_t in two and
71 // returns the off64_t result via a pointer because 32-bit kernels can't return 64-bit results.
72 off64_t lseek64(int fd, off64_t off, int whence) {
73   off64_t result;
74   unsigned long off_hi = static_cast<unsigned long>(off >> 32);
75   unsigned long off_lo = static_cast<unsigned long>(off);
76   if (__llseek(fd, off_hi, off_lo, &result, whence) < 0) {
77     return -1;
78   }
79   return result;
80 }
82 // There is no pread for 32-bit off_t, so we need to widen and call pread64.
83 ssize_t pread(int fd, void* buf, size_t byte_count, off_t offset) {
84   return pread64(fd, buf, byte_count, static_cast<off64_t>(offset));
85 }
87 // There is no pwrite for 32-bit off_t, so we need to widen and call pwrite64.
88 ssize_t pwrite(int fd, const void* buf, size_t byte_count, off_t offset) {
89   return pwrite64(fd, buf, byte_count, static_cast<off64_t>(offset));
90 }
92 // There is no fallocate for 32-bit off_t, so we need to widen and call fallocate64.
93 int fallocate(int fd, int mode, off_t offset, off_t length) {
94   return fallocate64(fd, mode, static_cast<off64_t>(offset), static_cast<off64_t>(length));
95 }
97 // There is no getrlimit64 system call, so we need to use prlimit64.
98 int getrlimit64(int resource, rlimit64* limits64) {
99   return prlimit64(0, resource, NULL, limits64);
102 // There is no setrlimit64 system call, so we need to use prlimit64.
103 int setrlimit64(int resource, const rlimit64* limits64) {
104   return prlimit64(0, resource, limits64, NULL);