Use mmap to create the pthread_internal_t
[android-sdk/platform-bionic.git] / libc / bionic / libc_init_common.cpp
1 /*
2  * Copyright (C) 2008 The Android Open Source Project
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *  * Redistributions of source code must retain the above copyright
9  *    notice, this list of conditions and the following disclaimer.
10  *  * Redistributions in binary form must reproduce the above copyright
11  *    notice, this list of conditions and the following disclaimer in
12  *    the documentation and/or other materials provided with the
13  *    distribution.
14  *
15  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
16  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
17  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS
18  * FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE
19  * COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT,
20  * INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING,
21  * BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS
22  * OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED
23  * AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
24  * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT
25  * OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF
26  * SUCH DAMAGE.
27  */
29 #include "libc_init_common.h"
31 #include <elf.h>
32 #include <errno.h>
33 #include <stddef.h>
34 #include <stdint.h>
35 #include <stdio.h>
36 #include <stdlib.h>
37 #include <sys/auxv.h>
38 #include <sys/time.h>
39 #include <unistd.h>
41 #include "private/bionic_auxv.h"
42 #include "private/bionic_ssp.h"
43 #include "private/bionic_tls.h"
44 #include "private/KernelArgumentBlock.h"
45 #include "pthread_internal.h"
47 extern "C" abort_msg_t** __abort_message_ptr;
48 extern "C" int __system_properties_init(void);
49 extern "C" int __set_tls(void* ptr);
50 extern "C" int __set_tid_address(int* tid_address);
52 __LIBC_HIDDEN__ void __libc_init_vdso();
54 // Not public, but well-known in the BSDs.
55 const char* __progname;
57 // Declared in <unistd.h>.
58 char** environ;
60 // Declared in "private/bionic_ssp.h".
61 uintptr_t __stack_chk_guard = 0;
63 /* Init TLS for the initial thread. Called by the linker _before_ libc is mapped
64  * in memory. Beware: all writes to libc globals from this function will
65  * apply to linker-private copies and will not be visible from libc later on.
66  *
67  * Note: this function creates a pthread_internal_t for the initial thread and
68  * stores the pointer in TLS, but does not add it to pthread's thread list. This
69  * has to be done later from libc itself (see __libc_init_common).
70  *
71  * This function also stores a pointer to the kernel argument block in a TLS slot to be
72  * picked up by the libc constructor.
73  */
74 void __libc_init_tls(KernelArgumentBlock& args) {
75   __libc_auxv = args.auxv;
77   static pthread_internal_t main_thread;
79   // Tell the kernel to clear our tid field when we exit, so we're like any other pthread.
80   // As a side-effect, this tells us our pid (which is the same as the main thread's tid).
81   main_thread.tid = __set_tid_address(&main_thread.tid);
82   main_thread.set_cached_pid(main_thread.tid);
84   // We don't want to free the main thread's stack even when the main thread exits
85   // because things like environment variables with global scope live on it.
86   // We also can't free the pthread_internal_t itself, since that lives on the main
87   // thread's stack rather than on the heap.
88   pthread_attr_init(&main_thread.attr);
89   main_thread.attr.flags = PTHREAD_ATTR_FLAG_USER_ALLOCATED_STACK | PTHREAD_ATTR_FLAG_MAIN_THREAD;
90   main_thread.attr.guard_size = 0; // The main thread has no guard page.
91   main_thread.attr.stack_size = 0; // User code should never see this; we'll compute it when asked.
92   // TODO: the main thread's sched_policy and sched_priority need to be queried.
94   __init_thread(&main_thread, false);
95   __init_tls(&main_thread);
96   __set_tls(main_thread.tls);
97   main_thread.tls[TLS_SLOT_BIONIC_PREINIT] = &args;
99   __init_alternate_signal_stack(&main_thread);
102 void __libc_init_common(KernelArgumentBlock& args) {
103   // Initialize various globals.
104   environ = args.envp;
105   errno = 0;
106   __libc_auxv = args.auxv;
107   __progname = args.argv[0] ? args.argv[0] : "<unknown>";
108   __abort_message_ptr = args.abort_message_ptr;
110   // AT_RANDOM is a pointer to 16 bytes of randomness on the stack.
111   __stack_chk_guard = *reinterpret_cast<uintptr_t*>(getauxval(AT_RANDOM));
113   // Get the main thread from TLS and add it to the thread list.
114   pthread_internal_t* main_thread = __get_thread();
115   _pthread_internal_add(main_thread);
117   __system_properties_init(); // Requires 'environ'.
119   __libc_init_vdso();
122 /* This function will be called during normal program termination
123  * to run the destructors that are listed in the .fini_array section
124  * of the executable, if any.
125  *
126  * 'fini_array' points to a list of function addresses. The first
127  * entry in the list has value -1, the last one has value 0.
128  */
129 void __libc_fini(void* array) {
130   void** fini_array = reinterpret_cast<void**>(array);
131   const size_t minus1 = ~(size_t)0; /* ensure proper sign extension */
133   /* Sanity check - first entry must be -1 */
134   if (array == NULL || (size_t)fini_array[0] != minus1) {
135     return;
136   }
138   /* skip over it */
139   fini_array += 1;
141   /* Count the number of destructors. */
142   int count = 0;
143   while (fini_array[count] != NULL) {
144     ++count;
145   }
147   /* Now call each destructor in reverse order. */
148   while (count > 0) {
149     void (*func)() = (void (*)()) fini_array[--count];
151     /* Sanity check, any -1 in the list is ignored */
152     if ((size_t)func == minus1) {
153       continue;
154     }
156     func();
157   }
159 #ifndef LIBC_STATIC
160   {
161     extern void __libc_postfini(void) __attribute__((weak));
162     if (__libc_postfini) {
163       __libc_postfini();
164     }
165   }
166 #endif