Use mmap to create the pthread_internal_t
[android-sdk/platform-bionic.git] / libc / bionic / pthread_create.cpp
1 /*
2  * Copyright (C) 2008 The Android Open Source Project
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *  * Redistributions of source code must retain the above copyright
9  *    notice, this list of conditions and the following disclaimer.
10  *  * Redistributions in binary form must reproduce the above copyright
11  *    notice, this list of conditions and the following disclaimer in
12  *    the documentation and/or other materials provided with the
13  *    distribution.
14  *
15  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
16  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
17  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS
18  * FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE
19  * COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT,
20  * INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING,
21  * BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS
22  * OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED
23  * AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
24  * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT
25  * OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF
26  * SUCH DAMAGE.
27  */
29 #include <pthread.h>
31 #include <errno.h>
32 #include <sys/mman.h>
33 #include <unistd.h>
35 #include "pthread_internal.h"
37 #include "private/bionic_macros.h"
38 #include "private/bionic_prctl.h"
39 #include "private/bionic_ssp.h"
40 #include "private/bionic_tls.h"
41 #include "private/libc_logging.h"
42 #include "private/ErrnoRestorer.h"
43 #include "private/ScopedPthreadMutexLocker.h"
45 // x86 uses segment descriptors rather than a direct pointer to TLS.
46 #if __i386__
47 #include <asm/ldt.h>
48 extern "C" __LIBC_HIDDEN__ void __init_user_desc(struct user_desc*, int, void*);
49 #endif
51 extern "C" int __isthreaded;
53 // This code is used both by each new pthread and the code that initializes the main thread.
54 void __init_tls(pthread_internal_t* thread) {
55   if (thread->user_allocated_stack()) {
56     // We don't know where the user got their stack, so assume the worst and zero the TLS area.
57     memset(&thread->tls[0], 0, BIONIC_TLS_SLOTS * sizeof(void*));
58   }
60   // Slot 0 must point to itself. The x86 Linux kernel reads the TLS from %fs:0.
61   thread->tls[TLS_SLOT_SELF] = thread->tls;
62   thread->tls[TLS_SLOT_THREAD_ID] = thread;
63   // GCC looks in the TLS for the stack guard on x86, so copy it there from our global.
64   thread->tls[TLS_SLOT_STACK_GUARD] = (void*) __stack_chk_guard;
65 }
67 void __init_alternate_signal_stack(pthread_internal_t* thread) {
68   // Create and set an alternate signal stack.
69   stack_t ss;
70   ss.ss_sp = mmap(NULL, SIGSTKSZ, PROT_READ|PROT_WRITE, MAP_PRIVATE|MAP_ANONYMOUS, -1, 0);
71   if (ss.ss_sp != MAP_FAILED) {
72     ss.ss_size = SIGSTKSZ;
73     ss.ss_flags = 0;
74     sigaltstack(&ss, NULL);
75     thread->alternate_signal_stack = ss.ss_sp;
77     // We can only use const static allocated string for mapped region name, as Android kernel
78     // uses the string pointer directly when dumping /proc/pid/maps.
79     prctl(PR_SET_VMA, PR_SET_VMA_ANON_NAME, ss.ss_sp, ss.ss_size, "thread signal stack");
80   }
81 }
83 int __init_thread(pthread_internal_t* thread, bool add_to_thread_list) {
84   int error = 0;
86   // Set the scheduling policy/priority of the thread.
87   if (thread->attr.sched_policy != SCHED_NORMAL) {
88     sched_param param;
89     param.sched_priority = thread->attr.sched_priority;
90     if (sched_setscheduler(thread->tid, thread->attr.sched_policy, &param) == -1) {
91 #if __LP64__
92       // For backwards compatibility reasons, we only report failures on 64-bit devices.
93       error = errno;
94 #endif
95       __libc_format_log(ANDROID_LOG_WARN, "libc",
96                         "pthread_create sched_setscheduler call failed: %s", strerror(errno));
97     }
98   }
100   thread->cleanup_stack = NULL;
102   if (add_to_thread_list) {
103     _pthread_internal_add(thread);
104   }
106   return error;
109 static void* __create_thread_stack(const pthread_attr_t& attr) {
110   // Create a new private anonymous map.
111   int prot = PROT_READ | PROT_WRITE;
112   int flags = MAP_PRIVATE | MAP_ANONYMOUS | MAP_NORESERVE;
113   void* stack = mmap(NULL, attr.stack_size, prot, flags, -1, 0);
114   if (stack == MAP_FAILED) {
115     __libc_format_log(ANDROID_LOG_WARN,
116                       "libc",
117                       "pthread_create failed: couldn't allocate %zd-byte stack: %s",
118                       attr.stack_size, strerror(errno));
119     return NULL;
120   }
122   // Set the guard region at the end of the stack to PROT_NONE.
123   if (mprotect(stack, attr.guard_size, PROT_NONE) == -1) {
124     __libc_format_log(ANDROID_LOG_WARN, "libc",
125                       "pthread_create failed: couldn't mprotect PROT_NONE %zd-byte stack guard region: %s",
126                       attr.guard_size, strerror(errno));
127     munmap(stack, attr.stack_size);
128     return NULL;
129   }
131   return stack;
134 static int __allocate_thread(pthread_attr_t* attr, pthread_internal_t** threadp, void** child_stack) {
135   if (attr->stack_base == NULL) {
136     // The caller didn't provide a stack, so allocate one.
137     // Make sure the stack size and guard size are multiples of PAGE_SIZE.
138     attr->stack_size = BIONIC_ALIGN(attr->stack_size, PAGE_SIZE);
139     attr->guard_size = BIONIC_ALIGN(attr->guard_size, PAGE_SIZE);
140     attr->stack_base = __create_thread_stack(*attr);
141     if (attr->stack_base == NULL) {
142       return EAGAIN;
143     }
144   } else {
145     // The caller did provide a stack, so remember we're not supposed to free it.
146     attr->flags |= PTHREAD_ATTR_FLAG_USER_ALLOCATED_STACK;
147   }
149   // Thread stack is used for two sections:
150   //   pthread_internal_t.
151   //   regular stack, from top to down.
152   uint8_t* stack_top = reinterpret_cast<uint8_t*>(attr->stack_base) + attr->stack_size;
153   stack_top -= sizeof(pthread_internal_t);
154   pthread_internal_t* thread = reinterpret_cast<pthread_internal_t*>(stack_top);
156   // No need to check stack_top alignment. The size of pthread_internal_t is 16-bytes aligned,
157   // and user allocated stack is guaranteed by pthread_attr_setstack.
159   thread->attr = *attr;
160   __init_tls(thread);
162   *threadp = thread;
163   *child_stack = stack_top;
164   return 0;
167 static int __pthread_start(void* arg) {
168   pthread_internal_t* thread = reinterpret_cast<pthread_internal_t*>(arg);
170   // Wait for our creating thread to release us. This lets it have time to
171   // notify gdb about this thread before we start doing anything.
172   // This also provides the memory barrier needed to ensure that all memory
173   // accesses previously made by the creating thread are visible to us.
174   pthread_mutex_lock(&thread->startup_handshake_mutex);
175   pthread_mutex_destroy(&thread->startup_handshake_mutex);
177   __init_alternate_signal_stack(thread);
179   void* result = thread->start_routine(thread->start_routine_arg);
180   pthread_exit(result);
182   return 0;
185 // A dummy start routine for pthread_create failures where we've created a thread but aren't
186 // going to run user code on it. We swap out the user's start routine for this and take advantage
187 // of the regular thread teardown to free up resources.
188 static void* __do_nothing(void*) {
189   return NULL;
192 int pthread_create(pthread_t* thread_out, pthread_attr_t const* attr,
193                    void* (*start_routine)(void*), void* arg) {
194   ErrnoRestorer errno_restorer;
196   // Inform the rest of the C library that at least one thread was created.
197   __isthreaded = 1;
199   pthread_attr_t thread_attr;
200   if (attr == NULL) {
201     pthread_attr_init(&thread_attr);
202   } else {
203     thread_attr = *attr;
204     attr = NULL; // Prevent misuse below.
205   }
207   pthread_internal_t* thread = NULL;
208   void* child_stack = NULL;
209   int result = __allocate_thread(&thread_attr, &thread, &child_stack);
210   if (result != 0) {
211     return result;
212   }
214   // Create a mutex for the thread in TLS to wait on once it starts so we can keep
215   // it from doing anything until after we notify the debugger about it
216   //
217   // This also provides the memory barrier we need to ensure that all
218   // memory accesses previously performed by this thread are visible to
219   // the new thread.
220   pthread_mutex_init(&thread->startup_handshake_mutex, NULL);
221   pthread_mutex_lock(&thread->startup_handshake_mutex);
223   thread->start_routine = start_routine;
224   thread->start_routine_arg = arg;
226   thread->set_cached_pid(getpid());
228   int flags = CLONE_VM | CLONE_FS | CLONE_FILES | CLONE_SIGHAND | CLONE_THREAD | CLONE_SYSVSEM |
229       CLONE_SETTLS | CLONE_PARENT_SETTID | CLONE_CHILD_CLEARTID;
230   void* tls = reinterpret_cast<void*>(thread->tls);
231 #if defined(__i386__)
232   // On x86 (but not x86-64), CLONE_SETTLS takes a pointer to a struct user_desc rather than
233   // a pointer to the TLS itself.
234   user_desc tls_descriptor;
235   __init_user_desc(&tls_descriptor, false, tls);
236   tls = &tls_descriptor;
237 #endif
238   int rc = clone(__pthread_start, child_stack, flags, thread, &(thread->tid), tls, &(thread->tid));
239   if (rc == -1) {
240     int clone_errno = errno;
241     // We don't have to unlock the mutex at all because clone(2) failed so there's no child waiting to
242     // be unblocked, but we're about to unmap the memory the mutex is stored in, so this serves as a
243     // reminder that you can't rewrite this function to use a ScopedPthreadMutexLocker.
244     pthread_mutex_unlock(&thread->startup_handshake_mutex);
245     if (!thread->user_allocated_stack()) {
246       munmap(thread->attr.stack_base, thread->attr.stack_size);
247     }
248     __libc_format_log(ANDROID_LOG_WARN, "libc", "pthread_create failed: clone failed: %s", strerror(errno));
249     return clone_errno;
250   }
252   int init_errno = __init_thread(thread, true);
253   if (init_errno != 0) {
254     // Mark the thread detached and replace its start_routine with a no-op.
255     // Letting the thread run is the easiest way to clean up its resources.
256     thread->attr.flags |= PTHREAD_ATTR_FLAG_DETACHED;
257     thread->start_routine = __do_nothing;
258     pthread_mutex_unlock(&thread->startup_handshake_mutex);
259     return init_errno;
260   }
262   // Publish the pthread_t and unlock the mutex to let the new thread start running.
263   *thread_out = reinterpret_cast<pthread_t>(thread);
264   pthread_mutex_unlock(&thread->startup_handshake_mutex);
266   return 0;