]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/platform-bionic.git/blob - libc/bionic/pthread_create.cpp
Merge "Switch to g_ for globals."
[android-sdk/platform-bionic.git] / libc / bionic / pthread_create.cpp
1 /*
2  * Copyright (C) 2008 The Android Open Source Project
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *  * Redistributions of source code must retain the above copyright
9  *    notice, this list of conditions and the following disclaimer.
10  *  * Redistributions in binary form must reproduce the above copyright
11  *    notice, this list of conditions and the following disclaimer in
12  *    the documentation and/or other materials provided with the
13  *    distribution.
14  *
15  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
16  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
17  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS
18  * FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE
19  * COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT,
20  * INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING,
21  * BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS
22  * OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED
23  * AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
24  * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT
25  * OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF
26  * SUCH DAMAGE.
27  */
29 #include <pthread.h>
31 #include <errno.h>
32 #include <sys/mman.h>
34 #include "pthread_internal.h"
36 #include "private/bionic_ssp.h"
37 #include "private/bionic_tls.h"
38 #include "private/libc_logging.h"
39 #include "private/ErrnoRestorer.h"
40 #include "private/ScopedPthreadMutexLocker.h"
42 // Used by gdb to track thread creation. See libthread_db.
43 #ifdef __i386__
44 extern "C" __attribute__((noinline)) __attribute__((fastcall)) void _thread_created_hook(pid_t) {}
45 #else
46 extern "C" __attribute__((noinline)) void _thread_created_hook(pid_t) {}
47 #endif
49 // x86 uses segment descriptors rather than a direct pointer to TLS.
50 #if __i386__
51 #include <asm/ldt.h>
52 extern "C" __LIBC_HIDDEN__ void __init_user_desc(struct user_desc*, int, void*);
53 #endif
55 static pthread_mutex_t g_pthread_stack_creation_ock = PTHREAD_MUTEX_INITIALIZER;
57 static pthread_mutex_t g_debugger_notification_lock = PTHREAD_MUTEX_INITIALIZER;
59 extern "C" int __isthreaded;
61 // This code is used both by each new pthread and the code that initializes the main thread.
62 void __init_tls(pthread_internal_t* thread) {
63   // Zero-initialize all the slots after TLS_SLOT_SELF and TLS_SLOT_THREAD_ID.
64   for (size_t i = TLS_SLOT_ERRNO; i < BIONIC_TLS_SLOTS; ++i) {
65     thread->tls[i] = NULL;
66   }
68   // Slot 0 must point to itself. The x86 Linux kernel reads the TLS from %fs:0.
69   thread->tls[TLS_SLOT_SELF] = thread->tls;
70   thread->tls[TLS_SLOT_THREAD_ID] = thread;
71   // GCC looks in the TLS for the stack guard on x86, so copy it there from our global.
72   thread->tls[TLS_SLOT_STACK_GUARD] = (void*) __stack_chk_guard;
73 }
75 void __init_alternate_signal_stack(pthread_internal_t* thread) {
76   // Create and set an alternate signal stack.
77   stack_t ss;
78   ss.ss_sp = mmap(NULL, SIGSTKSZ, PROT_READ|PROT_WRITE, MAP_PRIVATE|MAP_ANONYMOUS, 0, 0);
79   if (ss.ss_sp != MAP_FAILED) {
80     ss.ss_size = SIGSTKSZ;
81     ss.ss_flags = 0;
82     sigaltstack(&ss, NULL);
83     thread->alternate_signal_stack = ss.ss_sp;
84   }
85 }
87 int __init_thread(pthread_internal_t* thread, bool add_to_thread_list) {
88   int error = 0;
90   // Set the scheduling policy/priority of the thread.
91   if (thread->attr.sched_policy != SCHED_NORMAL) {
92     sched_param param;
93     param.sched_priority = thread->attr.sched_priority;
94     if (sched_setscheduler(thread->tid, thread->attr.sched_policy, &param) == -1) {
95 #if __LP64__
96       // For backwards compatibility reasons, we only report failures on 64-bit devices.
97       error = errno;
98 #endif
99       __libc_format_log(ANDROID_LOG_WARN, "libc",
100                         "pthread_create sched_setscheduler call failed: %s", strerror(errno));
101     }
102   }
104   thread->cleanup_stack = NULL;
106   if (add_to_thread_list) {
107     _pthread_internal_add(thread);
108   }
110   return error;
113 static void* __create_thread_stack(pthread_internal_t* thread) {
114   ScopedPthreadMutexLocker lock(&g_pthread_stack_creation_ock);
116   // Create a new private anonymous map.
117   int prot = PROT_READ | PROT_WRITE;
118   int flags = MAP_PRIVATE | MAP_ANONYMOUS | MAP_NORESERVE;
119   void* stack = mmap(NULL, thread->attr.stack_size, prot, flags, -1, 0);
120   if (stack == MAP_FAILED) {
121     __libc_format_log(ANDROID_LOG_WARN,
122                       "libc",
123                       "pthread_create failed: couldn't allocate %zd-byte stack: %s",
124                       thread->attr.stack_size, strerror(errno));
125     return NULL;
126   }
128   // Set the guard region at the end of the stack to PROT_NONE.
129   if (mprotect(stack, thread->attr.guard_size, PROT_NONE) == -1) {
130     __libc_format_log(ANDROID_LOG_WARN, "libc",
131                       "pthread_create failed: couldn't mprotect PROT_NONE %zd-byte stack guard region: %s",
132                       thread->attr.guard_size, strerror(errno));
133     munmap(stack, thread->attr.stack_size);
134     return NULL;
135   }
137   return stack;
140 static int __pthread_start(void* arg) {
141   pthread_internal_t* thread = reinterpret_cast<pthread_internal_t*>(arg);
143   // Wait for our creating thread to release us. This lets it have time to
144   // notify gdb about this thread before we start doing anything.
145   // This also provides the memory barrier needed to ensure that all memory
146   // accesses previously made by the creating thread are visible to us.
147   pthread_mutex_t* start_mutex = (pthread_mutex_t*) &thread->tls[TLS_SLOT_START_MUTEX];
148   pthread_mutex_lock(start_mutex);
149   pthread_mutex_destroy(start_mutex);
150   thread->tls[TLS_SLOT_START_MUTEX] = NULL;
152   __init_alternate_signal_stack(thread);
154   void* result = thread->start_routine(thread->start_routine_arg);
155   pthread_exit(result);
157   return 0;
160 // A dummy start routine for pthread_create failures where we've created a thread but aren't
161 // going to run user code on it. We swap out the user's start routine for this and take advantage
162 // of the regular thread teardown to free up resources.
163 static void* __do_nothing(void*) {
164   return NULL;
167 int pthread_create(pthread_t* thread_out, pthread_attr_t const* attr,
168                    void* (*start_routine)(void*), void* arg) {
169   ErrnoRestorer errno_restorer;
171   // Inform the rest of the C library that at least one thread was created.
172   __isthreaded = 1;
174   pthread_internal_t* thread = reinterpret_cast<pthread_internal_t*>(calloc(sizeof(*thread), 1));
175   if (thread == NULL) {
176     __libc_format_log(ANDROID_LOG_WARN, "libc", "pthread_create failed: couldn't allocate thread");
177     return EAGAIN;
178   }
180   if (attr == NULL) {
181     pthread_attr_init(&thread->attr);
182   } else {
183     thread->attr = *attr;
184     attr = NULL; // Prevent misuse below.
185   }
187   // Make sure the stack size and guard size are multiples of PAGE_SIZE.
188   thread->attr.stack_size = (thread->attr.stack_size + (PAGE_SIZE-1)) & ~(PAGE_SIZE-1);
189   thread->attr.guard_size = (thread->attr.guard_size + (PAGE_SIZE-1)) & ~(PAGE_SIZE-1);
191   if (thread->attr.stack_base == NULL) {
192     // The caller didn't provide a stack, so allocate one.
193     thread->attr.stack_base = __create_thread_stack(thread);
194     if (thread->attr.stack_base == NULL) {
195       free(thread);
196       return EAGAIN;
197     }
198   } else {
199     // The caller did provide a stack, so remember we're not supposed to free it.
200     thread->attr.flags |= PTHREAD_ATTR_FLAG_USER_ALLOCATED_STACK;
201   }
203   // Make room for the TLS area.
204   // The child stack is the same address, just growing in the opposite direction.
205   // At offsets >= 0, we have the TLS slots.
206   // At offsets < 0, we have the child stack.
207   thread->tls = (void**)((uint8_t*)(thread->attr.stack_base) + thread->attr.stack_size - BIONIC_TLS_SLOTS * sizeof(void*));
208   void* child_stack = thread->tls;
209   __init_tls(thread);
211   // Create a mutex for the thread in TLS to wait on once it starts so we can keep
212   // it from doing anything until after we notify the debugger about it
213   //
214   // This also provides the memory barrier we need to ensure that all
215   // memory accesses previously performed by this thread are visible to
216   // the new thread.
217   pthread_mutex_t* start_mutex = (pthread_mutex_t*) &thread->tls[TLS_SLOT_START_MUTEX];
218   pthread_mutex_init(start_mutex, NULL);
219   pthread_mutex_lock(start_mutex);
221   thread->start_routine = start_routine;
222   thread->start_routine_arg = arg;
224   int flags = CLONE_VM | CLONE_FS | CLONE_FILES | CLONE_SIGHAND | CLONE_THREAD | CLONE_SYSVSEM |
225       CLONE_SETTLS | CLONE_PARENT_SETTID | CLONE_CHILD_CLEARTID;
226   void* tls = thread->tls;
227 #if defined(__i386__)
228   // On x86 (but not x86-64), CLONE_SETTLS takes a pointer to a struct user_desc rather than
229   // a pointer to the TLS itself.
230   user_desc tls_descriptor;
231   __init_user_desc(&tls_descriptor, false, tls);
232   tls = &tls_descriptor;
233 #endif
234   int rc = clone(__pthread_start, child_stack, flags, thread, &(thread->tid), tls, &(thread->tid));
235   if (rc == -1) {
236     int clone_errno = errno;
237     // We don't have to unlock the mutex at all because clone(2) failed so there's no child waiting to
238     // be unblocked, but we're about to unmap the memory the mutex is stored in, so this serves as a
239     // reminder that you can't rewrite this function to use a ScopedPthreadMutexLocker.
240     pthread_mutex_unlock(start_mutex);
241     if ((thread->attr.flags & PTHREAD_ATTR_FLAG_USER_ALLOCATED_STACK) == 0) {
242       munmap(thread->attr.stack_base, thread->attr.stack_size);
243     }
244     free(thread);
245     __libc_format_log(ANDROID_LOG_WARN, "libc", "pthread_create failed: clone failed: %s", strerror(errno));
246     return clone_errno;
247   }
249   int init_errno = __init_thread(thread, true);
250   if (init_errno != 0) {
251     // Mark the thread detached and replace its start_routine with a no-op.
252     // Letting the thread run is the easiest way to clean up its resources.
253     thread->attr.flags |= PTHREAD_ATTR_FLAG_DETACHED;
254     thread->start_routine = __do_nothing;
255     pthread_mutex_unlock(start_mutex);
256     return init_errno;
257   }
259   // Notify any debuggers about the new thread.
260   {
261     ScopedPthreadMutexLocker debugger_locker(&g_debugger_notification_lock);
262     _thread_created_hook(thread->tid);
263   }
265   // Publish the pthread_t and unlock the mutex to let the new thread start running.
266   *thread_out = reinterpret_cast<pthread_t>(thread);
267   pthread_mutex_unlock(start_mutex);
269   return 0;