1 /*
2 * Copyright (C) 2008 The Android Open Source Project
3 * All rights reserved.
4 *
5 * Redistribution and use in source and binary forms, with or without
6 * modification, are permitted provided that the following conditions
7 * are met:
8 * * Redistributions of source code must retain the above copyright
9 * notice, this list of conditions and the following disclaimer.
10 * * Redistributions in binary form must reproduce the above copyright
11 * notice, this list of conditions and the following disclaimer in
12 * the documentation and/or other materials provided with the
13 * distribution.
14 *
15 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
16 * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
17 * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS
18 * FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE
19 * COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT,
20 * INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING,
21 * BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS
22 * OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED
23 * AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
24 * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT
25 * OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF
26 * SUCH DAMAGE.
27 */
29 #include <pthread.h>
31 #include <errno.h>
32 #include <sys/mman.h>
33 #include <unistd.h>
35 #include "pthread_internal.h"
37 #include "private/bionic_macros.h"
38 #include "private/bionic_ssp.h"
39 #include "private/bionic_tls.h"
40 #include "private/libc_logging.h"
41 #include "private/ErrnoRestorer.h"
42 #include "private/ScopedPthreadMutexLocker.h"
44 // x86 uses segment descriptors rather than a direct pointer to TLS.
45 #if __i386__
46 #include <asm/ldt.h>
47 extern "C" __LIBC_HIDDEN__ void __init_user_desc(struct user_desc*, int, void*);
48 #endif
50 extern "C" int __isthreaded;
52 // This code is used both by each new pthread and the code that initializes the main thread.
53 void __init_tls(pthread_internal_t* thread) {
54 if (thread->user_allocated_stack()) {
55 // We don't know where the user got their stack, so assume the worst and zero the TLS area.
56 memset(&thread->tls[0], 0, BIONIC_TLS_SLOTS * sizeof(void*));
57 }
59 // Slot 0 must point to itself. The x86 Linux kernel reads the TLS from %fs:0.
60 thread->tls[TLS_SLOT_SELF] = thread->tls;
61 thread->tls[TLS_SLOT_THREAD_ID] = thread;
62 // GCC looks in the TLS for the stack guard on x86, so copy it there from our global.
63 thread->tls[TLS_SLOT_STACK_GUARD] = (void*) __stack_chk_guard;
64 }
66 void __init_alternate_signal_stack(pthread_internal_t* thread) {
67 // Create and set an alternate signal stack.
68 stack_t ss;
69 ss.ss_sp = mmap(NULL, SIGSTKSZ, PROT_READ|PROT_WRITE, MAP_PRIVATE|MAP_ANONYMOUS, -1, 0);
70 if (ss.ss_sp != MAP_FAILED) {
71 ss.ss_size = SIGSTKSZ;
72 ss.ss_flags = 0;
73 sigaltstack(&ss, NULL);
74 thread->alternate_signal_stack = ss.ss_sp;
75 }
76 }
78 int __init_thread(pthread_internal_t* thread, bool add_to_thread_list) {
79 int error = 0;
81 // Set the scheduling policy/priority of the thread.
82 if (thread->attr.sched_policy != SCHED_NORMAL) {
83 sched_param param;
84 param.sched_priority = thread->attr.sched_priority;
85 if (sched_setscheduler(thread->tid, thread->attr.sched_policy, ¶m) == -1) {
86 #if __LP64__
87 // For backwards compatibility reasons, we only report failures on 64-bit devices.
88 error = errno;
89 #endif
90 __libc_format_log(ANDROID_LOG_WARN, "libc",
91 "pthread_create sched_setscheduler call failed: %s", strerror(errno));
92 }
93 }
95 thread->cleanup_stack = NULL;
97 if (add_to_thread_list) {
98 _pthread_internal_add(thread);
99 }
101 return error;
102 }
104 static void* __create_thread_stack(pthread_internal_t* thread) {
105 // Create a new private anonymous map.
106 int prot = PROT_READ | PROT_WRITE;
107 int flags = MAP_PRIVATE | MAP_ANONYMOUS | MAP_NORESERVE;
108 void* stack = mmap(NULL, thread->attr.stack_size, prot, flags, -1, 0);
109 if (stack == MAP_FAILED) {
110 __libc_format_log(ANDROID_LOG_WARN,
111 "libc",
112 "pthread_create failed: couldn't allocate %zd-byte stack: %s",
113 thread->attr.stack_size, strerror(errno));
114 return NULL;
115 }
117 // Set the guard region at the end of the stack to PROT_NONE.
118 if (mprotect(stack, thread->attr.guard_size, PROT_NONE) == -1) {
119 __libc_format_log(ANDROID_LOG_WARN, "libc",
120 "pthread_create failed: couldn't mprotect PROT_NONE %zd-byte stack guard region: %s",
121 thread->attr.guard_size, strerror(errno));
122 munmap(stack, thread->attr.stack_size);
123 return NULL;
124 }
126 return stack;
127 }
129 static int __pthread_start(void* arg) {
130 pthread_internal_t* thread = reinterpret_cast<pthread_internal_t*>(arg);
132 // Wait for our creating thread to release us. This lets it have time to
133 // notify gdb about this thread before we start doing anything.
134 // This also provides the memory barrier needed to ensure that all memory
135 // accesses previously made by the creating thread are visible to us.
136 pthread_mutex_lock(&thread->startup_handshake_mutex);
137 pthread_mutex_destroy(&thread->startup_handshake_mutex);
139 __init_alternate_signal_stack(thread);
141 void* result = thread->start_routine(thread->start_routine_arg);
142 pthread_exit(result);
144 return 0;
145 }
147 // A dummy start routine for pthread_create failures where we've created a thread but aren't
148 // going to run user code on it. We swap out the user's start routine for this and take advantage
149 // of the regular thread teardown to free up resources.
150 static void* __do_nothing(void*) {
151 return NULL;
152 }
154 int pthread_create(pthread_t* thread_out, pthread_attr_t const* attr,
155 void* (*start_routine)(void*), void* arg) {
156 ErrnoRestorer errno_restorer;
158 // Inform the rest of the C library that at least one thread was created.
159 __isthreaded = 1;
161 pthread_internal_t* thread = __create_thread_struct();
162 if (thread == NULL) {
163 return EAGAIN;
164 }
166 if (attr == NULL) {
167 pthread_attr_init(&thread->attr);
168 } else {
169 thread->attr = *attr;
170 attr = NULL; // Prevent misuse below.
171 }
173 // Make sure the stack size and guard size are multiples of PAGE_SIZE.
174 thread->attr.stack_size = BIONIC_ALIGN(thread->attr.stack_size, PAGE_SIZE);
175 thread->attr.guard_size = BIONIC_ALIGN(thread->attr.guard_size, PAGE_SIZE);
177 if (thread->attr.stack_base == NULL) {
178 // The caller didn't provide a stack, so allocate one.
179 thread->attr.stack_base = __create_thread_stack(thread);
180 if (thread->attr.stack_base == NULL) {
181 __free_thread_struct(thread);
182 return EAGAIN;
183 }
184 } else {
185 // The caller did provide a stack, so remember we're not supposed to free it.
186 thread->attr.flags |= PTHREAD_ATTR_FLAG_USER_ALLOCATED_STACK;
187 }
189 // Make room for the TLS area.
190 // The child stack is the same address, just growing in the opposite direction.
191 // At offsets >= 0, we have the TLS slots.
192 // At offsets < 0, we have the child stack.
193 thread->tls = reinterpret_cast<void**>(reinterpret_cast<uint8_t*>(thread->attr.stack_base) +
194 thread->attr.stack_size - BIONIC_TLS_SLOTS * sizeof(void*));
195 void* child_stack = thread->tls;
196 __init_tls(thread);
198 // Create a mutex for the thread in TLS to wait on once it starts so we can keep
199 // it from doing anything until after we notify the debugger about it
200 //
201 // This also provides the memory barrier we need to ensure that all
202 // memory accesses previously performed by this thread are visible to
203 // the new thread.
204 pthread_mutex_init(&thread->startup_handshake_mutex, NULL);
205 pthread_mutex_lock(&thread->startup_handshake_mutex);
207 thread->start_routine = start_routine;
208 thread->start_routine_arg = arg;
210 thread->set_cached_pid(getpid());
212 int flags = CLONE_VM | CLONE_FS | CLONE_FILES | CLONE_SIGHAND | CLONE_THREAD | CLONE_SYSVSEM |
213 CLONE_SETTLS | CLONE_PARENT_SETTID | CLONE_CHILD_CLEARTID;
214 void* tls = thread->tls;
215 #if defined(__i386__)
216 // On x86 (but not x86-64), CLONE_SETTLS takes a pointer to a struct user_desc rather than
217 // a pointer to the TLS itself.
218 user_desc tls_descriptor;
219 __init_user_desc(&tls_descriptor, false, tls);
220 tls = &tls_descriptor;
221 #endif
222 int rc = clone(__pthread_start, child_stack, flags, thread, &(thread->tid), tls, &(thread->tid));
223 if (rc == -1) {
224 int clone_errno = errno;
225 // We don't have to unlock the mutex at all because clone(2) failed so there's no child waiting to
226 // be unblocked, but we're about to unmap the memory the mutex is stored in, so this serves as a
227 // reminder that you can't rewrite this function to use a ScopedPthreadMutexLocker.
228 pthread_mutex_unlock(&thread->startup_handshake_mutex);
229 if (!thread->user_allocated_stack()) {
230 munmap(thread->attr.stack_base, thread->attr.stack_size);
231 }
232 __free_thread_struct(thread);
233 __libc_format_log(ANDROID_LOG_WARN, "libc", "pthread_create failed: clone failed: %s", strerror(errno));
234 return clone_errno;
235 }
237 int init_errno = __init_thread(thread, true);
238 if (init_errno != 0) {
239 // Mark the thread detached and replace its start_routine with a no-op.
240 // Letting the thread run is the easiest way to clean up its resources.
241 thread->attr.flags |= PTHREAD_ATTR_FLAG_DETACHED;
242 thread->start_routine = __do_nothing;
243 pthread_mutex_unlock(&thread->startup_handshake_mutex);
244 return init_errno;
245 }
247 // Publish the pthread_t and unlock the mutex to let the new thread start running.
248 *thread_out = reinterpret_cast<pthread_t>(thread);
249 pthread_mutex_unlock(&thread->startup_handshake_mutex);
251 return 0;
252 }