]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/platform-bionic.git/blob - libc/bionic/pthread_exit.cpp
Merge "Switch to OpenBSD res_random."
[android-sdk/platform-bionic.git] / libc / bionic / pthread_exit.cpp
1 /*
2  * Copyright (C) 2008 The Android Open Source Project
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *  * Redistributions of source code must retain the above copyright
9  *    notice, this list of conditions and the following disclaimer.
10  *  * Redistributions in binary form must reproduce the above copyright
11  *    notice, this list of conditions and the following disclaimer in
12  *    the documentation and/or other materials provided with the
13  *    distribution.
14  *
15  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
16  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
17  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS
18  * FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE
19  * COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT,
20  * INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING,
21  * BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS
22  * OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED
23  * AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
24  * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT
25  * OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF
26  * SUCH DAMAGE.
27  */
29 #include <pthread.h>
31 #include <signal.h>
32 #include <stdlib.h>
33 #include <sys/mman.h>
35 #include "pthread_internal.h"
37 extern "C" __noreturn void _exit_with_stack_teardown(void*, size_t);
38 extern "C" __noreturn void __exit(int);
39 extern "C" int __set_tid_address(int*);
41 /* CAVEAT: our implementation of pthread_cleanup_push/pop doesn't support C++ exceptions
42  *         and thread cancelation
43  */
45 void __pthread_cleanup_push(__pthread_cleanup_t* c, __pthread_cleanup_func_t routine, void* arg) {
46   pthread_internal_t* thread = __get_thread();
47   c->__cleanup_routine = routine;
48   c->__cleanup_arg = arg;
49   c->__cleanup_prev = thread->cleanup_stack;
50   thread->cleanup_stack = c;
51 }
53 void __pthread_cleanup_pop(__pthread_cleanup_t* c, int execute) {
54   pthread_internal_t* thread = __get_thread();
55   thread->cleanup_stack = c->__cleanup_prev;
56   if (execute) {
57     c->__cleanup_routine(c->__cleanup_arg);
58   }
59 }
61 void pthread_exit(void* return_value) {
62   pthread_internal_t* thread = __get_thread();
63   thread->return_value = return_value;
65   // Call the cleanup handlers first.
66   while (thread->cleanup_stack) {
67     __pthread_cleanup_t* c = thread->cleanup_stack;
68     thread->cleanup_stack = c->__cleanup_prev;
69     c->__cleanup_routine(c->__cleanup_arg);
70   }
72   // Call the TLS destructors. It is important to do that before removing this
73   // thread from the global list. This will ensure that if someone else deletes
74   // a TLS key, the corresponding value will be set to NULL in this thread's TLS
75   // space (see pthread_key_delete).
76   pthread_key_clean_all();
78   if (thread->alternate_signal_stack != NULL) {
79     // Tell the kernel to stop using the alternate signal stack.
80     stack_t ss;
81     ss.ss_sp = NULL;
82     ss.ss_flags = SS_DISABLE;
83     sigaltstack(&ss, NULL);
85     // Free it.
86     munmap(thread->alternate_signal_stack, SIGSTKSZ);
87     thread->alternate_signal_stack = NULL;
88   }
90   // Keep track of what we need to know about the stack before we lose the pthread_internal_t.
91   void* stack_base = thread->attr.stack_base;
92   size_t stack_size = thread->attr.stack_size;
93   bool user_allocated_stack = thread->user_allocated_stack();
95   pthread_mutex_lock(&g_thread_list_lock);
96   if ((thread->attr.flags & PTHREAD_ATTR_FLAG_DETACHED) != 0) {
97     // The thread is detached, so we can free the pthread_internal_t.
98     // First make sure that the kernel does not try to clear the tid field
99     // because we'll have freed the memory before the thread actually exits.
100     __set_tid_address(NULL);
101     _pthread_internal_remove_locked(thread);
102   } else {
103     // Make sure that the pthread_internal_t doesn't have stale pointers to a stack that
104     // will be unmapped after the exit call below.
105     if (!user_allocated_stack) {
106       thread->attr.stack_base = NULL;
107       thread->attr.stack_size = 0;
108       thread->tls = NULL;
109     }
110     // pthread_join is responsible for destroying the pthread_internal_t for non-detached threads.
111     // The kernel will futex_wake on the pthread_internal_t::tid field to wake pthread_join.
112   }
113   pthread_mutex_unlock(&g_thread_list_lock);
115   // Perform a second key cleanup. When using jemalloc, a call to free from
116   // _pthread_internal_remove_locked causes the memory associated with a key
117   // to be reallocated.
118   // TODO: When b/16847284 is fixed this call can be removed.
119   pthread_key_clean_all();
121   if (user_allocated_stack) {
122     // Cleaning up this thread's stack is the creator's responsibility, not ours.
123     __exit(0);
124   } else {
125     // We need to munmap the stack we're running on before calling exit.
126     // That's not something we can do in C.
128     // We don't want to take a signal after we've unmapped the stack.
129     // That's one last thing we can handle in C.
130     sigset_t mask;
131     sigfillset(&mask);
132     sigprocmask(SIG_SETMASK, &mask, NULL);
134     _exit_with_stack_teardown(stack_base, stack_size);
135   }