]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/platform-bionic.git/blob - libc/docs/CHANGES.TXT
merge from open-source master
[android-sdk/platform-bionic.git] / libc / docs / CHANGES.TXT
1 Bionic ChangeLog:
2 -----------------
4 Differences between current and Android 2.1:
6 - Add support for SH-4 CPU architecture !
8 - __atomic_swap(): use LDREX/STREX CPU instructions on ARMv6 and higher.
10 - <arpa/telnet.h>: New header (declarations only, no implementation).
12 - <err.h>: New header + implementation. GLibc compatibility.
14 - <warn.h>: New header + implementation. GLibc compatibility.
16 - <fts.h>: New header + implementation.
18 - <mntent.h>: Add missing <stdio.h> include.
20 - <regex.h>: New header + implementation.
22 - <signal.h>: Added killpg()
24 - <stdint.h>: Allow 64-bit type declarations on C99 builds.
26 - <stdio.h>: Add fdprintf() and vfdprintf(). Note that GLibc provides
27   the confusing 'dprintf' and 'vdprintf()' functions instead.
29 - <stdlib.h>: Fix ptsname_r(): the return type is int instead of char*.
30   The mistake comes from a GLibc man page bug (the man page listed a return
31   type of char*, while the implementation used int. Fixed in late 2009 only).
32   The Bionic implementation was incorrect. Technically, this is an ABI
33   breakage, but code that used this function probably never worked or
34   compiled properly anyway.
36 - <strings.h>: Add missing <sys/types.h> include.
38 - <sys/queue.h>: Added new header (no implementation - macro templates).
40 - <sys/resource.h>: Add rlim_t proper definition.
42 - <time64.h>: Add missing C++ header inclusion guards.
44 - <unistd.h>: Add getusershell(), setusershell() and endusershell(), though
45   implementation are bogus. GLibc compatibility.
47 - <wchar.h>: Add mbstowcs() and wcstombs()
49 - add clone() implementation for ARM (x86 and SH-4 not working yet).
51 - <sys/epoll.h>: <sys/system_properties.h>: Add missing C++ inclusion guards
53 - fix getpwnam() and getpwgrp() to accept "app_0" as a valid user name.
55 - fix sem_trywait() to return -1 and set errno to EAGAIN, instead of
56   returning EAGAIN directly.
58 - fix sem_post() to wake up multiple threads when called rapidly in
59   succession.
61 - DNS: partial implementation of RFC3484 (rule 1, 2, 5, 6, 8, 10 and
62   modified rule 9), for better address selection/sorting.
63   In the process, removed code that was previously used for "sortlist"
64   in /etc/resolv.conf. (resolv.conf is already ignored, so the latter
65   is a no-op for actual functionality.)
67 - fix pthread_sigmask() to properly return an error code without touching
68   errno. Previous implementation returned -1 on error, setting errno, which
69   is not Posix compliant.
71 - add sigaltstack() implementation for ARM.
73 - <time.h>: Properly implement the 'timezone' and 'daylight' global variables
74   (they were not defined previously, though declared in the header).
76 - <time.h>: Fix timezone management implementation to properly update
77   'tm_gmtoff' field in 'struct tm' structure.
79 - DNS: get rid of spurious random DNS queries when trying to resolve
80   an unknown domain name. Due to an initialization bug, a random DNS search
81   list was generated for each thread if net.dns.search is not defined.
83 - <pthread.h>: Add pthread_condattr_init/destroy/setpshared/getpshared functions
84   to enable proper shared conditional variable initialization.
86   Modify the pthread_mutex_t and pthread_cond_t implementation to use private
87   futexes for performance reasons. Mutexes and Condvars are no longer shareable
88   between processes by default anymore, unless you use PTHREAD_PROCESS_SHARED
89   with pthread_mutexattr_setpshared() and/or pthread_condattr_setpshared().
91 -------------------------------------------------------------------------------
92 Differences between Android 2.1 and 2.0.1:
94 - zoneinfo: updated data tables to version 2009s
97 -------------------------------------------------------------------------------
98 Differences between Android 2.0.1 and 2.0:
100 - abort(): ARM-specific hack to preserve the 'lr' register when abort()
101   is called (GCC does not preserve it by default since it thinks that
102   abort() never returns). This improves stack traces considerably.
105 -------------------------------------------------------------------------------
106 Differences between Android 2.0 and 1.6:
108 - memcmp(), memcpy(): ARMv7 optimized versions.
110 - pthread_mutexattr_setpshared(): implementation will not return ENOTSUP
111   if PTHREAD_PROCESS_SHARED is used, because our Mutex implementation can
112   work across multiple processes.
114   *HOWEVER* it does not use "robust futexes" which means that held mutexes
115   *are not* automatically released by the kernel when the owner process
116   crashes or exits. This is only done to simplify communication between
117   two always-live system processes, DO NOT USE THIS IN APPLICATIONS !
119 - pthread_mutex_lock_timeout_np(): New Android-specific function to
120   perform a timed lock (). In case of timeout, it returns EBUSY.
122 - pthread_cond_timedwait_monotonic_np(): Same as pthread_cond_timedwait()
123   but uses the monotonic clock(). Android-specific.
125 - pthread_cond_timedwait_relative_np(): Same as pthread_cond_timedwait()
126   but uses a relative timeout instead. Android-specific.
128 - <netinet/in.h>: Now includes <netinet/in6.h>.
130 - <netinet/in6.h>: Added IPV6_JOIN_GROUP, IPV6_LEAVE_GROUP, IN6ADDR_ANY_INIT
131   and ipv6mr_interface definitions.
133 - <time.h>:
134     * Add missing tzset() declaration.
135     * Add Android-specific strftime_tz().
137 - getaddrinfo():
138     Only perform IPv6 lookup for AF_UNSPEC if we have IPv6 connectivity.
139     This saves one DNS query per lookup on non-IPv6 systems.
141 - mktime(): Fix an infinite loop problen that appeared when switching to
142   GCC 4.4.0.
144 - strftime(): fix incorrect handling of dates > 2038 due to 64-bit issue
145   in original code.
147 -------------------------------------------------------------------------------
148 Differences between Android 1.6 and 1.5:
150 - C runtime: Fix runtime initialization to be called before any static C++
151   constructors. This allows these to use pthread functions properly.
153 - __aeabi_atexit(): Fix implementation to properly call C++ static destructors
154   when the program exits (or when a shared library is unloaded).
156 - <sys/stat.h>: added GLibc compatibility macros definitions:
158         #define  st_atimensec  st_atime_nsec
159         #define  st_mtimensec  st_mtime_nsec
160         #define  st_ctimensec  st_ctime_nsec
162 - getaddrinfo(): implementation will now allow numeric ports if ai_socktype is
163   set to ANY. This is to match the GLibc behaviour.
165 - getservent(): and getservent_r() incorrectly returned the port in host-endian
166   order in the s_port field. It now returns it in big-endian order.
168 - DNS: Allow underscore in the middle of DNS labels. While not really
169   standard, this extension is needed for some VPN configurations and is
170   supported by other operating systems.
172 - DNS: Support for DNS domain search lists through the new net.dns.search
173   system property. The corresponding value must be a space-separated list of
174   domain suffixes.