]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/platform-bionic.git/blob - libc/docs/CHANGES.TXT
syslog needs a valid socket path for _PATH_LOG
[android-sdk/platform-bionic.git] / libc / docs / CHANGES.TXT
1 Bionic ChangeLog:
2 -----------------
4 Differences between current and Android 2.3:
6 - <android/api-level.h>: Added new header to define __ANDROID_API__ to
7   a constant integer corresponding to the native API level. This header
8   also exists in the NDK's platform headers.
10 - <sys/cdefs.h>: Include <android/api-level.h>
12 - <time.h>: Add timegm(), timelocal(), time2posix() and posix2time()
14 - <sched.h>: Add sched_getcpu(), sched_getaffinity(), sched_setaffinity(),
15   cpu_set_t and related macros (e.g. CPU_SETSIZE, CPU_ZERO, CPU_SET, ...)
17 - <unistd.h>: Add ftruncate64().
19 - <signal.h>: Changed the definition of SIGRTMAX to 64. However, note that
20   sigset_t is only 32-bit and cannot deal with real-time signals.
22 -------------------------------------------------------------------------------
23 Differences between Android 2.3 and Android 2.2:
25 - <pthread.h>: Add reader/writer locks implementation. Add sanity
26   checking to pthread_mutex_destroy() (e.g. a locked mutex will return
27   EBUSY).
29 - <semaphore.h>: Use private futexes for semaphore implementation,
30   unless your set 'pshared' to non-0 when calling sem_init().
32   Also fixed a bug in sem_post() to make it wake up all waiting
33   threads, instead of one. As a consequence, the maximum semaphore
34   value is now reduced to 0x3fffffff.
36 - <math.h>: Added sincos(), sincosf() and sincosl() (GLibc compatibility).
38 - <sys/sysinfo.h>: Added missing sysinfo() system call implementation
39   (the function was already declared in the header though).
41 - sysconf() didn't work for some arguments due to a small bug in the
42   /proc line parser.
44 - <termio.h>: added missing header (just includes <termios.h>)
46 - <unistd.h>: add missing declaration for truncate(). The implementation
47   was already here since Android 1.5.
49   modify implementation of alarm() to return 0 in case of error (i.e.
50   if a value larger than 0x7fffffff seconds is passed to it). This
51   makes the implementation compliant with the GLibc behaviour.
53 - <wchar.h>: small fixes to really support wchar_t in Bionic (not there yet).
55      the size of wchar_t is still 32-bit (decided by the compiler)
57      WCHAR_MIN: changed from 0 to INT_MIN
58      WCHAR_MAX: changed from 255 to INT_MAX
60      wcpcpy(), wcpncpy(), wcscat(), wcschr(), wcscmp(),
61      wcscpy(), wcscspn(), wcsdup(), wcslcat(), wcslcpy(),
62      wcslen(), wcsncat(), wcsncmp(), wcsncpy(), wcsnlen(),
63      wcspbrk(), wcsrchr(), wcsrchr(), wcsspn(), wcsstr(),
64      wcstok(), wcswidth(), wmemchr(), wmemcmp(), wmemcpy(),
65      wmemmove(), wmemset(): Added proper implementations.
67      wcscasecmp(), wcsncasecmp(): Added implementation limited
68      to ASCII codes for lower/upper.
70      wcscoll(): added dummy implementation that calls wcscmp()
71      wcsxfrm(): added dummy implementation that calls wcsncpy()
73   NOTE: Technically, this breaks the ABI, but we never claimed to support
74         wchar_t anyway. The wchar_t support is still *NOT* official at this
75         point. We need better multi-byte support code, and wprintf/wscanf
76         stuff too.
78 - <inttypes.h>: add missing declarations for strntoimax abd strntoumax.
80 - <stdlib.h>: add missing declarations for drand48() and erand48().
82 - clearerr(): fix broken implementation.
84 - Feature test macros like _POSIX_C_SOURCE / _XOPEN_SOURCE / _C99_SOURCE
85   are now handled correctly by our C library headers (see <sys/cdefs.h>)
87 - <sys/select.h>: add missing declaration for pselect()
89 - <sys/vfs.h>: fixed implementation of fstatfs() (also fixes fpathconf()
90   which uses it).
92 - Added an implementation of pthread_atfork()
94 - <dlfcn.h>: fixed dlopen() implementation to support dlopen(NULL, ...).
95   This allows one to look at the dynamic symbols exported by an executable.
97 - <private/bionic_tls.h>: use kernel helper functions for static versions
98   of the C library. This is necessary because we don't know where the corresponding
99   machine code is going to run, and the optimization for __get_tls() might
100   not match the features of the target device where we run a static executable
101   linked to the C library. This fixes one of the bug that explains why gdbserver
102   didn't work well with threads.
104 -------------------------------------------------------------------------------
105 Differences between Android 2.2. and Android 2.1:
107 - Support FP register save/load in setjmp()/longjmp() on ARMv7 builds.
109 - Add support for SH-4 CPU architecture !
111 - __atomic_swap(): use LDREX/STREX CPU instructions on ARMv6 and higher.
113 - <arpa/telnet.h>: New header (declarations only, no implementation).
115 - <err.h>: New header + implementation. GLibc compatibility.
117 - <warn.h>: New header + implementation. GLibc compatibility.
119 - <fts.h>: New header + implementation.
121 - <mntent.h>: Add missing <stdio.h> include.
123 - <regex.h>: New header + implementation.
125 - <signal.h>: Added killpg()
127 - <stdint.h>: Allow 64-bit type declarations on C99 builds.
129 - <stdio.h>: Add fdprintf() and vfdprintf(). Note that GLibc provides
130   the confusing 'dprintf' and 'vdprintf()' functions instead.
132 - <stdlib.h>: Fix ptsname_r(): the return type is int instead of char*.
133   The mistake comes from a GLibc man page bug (the man page listed a return
134   type of char*, while the implementation used int. Fixed in late 2009 only).
135   The Bionic implementation was incorrect. Technically, this is an ABI
136   breakage, but code that used this function probably never worked or
137   compiled properly anyway.
139 - <strings.h>: Add missing <sys/types.h> include.
141 - <sys/queue.h>: Added new header (no implementation - macro templates).
143 - <sys/resource.h>: Add rlim_t proper definition.
145 - <time64.h>: Add missing C++ header inclusion guards.
147 - <unistd.h>: Add getusershell(), setusershell() and endusershell(), though
148   implementation are bogus. GLibc compatibility.
150 - <wchar.h>: Add mbstowcs() and wcstombs()
152 - add clone() implementation for ARM (x86 and SH-4 not working yet).
154 - <sys/epoll.h>: <sys/system_properties.h>: Add missing C++ inclusion guards
156 - fix getpwnam() and getpwgrp() to accept "app_0" as a valid user name.
158 - fix sem_trywait() to return -1 and set errno to EAGAIN, instead of
159   returning EAGAIN directly.
161 - fix sem_post() to wake up multiple threads when called rapidly in
162   succession.
164 - DNS: partial implementation of RFC3484 (rule 1, 2, 5, 6, 8, 10 and
165   modified rule 9), for better address selection/sorting.
166   In the process, removed code that was previously used for "sortlist"
167   in /etc/resolv.conf. (resolv.conf is already ignored, so the latter
168   is a no-op for actual functionality.)
170 - fix pthread_sigmask() to properly return an error code without touching
171   errno. Previous implementation returned -1 on error, setting errno, which
172   is not Posix compliant.
174 - add sigaltstack() implementation for ARM.
176 - <time.h>: Properly implement the 'timezone' and 'daylight' global variables
177   (they were not defined previously, though declared in the header).
179 - <time.h>: Fix timezone management implementation to properly update
180   'tm_gmtoff' field in 'struct tm' structure.
182 - DNS: get rid of spurious random DNS queries when trying to resolve
183   an unknown domain name. Due to an initialization bug, a random DNS search
184   list was generated for each thread if net.dns.search is not defined.
186 - <pthread.h>: Add pthread_condattr_init/destroy/setpshared/getpshared functions
187   to enable proper shared conditional variable initialization.
189   Modify the pthread_mutex_t and pthread_cond_t implementation to use private
190   futexes for performance reasons. Mutexes and Condvars are no longer shareable
191   between processes by default anymore, unless you use PTHREAD_PROCESS_SHARED
192   with pthread_mutexattr_setpshared() and/or pthread_condattr_setpshared().
194 -------------------------------------------------------------------------------
195 Differences between Android 2.1 and 2.0.1:
197 - zoneinfo: updated data tables to version 2009s
200 -------------------------------------------------------------------------------
201 Differences between Android 2.0.1 and 2.0:
203 - abort(): ARM-specific hack to preserve the 'lr' register when abort()
204   is called (GCC does not preserve it by default since it thinks that
205   abort() never returns). This improves stack traces considerably.
208 -------------------------------------------------------------------------------
209 Differences between Android 2.0 and 1.6:
211 - memcmp(), memcpy(): ARMv7 optimized versions.
213 - pthread_mutexattr_setpshared(): implementation will not return ENOTSUP
214   if PTHREAD_PROCESS_SHARED is used, because our Mutex implementation can
215   work across multiple processes.
217   *HOWEVER* it does not use "robust futexes" which means that held mutexes
218   *are not* automatically released by the kernel when the owner process
219   crashes or exits. This is only done to simplify communication between
220   two always-live system processes, DO NOT USE THIS IN APPLICATIONS !
222 - pthread_mutex_lock_timeout_np(): New Android-specific function to
223   perform a timed lock (). In case of timeout, it returns EBUSY.
225 - pthread_cond_timedwait_monotonic_np(): Same as pthread_cond_timedwait()
226   but uses the monotonic clock(). Android-specific.
228 - pthread_cond_timedwait_relative_np(): Same as pthread_cond_timedwait()
229   but uses a relative timeout instead. Android-specific.
231 - <netinet/in.h>: Now includes <netinet/in6.h>.
233 - <netinet/in6.h>: Added IPV6_JOIN_GROUP, IPV6_LEAVE_GROUP, IN6ADDR_ANY_INIT
234   and ipv6mr_interface definitions.
236 - <time.h>:
237     * Add missing tzset() declaration.
238     * Add Android-specific strftime_tz().
240 - getaddrinfo():
241     Only perform IPv6 lookup for AF_UNSPEC if we have IPv6 connectivity.
242     This saves one DNS query per lookup on non-IPv6 systems.
244 - mktime(): Fix an infinite loop problen that appeared when switching to
245   GCC 4.4.0.
247 - strftime(): fix incorrect handling of dates > 2038 due to 64-bit issue
248   in original code.
250 -------------------------------------------------------------------------------
251 Differences between Android 1.6 and 1.5:
253 - C runtime: Fix runtime initialization to be called before any static C++
254   constructors. This allows these to use pthread functions properly.
256 - __aeabi_atexit(): Fix implementation to properly call C++ static destructors
257   when the program exits (or when a shared library is unloaded).
259 - <sys/stat.h>: added GLibc compatibility macros definitions:
261         #define  st_atimensec  st_atime_nsec
262         #define  st_mtimensec  st_mtime_nsec
263         #define  st_ctimensec  st_ctime_nsec
265 - getaddrinfo(): implementation will now allow numeric ports if ai_socktype is
266   set to ANY. This is to match the GLibc behaviour.
268 - getservent(): and getservent_r() incorrectly returned the port in host-endian
269   order in the s_port field. It now returns it in big-endian order.
271 - DNS: Allow underscore in the middle of DNS labels. While not really
272   standard, this extension is needed for some VPN configurations and is
273   supported by other operating systems.
275 - DNS: Support for DNS domain search lists through the new net.dns.search
276   system property. The corresponding value must be a space-separated list of
277   domain suffixes.