1 Bionic C Library Overview:
2 ==========================
4 Introduction:
6 Core Philosophy:
8 The core idea behind Bionic's design is: KEEP IT REALLY SIMPLE.
10 This implies that the C library should only provide lightweight wrappers
11 around kernel facilities and not try to be too smart to deal with edge cases.
13 The name "Bionic" comes from the fact that it is part-BSD and part-Linux:
14 its source code consists in a mix of BSD C library pieces with custom
15 Linux-specific bits used to deal with threads, processes, signals and a few
16 others things.
18 All original BSD pieces carry the BSD copyright disclaimer. Bionic-specific
19 bits carry the Android Open Source Project copyright disclaimer. And
20 everything is released under the BSD license.
22 Architectures:
24 Bionic currently supports the ARM and x86 instruction sets. In theory, it
25 should be possible to support more, but this may require a little work (e.g.
26 adding system call IDs to SYSCALLS.TXT, described below, or modifying the
27 dynamic linker).
29 The ARM-specific code is under arch-arm/ and the x86-specific one is under
30 arch-x86/
32 Note that the x86 version is only meant to run on an x86 Android device. We
33 make absolutely no claim that you could build and use Bionic on a stock x86
34 Linux distribution (though that would be cool, so patches are welcomed :-))
36 Syscall stubs:
38 Each system call function is implemented by a tiny assembler source fragment
39 (called a "syscall stub"), which is generated automatically by
40 tools/gensyscalls.py which reads the SYSCALLS.TXT file for input.
42 SYSCALLS.TXT contains the list of all syscall stubs to generate, along with
43 the corresponding syscall numeric identifier (which may differ between ARM
44 and x86), and its signature
46 If you modify this file, you may want to use tools/checksyscalls.py which
47 checks its content against official Linux kernel header files, and will
48 report errors when invalid syscall ids are used.
50 Sometimes, the C library function is really a wrapper that calls the
51 corresponding syscall with another name. For example, the exit() function
52 is provided by the C library and calls the _exit() syscall stub.
54 See SYSCALLS.TXT for documentation and details.
57 time_t:
59 time_t is 32-bit as defined by the kernel on 32-bit CPUs. A 64-bit version
60 would be preferrable to avoid the Y2038 bug, but the kernel maintainers
61 consider that this is not needed at the moment.
63 Instead, Bionic provides a <time64.h> header that defines a time64_t type,
64 and related functions like mktime64(), localtime64(), etc...
67 Timezone management:
69 The name of the current timezone is taken from the TZ environment variable,
70 if defined. Otherwise, the system property named 'persist.sys.timezone' is
71 checked instead.
73 The zoneinfo timezone database and index files are located under directory
74 /system/usr/share/zoneinfo, instead of the more Posix-compliant path of
75 /usr/share/zoneinfo
78 off_t:
80 For similar reasons, off_t is 32-bit. We define loff_t as the 64-bit variant
81 due to BSD inheritance, but off64_t should be available as a typedef to ease
82 porting of current Linux-specific code.
85 Linux kernel headers:
87 Bionic comes with its own set of "clean" Linux kernel headers to allow
88 user-space code to use kernel-specific declarations (e.g. IOCTLs, structure
89 declarations, constants, etc...). They are located in:
91 ./kernel/common,
92 ./kernel/arch-arm
93 ./kernel/arch-x86
95 These headers have been generated by a tool (kernel/tools/update-all.py) to
96 only include the public definitions from the original Linux kernel headers.
98 If you want to know why and how this is done, read kernel/README.TXT to get
99 all the (gory) details.
102 PThread implementation:
104 Bionic's C library comes with its own pthread implementation bundled in.
105 This is different from other historical C libraries which:
107 - place it in an external library (-lpthread)
108 - play linker tricks with weak symbols at dynamic link time
110 The support for real-time features (a.k.a. -lrt) is also bundled in the
111 C library.
113 The implementation is based on futexes and strives to provide *very* short
114 code paths for common operations. Notable features are the following:
116 - pthread_mutex_t, pthread_cond_t are only 4 bytes each.
118 - Normal, recursive and error-check mutexes are supported, and the code
119 path is heavily optimized for the normal case, which is used most of
120 the time.
122 - Process-shared mutexes and condition variables are not supported.
123 Their implementation requires far more complexity and was absolutely
124 not needed for Android (which uses other inter-process synchronization
125 capabilities).
127 Note that they could be added in the future without breaking the ABI
128 by specifying more sophisticated code paths (which may make the common
129 paths slightly slower though).
131 - There is currently no support for read/write locks, priority-ceiling in
132 mutexes and other more advanced features. Again, the main idea being
133 that this was not needed for Android at all but could be added in the
134 future.
136 pthread_cancel():
138 pthread_cancel() will *not* be supported in Bionic, because doing this would
139 involve making the C library significantly bigger for very little benefit.
141 Consider that:
143 - A proper implementation must insert pthread cancellation checks in a lot
144 of different places of the C library. And conformance is very difficult
145 to test properly.
147 - A proper implementation must also clean up resources, like releasing
148 memory, or unlocking mutexes, properly if the cancellation happens in a
149 complex function (e.g. inside gethostbyname() or fprintf() + complex
150 formatting rules). This tends to slow down the path of many functions.
152 - pthread cancellation cannot stop all threads: e.g. it can't do anything
153 against an infinite loop
155 - pthread cancellation itself has short-comings and isn't very portable
156 (see http://advogato.org/person/slamb/diary.html?start=49 for example).
158 All of this is contrary to the Bionic design goals. If your code depends on
159 thread cancellation, please consider alternatives.
161 Note however that Bionic does implement pthread_cleanup_push() and
162 pthread_cleanup_pop(), which can be used to handle cleanups that happen when
163 a thread voluntarily exits through pthread_exit() or returning from its
164 main function.
167 pthread_once():
169 Do not call fork() within a callback provided to pthread_once(). Doing this
170 may result in a deadlock in the child process the next time it calls
171 pthread_once().
173 Also, you can't throw a C++ Exception from the callback (see C++ Exception
174 Support below).
176 The current implementation of pthread_once() lacks the necessary support of
177 multi-core-safe double-checked-locking (read and write barriers).
180 Thread-specific data
182 The thread-specific storage only provides for a bit less than 64
183 pthread_key_t objects to each process. The implementation provides 64 real
184 slots but also uses about 5 of them (exact number may depend on
185 implementation) for its own use (e.g. two slots are pre-allocated by the C
186 library to speed-up the Android OpenGL sub-system).
188 Note that Posix mandates a minimum of 128 slots, but we do not claim to be
189 Posix-compliant.
191 Except for the main thread, the TLS area is stored at the top of the stack.
192 See comments in bionic/libc/bionic/pthread.c for details.
194 At the moment, thread-local storage defined through the __thread compiler
195 keyword is not supported by the Bionic C library and dynamic linker.
198 Multi-core support
200 At the moment, Bionic does not provide or use read/write memory barriers.
201 This means that using it on certain multi-core systems might not be
202 supported, depending on its exact CPU architecture.
205 Android-specific features:
207 Bionic provides a small number of Android-specific features to its clients:
209 - access to system properties:
211 Android provides a simple shared value/key space to all processes on the
212 system. It stores a liberal number of 'properties', each of them being a
213 simple size-limited string that can be associated to a size-limited
214 string value.
216 The header <sys/system_properties.h> can be used to read system
217 properties and also defines the maximum size of keys and values.
219 - Android-specific user/group management:
221 There is no /etc/passwd or /etc/groups in Android. By design, it is
222 meant to be used by a single handset user. On the other hand, Android
223 uses the Linux user/group management features extensively to secure
224 process permissions, like access to various filesystem directories.
226 In the Android scheme, each installed application gets its own
227 uid_t/gid_t starting from 10000; lower numerical ids are reserved for
228 system daemons.
230 getpwnam() recognizes some hard-coded subsystems names (e.g. "radio")
231 and will translate them to their low-user-id values. It also recognizes
232 "app_1234" as the synthetic name of the application that was installed
233 with uid 10000 + 1234, which is 11234. getgrnam() works similarly
235 getgrouplist() will always return a single group for any user name,
236 which is the one passed as an input parameter.
238 getgrgid() will similarly only return a structure that contains a
239 single-element members list, corresponding to the user with the same
240 numerical value than the group.
242 See bionic/libc/bionic/stubs.c for more details.
244 - getservent()
246 There is no /etc/services on Android. Instead the C library embeds a
247 constant list of services in its executable, which is parsed on demand
248 by the various functions that depend on it. See
249 bionic/libc/netbsd/net/getservent.c and
250 bionic/libc/netbsd/net/services.h
252 The list of services defined internally might change liberally in the
253 future. This feature is mostly historically and is very rarely used.
255 The getservent() returns thread-local data. getservbyport() and
256 getservbyname() are also implemented in a similar fashion.
258 - getprotoent()
260 There is no /etc/protocol on Android. Bionic does not currently
261 implement getprotoent() and related functions. If added, it will
262 likely be done in a way similar to getservent()
264 DNS resolver:
266 Bionic uses a NetBSD-derived resolver library which has been modified in
267 the following ways:
269 - don't implement the name-server-switch feature (a.k.a. <nsswitch.h>)
271 - read /system/etc/resolv.conf instead of /etc/resolv.conf
273 - read the list of servers from system properties. the code looks for
274 'net.dns1', 'net.dns2', etc.. Each property should contain the IP
275 address of a DNS server.
277 these properties are set/modified by other parts of the Android system
278 (e.g. the dhcpd daemon).
280 the implementation also supports per-process DNS server list, using the
281 properties 'net.dns1.<pid>', 'net.dns2.<pid>', etc... Where <pid> stands
282 for the numerical ID of the current process.
284 - when performing a query, use a properly randomized Query ID (instead of
285 a incremented one), for increased security.
287 - when performing a query, bind the local client socket to a random port
288 for increased security.
290 - get rid of *many* unfortunate thread-safety issues in the original code
292 Bionic does *not* expose implementation details of its DNS resolver; the
293 content of <arpa/nameser.h> is intentionally blank. The resolver
294 implementation might change completely in the future.
297 PThread Real-Time Timers:
299 timer_create(), timer_gettime(), timer_settime() and timer_getoverrun() are
300 supported.
302 Bionic also now supports SIGEV_THREAD real-time timers (see timer_create()).
303 The implementation simply uses a single thread per timer, unlike GLibc which
304 uses complex heuristics to try to use the less threads possible when several
305 timers with compatible properties are used.
307 This means that if your code uses a lot of SIGEV_THREAD timers, your program
308 may consume a lot of memory. However, if your program needs many of these
309 timers, it'd better handle timeout events directly instead.
311 Other timers (e.g. SIGEV_SIGNAL) are handled by the kernel and use much less
312 system resources.
315 Binary Compatibility:
317 Bionic is *not* in any way binary-compatible with the GNU C Library, ucLibc
318 or any known Linux C library. This means several things:
320 - You cannot expect to build something against the GNU C Library headers and
321 have it dynamically link properly to Bionic later.
323 - You should *really* use the Android toolchain to build your program against
324 Bionic. The toolchain deals with many important details that are crucial
325 to get something working properly.
327 Failure to do so will usually result in the inability to run or link your
328 program, or even runtime crashes. Several random web pages on the Internet
329 describe how you can succesfully write a "hello-world" program with the
330 ARM GNU toolchain. These examples usually work by chance, if anything else,
331 and you should not follow these instructions unless you want to waste a lot
332 of your time in the process.
334 Note however that you *can* generate a binary that is built against the
335 GNU C Library headers and then statically linked to it. The corresponding
336 executable should be able to run (if it doesn't use dlopen()/dlsym())
339 Dynamic Linker:
341 Bionic comes with its own dynamic linker (just like ld.so on Linux really
342 comes from GLibc). This linker does not support all the relocations
343 generated by other GCC ARM toolchains.
346 C++ Exceptions Support:
348 At the moment, Bionic doesn't support C++ exceptions, what this really means
349 is the following:
351 - If pthread_once() is called with a C++ callback that throws an exception,
352 then the C library will keep the corresponding pthread_once_t mutex
353 locked. Any further call to pthread_once() will result in a deadlock.
355 A proper implementation should be able to register a C++ exception
356 cleanup handler before the callback to properly unlock the
357 pthread_once_t. Unfortunately this requires tricky assembly code that
358 is highly dependent on the compiler.
360 This feature is not planned to be supported anytime soon.
362 - The same problem may arise if you throw an exception within a callback
363 called from the C library. Fortunately, these cases are very rare in the
364 real-world, but any callback you provide to the C library should *not*
365 throw an exception.
367 - Bionic lacks a few support functions to have exception support work
368 properly.
370 System V IPCs:
372 Bionic intentionally does not provide support for System-V IPCs mechanisms,
373 like the ones provided by semget(), shmget(), msgget(). The reason for this
374 is to avoid denial-of-service. For a detailed rationale about this, please
375 read the file docs/SYSV-IPCS.TXT.
377 Include Paths:
379 The Android build system should automatically provide the necessary include
380 paths required to build against the C library headers. However, if you want
381 to do that yourself, you will need to add:
383 libc/arch-$ARCH/include
384 libc/include
385 libc/kernel/common
386 libc/kernel/arch-$ARCH
388 to your C include path.