1 /* $NetBSD: cdefs.h,v 1.58 2004/12/11 05:59:00 christos Exp $ */
3 /*
4 * Copyright (c) 1991, 1993
5 * The Regents of the University of California. All rights reserved.
6 *
7 * This code is derived from software contributed to Berkeley by
8 * Berkeley Software Design, Inc.
9 *
10 * Redistribution and use in source and binary forms, with or without
11 * modification, are permitted provided that the following conditions
12 * are met:
13 * 1. Redistributions of source code must retain the above copyright
14 * notice, this list of conditions and the following disclaimer.
15 * 2. Redistributions in binary form must reproduce the above copyright
16 * notice, this list of conditions and the following disclaimer in the
17 * documentation and/or other materials provided with the distribution.
18 * 3. Neither the name of the University nor the names of its contributors
19 * may be used to endorse or promote products derived from this software
20 * without specific prior written permission.
21 *
22 * THIS SOFTWARE IS PROVIDED BY THE REGENTS AND CONTRIBUTORS ``AS IS'' AND
23 * ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
24 * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
25 * ARE DISCLAIMED. IN NO EVENT SHALL THE REGENTS OR CONTRIBUTORS BE LIABLE
26 * FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL
27 * DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS
28 * OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION)
29 * HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT
30 * LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY
31 * OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF
32 * SUCH DAMAGE.
33 *
34 * @(#)cdefs.h 8.8 (Berkeley) 1/9/95
35 */
37 #ifndef _SYS_CDEFS_H_
38 #define _SYS_CDEFS_H_
40 /*
41 * Testing against Clang-specific extensions.
42 */
44 #ifndef __has_extension
45 #define __has_extension __has_feature
46 #endif
47 #ifndef __has_feature
48 #define __has_feature(x) 0
49 #endif
50 #ifndef __has_include
51 #define __has_include(x) 0
52 #endif
53 #ifndef __has_builtin
54 #define __has_builtin(x) 0
55 #endif
58 /*
59 * Macro to test if we're using a GNU C compiler of a specific vintage
60 * or later, for e.g. features that appeared in a particular version
61 * of GNU C. Usage:
62 *
63 * #if __GNUC_PREREQ__(major, minor)
64 * ...cool feature...
65 * #else
66 * ...delete feature...
67 * #endif
68 */
69 #ifdef __GNUC__
70 #define __GNUC_PREREQ__(x, y) \
71 ((__GNUC__ == (x) && __GNUC_MINOR__ >= (y)) || \
72 (__GNUC__ > (x)))
73 #else
74 #define __GNUC_PREREQ__(x, y) 0
75 #endif
77 #include <sys/cdefs_elf.h>
79 #if defined(__cplusplus)
80 #define __BEGIN_DECLS extern "C" {
81 #define __END_DECLS }
82 #define __static_cast(x,y) static_cast<x>(y)
83 #else
84 #define __BEGIN_DECLS
85 #define __END_DECLS
86 #define __static_cast(x,y) (x)y
87 #endif
89 /*
90 * The __CONCAT macro is used to concatenate parts of symbol names, e.g.
91 * with "#define OLD(foo) __CONCAT(old,foo)", OLD(foo) produces oldfoo.
92 * The __CONCAT macro is a bit tricky -- make sure you don't put spaces
93 * in between its arguments. __CONCAT can also concatenate double-quoted
94 * strings produced by the __STRING macro, but this only works with ANSI C.
95 */
97 #define ___STRING(x) __STRING(x)
98 #define ___CONCAT(x,y) __CONCAT(x,y)
100 #if defined(__STDC__) || defined(__cplusplus)
101 #define __P(protos) protos /* full-blown ANSI C */
102 #define __CONCAT(x,y) x ## y
103 #define __STRING(x) #x
105 #define __const const /* define reserved names to standard */
106 #define __signed signed
107 #define __volatile volatile
108 #if defined(__cplusplus)
109 #define __inline inline /* convert to C++ keyword */
110 #else
111 #if !defined(__GNUC__) && !defined(__lint__)
112 #define __inline /* delete GCC keyword */
113 #endif /* !__GNUC__ && !__lint__ */
114 #endif /* !__cplusplus */
116 #else /* !(__STDC__ || __cplusplus) */
117 #define __P(protos) () /* traditional C preprocessor */
118 #define __CONCAT(x,y) x/**/y
119 #define __STRING(x) "x"
121 #ifndef __GNUC__
122 #define __const /* delete pseudo-ANSI C keywords */
123 #define __inline
124 #define __signed
125 #define __volatile
126 #endif /* !__GNUC__ */
128 /*
129 * In non-ANSI C environments, new programs will want ANSI-only C keywords
130 * deleted from the program and old programs will want them left alone.
131 * Programs using the ANSI C keywords const, inline etc. as normal
132 * identifiers should define -DNO_ANSI_KEYWORDS.
133 */
134 #ifndef NO_ANSI_KEYWORDS
135 #define const __const /* convert ANSI C keywords */
136 #define inline __inline
137 #define signed __signed
138 #define volatile __volatile
139 #endif /* !NO_ANSI_KEYWORDS */
140 #endif /* !(__STDC__ || __cplusplus) */
142 /*
143 * Used for internal auditing of the NetBSD source tree.
144 */
145 #ifdef __AUDIT__
146 #define __aconst __const
147 #else
148 #define __aconst
149 #endif
151 /*
152 * The following macro is used to remove const cast-away warnings
153 * from gcc -Wcast-qual; it should be used with caution because it
154 * can hide valid errors; in particular most valid uses are in
155 * situations where the API requires it, not to cast away string
156 * constants. We don't use *intptr_t on purpose here and we are
157 * explicit about unsigned long so that we don't have additional
158 * dependencies.
159 */
160 #define __UNCONST(a) ((void *)(unsigned long)(const void *)(a))
162 /*
163 * GCC2 provides __extension__ to suppress warnings for various GNU C
164 * language extensions under "-ansi -pedantic".
165 */
166 #if !__GNUC_PREREQ__(2, 0)
167 #define __extension__ /* delete __extension__ if non-gcc or gcc1 */
168 #endif
170 /*
171 * GCC1 and some versions of GCC2 declare dead (non-returning) and
172 * pure (no side effects) functions using "volatile" and "const";
173 * unfortunately, these then cause warnings under "-ansi -pedantic".
174 * GCC2 uses a new, peculiar __attribute__((attrs)) style. All of
175 * these work for GNU C++ (modulo a slight glitch in the C++ grammar
176 * in the distribution version of 2.5.5).
177 */
178 #if !__GNUC_PREREQ__(2, 5)
179 #define __attribute__(x) /* delete __attribute__ if non-gcc or gcc1 */
180 #if defined(__GNUC__) && !defined(__STRICT_ANSI__)
181 #define __dead __volatile
182 #define __pure __const
183 #endif
184 #endif
186 /* Delete pseudo-keywords wherever they are not available or needed. */
187 #ifndef __dead
188 #define __dead
189 #define __pure
190 #endif
192 #if __GNUC_PREREQ__(2, 7)
193 #define __unused __attribute__((__unused__))
194 #else
195 #define __unused /* delete */
196 #endif
198 #define __pure2 __attribute__((__const__)) /* Android-added: used by FreeBSD libm */
200 #if __GNUC_PREREQ__(3, 1)
201 #define __used __attribute__((__used__))
202 #else
203 #define __used /* delete */
204 #endif
206 #if __GNUC_PREREQ__(2, 7)
207 #define __packed __attribute__((__packed__))
208 #define __aligned(x) __attribute__((__aligned__(x)))
209 #define __section(x) __attribute__((__section__(x)))
210 #elif defined(__lint__)
211 #define __packed /* delete */
212 #define __aligned(x) /* delete */
213 #define __section(x) /* delete */
214 #else
215 #define __packed error: no __packed for this compiler
216 #define __aligned(x) error: no __aligned for this compiler
217 #define __section(x) error: no __section for this compiler
218 #endif
220 #if !__GNUC_PREREQ__(2, 8)
221 #define __extension__
222 #endif
224 #if __GNUC_PREREQ__(2, 8)
225 #define __statement(x) __extension__(x)
226 #elif defined(lint)
227 #define __statement(x) (0)
228 #else
229 #define __statement(x) (x)
230 #endif
232 #define __nonnull(args) __attribute__((__nonnull__ args))
234 #define __printflike(x, y) __attribute__((__format__(printf, x, y))) __nonnull((x))
235 #define __scanflike(x, y) __attribute__((__format__(scanf, x, y))) __nonnull((x))
237 /*
238 * C99 defines the restrict type qualifier keyword, which was made available
239 * in GCC 2.92.
240 */
241 #if defined(__STDC__VERSION__) && __STDC_VERSION__ >= 199901L
242 #define __restrict restrict
243 #else
244 #if !__GNUC_PREREQ__(2, 92)
245 #define __restrict /* delete __restrict when not supported */
246 #endif
247 #endif
249 /*
250 * C99 defines __func__ predefined identifier, which was made available
251 * in GCC 2.95.
252 */
253 #if !defined(__STDC_VERSION__) || !(__STDC_VERSION__ >= 199901L)
254 #if __GNUC_PREREQ__(2, 6)
255 #define __func__ __PRETTY_FUNCTION__
256 #elif __GNUC_PREREQ__(2, 4)
257 #define __func__ __FUNCTION__
258 #else
259 #define __func__ ""
260 #endif
261 #endif /* !(__STDC_VERSION__ >= 199901L) */
263 #if defined(_KERNEL)
264 #if defined(NO_KERNEL_RCSIDS)
265 #undef __KERNEL_RCSID
266 #define __KERNEL_RCSID(_n, _s) /* nothing */
267 #endif /* NO_KERNEL_RCSIDS */
268 #endif /* _KERNEL */
270 /*
271 * A barrier to stop the optimizer from moving code or assume live
272 * register values. This is gcc specific, the version is more or less
273 * arbitrary, might work with older compilers.
274 */
275 #if __GNUC_PREREQ__(2, 95)
276 #define __insn_barrier() __asm __volatile("":::"memory")
277 #else
278 #define __insn_barrier() /* */
279 #endif
281 /*
282 * GNU C version 2.96 adds explicit branch prediction so that
283 * the CPU back-end can hint the processor and also so that
284 * code blocks can be reordered such that the predicted path
285 * sees a more linear flow, thus improving cache behavior, etc.
286 *
287 * The following two macros provide us with a way to use this
288 * compiler feature. Use __predict_true() if you expect the expression
289 * to evaluate to true, and __predict_false() if you expect the
290 * expression to evaluate to false.
291 *
292 * A few notes about usage:
293 *
294 * * Generally, __predict_false() error condition checks (unless
295 * you have some _strong_ reason to do otherwise, in which case
296 * document it), and/or __predict_true() `no-error' condition
297 * checks, assuming you want to optimize for the no-error case.
298 *
299 * * Other than that, if you don't know the likelihood of a test
300 * succeeding from empirical or other `hard' evidence, don't
301 * make predictions.
302 *
303 * * These are meant to be used in places that are run `a lot'.
304 * It is wasteful to make predictions in code that is run
305 * seldomly (e.g. at subsystem initialization time) as the
306 * basic block reordering that this affects can often generate
307 * larger code.
308 */
309 #if __GNUC_PREREQ__(2, 96)
310 #define __predict_true(exp) __builtin_expect((exp) != 0, 1)
311 #define __predict_false(exp) __builtin_expect((exp) != 0, 0)
312 #else
313 #define __predict_true(exp) (exp)
314 #define __predict_false(exp) (exp)
315 #endif
317 #if __GNUC_PREREQ__(2, 96)
318 #define __noreturn __attribute__((__noreturn__))
319 #define __mallocfunc __attribute__((malloc))
320 #define __purefunc __attribute__((pure))
321 #else
322 #define __noreturn
323 #define __mallocfunc
324 #define __purefunc
325 #endif
327 #if __GNUC_PREREQ__(3, 1)
328 #define __always_inline __attribute__((__always_inline__))
329 #else
330 #define __always_inline
331 #endif
333 #if __GNUC_PREREQ__(3, 4)
334 #define __wur __attribute__((__warn_unused_result__))
335 #else
336 #define __wur
337 #endif
339 #if __GNUC_PREREQ__(4, 3)
340 #define __errordecl(name, msg) extern void name(void) __attribute__((__error__(msg)))
341 #define __warnattr(msg) __attribute__((__warning__(msg)))
342 #else
343 #define __errordecl(name, msg) extern void name(void)
344 #define __warnattr(msg)
345 #endif
347 /*
348 * Some BSD source needs these macros.
349 * Originally they embedded the rcs versions of each source file
350 * in the generated binary. We strip strings during build anyway,.
351 */
352 #define __IDSTRING(_prefix,_s) /* nothing */
353 #define __COPYRIGHT(_s) /* nothing */
354 #define __FBSDID(_s) /* nothing */
355 #define __RCSID(_s) /* nothing */
356 #define __SCCSID(_s) /* nothing */
358 /*
359 * _BSD_SOURCE and _GNU_SOURCE are expected to be defined by callers before
360 * any standard header file is included. In those header files we test
361 * against __USE_BSD and __USE_GNU. glibc does this in <features.h> but we
362 * do it in <sys/cdefs.h> instead because that's where our existing
363 * _POSIX_C_SOURCE tests were, and we're already confident that <sys/cdefs.h>
364 * is included everywhere it should be.
365 */
366 #if defined(_BSD_SOURCE)
367 # define __USE_BSD 1
368 #endif
370 #if defined(_GNU_SOURCE)
371 # define __USE_GNU 1
372 #endif
374 /*-
375 * POSIX.1 requires that the macros we test be defined before any standard
376 * header file is included.
377 *
378 * Here's a quick run-down of the versions:
379 * defined(_POSIX_SOURCE) 1003.1-1988
380 * _POSIX_C_SOURCE == 1 1003.1-1990
381 * _POSIX_C_SOURCE == 2 1003.2-1992 C Language Binding Option
382 * _POSIX_C_SOURCE == 199309 1003.1b-1993
383 * _POSIX_C_SOURCE == 199506 1003.1c-1995, 1003.1i-1995,
384 * and the omnibus ISO/IEC 9945-1: 1996
385 * _POSIX_C_SOURCE == 200112 1003.1-2001
386 * _POSIX_C_SOURCE == 200809 1003.1-2008
387 *
388 * In addition, the X/Open Portability Guide, which is now the Single UNIX
389 * Specification, defines a feature-test macro which indicates the version of
390 * that specification, and which subsumes _POSIX_C_SOURCE.
391 *
392 * Our macros begin with two underscores to avoid namespace screwage.
393 */
395 /* Deal with IEEE Std. 1003.1-1990, in which _POSIX_C_SOURCE == 1. */
396 #if defined(_POSIX_C_SOURCE) && _POSIX_C_SOURCE == 1
397 #undef _POSIX_C_SOURCE /* Probably illegal, but beyond caring now. */
398 #define _POSIX_C_SOURCE 199009
399 #endif
401 /* Deal with IEEE Std. 1003.2-1992, in which _POSIX_C_SOURCE == 2. */
402 #if defined(_POSIX_C_SOURCE) && _POSIX_C_SOURCE == 2
403 #undef _POSIX_C_SOURCE
404 #define _POSIX_C_SOURCE 199209
405 #endif
407 /* Deal with various X/Open Portability Guides and Single UNIX Spec. */
408 #ifdef _XOPEN_SOURCE
409 #if _XOPEN_SOURCE - 0 >= 700
410 #define __XSI_VISIBLE 700
411 #undef _POSIX_C_SOURCE
412 #define _POSIX_C_SOURCE 200809
413 #elif _XOPEN_SOURCE - 0 >= 600
414 #define __XSI_VISIBLE 600
415 #undef _POSIX_C_SOURCE
416 #define _POSIX_C_SOURCE 200112
417 #elif _XOPEN_SOURCE - 0 >= 500
418 #define __XSI_VISIBLE 500
419 #undef _POSIX_C_SOURCE
420 #define _POSIX_C_SOURCE 199506
421 #endif
422 #endif
424 /*
425 * Deal with all versions of POSIX. The ordering relative to the tests above is
426 * important.
427 */
428 #if defined(_POSIX_SOURCE) && !defined(_POSIX_C_SOURCE)
429 #define _POSIX_C_SOURCE 198808
430 #endif
431 #ifdef _POSIX_C_SOURCE
432 #if _POSIX_C_SOURCE >= 200809
433 #define __POSIX_VISIBLE 200809
434 #define __ISO_C_VISIBLE 1999
435 #elif _POSIX_C_SOURCE >= 200112
436 #define __POSIX_VISIBLE 200112
437 #define __ISO_C_VISIBLE 1999
438 #elif _POSIX_C_SOURCE >= 199506
439 #define __POSIX_VISIBLE 199506
440 #define __ISO_C_VISIBLE 1990
441 #elif _POSIX_C_SOURCE >= 199309
442 #define __POSIX_VISIBLE 199309
443 #define __ISO_C_VISIBLE 1990
444 #elif _POSIX_C_SOURCE >= 199209
445 #define __POSIX_VISIBLE 199209
446 #define __ISO_C_VISIBLE 1990
447 #elif _POSIX_C_SOURCE >= 199009
448 #define __POSIX_VISIBLE 199009
449 #define __ISO_C_VISIBLE 1990
450 #else
451 #define __POSIX_VISIBLE 198808
452 #define __ISO_C_VISIBLE 0
453 #endif /* _POSIX_C_SOURCE */
454 #else
455 /*-
456 * Deal with _ANSI_SOURCE:
457 * If it is defined, and no other compilation environment is explicitly
458 * requested, then define our internal feature-test macros to zero. This
459 * makes no difference to the preprocessor (undefined symbols in preprocessing
460 * expressions are defined to have value zero), but makes it more convenient for
461 * a test program to print out the values.
462 *
463 * If a program mistakenly defines _ANSI_SOURCE and some other macro such as
464 * _POSIX_C_SOURCE, we will assume that it wants the broader compilation
465 * environment (and in fact we will never get here).
466 */
467 #if defined(_ANSI_SOURCE) /* Hide almost everything. */
468 #define __POSIX_VISIBLE 0
469 #define __XSI_VISIBLE 0
470 #define __BSD_VISIBLE 0
471 #define __ISO_C_VISIBLE 1990
472 #elif defined(_C99_SOURCE) /* Localism to specify strict C99 env. */
473 #define __POSIX_VISIBLE 0
474 #define __XSI_VISIBLE 0
475 #define __BSD_VISIBLE 0
476 #define __ISO_C_VISIBLE 1999
477 #else /* Default environment: show everything. */
478 #define __POSIX_VISIBLE 200809
479 #define __XSI_VISIBLE 700
480 #define __BSD_VISIBLE 1
481 #define __ISO_C_VISIBLE 1999
482 #endif
483 #endif
485 /*
486 * Default values.
487 */
488 #ifndef __XPG_VISIBLE
489 # define __XPG_VISIBLE 700
490 #endif
491 #ifndef __POSIX_VISIBLE
492 # define __POSIX_VISIBLE 200809
493 #endif
494 #ifndef __ISO_C_VISIBLE
495 # define __ISO_C_VISIBLE 1999
496 #endif
497 #ifndef __BSD_VISIBLE
498 # define __BSD_VISIBLE 1
499 #endif
501 #define __BIONIC__ 1
502 #include <android/api-level.h>
504 /* glibc compatibility. */
505 #if __LP64__
506 #define __WORDSIZE 64
507 #else
508 #define __WORDSIZE 32
509 #endif
511 /*
512 * When _FORTIFY_SOURCE is defined, automatic bounds checking is
513 * added to commonly used libc functions. If a buffer overrun is
514 * detected, the program is safely aborted.
515 *
516 * See
517 * http://gcc.gnu.org/onlinedocs/gcc/Object-Size-Checking.html for details.
518 */
519 #if defined(_FORTIFY_SOURCE) && _FORTIFY_SOURCE > 0 && defined(__OPTIMIZE__) && __OPTIMIZE__ > 0
520 #define __BIONIC_FORTIFY 1
521 #if _FORTIFY_SOURCE == 2
522 #define __bos(s) __builtin_object_size((s), 1)
523 #else
524 #define __bos(s) __builtin_object_size((s), 0)
525 #endif
526 #define __bos0(s) __builtin_object_size((s), 0)
528 #define __BIONIC_FORTIFY_INLINE extern __inline__ __always_inline __attribute__((gnu_inline))
529 #endif
530 #define __BIONIC_FORTIFY_UNKNOWN_SIZE ((size_t) -1)
532 /* Used to tag non-static symbols that are private and never exposed by the shared library. */
533 #define __LIBC_HIDDEN__ __attribute__((visibility("hidden")))
535 /* Like __LIBC_HIDDEN__, but preserves binary compatibility for LP32. */
536 #ifdef __LP64__
537 #define __LIBC64_HIDDEN__ __LIBC_HIDDEN__
538 #else
539 #define __LIBC64_HIDDEN__ __LIBC_ABI_PUBLIC__
540 #endif
542 /* Used to tag non-static symbols that are public and exposed by the shared library. */
543 #define __LIBC_ABI_PUBLIC__ __attribute__((visibility ("default")))
545 /* Used to rename functions so that the compiler emits a call to 'x' rather than the function this was applied to. */
546 #define __RENAME(x) __asm__(#x)
548 #endif /* !_SYS_CDEFS_H_ */