]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/platform-bionic.git/blob - libc/include/sys/cdefs.h
am 081db840: Allow overlap in resolv uid => DNS iface mapping
[android-sdk/platform-bionic.git] / libc / include / sys / cdefs.h
1 /*      $NetBSD: cdefs.h,v 1.58 2004/12/11 05:59:00 christos Exp $      */
3 /*
4  * Copyright (c) 1991, 1993
5  *      The Regents of the University of California.  All rights reserved.
6  *
7  * This code is derived from software contributed to Berkeley by
8  * Berkeley Software Design, Inc.
9  *
10  * Redistribution and use in source and binary forms, with or without
11  * modification, are permitted provided that the following conditions
12  * are met:
13  * 1. Redistributions of source code must retain the above copyright
14  *    notice, this list of conditions and the following disclaimer.
15  * 2. Redistributions in binary form must reproduce the above copyright
16  *    notice, this list of conditions and the following disclaimer in the
17  *    documentation and/or other materials provided with the distribution.
18  * 3. Neither the name of the University nor the names of its contributors
19  *    may be used to endorse or promote products derived from this software
20  *    without specific prior written permission.
21  *
22  * THIS SOFTWARE IS PROVIDED BY THE REGENTS AND CONTRIBUTORS ``AS IS'' AND
23  * ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
24  * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
25  * ARE DISCLAIMED.  IN NO EVENT SHALL THE REGENTS OR CONTRIBUTORS BE LIABLE
26  * FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL
27  * DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS
28  * OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION)
29  * HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT
30  * LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY
31  * OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF
32  * SUCH DAMAGE.
33  *
34  *      @(#)cdefs.h     8.8 (Berkeley) 1/9/95
35  */
37 #ifndef _SYS_CDEFS_H_
38 #define _SYS_CDEFS_H_
40 /*
41  * Macro to test if we're using a GNU C compiler of a specific vintage
42  * or later, for e.g. features that appeared in a particular version
43  * of GNU C.  Usage:
44  *
45  *      #if __GNUC_PREREQ__(major, minor)
46  *      ...cool feature...
47  *      #else
48  *      ...delete feature...
49  *      #endif
50  */
51 #ifdef __GNUC__
52 #define __GNUC_PREREQ__(x, y)                                           \
53         ((__GNUC__ == (x) && __GNUC_MINOR__ >= (y)) ||                  \
54          (__GNUC__ > (x)))
55 #else
56 #define __GNUC_PREREQ__(x, y)   0
57 #endif
59 #include <sys/cdefs_elf.h>
61 #if defined(__cplusplus)
62 #define __BEGIN_DECLS           extern "C" {
63 #define __END_DECLS             }
64 #define __static_cast(x,y)      static_cast<x>(y)
65 #else
66 #define __BEGIN_DECLS
67 #define __END_DECLS
68 #define __static_cast(x,y)      (x)y
69 #endif
71 /*
72  * The __CONCAT macro is used to concatenate parts of symbol names, e.g.
73  * with "#define OLD(foo) __CONCAT(old,foo)", OLD(foo) produces oldfoo.
74  * The __CONCAT macro is a bit tricky -- make sure you don't put spaces
75  * in between its arguments.  __CONCAT can also concatenate double-quoted
76  * strings produced by the __STRING macro, but this only works with ANSI C.
77  */
79 #define ___STRING(x)    __STRING(x)
80 #define ___CONCAT(x,y)  __CONCAT(x,y)
82 #if defined(__STDC__) || defined(__cplusplus)
83 #define __P(protos)     protos          /* full-blown ANSI C */
84 #define __CONCAT(x,y)   x ## y
85 #define __STRING(x)     #x
87 #define __const         const           /* define reserved names to standard */
88 #define __signed        signed
89 #define __volatile      volatile
90 #if defined(__cplusplus)
91 #define __inline        inline          /* convert to C++ keyword */
92 #else
93 #if !defined(__GNUC__) && !defined(__lint__)
94 #define __inline                        /* delete GCC keyword */
95 #endif /* !__GNUC__  && !__lint__ */
96 #endif /* !__cplusplus */
98 #else   /* !(__STDC__ || __cplusplus) */
99 #define __P(protos)     ()              /* traditional C preprocessor */
100 #define __CONCAT(x,y)   x/**/y
101 #define __STRING(x)     "x"
103 #ifndef __GNUC__
104 #define __const                         /* delete pseudo-ANSI C keywords */
105 #define __inline
106 #define __signed
107 #define __volatile
108 #endif  /* !__GNUC__ */
110 /*
111  * In non-ANSI C environments, new programs will want ANSI-only C keywords
112  * deleted from the program and old programs will want them left alone.
113  * Programs using the ANSI C keywords const, inline etc. as normal
114  * identifiers should define -DNO_ANSI_KEYWORDS.
115  */
116 #ifndef NO_ANSI_KEYWORDS
117 #define const           __const         /* convert ANSI C keywords */
118 #define inline          __inline
119 #define signed          __signed
120 #define volatile        __volatile
121 #endif /* !NO_ANSI_KEYWORDS */
122 #endif  /* !(__STDC__ || __cplusplus) */
124 /*
125  * Used for internal auditing of the NetBSD source tree.
126  */
127 #ifdef __AUDIT__
128 #define __aconst        __const
129 #else
130 #define __aconst
131 #endif
133 /*
134  * The following macro is used to remove const cast-away warnings
135  * from gcc -Wcast-qual; it should be used with caution because it
136  * can hide valid errors; in particular most valid uses are in
137  * situations where the API requires it, not to cast away string
138  * constants. We don't use *intptr_t on purpose here and we are
139  * explicit about unsigned long so that we don't have additional
140  * dependencies.
141  */
142 #define __UNCONST(a)    ((void *)(unsigned long)(const void *)(a))
144 /*
145  * GCC2 provides __extension__ to suppress warnings for various GNU C
146  * language extensions under "-ansi -pedantic".
147  */
148 #if !__GNUC_PREREQ__(2, 0)
149 #define __extension__           /* delete __extension__ if non-gcc or gcc1 */
150 #endif
152 /*
153  * GCC1 and some versions of GCC2 declare dead (non-returning) and
154  * pure (no side effects) functions using "volatile" and "const";
155  * unfortunately, these then cause warnings under "-ansi -pedantic".
156  * GCC2 uses a new, peculiar __attribute__((attrs)) style.  All of
157  * these work for GNU C++ (modulo a slight glitch in the C++ grammar
158  * in the distribution version of 2.5.5).
159  */
160 #if !__GNUC_PREREQ__(2, 5)
161 #define __attribute__(x)        /* delete __attribute__ if non-gcc or gcc1 */
162 #if defined(__GNUC__) && !defined(__STRICT_ANSI__)
163 #define __dead          __volatile
164 #define __pure          __const
165 #endif
166 #endif
168 /* Delete pseudo-keywords wherever they are not available or needed. */
169 #ifndef __dead
170 #define __dead
171 #define __pure
172 #endif
174 #if __GNUC_PREREQ__(2, 7)
175 #define __unused        __attribute__((__unused__))
176 #else
177 #define __unused        /* delete */
178 #endif
180 #define __pure2 __attribute__((__const__)) /* Android-added: used by FreeBSD libm */
182 #if __GNUC_PREREQ__(3, 1)
183 #define __used          __attribute__((__used__))
184 #else
185 #define __used          /* delete */
186 #endif
188 #if __GNUC_PREREQ__(2, 7)
189 #define __packed        __attribute__((__packed__))
190 #define __aligned(x)    __attribute__((__aligned__(x)))
191 #define __section(x)    __attribute__((__section__(x)))
192 #elif defined(__lint__)
193 #define __packed        /* delete */
194 #define __aligned(x)    /* delete */
195 #define __section(x)    /* delete */
196 #else
197 #define __packed        error: no __packed for this compiler
198 #define __aligned(x)    error: no __aligned for this compiler
199 #define __section(x)    error: no __section for this compiler
200 #endif
202 #if !__GNUC_PREREQ__(2, 8)
203 #define __extension__
204 #endif
206 #if __GNUC_PREREQ__(2, 8)
207 #define __statement(x)  __extension__(x)
208 #elif defined(lint)
209 #define __statement(x)  (0)
210 #else
211 #define __statement(x)  (x)
212 #endif
214 #define __nonnull(args) __attribute__((__nonnull__ args))
216 #define __printflike(x, y) __attribute__((__format__(printf, x, y))) __nonnull((x))
217 #define __scanflike(x, y) __attribute__((__format__(scanf, x, y))) __nonnull((x))
219 /*
220  * C99 defines the restrict type qualifier keyword, which was made available
221  * in GCC 2.92.
222  */
223 #if defined(__STDC__VERSION__) && __STDC_VERSION__ >= 199901L
224 #define __restrict      restrict
225 #else
226 #if !__GNUC_PREREQ__(2, 92)
227 #define __restrict      /* delete __restrict when not supported */
228 #endif
229 #endif
231 /*
232  * C99 defines __func__ predefined identifier, which was made available
233  * in GCC 2.95.
234  */
235 #if !defined(__STDC_VERSION__) || !(__STDC_VERSION__ >= 199901L)
236 #if __GNUC_PREREQ__(2, 6)
237 #define __func__        __PRETTY_FUNCTION__
238 #elif __GNUC_PREREQ__(2, 4)
239 #define __func__        __FUNCTION__
240 #else
241 #define __func__        ""
242 #endif
243 #endif /* !(__STDC_VERSION__ >= 199901L) */
245 #if defined(_KERNEL)
246 #if defined(NO_KERNEL_RCSIDS)
247 #undef __KERNEL_RCSID
248 #define __KERNEL_RCSID(_n, _s)          /* nothing */
249 #endif /* NO_KERNEL_RCSIDS */
250 #endif /* _KERNEL */
252 #if !defined(_STANDALONE) && !defined(_KERNEL)
253 #ifdef __GNUC__
254 #define __RENAME(x)     ___RENAME(x)
255 #else
256 #ifdef __lint__
257 #define __RENAME(x)     __symbolrename(x)
258 #else
259 #error "No function renaming possible"
260 #endif /* __lint__ */
261 #endif /* __GNUC__ */
262 #else /* _STANDALONE || _KERNEL */
263 #define __RENAME(x)     no renaming in kernel or standalone environment
264 #endif
266 /*
267  * A barrier to stop the optimizer from moving code or assume live
268  * register values. This is gcc specific, the version is more or less
269  * arbitrary, might work with older compilers.
270  */
271 #if __GNUC_PREREQ__(2, 95)
272 #define __insn_barrier()        __asm __volatile("":::"memory")
273 #else
274 #define __insn_barrier()        /* */
275 #endif
277 /*
278  * GNU C version 2.96 adds explicit branch prediction so that
279  * the CPU back-end can hint the processor and also so that
280  * code blocks can be reordered such that the predicted path
281  * sees a more linear flow, thus improving cache behavior, etc.
282  *
283  * The following two macros provide us with a way to use this
284  * compiler feature.  Use __predict_true() if you expect the expression
285  * to evaluate to true, and __predict_false() if you expect the
286  * expression to evaluate to false.
287  *
288  * A few notes about usage:
289  *
290  *      * Generally, __predict_false() error condition checks (unless
291  *        you have some _strong_ reason to do otherwise, in which case
292  *        document it), and/or __predict_true() `no-error' condition
293  *        checks, assuming you want to optimize for the no-error case.
294  *
295  *      * Other than that, if you don't know the likelihood of a test
296  *        succeeding from empirical or other `hard' evidence, don't
297  *        make predictions.
298  *
299  *      * These are meant to be used in places that are run `a lot'.
300  *        It is wasteful to make predictions in code that is run
301  *        seldomly (e.g. at subsystem initialization time) as the
302  *        basic block reordering that this affects can often generate
303  *        larger code.
304  */
305 #if __GNUC_PREREQ__(2, 96)
306 #define __predict_true(exp)     __builtin_expect((exp) != 0, 1)
307 #define __predict_false(exp)    __builtin_expect((exp) != 0, 0)
308 #else
309 #define __predict_true(exp)     (exp)
310 #define __predict_false(exp)    (exp)
311 #endif
313 #if __GNUC_PREREQ__(2, 96)
314 #define __noreturn    __attribute__((__noreturn__))
315 #define __mallocfunc  __attribute__((malloc))
316 #define __purefunc    __attribute__((pure))
317 #else
318 #define __noreturn
319 #define __mallocfunc
320 #define __purefunc
321 #endif
323 #if __GNUC_PREREQ__(3, 1)
324 #define __always_inline __attribute__((__always_inline__))
325 #else
326 #define __always_inline
327 #endif
329 #if __GNUC_PREREQ__(3, 4)
330 #define __wur __attribute__((__warn_unused_result__))
331 #else
332 #define __wur
333 #endif
335 #if __GNUC_PREREQ__(4, 3)
336 #define __errordecl(name, msg) extern void name(void) __attribute__((__error__(msg)))
337 #define __warnattr(msg) __attribute__((__warning__(msg)))
338 #else
339 #define __errordecl(name, msg) extern void name(void)
340 #define __warnattr(msg)
341 #endif
343 /*
344  * Macros for manipulating "link sets".  Link sets are arrays of pointers
345  * to objects, which are gathered up by the linker.
346  *
347  * Object format-specific code has provided us with the following macros:
348  *
349  *      __link_set_add_text(set, sym)
350  *              Add a reference to the .text symbol `sym' to `set'.
351  *
352  *      __link_set_add_rodata(set, sym)
353  *              Add a reference to the .rodata symbol `sym' to `set'.
354  *
355  *      __link_set_add_data(set, sym)
356  *              Add a reference to the .data symbol `sym' to `set'.
357  *
358  *      __link_set_add_bss(set, sym)
359  *              Add a reference to the .bss symbol `sym' to `set'.
360  *
361  *      __link_set_decl(set, ptype)
362  *              Provide an extern declaration of the set `set', which
363  *              contains an array of the pointer type `ptype'.  This
364  *              macro must be used by any code which wishes to reference
365  *              the elements of a link set.
366  *
367  *      __link_set_start(set)
368  *              This points to the first slot in the link set.
369  *
370  *      __link_set_end(set)
371  *              This points to the (non-existent) slot after the last
372  *              entry in the link set.
373  *
374  *      __link_set_count(set)
375  *              Count the number of entries in link set `set'.
376  *
377  * In addition, we provide the following macros for accessing link sets:
378  *
379  *      __link_set_foreach(pvar, set)
380  *              Iterate over the link set `set'.  Because a link set is
381  *              an array of pointers, pvar must be declared as "type **pvar",
382  *              and the actual entry accessed as "*pvar".
383  *
384  *      __link_set_entry(set, idx)
385  *              Access the link set entry at index `idx' from set `set'.
386  */
387 #define __link_set_foreach(pvar, set)                                   \
388         for (pvar = __link_set_start(set); pvar < __link_set_end(set); pvar++)
390 #define __link_set_entry(set, idx)      (__link_set_begin(set)[idx])
392 /*
393  * Some of the FreeBSD sources used in Bionic need this.
394  * Originally, this is used to embed the rcs versions of each source file
395  * in the generated binary. We certainly don't want this in Bionic.
396  */
397 #define __FBSDID(s) /* nothing */
399 /*-
400  * The following definitions are an extension of the behavior originally
401  * implemented in <sys/_posix.h>, but with a different level of granularity.
402  * POSIX.1 requires that the macros we test be defined before any standard
403  * header file is included.
404  *
405  * Here's a quick run-down of the versions:
406  *  defined(_POSIX_SOURCE)              1003.1-1988
407  *  _POSIX_C_SOURCE == 1                1003.1-1990
408  *  _POSIX_C_SOURCE == 2                1003.2-1992 C Language Binding Option
409  *  _POSIX_C_SOURCE == 199309           1003.1b-1993
410  *  _POSIX_C_SOURCE == 199506           1003.1c-1995, 1003.1i-1995,
411  *                                      and the omnibus ISO/IEC 9945-1: 1996
412  *  _POSIX_C_SOURCE == 200112           1003.1-2001
413  *  _POSIX_C_SOURCE == 200809           1003.1-2008
414  *
415  * In addition, the X/Open Portability Guide, which is now the Single UNIX
416  * Specification, defines a feature-test macro which indicates the version of
417  * that specification, and which subsumes _POSIX_C_SOURCE.
418  *
419  * Our macros begin with two underscores to avoid namespace screwage.
420  */
422 /* Deal with IEEE Std. 1003.1-1990, in which _POSIX_C_SOURCE == 1. */
423 #if defined(_POSIX_C_SOURCE) && _POSIX_C_SOURCE == 1
424 #undef _POSIX_C_SOURCE          /* Probably illegal, but beyond caring now. */
425 #define _POSIX_C_SOURCE         199009
426 #endif
428 /* Deal with IEEE Std. 1003.2-1992, in which _POSIX_C_SOURCE == 2. */
429 #if defined(_POSIX_C_SOURCE) && _POSIX_C_SOURCE == 2
430 #undef _POSIX_C_SOURCE
431 #define _POSIX_C_SOURCE         199209
432 #endif
434 /* Deal with various X/Open Portability Guides and Single UNIX Spec. */
435 #ifdef _XOPEN_SOURCE
436 #if _XOPEN_SOURCE - 0 >= 700
437 #define __XSI_VISIBLE           700
438 #undef _POSIX_C_SOURCE
439 #define _POSIX_C_SOURCE         200809
440 #elif _XOPEN_SOURCE - 0 >= 600
441 #define __XSI_VISIBLE           600
442 #undef _POSIX_C_SOURCE
443 #define _POSIX_C_SOURCE         200112
444 #elif _XOPEN_SOURCE - 0 >= 500
445 #define __XSI_VISIBLE           500
446 #undef _POSIX_C_SOURCE
447 #define _POSIX_C_SOURCE         199506
448 #endif
449 #endif
451 /*
452  * Deal with all versions of POSIX.  The ordering relative to the tests above is
453  * important.
454  */
455 #if defined(_POSIX_SOURCE) && !defined(_POSIX_C_SOURCE)
456 #define _POSIX_C_SOURCE         198808
457 #endif
458 #ifdef _POSIX_C_SOURCE
459 #if _POSIX_C_SOURCE >= 200809
460 #define __POSIX_VISIBLE         200809
461 #define __ISO_C_VISIBLE         1999
462 #elif _POSIX_C_SOURCE >= 200112
463 #define __POSIX_VISIBLE         200112
464 #define __ISO_C_VISIBLE         1999
465 #elif _POSIX_C_SOURCE >= 199506
466 #define __POSIX_VISIBLE         199506
467 #define __ISO_C_VISIBLE         1990
468 #elif _POSIX_C_SOURCE >= 199309
469 #define __POSIX_VISIBLE         199309
470 #define __ISO_C_VISIBLE         1990
471 #elif _POSIX_C_SOURCE >= 199209
472 #define __POSIX_VISIBLE         199209
473 #define __ISO_C_VISIBLE         1990
474 #elif _POSIX_C_SOURCE >= 199009
475 #define __POSIX_VISIBLE         199009
476 #define __ISO_C_VISIBLE         1990
477 #else
478 #define __POSIX_VISIBLE         198808
479 #define __ISO_C_VISIBLE         0
480 #endif /* _POSIX_C_SOURCE */
481 #else
482 /*-
483  * Deal with _ANSI_SOURCE:
484  * If it is defined, and no other compilation environment is explicitly
485  * requested, then define our internal feature-test macros to zero.  This
486  * makes no difference to the preprocessor (undefined symbols in preprocessing
487  * expressions are defined to have value zero), but makes it more convenient for
488  * a test program to print out the values.
489  *
490  * If a program mistakenly defines _ANSI_SOURCE and some other macro such as
491  * _POSIX_C_SOURCE, we will assume that it wants the broader compilation
492  * environment (and in fact we will never get here).
493  */
494 #if defined(_ANSI_SOURCE)       /* Hide almost everything. */
495 #define __POSIX_VISIBLE         0
496 #define __XSI_VISIBLE           0
497 #define __BSD_VISIBLE           0
498 #define __ISO_C_VISIBLE         1990
499 #elif defined(_C99_SOURCE)      /* Localism to specify strict C99 env. */
500 #define __POSIX_VISIBLE         0
501 #define __XSI_VISIBLE           0
502 #define __BSD_VISIBLE           0
503 #define __ISO_C_VISIBLE         1999
504 #else                           /* Default environment: show everything. */
505 #define __POSIX_VISIBLE         200809
506 #define __XSI_VISIBLE           700
507 #define __BSD_VISIBLE           1
508 #define __ISO_C_VISIBLE         1999
509 #endif
510 #endif
512 /*
513  * Default values.
514  */
515 #ifndef __XPG_VISIBLE
516 # define __XPG_VISIBLE          700
517 #endif
518 #ifndef __POSIX_VISIBLE
519 # define __POSIX_VISIBLE        200809
520 #endif
521 #ifndef __ISO_C_VISIBLE
522 # define __ISO_C_VISIBLE        1999
523 #endif
524 #ifndef __BSD_VISIBLE
525 # define __BSD_VISIBLE          1
526 #endif
528 #define  __BIONIC__   1
529 #include <android/api-level.h>
531 /*
532  * When _FORTIFY_SOURCE is defined, automatic bounds checking is
533  * added to commonly used libc functions. If a buffer overrun is
534  * detected, the program is safely aborted.
535  *
536  * See
537  * http://gcc.gnu.org/onlinedocs/gcc/Object-Size-Checking.html for details.
538  */
539 #if defined(_FORTIFY_SOURCE) && _FORTIFY_SOURCE > 0 && defined(__OPTIMIZE__) && __OPTIMIZE__ > 0
540 #define __BIONIC_FORTIFY 1
541 #if _FORTIFY_SOURCE == 2
542 #define __bos(s) __builtin_object_size((s), 1)
543 #else
544 #define __bos(s) __builtin_object_size((s), 0)
545 #endif
546 #define __bos0(s) __builtin_object_size((s), 0)
548 #define __BIONIC_FORTIFY_INLINE \
549     extern inline \
550     __attribute__ ((always_inline)) \
551     __attribute__ ((gnu_inline))
552 #endif
553 #define __BIONIC_FORTIFY_UNKNOWN_SIZE ((size_t) -1)
555 #endif /* !_SYS_CDEFS_H_ */