]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/platform-bionic.git/blob - libc/include/sys/cdefs.h
am cb093d1f: Merge "Upgrade bionic to tzdata2014g." into lmp-dev
[android-sdk/platform-bionic.git] / libc / include / sys / cdefs.h
1 /*      $NetBSD: cdefs.h,v 1.58 2004/12/11 05:59:00 christos Exp $      */
3 /*
4  * Copyright (c) 1991, 1993
5  *      The Regents of the University of California.  All rights reserved.
6  *
7  * This code is derived from software contributed to Berkeley by
8  * Berkeley Software Design, Inc.
9  *
10  * Redistribution and use in source and binary forms, with or without
11  * modification, are permitted provided that the following conditions
12  * are met:
13  * 1. Redistributions of source code must retain the above copyright
14  *    notice, this list of conditions and the following disclaimer.
15  * 2. Redistributions in binary form must reproduce the above copyright
16  *    notice, this list of conditions and the following disclaimer in the
17  *    documentation and/or other materials provided with the distribution.
18  * 3. Neither the name of the University nor the names of its contributors
19  *    may be used to endorse or promote products derived from this software
20  *    without specific prior written permission.
21  *
22  * THIS SOFTWARE IS PROVIDED BY THE REGENTS AND CONTRIBUTORS ``AS IS'' AND
23  * ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
24  * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
25  * ARE DISCLAIMED.  IN NO EVENT SHALL THE REGENTS OR CONTRIBUTORS BE LIABLE
26  * FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL
27  * DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS
28  * OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION)
29  * HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT
30  * LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY
31  * OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF
32  * SUCH DAMAGE.
33  *
34  *      @(#)cdefs.h     8.8 (Berkeley) 1/9/95
35  */
37 #ifndef _SYS_CDEFS_H_
38 #define _SYS_CDEFS_H_
40 /*
41  * Testing against Clang-specific extensions.
42  */
44 #ifndef __has_extension
45 #define __has_extension         __has_feature
46 #endif
47 #ifndef __has_feature
48 #define __has_feature(x)        0
49 #endif
50 #ifndef __has_include
51 #define __has_include(x)        0
52 #endif
53 #ifndef __has_builtin
54 #define __has_builtin(x)        0
55 #endif
58 /*
59  * Macro to test if we're using a GNU C compiler of a specific vintage
60  * or later, for e.g. features that appeared in a particular version
61  * of GNU C.  Usage:
62  *
63  *      #if __GNUC_PREREQ(major, minor)
64  *      ...cool feature...
65  *      #else
66  *      ...delete feature...
67  *      #endif
68  */
69 #ifdef __GNUC__
70 #define __GNUC_PREREQ(x, y)                                             \
71         ((__GNUC__ == (x) && __GNUC_MINOR__ >= (y)) ||                  \
72          (__GNUC__ > (x)))
73 #else
74 #define __GNUC_PREREQ(x, y)     0
75 #endif
77 #include <sys/cdefs_elf.h>
79 #if defined(__cplusplus)
80 #define __BEGIN_DECLS           extern "C" {
81 #define __END_DECLS             }
82 #define __static_cast(x,y)      static_cast<x>(y)
83 #else
84 #define __BEGIN_DECLS
85 #define __END_DECLS
86 #define __static_cast(x,y)      (x)y
87 #endif
89 /*
90  * The __CONCAT macro is used to concatenate parts of symbol names, e.g.
91  * with "#define OLD(foo) __CONCAT(old,foo)", OLD(foo) produces oldfoo.
92  * The __CONCAT macro is a bit tricky -- make sure you don't put spaces
93  * in between its arguments.  __CONCAT can also concatenate double-quoted
94  * strings produced by the __STRING macro, but this only works with ANSI C.
95  */
97 #define ___STRING(x)    __STRING(x)
98 #define ___CONCAT(x,y)  __CONCAT(x,y)
100 #if defined(__STDC__) || defined(__cplusplus)
101 #define __P(protos)     protos          /* full-blown ANSI C */
102 #define __CONCAT(x,y)   x ## y
103 #define __STRING(x)     #x
105 #define __const         const           /* define reserved names to standard */
106 #define __signed        signed
107 #define __volatile      volatile
108 #if defined(__cplusplus)
109 #define __inline        inline          /* convert to C++ keyword */
110 #else
111 #if !defined(__GNUC__) && !defined(__lint__)
112 #define __inline                        /* delete GCC keyword */
113 #endif /* !__GNUC__  && !__lint__ */
114 #endif /* !__cplusplus */
116 #else   /* !(__STDC__ || __cplusplus) */
117 #define __P(protos)     ()              /* traditional C preprocessor */
118 #define __CONCAT(x,y)   x/**/y
119 #define __STRING(x)     "x"
121 #ifndef __GNUC__
122 #define __const                         /* delete pseudo-ANSI C keywords */
123 #define __inline
124 #define __signed
125 #define __volatile
126 #endif  /* !__GNUC__ */
128 /*
129  * In non-ANSI C environments, new programs will want ANSI-only C keywords
130  * deleted from the program and old programs will want them left alone.
131  * Programs using the ANSI C keywords const, inline etc. as normal
132  * identifiers should define -DNO_ANSI_KEYWORDS.
133  */
134 #ifndef NO_ANSI_KEYWORDS
135 #define const           __const         /* convert ANSI C keywords */
136 #define inline          __inline
137 #define signed          __signed
138 #define volatile        __volatile
139 #endif /* !NO_ANSI_KEYWORDS */
140 #endif  /* !(__STDC__ || __cplusplus) */
142 /*
143  * Used for internal auditing of the NetBSD source tree.
144  */
145 #ifdef __AUDIT__
146 #define __aconst        __const
147 #else
148 #define __aconst
149 #endif
151 /*
152  * The following macro is used to remove const cast-away warnings
153  * from gcc -Wcast-qual; it should be used with caution because it
154  * can hide valid errors; in particular most valid uses are in
155  * situations where the API requires it, not to cast away string
156  * constants. We don't use *intptr_t on purpose here and we are
157  * explicit about unsigned long so that we don't have additional
158  * dependencies.
159  */
160 #define __UNCONST(a)    ((void *)(unsigned long)(const void *)(a))
162 /*
163  * GCC2 provides __extension__ to suppress warnings for various GNU C
164  * language extensions under "-ansi -pedantic".
165  */
166 #if !__GNUC_PREREQ(2, 0)
167 #define __extension__           /* delete __extension__ if non-gcc or gcc1 */
168 #endif
170 /*
171  * GCC1 and some versions of GCC2 declare dead (non-returning) and
172  * pure (no side effects) functions using "volatile" and "const";
173  * unfortunately, these then cause warnings under "-ansi -pedantic".
174  * GCC2 uses a new, peculiar __attribute__((attrs)) style.  All of
175  * these work for GNU C++ (modulo a slight glitch in the C++ grammar
176  * in the distribution version of 2.5.5).
177  */
178 #if !__GNUC_PREREQ(2, 5)
179 #define __attribute__(x)        /* delete __attribute__ if non-gcc or gcc1 */
180 #if defined(__GNUC__) && !defined(__STRICT_ANSI__)
181 #define __dead          __volatile
182 #define __pure          __const
183 #endif
184 #endif
186 /* Delete pseudo-keywords wherever they are not available or needed. */
187 #ifndef __dead
188 #define __dead
189 #define __pure
190 #endif
192 #if __GNUC_PREREQ(2, 7)
193 #define __unused        __attribute__((__unused__))
194 #else
195 #define __unused        /* delete */
196 #endif
198 #define __pure2 __attribute__((__const__)) /* Android-added: used by FreeBSD libm */
200 #if __GNUC_PREREQ(3, 1)
201 #define __used          __attribute__((__used__))
202 #else
203 #define __used          /* delete */
204 #endif
206 #if __GNUC_PREREQ(2, 7)
207 #define __packed        __attribute__((__packed__))
208 #define __aligned(x)    __attribute__((__aligned__(x)))
209 #define __section(x)    __attribute__((__section__(x)))
210 #elif defined(__lint__)
211 #define __packed        /* delete */
212 #define __aligned(x)    /* delete */
213 #define __section(x)    /* delete */
214 #else
215 #define __packed        error: no __packed for this compiler
216 #define __aligned(x)    error: no __aligned for this compiler
217 #define __section(x)    error: no __section for this compiler
218 #endif
220 #if !__GNUC_PREREQ(2, 8)
221 #define __extension__
222 #endif
224 #if __GNUC_PREREQ(2, 8)
225 #define __statement(x)  __extension__(x)
226 #elif defined(lint)
227 #define __statement(x)  (0)
228 #else
229 #define __statement(x)  (x)
230 #endif
232 #define __nonnull(args) __attribute__((__nonnull__ args))
234 #define __printflike(x, y) __attribute__((__format__(printf, x, y))) __nonnull((x))
235 #define __scanflike(x, y) __attribute__((__format__(scanf, x, y))) __nonnull((x))
237 /*
238  * C99 defines the restrict type qualifier keyword, which was made available
239  * in GCC 2.92.
240  */
241 #if defined(__STDC__VERSION__) && __STDC_VERSION__ >= 199901L
242 #define __restrict      restrict
243 #else
244 #if !__GNUC_PREREQ(2, 92)
245 #define __restrict      /* delete __restrict when not supported */
246 #endif
247 #endif
249 /*
250  * C99 defines __func__ predefined identifier, which was made available
251  * in GCC 2.95.
252  */
253 #if !defined(__STDC_VERSION__) || !(__STDC_VERSION__ >= 199901L)
254 #if __GNUC_PREREQ(2, 6)
255 #define __func__        __PRETTY_FUNCTION__
256 #elif __GNUC_PREREQ(2, 4)
257 #define __func__        __FUNCTION__
258 #else
259 #define __func__        ""
260 #endif
261 #endif /* !(__STDC_VERSION__ >= 199901L) */
263 #if defined(_KERNEL)
264 #if defined(NO_KERNEL_RCSIDS)
265 #undef __KERNEL_RCSID
266 #define __KERNEL_RCSID(_n, _s)          /* nothing */
267 #endif /* NO_KERNEL_RCSIDS */
268 #endif /* _KERNEL */
270 /*
271  * A barrier to stop the optimizer from moving code or assume live
272  * register values. This is gcc specific, the version is more or less
273  * arbitrary, might work with older compilers.
274  */
275 #if __GNUC_PREREQ(2, 95)
276 #define __insn_barrier()        __asm __volatile("":::"memory")
277 #else
278 #define __insn_barrier()        /* */
279 #endif
281 /*
282  * GNU C version 2.96 adds explicit branch prediction so that
283  * the CPU back-end can hint the processor and also so that
284  * code blocks can be reordered such that the predicted path
285  * sees a more linear flow, thus improving cache behavior, etc.
286  *
287  * The following two macros provide us with a way to use this
288  * compiler feature.  Use __predict_true() if you expect the expression
289  * to evaluate to true, and __predict_false() if you expect the
290  * expression to evaluate to false.
291  *
292  * A few notes about usage:
293  *
294  *      * Generally, __predict_false() error condition checks (unless
295  *        you have some _strong_ reason to do otherwise, in which case
296  *        document it), and/or __predict_true() `no-error' condition
297  *        checks, assuming you want to optimize for the no-error case.
298  *
299  *      * Other than that, if you don't know the likelihood of a test
300  *        succeeding from empirical or other `hard' evidence, don't
301  *        make predictions.
302  *
303  *      * These are meant to be used in places that are run `a lot'.
304  *        It is wasteful to make predictions in code that is run
305  *        seldomly (e.g. at subsystem initialization time) as the
306  *        basic block reordering that this affects can often generate
307  *        larger code.
308  */
309 #if __GNUC_PREREQ(2, 96)
310 #define __predict_true(exp)     __builtin_expect((exp) != 0, 1)
311 #define __predict_false(exp)    __builtin_expect((exp) != 0, 0)
312 #else
313 #define __predict_true(exp)     (exp)
314 #define __predict_false(exp)    (exp)
315 #endif
317 #if __GNUC_PREREQ(2, 96)
318 #define __noreturn    __attribute__((__noreturn__))
319 #define __mallocfunc  __attribute__((malloc))
320 #define __purefunc    __attribute__((pure))
321 #else
322 #define __noreturn
323 #define __mallocfunc
324 #define __purefunc
325 #endif
327 #if __GNUC_PREREQ(3, 1)
328 #define __always_inline __attribute__((__always_inline__))
329 #else
330 #define __always_inline
331 #endif
333 #if __GNUC_PREREQ(3, 4)
334 #define __wur __attribute__((__warn_unused_result__))
335 #else
336 #define __wur
337 #endif
339 #if __GNUC_PREREQ(4, 3)
340 #define __errordecl(name, msg) extern void name(void) __attribute__((__error__(msg)))
341 #define __warnattr(msg) __attribute__((__warning__(msg)))
342 #else
343 #define __errordecl(name, msg) extern void name(void)
344 #define __warnattr(msg)
345 #endif
347 /*
348  * Some BSD source needs these macros.
349  * Originally they embedded the rcs versions of each source file
350  * in the generated binary. We strip strings during build anyway,.
351  */
352 #define __IDSTRING(_prefix,_s) /* nothing */
353 #define __COPYRIGHT(_s) /* nothing */
354 #define __FBSDID(_s) /* nothing */
355 #define __RCSID(_s) /* nothing */
356 #define __SCCSID(_s) /* nothing */
358 /*
359  * _BSD_SOURCE and _GNU_SOURCE are expected to be defined by callers before
360  * any standard header file is included. In those header files we test
361  * against __USE_BSD and __USE_GNU. glibc does this in <features.h> but we
362  * do it in <sys/cdefs.h> instead because that's where our existing
363  * _POSIX_C_SOURCE tests were, and we're already confident that <sys/cdefs.h>
364  * is included everywhere it should be.
365  */
366 #if defined(_BSD_SOURCE)
367 # define __USE_BSD 1
368 #endif
370 #if defined(_GNU_SOURCE)
371 # define __USE_GNU 1
372 #endif
374 /*-
375  * POSIX.1 requires that the macros we test be defined before any standard
376  * header file is included.
377  *
378  * Here's a quick run-down of the versions:
379  *  defined(_POSIX_SOURCE)              1003.1-1988
380  *  _POSIX_C_SOURCE == 1                1003.1-1990
381  *  _POSIX_C_SOURCE == 2                1003.2-1992 C Language Binding Option
382  *  _POSIX_C_SOURCE == 199309           1003.1b-1993
383  *  _POSIX_C_SOURCE == 199506           1003.1c-1995, 1003.1i-1995,
384  *                                      and the omnibus ISO/IEC 9945-1: 1996
385  *  _POSIX_C_SOURCE == 200112           1003.1-2001
386  *  _POSIX_C_SOURCE == 200809           1003.1-2008
387  *
388  * In addition, the X/Open Portability Guide, which is now the Single UNIX
389  * Specification, defines a feature-test macro which indicates the version of
390  * that specification, and which subsumes _POSIX_C_SOURCE.
391  *
392  * Our macros begin with two underscores to avoid namespace screwage.
393  */
395 /* Deal with IEEE Std. 1003.1-1990, in which _POSIX_C_SOURCE == 1. */
396 #if defined(_POSIX_C_SOURCE) && _POSIX_C_SOURCE == 1
397 #undef _POSIX_C_SOURCE          /* Probably illegal, but beyond caring now. */
398 #define _POSIX_C_SOURCE         199009
399 #endif
401 /* Deal with IEEE Std. 1003.2-1992, in which _POSIX_C_SOURCE == 2. */
402 #if defined(_POSIX_C_SOURCE) && _POSIX_C_SOURCE == 2
403 #undef _POSIX_C_SOURCE
404 #define _POSIX_C_SOURCE         199209
405 #endif
407 /* Deal with various X/Open Portability Guides and Single UNIX Spec. */
408 #ifdef _XOPEN_SOURCE
409 #if _XOPEN_SOURCE - 0 >= 700
410 #define __XSI_VISIBLE           700
411 #undef _POSIX_C_SOURCE
412 #define _POSIX_C_SOURCE         200809
413 #elif _XOPEN_SOURCE - 0 >= 600
414 #define __XSI_VISIBLE           600
415 #undef _POSIX_C_SOURCE
416 #define _POSIX_C_SOURCE         200112
417 #elif _XOPEN_SOURCE - 0 >= 500
418 #define __XSI_VISIBLE           500
419 #undef _POSIX_C_SOURCE
420 #define _POSIX_C_SOURCE         199506
421 #endif
422 #endif
424 /*
425  * Deal with all versions of POSIX.  The ordering relative to the tests above is
426  * important.
427  */
428 #if defined(_POSIX_SOURCE) && !defined(_POSIX_C_SOURCE)
429 #define _POSIX_C_SOURCE         198808
430 #endif
431 #ifdef _POSIX_C_SOURCE
432 #if _POSIX_C_SOURCE >= 200809
433 #define __POSIX_VISIBLE         200809
434 #define __ISO_C_VISIBLE         1999
435 #elif _POSIX_C_SOURCE >= 200112
436 #define __POSIX_VISIBLE         200112
437 #define __ISO_C_VISIBLE         1999
438 #elif _POSIX_C_SOURCE >= 199506
439 #define __POSIX_VISIBLE         199506
440 #define __ISO_C_VISIBLE         1990
441 #elif _POSIX_C_SOURCE >= 199309
442 #define __POSIX_VISIBLE         199309
443 #define __ISO_C_VISIBLE         1990
444 #elif _POSIX_C_SOURCE >= 199209
445 #define __POSIX_VISIBLE         199209
446 #define __ISO_C_VISIBLE         1990
447 #elif _POSIX_C_SOURCE >= 199009
448 #define __POSIX_VISIBLE         199009
449 #define __ISO_C_VISIBLE         1990
450 #else
451 #define __POSIX_VISIBLE         198808
452 #define __ISO_C_VISIBLE         0
453 #endif /* _POSIX_C_SOURCE */
454 #else
455 /*-
456  * Deal with _ANSI_SOURCE:
457  * If it is defined, and no other compilation environment is explicitly
458  * requested, then define our internal feature-test macros to zero.  This
459  * makes no difference to the preprocessor (undefined symbols in preprocessing
460  * expressions are defined to have value zero), but makes it more convenient for
461  * a test program to print out the values.
462  *
463  * If a program mistakenly defines _ANSI_SOURCE and some other macro such as
464  * _POSIX_C_SOURCE, we will assume that it wants the broader compilation
465  * environment (and in fact we will never get here).
466  */
467 #if defined(_ANSI_SOURCE)       /* Hide almost everything. */
468 #define __POSIX_VISIBLE         0
469 #define __XSI_VISIBLE           0
470 #define __BSD_VISIBLE           0
471 #define __ISO_C_VISIBLE         1990
472 #elif defined(_C99_SOURCE)      /* Localism to specify strict C99 env. */
473 #define __POSIX_VISIBLE         0
474 #define __XSI_VISIBLE           0
475 #define __BSD_VISIBLE           0
476 #define __ISO_C_VISIBLE         1999
477 #else                           /* Default environment: show everything. */
478 #define __POSIX_VISIBLE         200809
479 #define __XSI_VISIBLE           700
480 #define __BSD_VISIBLE           1
481 #define __ISO_C_VISIBLE         1999
482 #endif
483 #endif
485 /*
486  * Default values.
487  */
488 #ifndef __XPG_VISIBLE
489 # define __XPG_VISIBLE          700
490 #endif
491 #ifndef __POSIX_VISIBLE
492 # define __POSIX_VISIBLE        200809
493 #endif
494 #ifndef __ISO_C_VISIBLE
495 # define __ISO_C_VISIBLE        1999
496 #endif
497 #ifndef __BSD_VISIBLE
498 # define __BSD_VISIBLE          1
499 #endif
501 #define  __BIONIC__   1
502 #include <android/api-level.h>
504 /* glibc compatibility. */
505 #if __LP64__
506 #define __WORDSIZE 64
507 #else
508 #define __WORDSIZE 32
509 #endif
511 /*
512  * When _FORTIFY_SOURCE is defined, automatic bounds checking is
513  * added to commonly used libc functions. If a buffer overrun is
514  * detected, the program is safely aborted.
515  *
516  * See
517  * http://gcc.gnu.org/onlinedocs/gcc/Object-Size-Checking.html for details.
518  */
519 #if defined(_FORTIFY_SOURCE) && _FORTIFY_SOURCE > 0 && defined(__OPTIMIZE__) && __OPTIMIZE__ > 0
520 #define __BIONIC_FORTIFY 1
521 #if _FORTIFY_SOURCE == 2
522 #define __bos(s) __builtin_object_size((s), 1)
523 #else
524 #define __bos(s) __builtin_object_size((s), 0)
525 #endif
526 #define __bos0(s) __builtin_object_size((s), 0)
528 #define __BIONIC_FORTIFY_INLINE extern __inline__ __always_inline __attribute__((gnu_inline))
529 #endif
530 #define __BIONIC_FORTIFY_UNKNOWN_SIZE ((size_t) -1)
532 /* Used to tag non-static symbols that are private and never exposed by the shared library. */
533 #define __LIBC_HIDDEN__ __attribute__((visibility("hidden")))
535 /* Like __LIBC_HIDDEN__, but preserves binary compatibility for LP32. */
536 #ifdef __LP64__
537 #define __LIBC64_HIDDEN__ __LIBC_HIDDEN__
538 #else
539 #define __LIBC64_HIDDEN__ __LIBC_ABI_PUBLIC__
540 #endif
542 /* Used to tag non-static symbols that are public and exposed by the shared library. */
543 #define __LIBC_ABI_PUBLIC__ __attribute__((visibility ("default")))
545 /* Used to rename functions so that the compiler emits a call to 'x' rather than the function this was applied to. */
546 #define __RENAME(x) __asm__(#x)
548 #endif /* !_SYS_CDEFS_H_ */