am 731f9273: am 2d94ee29: Merge "Revert "Revert "Hide _tolower_tab_ and _toupper_tab_...
[android-sdk/platform-bionic.git] / libc / include / sys / cdefs_elf.h
1 /*      $NetBSD: cdefs_elf.h,v 1.22 2005/02/26 22:25:34 perry Exp $     */
3 /*
4  * Copyright (c) 1995, 1996 Carnegie-Mellon University.
5  * All rights reserved.
6  *
7  * Author: Chris G. Demetriou
8  *
9  * Permission to use, copy, modify and distribute this software and
10  * its documentation is hereby granted, provided that both the copyright
11  * notice and this permission notice appear in all copies of the
12  * software, derivative works or modified versions, and any portions
13  * thereof, and that both notices appear in supporting documentation.
14  *
15  * CARNEGIE MELLON ALLOWS FREE USE OF THIS SOFTWARE IN ITS "AS IS"
16  * CONDITION.  CARNEGIE MELLON DISCLAIMS ANY LIABILITY OF ANY KIND
17  * FOR ANY DAMAGES WHATSOEVER RESULTING FROM THE USE OF THIS SOFTWARE.
18  *
19  * Carnegie Mellon requests users of this software to return to
20  *
21  *  Software Distribution Coordinator  or  Software.Distribution@CS.CMU.EDU
22  *  School of Computer Science
23  *  Carnegie Mellon University
24  *  Pittsburgh PA 15213-3890
25  *
26  * any improvements or extensions that they make and grant Carnegie the
27  * rights to redistribute these changes.
28  */
30 #ifndef _SYS_CDEFS_ELF_H_
31 #define _SYS_CDEFS_ELF_H_
33 #ifdef __LEADING_UNDERSCORE
34 #define _C_LABEL(x)     __CONCAT(_,x)
35 #define _C_LABEL_STRING(x)      "_"x
36 #else
37 #define _C_LABEL(x)     x
38 #define _C_LABEL_STRING(x)      x
39 #endif
41 #define ___RENAME(x)    __asm__(___STRING(_C_LABEL(x)))
43 #define __indr_reference(sym,alias)     /* nada, since we do weak refs */
45 #define __strong_alias(alias,sym)                                       \
46     __asm__(".global " _C_LABEL_STRING(#alias) "\n"                     \
47             _C_LABEL_STRING(#alias) " = " _C_LABEL_STRING(#sym));
49 #define __weak_alias(alias,sym)                                         \
50     __asm__(".weak " _C_LABEL_STRING(#alias) "\n"                       \
51             _C_LABEL_STRING(#alias) " = " _C_LABEL_STRING(#sym));
52 #define __weak_extern(sym)                                              \
53     __asm__(".weak " _C_LABEL_STRING(#sym));
55 /* We use __warnattr instead of __warn_references.
56  * TODO: remove this and put an empty definition in one of the upstream-* compatibility headers.
57  */
58 #define __warn_references(sym,msg)                                      \
59     /*__asm__(".section .gnu.warning." #sym "\n\t.ascii \"" msg "\"\n\t.text");*/
61 #define __SECTIONSTRING(_sec, _str)                                     \
62         __asm__(".section " #_sec "\n\t.asciz \"" _str "\"\n\t.previous")
64 /* Used to tag non-static symbols that are private and never exposed by the shared library. */
65 #define __LIBC_HIDDEN__ __attribute__((visibility ("hidden")))
67 /* Like __LIBC_HIDDEN__, but preserves binary compatibility for LP32. */
68 #ifdef __LP64__
69 #define __LIBC64_HIDDEN__ __LIBC_HIDDEN__
70 #else
71 #define __LIBC64_HIDDEN__
72 #endif
74 /* Used to tag non-static symbols that are public and exposed by the shared library. */
75 #define __LIBC_ABI_PUBLIC__ __attribute__((visibility ("default")))
77 #define __IDSTRING(_n,_s)               __SECTIONSTRING(.ident,_s)
79 #define __RCSID(_s)                     __IDSTRING(rcsid,_s)
80 #define __SCCSID(_s)
81 #define __SCCSID2(_s)
82 #if 0   /* XXX userland __COPYRIGHTs have \ns in them */
83 #define __COPYRIGHT(_s)                 __SECTIONSTRING(.copyright,_s)
84 #else
85 #define __COPYRIGHT(_s)                                                 \
86         static const char copyright[]                                   \
87             __attribute__((__unused__,__section__(".copyright"))) = _s
88 #endif
90 #define __KERNEL_RCSID(_n, _s)          __RCSID(_s)
91 #define __KERNEL_SCCSID(_n, _s)
92 #if 0   /* XXX see above */
93 #define __KERNEL_COPYRIGHT(_n, _s)      __COPYRIGHT(_s)
94 #else
95 #define __KERNEL_COPYRIGHT(_n, _s)      __SECTIONSTRING(.copyright, _s)
96 #endif
98 #ifndef __lint__
99 #define __link_set_make_entry(set, sym)                                 \
100         static void const * const __link_set_##set##_sym_##sym          \
101             __section("link_set_" #set) __used = &sym
102 #define __link_set_make_entry2(set, sym, n)                             \
103         static void const * const __link_set_##set##_sym_##sym##_##n    \
104             __section("link_set_" #set) __used = &sym[n]
105 #else
106 #define __link_set_make_entry(set, sym)                                 \
107         extern void const * const __link_set_##set##_sym_##sym
108 #define __link_set_make_entry2(set, sym, n)                             \
109         extern void const * const __link_set_##set##_sym_##sym##_##n
110 #endif /* __lint__ */
112 #define __link_set_add_text(set, sym)   __link_set_make_entry(set, sym)
113 #define __link_set_add_rodata(set, sym) __link_set_make_entry(set, sym)
114 #define __link_set_add_data(set, sym)   __link_set_make_entry(set, sym)
115 #define __link_set_add_bss(set, sym)    __link_set_make_entry(set, sym)
116 #define __link_set_add_text2(set, sym, n)   __link_set_make_entry2(set, sym, n)
117 #define __link_set_add_rodata2(set, sym, n) __link_set_make_entry2(set, sym, n)
118 #define __link_set_add_data2(set, sym, n)   __link_set_make_entry2(set, sym, n)
119 #define __link_set_add_bss2(set, sym, n)    __link_set_make_entry2(set, sym, n)
121 #define __link_set_decl(set, ptype)                                     \
122         extern ptype * const __start_link_set_##set[];                  \
123         extern ptype * const __stop_link_set_##set[]                    \
125 #define __link_set_start(set)   (__start_link_set_##set)
126 #define __link_set_end(set)     (__stop_link_set_##set)
128 #define __link_set_count(set)                                           \
129         (__link_set_end(set) - __link_set_start(set))
131 #endif /* !_SYS_CDEFS_ELF_H_ */