1 /****************************************************************************
2 ****************************************************************************
3 ***
4 *** This header was automatically generated from a Linux kernel header
5 *** of the same name, to make information necessary for userspace to
6 *** call into the kernel available to libc. It contains only constants,
7 *** structures, and macros generated from the original header, and thus,
8 *** contains no copyrightable information.
9 ***
10 *** To edit the content of this header, modify the corresponding
11 *** source file (e.g. under external/kernel-headers/original/) then
12 *** run bionic/libc/kernel/tools/update_all.py
13 ***
14 *** Any manual change here will be lost the next time this script will
15 *** be run. You've been warned!
16 ***
17 ****************************************************************************
18 ****************************************************************************/
19 #ifndef _ASM_DMA_H
20 #define _ASM_DMA_H
21 #include <asm/io.h>
22 #include <linux/spinlock.h>
23 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
24 #include <linux/delay.h>
25 #include <asm/system.h>
26 #ifdef HAVE_REALLY_SLOW_DMA_CONTROLLER
27 #define dma_outb outb_p
28 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
29 #else
30 #define dma_outb outb
31 #endif
32 #define dma_inb inb
33 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
34 #define MAX_DMA_CHANNELS 8
35 #define MAX_DMA_ADDRESS (PAGE_OFFSET + 0x01000000)
36 #define MAX_DMA_PFN PFN_DOWN(virt_to_phys((void *)MAX_DMA_ADDRESS))
37 #define MAX_DMA32_PFN (1UL << (32 - PAGE_SHIFT))
38 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
39 #define IO_DMA1_BASE 0x00
40 #define IO_DMA2_BASE 0xC0
41 #define DMA1_CMD_REG 0x08
42 #define DMA1_STAT_REG 0x08
43 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
44 #define DMA1_REQ_REG 0x09
45 #define DMA1_MASK_REG 0x0A
46 #define DMA1_MODE_REG 0x0B
47 #define DMA1_CLEAR_FF_REG 0x0C
48 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
49 #define DMA1_TEMP_REG 0x0D
50 #define DMA1_RESET_REG 0x0D
51 #define DMA1_CLR_MASK_REG 0x0E
52 #define DMA1_MASK_ALL_REG 0x0F
53 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
54 #define DMA2_CMD_REG 0xD0
55 #define DMA2_STAT_REG 0xD0
56 #define DMA2_REQ_REG 0xD2
57 #define DMA2_MASK_REG 0xD4
58 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
59 #define DMA2_MODE_REG 0xD6
60 #define DMA2_CLEAR_FF_REG 0xD8
61 #define DMA2_TEMP_REG 0xDA
62 #define DMA2_RESET_REG 0xDA
63 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
64 #define DMA2_CLR_MASK_REG 0xDC
65 #define DMA2_MASK_ALL_REG 0xDE
66 #define DMA_ADDR_0 0x00
67 #define DMA_ADDR_1 0x02
68 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
69 #define DMA_ADDR_2 0x04
70 #define DMA_ADDR_3 0x06
71 #define DMA_ADDR_4 0xC0
72 #define DMA_ADDR_5 0xC4
73 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
74 #define DMA_ADDR_6 0xC8
75 #define DMA_ADDR_7 0xCC
76 #define DMA_CNT_0 0x01
77 #define DMA_CNT_1 0x03
78 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
79 #define DMA_CNT_2 0x05
80 #define DMA_CNT_3 0x07
81 #define DMA_CNT_4 0xC2
82 #define DMA_CNT_5 0xC6
83 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
84 #define DMA_CNT_6 0xCA
85 #define DMA_CNT_7 0xCE
86 #define DMA_PAGE_0 0x87
87 #define DMA_PAGE_1 0x83
88 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
89 #define DMA_PAGE_2 0x81
90 #define DMA_PAGE_3 0x82
91 #define DMA_PAGE_5 0x8B
92 #define DMA_PAGE_6 0x89
93 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
94 #define DMA_PAGE_7 0x8A
95 #define DMA_MODE_READ 0x44
96 #define DMA_MODE_WRITE 0x48
97 #define DMA_MODE_CASCADE 0xC0
98 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
99 #define DMA_AUTOINIT 0x10
100 #define isa_dma_bridge_buggy (0)
101 #endif