]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/platform-bionic.git/blob - libc/kernel/arch-x86/asm/alternative_32.h
Merge "syslog needs a valid socket path for _PATH_LOG"
[android-sdk/platform-bionic.git] / libc / kernel / arch-x86 / asm / alternative_32.h
1 /****************************************************************************
2  ****************************************************************************
3  ***
4  ***   This header was automatically generated from a Linux kernel header
5  ***   of the same name, to make information necessary for userspace to
6  ***   call into the kernel available to libc.  It contains only constants,
7  ***   structures, and macros generated from the original header, and thus,
8  ***   contains no copyrightable information.
9  ***
10  ***   To edit the content of this header, modify the corresponding
11  ***   source file (e.g. under external/kernel-headers/original/) then
12  ***   run bionic/libc/kernel/tools/update_all.py
13  ***
14  ***   Any manual change here will be lost the next time this script will
15  ***   be run. You've been warned!
16  ***
17  ****************************************************************************
18  ****************************************************************************/
19 #ifndef _I386_ALTERNATIVE_H
20 #define _I386_ALTERNATIVE_H
21 #include <asm/types.h>
22 #include <linux/stddef.h>
23 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
24 #include <linux/types.h>
25 struct alt_instr {
26  u8 *instr;
27  u8 *replacement;
28 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
29  u8 cpuid;
30  u8 instrlen;
31  u8 replacementlen;
32  u8 pad;
33 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
34 };
35 struct module;
36 #define alternative(oldinstr, newinstr, feature)   asm volatile ("661:\n\t" oldinstr "\n662:\n"   ".section .altinstructions,\"a\"\n"   "  .align 4\n"   "  .long 661b\n"     "  .long 663f\n"     "  .byte %c0\n"     "  .byte 662b-661b\n"     "  .byte 664f-663f\n"     ".previous\n"   ".section .altinstr_replacement,\"ax\"\n"   "663:\n\t" newinstr "\n664:\n"    ".previous" :: "i" (feature) : "memory")
37 #define alternative_input(oldinstr, newinstr, feature, input...)   asm volatile ("661:\n\t" oldinstr "\n662:\n"   ".section .altinstructions,\"a\"\n"   "  .align 4\n"   "  .long 661b\n"     "  .long 663f\n"     "  .byte %c0\n"     "  .byte 662b-661b\n"     "  .byte 664f-663f\n"     ".previous\n"   ".section .altinstr_replacement,\"ax\"\n"   "663:\n\t" newinstr "\n664:\n"    ".previous" :: "i" (feature), ##input)
38 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
39 #define alternative_io(oldinstr, newinstr, feature, output, input...)   asm volatile ("661:\n\t" oldinstr "\n662:\n"   ".section .altinstructions,\"a\"\n"   "  .align 4\n"   "  .long 661b\n"     "  .long 663f\n"     "  .byte %c[feat]\n"     "  .byte 662b-661b\n"     "  .byte 664f-663f\n"     ".previous\n"   ".section .altinstr_replacement,\"ax\"\n"   "663:\n\t" newinstr "\n664:\n"     ".previous" : output : [feat] "i" (feature), ##input)
40 #define ASM_OUTPUT2(a, b) a, b
41 #define LOCK_PREFIX ""
42 struct paravirt_patch_site;
43 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
44 #define __parainstructions NULL
45 #define __parainstructions_end NULL
46 #endif