1 #!/usr/bin/env python
2 #
3 # this program is used to find source code that includes linux kernel headers directly
4 # (e.g. with #include <linux/...> or #include <asm/...>)
5 #
6 # then it lists
8 import sys, cpp, glob, os, re, getopt, kernel
9 from utils import *
10 from defaults import *
12 program_dir = find_program_dir()
14 wanted_archs = kernel_archs
15 wanted_include = os.path.normpath(program_dir + '/../original')
16 wanted_config = os.path.normpath(program_dir + '/../original/config')
18 def usage():
19 print """\
20 usage: find_headers.py [options] (file|directory|@listfile)+
22 options:
23 -d <include-dir> specify alternate kernel headers
24 'include' directory
25 ('%s' by default)
27 -c <file> specify alternate .config file
28 ('%s' by default)
30 -a <archs> used to specify an alternative list
31 of architectures to support
32 ('%s' by default)
34 -v enable verbose mode
36 this program is used to find all the kernel headers that are used
37 by a set of source files or directories containing them. the search
38 is recursive to find *all* required files.
40 """ % ( wanted_include, wanted_config, string.join(kernel_archs,",") )
41 sys.exit(1)
44 try:
45 optlist, args = getopt.getopt( sys.argv[1:], 'vc:d:a:' )
46 except:
47 # unrecognized option
48 print "error: unrecognized option"
49 usage()
51 for opt, arg in optlist:
52 if opt == '-a':
53 wanted_archs = string.split(arg,',')
54 elif opt == '-d':
55 wanted_include = arg
56 elif opt == '-c':
57 wanted_config = arg
58 elif opt == '-v':
59 kernel.verboseSearch = 1
60 kernel.verboseFind = 1
61 verbose = 1
62 else:
63 usage()
65 if len(args) < 1:
66 usage()
68 kernel_root = wanted_include
69 if not os.path.exists(kernel_root):
70 sys.stderr.write( "error: directory '%s' does not exist\n" % kernel_root )
71 sys.exit(1)
73 if not os.path.isdir(kernel_root):
74 sys.stderr.write( "error: '%s' is not a directory\n" % kernel_root )
75 sys.exit(1)
77 if not os.path.isdir(kernel_root+"/linux"):
78 sys.stderr.write( "error: '%s' does not have a 'linux' directory\n" % kernel_root )
79 sys.exit(1)
81 if not os.path.exists(wanted_config):
82 sys.stderr.write( "error: file '%s' does not exist\n" % wanted_config )
83 sys.exit(1)
85 if not os.path.isfile(wanted_config):
86 sys.stderr.write( "error: '%s' is not a file\n" % wanted_config )
87 sys.exit(1)
89 # find all architectures in the kernel tree
90 re_asm_ = re.compile(r"asm-(\w+)")
91 archs = []
92 for dir in os.listdir(kernel_root):
93 m = re_asm_.match(dir)
94 if m:
95 if verbose: print ">> found kernel arch '%s'" % m.group(1)
96 archs.append(m.group(1))
98 # if we're using the 'kernel_headers' directory, there is only asm/
99 # and no other asm-<arch> directories (arm is assumed, which sucks)
100 #
101 in_kernel_headers = False
102 if len(archs) == 0:
103 # this can happen when we're using the 'kernel_headers' directory
104 if os.path.isdir(kernel_root+"/asm"):
105 in_kernel_headers = True
106 archs = [ "arm" ]
108 # if the user has specified some architectures with -a <archs> ensure that
109 # all those he wants are available from the kernel include tree
110 if wanted_archs != None:
111 if in_kernel_headers and wanted_archs != [ "arm" ]:
112 sys.stderr.write( "error: when parsing kernel_headers, 'arm' architecture only is supported at the moment\n" )
113 sys.exit(1)
114 missing = []
115 for arch in wanted_archs:
116 if arch not in archs:
117 missing.append(arch)
118 if len(missing) > 0:
119 sys.stderr.write( "error: the following requested architectures are not in the kernel tree: " )
120 for a in missing:
121 sys.stderr.write( " %s" % a )
122 sys.stderr.write( "\n" )
123 sys.exit(1)
125 archs = wanted_archs
127 # helper function used to walk the user files
128 def parse_file(path, parser):
129 parser.parseFile(path)
132 # remove previous destination directory
133 #destdir = "/tmp/bionic-kernel-headers/"
134 #cleanup_dir(destdir)
136 # try to read the config file
137 try:
138 cparser = kernel.ConfigParser()
139 cparser.parseFile( wanted_config )
140 except:
141 sys.stderr.write( "error: can't parse '%s'" % wanted_config )
142 sys.exit(1)
144 kernel_config = cparser.getDefinitions()
146 # first, obtain the list of kernel files used by our clients
147 fparser = kernel.HeaderScanner()
148 walk_source_files( args, parse_file, fparser, excludes=["kernel_headers"] )
149 headers = fparser.getHeaders()
150 files = fparser.getFiles()
152 # now recursively scan the kernel headers for additionnal sub-included headers
153 hparser = kernel.KernelHeaderFinder(headers,archs,kernel_root,kernel_config)
154 headers = hparser.scanForAllArchs()
156 if 0: # just for debugging
157 dumpHeaderUsers = False
159 print "the following %d headers:" % len(headers)
160 for h in sorted(headers):
161 if dumpHeaderUsers:
162 print " %s (%s)" % (h, repr(hparser.getHeaderUsers(h)))
163 else:
164 print " %s" % h
166 print "are used by the following %d files:" % len(files)
167 for f in sorted(files):
168 print " %s" % f
170 sys.exit(0)
172 for h in sorted(headers):
173 print h
175 sys.exit(0)