1 /* $NetBSD: reentrant.h,v 1.10 2004/12/14 00:23:19 nathanw Exp $ */
3 /*-
4 * Copyright (c) 1997, 1998, 2003 The NetBSD Foundation, Inc.
5 * All rights reserved.
6 *
7 * This code is derived from software contributed to The NetBSD Foundation
8 * by J.T. Conklin, by Nathan J. Williams, and by Jason R. Thorpe.
9 *
10 * Redistribution and use in source and binary forms, with or without
11 * modification, are permitted provided that the following conditions
12 * are met:
13 * 1. Redistributions of source code must retain the above copyright
14 * notice, this list of conditions and the following disclaimer.
15 * 2. Redistributions in binary form must reproduce the above copyright
16 * notice, this list of conditions and the following disclaimer in the
17 * documentation and/or other materials provided with the distribution.
18 * 3. All advertising materials mentioning features or use of this software
19 * must display the following acknowledgement:
20 * This product includes software developed by the NetBSD
21 * Foundation, Inc. and its contributors.
22 * 4. Neither the name of The NetBSD Foundation nor the names of its
23 * contributors may be used to endorse or promote products derived
24 * from this software without specific prior written permission.
25 *
26 * THIS SOFTWARE IS PROVIDED BY THE NETBSD FOUNDATION, INC. AND CONTRIBUTORS
27 * ``AS IS'' AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED
28 * TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
29 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE FOUNDATION OR CONTRIBUTORS
30 * BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
31 * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
32 * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
33 * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
34 * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
35 * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
36 * POSSIBILITY OF SUCH DAMAGE.
37 */
39 /*
40 * Requirements:
41 *
42 * 1. The thread safe mechanism should be lightweight so the library can
43 * be used by non-threaded applications without unreasonable overhead.
44 *
45 * 2. There should be no dependency on a thread engine for non-threaded
46 * applications.
47 *
48 * 3. There should be no dependency on any particular thread engine.
49 *
50 * 4. The library should be able to be compiled without support for thread
51 * safety.
52 *
53 *
54 * Rationale:
55 *
56 * One approach for thread safety is to provide discrete versions of the
57 * library: one thread safe, the other not. The disadvantage of this is
58 * that libc is rather large, and two copies of a library which are 99%+
59 * identical is not an efficent use of resources.
60 *
61 * Another approach is to provide a single thread safe library. However,
62 * it should not add significant run time or code size overhead to non-
63 * threaded applications.
64 *
65 * Since the NetBSD C library is used in other projects, it should be
66 * easy to replace the mutual exclusion primitives with ones provided by
67 * another system. Similarly, it should also be easy to remove all
68 * support for thread safety completely if the target environment does
69 * not support threads.
70 *
71 *
72 * Implementation Details:
73 *
74 * The thread primitives used by the library (mutex_t, mutex_lock, etc.)
75 * are macros which expand to the cooresponding primitives provided by
76 * the thread engine or to nothing. The latter is used so that code is
77 * not unreasonably cluttered with #ifdefs when all thread safe support
78 * is removed.
79 *
80 * The thread macros can be directly mapped to the mutex primitives from
81 * pthreads, however it should be reasonably easy to wrap another mutex
82 * implementation so it presents a similar interface.
83 *
84 * The thread functions operate by dispatching to symbols which are, by
85 * default, weak-aliased to no-op functions in thread-stub/thread-stub.c
86 * (some uses of thread operations are conditional on __isthreaded, but
87 * not all of them are).
88 *
89 * When the thread library is linked in, it provides strong-alias versions
90 * of those symbols which dispatch to its own real thread operations.
91 *
92 */
94 #ifdef _REENTRANT
96 /*
97 * Abtract thread interface for thread-safe libraries. These routines
98 * will use stubs in libc if the application is not linked against the
99 * pthread library, and the real function in the pthread library if it
100 * is.
101 */
103 #include <pthread.h>
104 #include <signal.h>
105 #include <sys/cdefs.h>
107 #define mutex_t pthread_mutex_t
108 #define MUTEX_INITIALIZER PTHREAD_MUTEX_INITIALIZER
110 #define mutexattr_t pthread_mutexattr_t
112 #define MUTEX_TYPE_NORMAL PTHREAD_MUTEX_NORMAL
113 #define MUTEX_TYPE_ERRORCHECK PTHREAD_MUTEX_ERRORCHECK
114 #define MUTEX_TYPE_RECURSIVE PTHREAD_MUTEX_RECURSIVE
116 #define cond_t pthread_cond_t
117 #define COND_INITIALIZER PTHREAD_COND_INITIALIZER
119 #define condattr_t pthread_condattr_t
121 #define rwlock_t pthread_rwlock_t
122 #define RWLOCK_INITIALIZER PTHREAD_RWLOCK_INITIALIZER
124 #define rwlockattr_t pthread_rwlockattr_t
126 #define thread_key_t pthread_key_t
128 #define thr_t pthread_t
130 #define thrattr_t pthread_attr_t
132 #define once_t pthread_once_t
133 #define ONCE_INITIALIZER PTHREAD_ONCE_INIT
135 #ifndef __LIBC_THREAD_STUBS
137 __BEGIN_DECLS
138 int __libc_mutex_init(mutex_t *, const mutexattr_t *);
139 int __libc_mutex_lock(mutex_t *);
140 int __libc_mutex_trylock(mutex_t *);
141 int __libc_mutex_unlock(mutex_t *);
142 int __libc_mutex_destroy(mutex_t *);
144 int __libc_mutexattr_init(mutexattr_t *);
145 int __libc_mutexattr_settype(mutexattr_t *, int);
146 int __libc_mutexattr_destroy(mutexattr_t *);
147 __END_DECLS
149 #define mutex_init(m, a) __libc_mutex_init((m), (a))
150 #define mutex_lock(m) __libc_mutex_lock((m))
151 #define mutex_trylock(m) __libc_mutex_trylock((m))
152 #define mutex_unlock(m) __libc_mutex_unlock((m))
153 #define mutex_destroy(m) __libc_mutex_destroy((m))
155 #define mutexattr_init(ma) __libc_mutexattr_init((ma))
156 #define mutexattr_settype(ma, t) __libc_mutexattr_settype((ma), (t))
157 #define mutexattr_destroy(ma) __libc_mutexattr_destroy((ma))
159 __BEGIN_DECLS
160 int __libc_cond_init(cond_t *, const condattr_t *);
161 int __libc_cond_signal(cond_t *);
162 int __libc_cond_broadcast(cond_t *);
163 int __libc_cond_wait(cond_t *, mutex_t *);
164 int __libc_cond_timedwait(cond_t *, mutex_t *, const struct timespec *);
165 int __libc_cond_destroy(cond_t *);
166 __END_DECLS
168 #define cond_init(c, t, a) __libc_cond_init((c), (a))
169 #define cond_signal(c) __libc_cond_signal((c))
170 #define cond_broadcast(c) __libc_cond_broadcast((c))
171 #define cond_wait(c, m) __libc_cond_wait((c), (m))
172 #define cond_timedwait(c, m, t) __libc_cond_timedwait((c), (m), (t))
173 #define cond_destroy(c) __libc_cond_destroy((c))
175 __BEGIN_DECLS
176 int __libc_rwlock_init(rwlock_t *, const rwlockattr_t *);
177 int __libc_rwlock_rdlock(rwlock_t *);
178 int __libc_rwlock_wrlock(rwlock_t *);
179 int __libc_rwlock_tryrdlock(rwlock_t *);
180 int __libc_rwlock_trywrlock(rwlock_t *);
181 int __libc_rwlock_unlock(rwlock_t *);
182 int __libc_rwlock_destroy(rwlock_t *);
183 __END_DECLS
185 #define rwlock_init(l, a) __libc_rwlock_init((l), (a))
186 #define rwlock_rdlock(l) __libc_rwlock_rdlock((l))
187 #define rwlock_wrlock(l) __libc_rwlock_wrlock((l))
188 #define rwlock_tryrdlock(l) __libc_rwlock_tryrdlock((l))
189 #define rwlock_trywrlock(l) __libc_rwlock_trywrlock((l))
190 #define rwlock_unlock(l) __libc_rwlock_unlock((l))
191 #define rwlock_destroy(l) __libc_rwlock_destroy((l))
193 __BEGIN_DECLS
194 int __libc_thr_keycreate(thread_key_t *, void (*)(void *));
195 int __libc_thr_setspecific(thread_key_t, const void *);
196 void *__libc_thr_getspecific(thread_key_t);
197 int __libc_thr_keydelete(thread_key_t);
198 __END_DECLS
200 #define thr_keycreate(k, d) __libc_thr_keycreate((k), (d))
201 #define thr_setspecific(k, p) __libc_thr_setspecific((k), (p))
202 #define thr_getspecific(k) __libc_thr_getspecific((k))
203 #define thr_keydelete(k) __libc_thr_keydelete((k))
205 __BEGIN_DECLS
206 int __libc_thr_once(once_t *, void (*)(void));
207 int __libc_thr_sigsetmask(int, const sigset_t *, sigset_t *);
208 thr_t __libc_thr_self(void);
209 int __libc_thr_yield(void);
210 void __libc_thr_create(thr_t *, const thrattr_t *,
211 void *(*)(void *), void *);
212 void __libc_thr_exit(void *) __attribute__((__noreturn__));
213 int *__libc_thr_errno(void);
214 int __libc_thr_setcancelstate(int, int *);
216 extern int __isthreaded;
217 __END_DECLS
219 #define thr_once(o, f) __libc_thr_once((o), (f))
220 #define thr_sigsetmask(f, n, o) __libc_thr_sigsetmask((f), (n), (o))
221 #define thr_self() __libc_thr_self()
222 #define thr_yield() __libc_thr_yield()
223 #define thr_create(tp, ta, f, a) __libc_thr_create((tp), (ta), (f), (a))
224 #define thr_exit(v) __libc_thr_exit((v))
225 #define thr_errno() __libc_thr_errno()
226 #define thr_enabled() (__isthreaded)
227 #define thr_setcancelstate(n, o) __libc_thr_setcancelstate((n),(o))
228 #endif /* __LIBC_THREAD_STUBS */
230 #define FLOCKFILE(fp) __flockfile_internal(fp, 1)
231 #define FUNLOCKFILE(fp) __funlockfile_internal(fp, 1)
233 #else /* _REENTRANT */
235 #define mutex_init(m, a)
236 #define mutex_lock(m)
237 #define mutex_trylock(m)
238 #define mutex_unlock(m)
239 #define mutex_destroy(m)
241 #define cond_init(c, t, a)
242 #define cond_signal(c)
243 #define cond_broadcast(c)
244 #define cond_wait(c, m)
245 #define cond_timedwait(c, m, t)
246 #define cond_destroy(c)
248 #define rwlock_init(l, a)
249 #define rwlock_rdlock(l)
250 #define rwlock_wrlock(l)
251 #define rwlock_tryrdlock(l)
252 #define rwlock_trywrlock(l)
253 #define rwlock_unlock(l)
254 #define rwlock_destroy(l)
256 #define thr_keycreate(k, d)
257 #define thr_setspecific(k, p)
258 #define thr_getspecific(k)
259 #define thr_keydelete(k)
261 #define thr_once(o, f)
262 #define thr_sigsetmask(f, n, o)
263 #define thr_self()
264 #define thr_errno()
266 #define FLOCKFILE(fp)
267 #define FUNLOCKFILE(fp)
269 #endif /* _REENTRANT */