]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/platform-bionic.git/blob - libc/private/bionic_atomic_arm.h
Merge "Kexec header generated from linux header 3.10"
[android-sdk/platform-bionic.git] / libc / private / bionic_atomic_arm.h
1 /*
2  * Copyright (C) 2011 The Android Open Source Project
3  *
4  * Licensed under the Apache License, Version 2.0 (the "License");
5  * you may not use this file except in compliance with the License.
6  * You may obtain a copy of the License at
7  *
8  *      http://www.apache.org/licenses/LICENSE-2.0
9  *
10  * Unless required by applicable law or agreed to in writing, software
11  * distributed under the License is distributed on an "AS IS" BASIS,
12  * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13  * See the License for the specific language governing permissions and
14  * limitations under the License.
15  */
16 #ifndef BIONIC_ATOMIC_ARM_H
17 #define BIONIC_ATOMIC_ARM_H
19 #include <machine/cpu-features.h>
21 /* Some of the harware instructions used below are not available in Thumb-1
22  * mode (they are if you build in ARM or Thumb-2 mode though). To solve this
23  * problem, we're going to use the same technique than libatomics_ops,
24  * which is to temporarily switch to ARM, do the operation, then switch
25  * back to Thumb-1.
26  *
27  * This results in two 'bx' jumps, just like a normal function call, but
28  * everything is kept inlined, avoids loading or computing the function's
29  * address, and prevents a little I-cache trashing too.
30  *
31  * However, it is highly recommended to avoid compiling any C library source
32  * file that use these functions in Thumb-1 mode.
33  *
34  * Define three helper macros to implement this:
35  */
36 #if defined(__thumb__) && !defined(__thumb2__)
37 #  define  __ATOMIC_SWITCH_TO_ARM \
38             "adr r3, 5f\n" \
39             "bx  r3\n" \
40             ".align\n" \
41             ".arm\n" \
42         "5:\n"
43 /* note: the leading \n below is intentional */
44 #  define __ATOMIC_SWITCH_TO_THUMB \
45             "\n" \
46             "adr r3, 6f\n" \
47             "bx  r3\n" \
48             ".thumb" \
49         "6:\n"
51 #  define __ATOMIC_CLOBBERS   "r3"  /* list of clobbered registers */
53 /* Warn the user that ARM mode should really be preferred! */
54 #  warning Rebuilding this source file in ARM mode is highly recommended for performance!!
56 #else
57 #  define  __ATOMIC_SWITCH_TO_ARM   /* nothing */
58 #  define  __ATOMIC_SWITCH_TO_THUMB /* nothing */
59 #  define  __ATOMIC_CLOBBERS        /* nothing */
60 #endif
63 /* Define a full memory barrier, this is only needed if we build the
64  * platform for a multi-core device. For the record, using a 'dmb'
65  * instruction on a Nexus One device can take up to 180 ns even if
66  * it is completely un-necessary on this device.
67  *
68  * NOTE: This is where the platform and NDK headers atomic headers are
69  *        going to diverge. With the NDK, we don't know if the generated
70  *        code is going to run on a single or multi-core device, so we
71  *        need to be cautious.
72  *
73  *        I.e. on single-core devices, the helper immediately returns,
74  *        on multi-core devices, it uses "dmb" or any other means to
75  *        perform a full-memory barrier.
76  *
77  * There are three cases to consider for the platform:
78  *
79  *    - multi-core ARMv7-A       => use the 'dmb' hardware instruction
80  *    - multi-core ARMv6         => use the coprocessor
81  *    - single core ARMv6+       => do not use any hardware barrier
82  */
83 #if defined(ANDROID_SMP) && ANDROID_SMP == 1
85 /* Sanity check, multi-core is only supported starting from ARMv6 */
86 #  if __ARM_ARCH__ < 6
87 #    error ANDROID_SMP should not be set to 1 for an ARM architecture less than 6
88 #  endif
90 #  ifdef __ARM_HAVE_DMB
91 /* For ARMv7-A, we can use the 'dmb' instruction directly */
92 __ATOMIC_INLINE__ void
93 __bionic_memory_barrier(void)
94 {
95     /* Note: we always build in ARM or Thumb-2 on ARMv7-A, so don't
96      * bother with __ATOMIC_SWITCH_TO_ARM */
97     __asm__ __volatile__ ( "dmb" : : : "memory" );
98 }
99 #  else /* !__ARM_HAVE_DMB */
100 /* Otherwise, i.e. for multi-core ARMv6, we need to use the coprocessor,
101  * which requires the use of a general-purpose register, which is slightly
102  * less efficient.
103  */
104 __ATOMIC_INLINE__ void
105 __bionic_memory_barrier(void)
107     __asm__ __volatile__ (
108         __SWITCH_TO_ARM
109         "mcr p15, 0, %0, c7, c10, 5"
110         __SWITCH_TO_THUMB
111         : : "r" (0) : __ATOMIC_CLOBBERS "memory");
113 #  endif /* !__ARM_HAVE_DMB */
114 #else /* !ANDROID_SMP */
115 __ATOMIC_INLINE__ void
116 __bionic_memory_barrier(void)
118     /* A simple compiler barrier */
119     __asm__ __volatile__ ( "" : : : "memory" );
121 #endif /* !ANDROID_SMP */
123 #ifndef __ARM_HAVE_LDREX_STREX
124 #error Only ARM devices which have LDREX / STREX are supported
125 #endif
127 /* Compare-and-swap, without any explicit barriers. Note that this functions
128  * returns 0 on success, and 1 on failure. The opposite convention is typically
129  * used on other platforms.
130  */
131 __ATOMIC_INLINE__ int
132 __bionic_cmpxchg(int32_t old_value, int32_t new_value, volatile int32_t* ptr)
134     int32_t prev, status;
135     do {
136         __asm__ __volatile__ (
137             __ATOMIC_SWITCH_TO_ARM
138             "ldrex %0, [%3]\n"
139             "mov %1, #0\n"
140             "teq %0, %4\n"
141 #ifdef __thumb2__
142             "it eq\n"
143 #endif
144             "strexeq %1, %5, [%3]"
145             __ATOMIC_SWITCH_TO_THUMB
146             : "=&r" (prev), "=&r" (status), "+m"(*ptr)
147             : "r" (ptr), "Ir" (old_value), "r" (new_value)
148             : __ATOMIC_CLOBBERS "cc");
149     } while (__builtin_expect(status != 0, 0));
150     return prev != old_value;
153 /* Swap operation, without any explicit barriers. */
154 __ATOMIC_INLINE__ int32_t
155 __bionic_swap(int32_t new_value, volatile int32_t* ptr)
157     int32_t prev, status;
158     do {
159         __asm__ __volatile__ (
160             __ATOMIC_SWITCH_TO_ARM
161             "ldrex %0, [%3]\n"
162             "strex %1, %4, [%3]"
163             __ATOMIC_SWITCH_TO_THUMB
164             : "=&r" (prev), "=&r" (status), "+m" (*ptr)
165             : "r" (ptr), "r" (new_value)
166             : __ATOMIC_CLOBBERS "cc");
167     } while (__builtin_expect(status != 0, 0));
168     return prev;
171 /* Atomic increment - without any barriers
172  * This returns the old value
173  */
174 __ATOMIC_INLINE__ int32_t
175 __bionic_atomic_inc(volatile int32_t* ptr)
177     int32_t prev, tmp, status;
178     do {
179         __asm__ __volatile__ (
180             __ATOMIC_SWITCH_TO_ARM
181             "ldrex %0, [%4]\n"
182             "add %1, %0, #1\n"
183             "strex %2, %1, [%4]"
184             __ATOMIC_SWITCH_TO_THUMB
185             : "=&r" (prev), "=&r" (tmp), "=&r" (status), "+m"(*ptr)
186             : "r" (ptr)
187             : __ATOMIC_CLOBBERS "cc");
188     } while (__builtin_expect(status != 0, 0));
189     return prev;
192 /* Atomic decrement - without any barriers
193  * This returns the old value.
194  */
195 __ATOMIC_INLINE__ int32_t
196 __bionic_atomic_dec(volatile int32_t* ptr)
198     int32_t prev, tmp, status;
199     do {
200         __asm__ __volatile__ (
201             __ATOMIC_SWITCH_TO_ARM
202             "ldrex %0, [%4]\n"
203             "sub %1, %0, #1\n"
204             "strex %2, %1, [%4]"
205             __ATOMIC_SWITCH_TO_THUMB
206             : "=&r" (prev), "=&r" (tmp), "=&r" (status), "+m"(*ptr)
207             : "r" (ptr)
208             : __ATOMIC_CLOBBERS "cc");
209     } while (__builtin_expect(status != 0, 0));
210     return prev;
213 #endif /* SYS_ATOMICS_ARM_H */