]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/platform-bionic.git/blob - libc/private/bionic_atomic_mips.h
am 04583ce9: Upgrade to tzdata2014a.
[android-sdk/platform-bionic.git] / libc / private / bionic_atomic_mips.h
1 /*
2  * Copyright (C) 2011 The Android Open Source Project
3  *
4  * Licensed under the Apache License, Version 2.0 (the "License");
5  * you may not use this file except in compliance with the License.
6  * You may obtain a copy of the License at
7  *
8  *      http://www.apache.org/licenses/LICENSE-2.0
9  *
10  * Unless required by applicable law or agreed to in writing, software
11  * distributed under the License is distributed on an "AS IS" BASIS,
12  * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13  * See the License for the specific language governing permissions and
14  * limitations under the License.
15  */
16 #ifndef BIONIC_ATOMIC_MIPS_H
17 #define BIONIC_ATOMIC_MIPS_H
19 /* Define a full memory barrier, this is only needed if we build the
20  * platform for a multi-core device.
21  */
23 __ATOMIC_INLINE__ void __bionic_memory_barrier() {
24 #if defined(ANDROID_SMP) && ANDROID_SMP == 1
25   __asm__ __volatile__ ( "sync" : : : "memory" );
26 #else
27   /* A simple compiler barrier. */
28   __asm__ __volatile__ ( "" : : : "memory" );
29 #endif
30 }
32 /* Compare-and-swap, without any explicit barriers. Note that this function
33  * returns 0 on success, and 1 on failure. The opposite convention is typically
34  * used on other platforms.
35  */
36 __ATOMIC_INLINE__ int __bionic_cmpxchg(int32_t old_value, int32_t new_value, volatile int32_t* ptr) {
37   int32_t prev, status;
38   __asm__ __volatile__ ("1: move %[status], %[new_value]  \n"
39                         "   ll %[prev], 0(%[ptr])         \n"
40                         "   bne %[old_value], %[prev], 2f \n"
41                         "   sc   %[status], 0(%[ptr])     \n"
42                         "   beqz %[status], 1b            \n"
43                         "2:                               \n"
44                         : [prev]"=&r"(prev), [status]"=&r"(status), "+m"(*ptr)
45                         : [new_value]"r"(new_value), [old_value]"r"(old_value), [ptr]"r"(ptr)
46                         : "memory");
47   return prev != old_value;
48 }
50 /* Swap, without any explicit barriers. */
51 __ATOMIC_INLINE__ int32_t __bionic_swap(int32_t new_value, volatile int32_t* ptr) {
52   int32_t prev, status;
53   __asm__ __volatile__ ("1:  move %[status], %[new_value] \n"
54                         "    ll %[prev], 0(%[ptr])        \n"
55                         "    sc %[status], 0(%[ptr])      \n"
56                         "    beqz %[status], 1b           \n"
57                         : [prev]"=&r"(prev), [status]"=&r"(status), "+m"(*ptr)
58                         : [ptr]"r"(ptr), [new_value]"r"(new_value)
59                         : "memory");
60   return prev;
61 }
63 /* Atomic decrement, without explicit barriers. */
64 __ATOMIC_INLINE__ int32_t __bionic_atomic_dec(volatile int32_t* ptr) {
65   int32_t prev, status;
66   __asm__ __volatile__ ("1:  ll %[prev], 0(%[ptr])        \n"
67                         "    addiu %[status], %[prev], -1 \n"
68                         "    sc   %[status], 0(%[ptr])    \n"
69                         "    beqz %[status], 1b           \n"
70                         : [prev]"=&r" (prev), [status]"=&r"(status), "+m" (*ptr)
71                         : [ptr]"r"(ptr)
72                         : "memory");
73   return prev;
74 }
76 #endif /* BIONIC_ATOMIC_MIPS_H */