]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/platform-bionic.git/blob - libc/private/bionic_atomic_x86.h
am 2b89f1e3: Merge "Fix sysconf(_SC_NPROCESSORS_CONF) on ARM."
[android-sdk/platform-bionic.git] / libc / private / bionic_atomic_x86.h
1 /*
2  * Copyright (C) 2011 The Android Open Source Project
3  *
4  * Licensed under the Apache License, Version 2.0 (the "License");
5  * you may not use this file except in compliance with the License.
6  * You may obtain a copy of the License at
7  *
8  *      http://www.apache.org/licenses/LICENSE-2.0
9  *
10  * Unless required by applicable law or agreed to in writing, software
11  * distributed under the License is distributed on an "AS IS" BASIS,
12  * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13  * See the License for the specific language governing permissions and
14  * limitations under the License.
15  */
16 #ifndef BIONIC_ATOMIC_X86_H
17 #define BIONIC_ATOMIC_X86_H
19 /* Define a full memory barrier, this is only needed if we build the
20  * platform for a multi-core device.
21  */
22 #if defined(ANDROID_SMP) && ANDROID_SMP == 1
23 __ATOMIC_INLINE__ void
24 __bionic_memory_barrier()
25 {
26     __asm__ __volatile__ ( "mfence" : : : "memory" );
27 }
28 #else
29 __ATOMIC_INLINE__ void
30 __bionic_memory_barrier()
31 {
32     /* A simple compiler barrier */
33     __asm__ __volatile__ ( "" : : : "memory" );
34 }
35 #endif
37 /* Compare-and-swap, without any explicit barriers. Note that this function
38  * returns 0 on success, and 1 on failure. The opposite convention is typically
39  * used on other platforms.
40  */
41 __ATOMIC_INLINE__ int
42 __bionic_cmpxchg(int32_t old_value, int32_t new_value, volatile int32_t* ptr)
43 {
44     int32_t prev;
45     __asm__ __volatile__ ("lock; cmpxchgl %1, %2"
46                           : "=a" (prev)
47                           : "q" (new_value), "m" (*ptr), "0" (old_value)
48                           : "memory");
49     return prev != old_value;
50 }
53 /* Swap, without any explicit barriers */
54 __ATOMIC_INLINE__ int32_t
55 __bionic_swap(int32_t new_value, volatile int32_t *ptr)
56 {
57     __asm__ __volatile__ ("xchgl %1, %0"
58                           : "=r" (new_value)
59                           : "m" (*ptr), "0" (new_value)
60                           : "memory");
61     return new_value;
62 }
64 /* Atomic increment, without explicit barriers */
65 __ATOMIC_INLINE__ int32_t
66 __bionic_atomic_inc(volatile int32_t *ptr)
67 {
68     int increment = 1;
69     __asm__ __volatile__ ("lock; xaddl %0, %1"
70                           : "+r" (increment), "+m" (*ptr)
71                           : : "memory");
72     /* increment now holds the old value of *ptr */
73     return increment;
74 }
76 /* Atomic decrement, without explicit barriers */
77 __ATOMIC_INLINE__ int32_t
78 __bionic_atomic_dec(volatile int32_t *ptr)
79 {
80     int increment = -1;
81     __asm__ __volatile__ ("lock; xaddl %0, %1"
82                           : "+r" (increment), "+m" (*ptr)
83                           : : "memory");
84     /* increment now holds the old value of *ptr */
85     return increment;
86 }
88 #endif /* BIONIC_ATOMIC_X86_H */