1 /*
2 * Copyright (C) 2011 The Android Open Source Project
3 * All rights reserved.
4 *
5 * Redistribution and use in source and binary forms, with or without
6 * modification, are permitted provided that the following conditions
7 * are met:
8 * * Redistributions of source code must retain the above copyright
9 * notice, this list of conditions and the following disclaimer.
10 * * Redistributions in binary form must reproduce the above copyright
11 * notice, this list of conditions and the following disclaimer in
12 * the documentation and/or other materials provided with the
13 * distribution.
14 *
15 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
16 * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
17 * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS
18 * FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE
19 * COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT,
20 * INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING,
21 * BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS
22 * OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED
23 * AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
24 * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT
25 * OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF
26 * SUCH DAMAGE.
27 */
28 #ifndef _RESOLV_IFACE_H
29 #define _RESOLV_IFACE_H
31 /* This header contains declarations related to per-interface DNS
32 * server selection. They are used by system/netd/ and should not be
33 * exposed by the C library's public NDK headers.
34 *
35 * NOTE: <resolv.h> contains the same declarations, this will be removed
36 * when we change system/netd to use this header instead.
37 */
38 #include <sys/cdefs.h>
39 #include <netinet/in.h>
41 __BEGIN_DECLS
43 /* Use a guard macro until we remove the same definitions from <resolv.h> */
44 #ifndef _BIONIC_RESOLV_IFACE_FUNCTIONS_DECLARED
45 #define _BIONIC_RESOLV_IFACE_FUNCTIONS_DECLARED
47 /* Set name of default interface */
48 extern void _resolv_set_default_iface(const char* ifname);
50 /* set name servers for an interface */
51 extern void _resolv_set_nameservers_for_iface(const char* ifname, const char** servers, int numservers,
52 const char *domains);
54 /* tell resolver of the address of an interface */
55 extern void _resolv_set_addr_of_iface(const char* ifname, struct in_addr* addr);
57 /* flush the cache associated with the default interface */
58 extern void _resolv_flush_cache_for_default_iface();
60 /* flush the cache associated with a certain interface */
61 extern void _resolv_flush_cache_for_iface(const char* ifname);
63 /* set a pid to use the name servers of the specified interface */
64 extern void _resolv_set_iface_for_pid(const char* ifname, int pid);
66 /* clear pid from being associated with an interface */
67 extern void _resolv_clear_iface_for_pid(int pid);
69 /* clear the entire mapping of pids to interfaces. */
70 extern void _resolv_clear_iface_pid_mapping();
72 /** Gets the name of the interface to which the pid is attached.
73 * On error, -1 is returned.
74 * If no interface is found, 0 is returned and buff is set to empty ('\0').
75 * If an interface is found, the name is copied to buff and the length of the name is returned.
76 * Arguments: pid The pid to find an interface for
77 * buff A buffer to copy the result to
78 * buffLen Length of buff. An interface is at most IF_NAMESIZE in length */
79 extern int _resolv_get_pids_associated_interface(int pid, char* buff, int buffLen);
82 /** set a uid range to use the name servers of the specified interface
83 * If [low,high] overlaps with an already existing rule -1 is returned */
84 extern int _resolv_set_iface_for_uid_range(const char* ifname, int uid_start, int uid_end);
86 /* clear a uid range from being associated with an interface
87 * If the range given is not mapped -1 is returned. */
88 extern int _resolv_clear_iface_for_uid_range(int uid_start, int uid_end);
90 /* clear the entire mapping of uid ranges to interfaces. */
91 extern void _resolv_clear_iface_uid_range_mapping();
93 /** Gets the name of the interface to which the uid is attached.
94 * On error, -1 is returned.
95 * If no interface is found, 0 is returned and buff is set to empty ('\0').
96 * If an interface is found, the name is copied to buff and the length of the name is returned.
97 * Arguments: uid The uid to find an interface for
98 * buff A buffer to copy the result to
99 * buffLen Length of buff. An interface is at most IF_NAMESIZE in length */
100 extern int _resolv_get_uids_associated_interface(int uid, char* buff, int buffLen);
102 #endif /* _BIONIC_RESOLV_IFACE_FUNCTIONS_DECLARED */
104 __END_DECLS
106 #endif /* _RESOLV_IFACE_H */