1 /* $OpenBSD: fseek.c,v 1.7 2005/08/08 08:05:36 espie Exp $ */
2 /*-
3 * Copyright (c) 1990, 1993
4 * The Regents of the University of California. All rights reserved.
5 *
6 * This code is derived from software contributed to Berkeley by
7 * Chris Torek.
8 *
9 * Redistribution and use in source and binary forms, with or without
10 * modification, are permitted provided that the following conditions
11 * are met:
12 * 1. Redistributions of source code must retain the above copyright
13 * notice, this list of conditions and the following disclaimer.
14 * 2. Redistributions in binary form must reproduce the above copyright
15 * notice, this list of conditions and the following disclaimer in the
16 * documentation and/or other materials provided with the distribution.
17 * 3. Neither the name of the University nor the names of its contributors
18 * may be used to endorse or promote products derived from this software
19 * without specific prior written permission.
20 *
21 * THIS SOFTWARE IS PROVIDED BY THE REGENTS AND CONTRIBUTORS ``AS IS'' AND
22 * ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
23 * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
24 * ARE DISCLAIMED. IN NO EVENT SHALL THE REGENTS OR CONTRIBUTORS BE LIABLE
25 * FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL
26 * DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS
27 * OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION)
28 * HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT
29 * LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY
30 * OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF
31 * SUCH DAMAGE.
32 */
34 #include <sys/types.h>
35 #include <sys/stat.h>
36 #include <fcntl.h>
37 #include <stdio.h>
38 #include <stdlib.h>
39 #include <errno.h>
40 #include "local.h"
42 #define POS_ERR (-(fpos_t)1)
44 /*
45 * Seek the given file to the given offset.
46 * `Whence' must be one of the three SEEK_* macros.
47 */
48 int
49 fseeko(FILE *fp, off_t offset, int whence)
50 {
51 fpos_t (*seekfn)(void *, fpos_t, int);
52 fpos_t target, curoff;
53 size_t n;
54 struct stat st;
55 int havepos;
57 /* make sure stdio is set up */
58 if (!__sdidinit)
59 __sinit();
61 /*
62 * Have to be able to seek.
63 */
64 if ((seekfn = fp->_seek) == NULL) {
65 errno = ESPIPE; /* historic practice */
66 return (EOF);
67 }
69 /*
70 * Change any SEEK_CUR to SEEK_SET, and check `whence' argument.
71 * After this, whence is either SEEK_SET or SEEK_END.
72 */
73 switch (whence) {
75 case SEEK_CUR:
76 /*
77 * In order to seek relative to the current stream offset,
78 * we have to first find the current stream offset a la
79 * ftell (see ftell for details).
80 */
81 __sflush(fp); /* may adjust seek offset on append stream */
82 if (fp->_flags & __SOFF)
83 curoff = fp->_offset;
84 else {
85 curoff = (*seekfn)(fp->_cookie, (fpos_t)0, SEEK_CUR);
86 if (curoff == (fpos_t)-1)
87 return (EOF);
88 }
89 if (fp->_flags & __SRD) {
90 curoff -= fp->_r;
91 if (HASUB(fp))
92 curoff -= fp->_ur;
93 } else if (fp->_flags & __SWR && fp->_p != NULL)
94 curoff += fp->_p - fp->_bf._base;
96 offset += curoff;
97 whence = SEEK_SET;
98 havepos = 1;
99 break;
101 case SEEK_SET:
102 case SEEK_END:
103 curoff = 0; /* XXX just to keep gcc quiet */
104 havepos = 0;
105 break;
107 default:
108 errno = EINVAL;
109 return (EOF);
110 }
112 /*
113 * Can only optimise if:
114 * reading (and not reading-and-writing);
115 * not unbuffered; and
116 * this is a `regular' Unix file (and hence seekfn==__sseek).
117 * We must check __NBF first, because it is possible to have __NBF
118 * and __SOPT both set.
119 */
120 if (fp->_bf._base == NULL)
121 __smakebuf(fp);
122 if (fp->_flags & (__SWR | __SRW | __SNBF | __SNPT))
123 goto dumb;
124 if ((fp->_flags & __SOPT) == 0) {
125 if (seekfn != __sseek ||
126 fp->_file < 0 || fstat(fp->_file, &st) ||
127 (st.st_mode & S_IFMT) != S_IFREG) {
128 fp->_flags |= __SNPT;
129 goto dumb;
130 }
131 fp->_blksize = st.st_blksize;
132 fp->_flags |= __SOPT;
133 }
135 /*
136 * We are reading; we can try to optimise.
137 * Figure out where we are going and where we are now.
138 */
139 if (whence == SEEK_SET)
140 target = offset;
141 else {
142 if (fstat(fp->_file, &st))
143 goto dumb;
144 target = st.st_size + offset;
145 }
147 if (!havepos) {
148 if (fp->_flags & __SOFF)
149 curoff = fp->_offset;
150 else {
151 curoff = (*seekfn)(fp->_cookie, (fpos_t)0, SEEK_CUR);
152 if (curoff == POS_ERR)
153 goto dumb;
154 }
155 curoff -= fp->_r;
156 if (HASUB(fp))
157 curoff -= fp->_ur;
158 }
160 /*
161 * Compute the number of bytes in the input buffer (pretending
162 * that any ungetc() input has been discarded). Adjust current
163 * offset backwards by this count so that it represents the
164 * file offset for the first byte in the current input buffer.
165 */
166 if (HASUB(fp)) {
167 curoff += fp->_r; /* kill off ungetc */
168 n = fp->_up - fp->_bf._base;
169 curoff -= n;
170 n += fp->_ur;
171 } else {
172 n = fp->_p - fp->_bf._base;
173 curoff -= n;
174 n += fp->_r;
175 }
177 /*
178 * If the target offset is within the current buffer,
179 * simply adjust the pointers, clear EOF, undo ungetc(),
180 * and return. (If the buffer was modified, we have to
181 * skip this; see fgetln.c.)
182 */
183 if ((fp->_flags & __SMOD) == 0 &&
184 target >= curoff && target < (fpos_t)(curoff + n)) {
185 int o = target - curoff;
187 fp->_p = fp->_bf._base + o;
188 fp->_r = n - o;
189 if (HASUB(fp))
190 FREEUB(fp);
191 fp->_flags &= ~__SEOF;
192 return (0);
193 }
195 /*
196 * The place we want to get to is not within the current buffer,
197 * but we can still be kind to the kernel copyout mechanism.
198 * By aligning the file offset to a block boundary, we can let
199 * the kernel use the VM hardware to map pages instead of
200 * copying bytes laboriously. Using a block boundary also
201 * ensures that we only read one block, rather than two.
202 */
203 curoff = target & ~(fp->_blksize - 1);
204 if ((*seekfn)(fp->_cookie, curoff, SEEK_SET) == POS_ERR)
205 goto dumb;
206 fp->_r = 0;
207 fp->_p = fp->_bf._base;
208 if (HASUB(fp))
209 FREEUB(fp);
210 fp->_flags &= ~__SEOF;
211 n = target - curoff;
212 if (n) {
213 if (__srefill(fp) || (size_t)fp->_r < n)
214 goto dumb;
215 fp->_p += n;
216 fp->_r -= n;
217 }
218 return (0);
220 /*
221 * We get here if we cannot optimise the seek ... just
222 * do it. Allow the seek function to change fp->_bf._base.
223 */
224 dumb:
225 if (__sflush(fp) ||
226 (*seekfn)(fp->_cookie, (fpos_t)offset, whence) == POS_ERR) {
227 return (EOF);
228 }
229 /* success: clear EOF indicator and discard ungetc() data */
230 if (HASUB(fp))
231 FREEUB(fp);
232 fp->_p = fp->_bf._base;
233 fp->_r = 0;
234 /* fp->_w = 0; */ /* unnecessary (I think...) */
235 fp->_flags &= ~__SEOF;
236 return (0);
237 }
239 /*
240 * fseek()'s offset is a long and sizeof(off_t) != sizeof(long) on all arches
241 */
242 #if defined(__alpha__) && defined(__indr_reference)
243 __indr_reference(fseeko, fseek);
244 #else
245 int
246 fseek(FILE *fp, long offset, int whence)
247 {
248 off_t off = offset;
250 return(fseeko(fp, off, whence));
251 }
252 #endif