1 /*-
2 * Copyright (c) 2004-2005 David Schultz <das@FreeBSD.ORG>
3 * All rights reserved.
4 *
5 * Redistribution and use in source and binary forms, with or without
6 * modification, are permitted provided that the following conditions
7 * are met:
8 * 1. Redistributions of source code must retain the above copyright
9 * notice, this list of conditions and the following disclaimer.
10 * 2. Redistributions in binary form must reproduce the above copyright
11 * notice, this list of conditions and the following disclaimer in the
12 * documentation and/or other materials provided with the distribution.
13 *
14 * THIS SOFTWARE IS PROVIDED BY THE AUTHOR AND CONTRIBUTORS ``AS IS'' AND
15 * ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
16 * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
17 * ARE DISCLAIMED. IN NO EVENT SHALL THE AUTHOR OR CONTRIBUTORS BE LIABLE
18 * FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL
19 * DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS
20 * OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION)
21 * HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT
22 * LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY
23 * OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF
24 * SUCH DAMAGE.
25 *
26 * $FreeBSD: src/lib/msun/i387/fenv.h,v 1.4 2005/03/17 22:21:46 das Exp $
27 */
29 #ifndef _FENV_H_
30 #define _FENV_H_
32 #include <sys/cdefs.h>
33 #include <sys/_types.h>
35 /*
36 * To preserve binary compatibility with FreeBSD 5.3, we pack the
37 * mxcsr into some reserved fields, rather than changing sizeof(fenv_t).
38 */
39 typedef struct {
40 __uint16_t __control;
41 __uint16_t __mxcsr_hi;
42 __uint16_t __status;
43 __uint16_t __mxcsr_lo;
44 __uint32_t __tag;
45 char __other[16];
46 } fenv_t;
48 #define __get_mxcsr(env) (((env).__mxcsr_hi << 16) | \
49 ((env).__mxcsr_lo))
50 #define __set_mxcsr(env, x) do { \
51 (env).__mxcsr_hi = (__uint32_t)(x) >> 16; \
52 (env).__mxcsr_lo = (__uint16_t)(x); \
53 } while (0)
55 typedef __uint16_t fexcept_t;
57 /* Exception flags */
58 #define FE_INVALID 0x01
59 #define FE_DENORMAL 0x02
60 #define FE_DIVBYZERO 0x04
61 #define FE_OVERFLOW 0x08
62 #define FE_UNDERFLOW 0x10
63 #define FE_INEXACT 0x20
64 #define FE_ALL_EXCEPT (FE_DIVBYZERO | FE_DENORMAL | FE_INEXACT | \
65 FE_INVALID | FE_OVERFLOW | FE_UNDERFLOW)
67 /* Rounding modes */
68 #define FE_TONEAREST 0x0000
69 #define FE_DOWNWARD 0x0400
70 #define FE_UPWARD 0x0800
71 #define FE_TOWARDZERO 0x0c00
72 #define _ROUND_MASK (FE_TONEAREST | FE_DOWNWARD | \
73 FE_UPWARD | FE_TOWARDZERO)
75 /*
76 * As compared to the x87 control word, the SSE unit's control word
77 * has the rounding control bits offset by 3 and the exception mask
78 * bits offset by 7.
79 */
80 #define _SSE_ROUND_SHIFT 3
81 #define _SSE_EMASK_SHIFT 7
83 /* After testing for SSE support once, we cache the result in __has_sse. */
84 enum __sse_support { __SSE_YES, __SSE_NO, __SSE_UNK };
85 extern enum __sse_support __has_sse;
86 int __test_sse(void);
87 #ifdef __SSE__
88 #define __HAS_SSE() 1
89 #else
90 #define __HAS_SSE() (__has_sse == __SSE_YES || \
91 (__has_sse == __SSE_UNK && __test_sse()))
92 #endif
94 __BEGIN_DECLS
96 /* Default floating-point environment */
97 extern const fenv_t __fe_dfl_env;
98 #define FE_DFL_ENV (&__fe_dfl_env)
100 #define __fldcw(__cw) __asm __volatile("fldcw %0" : : "m" (__cw))
101 #define __fldenv(__env) __asm __volatile("fldenv %0" : : "m" (__env))
102 #define __fnclex() __asm __volatile("fnclex")
103 #define __fnstenv(__env) __asm __volatile("fnstenv %0" : "=m" (*(__env)))
104 #define __fnstcw(__cw) __asm __volatile("fnstcw %0" : "=m" (*(__cw)))
105 #define __fnstsw(__sw) __asm __volatile("fnstsw %0" : "=am" (*(__sw)))
106 #define __fwait() __asm __volatile("fwait")
107 #define __ldmxcsr(__csr) __asm __volatile("ldmxcsr %0" : : "m" (__csr))
108 #define __stmxcsr(__csr) __asm __volatile("stmxcsr %0" : "=m" (*(__csr)))
110 static __inline int
111 feclearexcept(int __excepts)
112 {
113 fenv_t __env;
114 int __mxcsr;
116 if (__excepts == FE_ALL_EXCEPT) {
117 __fnclex();
118 } else {
119 __fnstenv(&__env);
120 __env.__status &= ~__excepts;
121 __fldenv(__env);
122 }
123 if (__HAS_SSE()) {
124 __stmxcsr(&__mxcsr);
125 __mxcsr &= ~__excepts;
126 __ldmxcsr(__mxcsr);
127 }
128 return (0);
129 }
131 static __inline int
132 fegetexceptflag(fexcept_t *__flagp, int __excepts)
133 {
134 int __mxcsr, __status;
136 __fnstsw(&__status);
137 if (__HAS_SSE())
138 __stmxcsr(&__mxcsr);
139 else
140 __mxcsr = 0;
141 *__flagp = (__mxcsr | __status) & __excepts;
142 return (0);
143 }
145 int fesetexceptflag(const fexcept_t *__flagp, int __excepts);
146 int feraiseexcept(int __excepts);
148 static __inline int
149 fetestexcept(int __excepts)
150 {
151 int __mxcsr, __status;
153 __fnstsw(&__status);
154 if (__HAS_SSE())
155 __stmxcsr(&__mxcsr);
156 else
157 __mxcsr = 0;
158 return ((__status | __mxcsr) & __excepts);
159 }
161 static __inline int
162 fegetround(void)
163 {
164 int __control;
166 /*
167 * We assume that the x87 and the SSE unit agree on the
168 * rounding mode. Reading the control word on the x87 turns
169 * out to be about 5 times faster than reading it on the SSE
170 * unit on an Opteron 244.
171 */
172 __fnstcw(&__control);
173 return (__control & _ROUND_MASK);
174 }
176 static __inline int
177 fesetround(int __round)
178 {
179 int __mxcsr, __control;
181 if (__round & ~_ROUND_MASK)
182 return (-1);
184 __fnstcw(&__control);
185 __control &= ~_ROUND_MASK;
186 __control |= __round;
187 __fldcw(__control);
189 if (__HAS_SSE()) {
190 __stmxcsr(&__mxcsr);
191 __mxcsr &= ~(_ROUND_MASK << _SSE_ROUND_SHIFT);
192 __mxcsr |= __round << _SSE_ROUND_SHIFT;
193 __ldmxcsr(__mxcsr);
194 }
196 return (0);
197 }
199 int fegetenv(fenv_t *__envp);
200 int feholdexcept(fenv_t *__envp);
202 static __inline int
203 fesetenv(const fenv_t *__envp)
204 {
205 fenv_t __env = *__envp;
206 int __mxcsr;
208 __mxcsr = __get_mxcsr(__env);
209 __set_mxcsr(__env, 0xffffffff);
210 __fldenv(__env);
211 if (__HAS_SSE())
212 __ldmxcsr(__mxcsr);
213 return (0);
214 }
216 int feupdateenv(const fenv_t *__envp);
218 #if __BSD_VISIBLE
220 int feenableexcept(int __mask);
221 int fedisableexcept(int __mask);
223 static __inline int
224 fegetexcept(void)
225 {
226 int __control;
228 /*
229 * We assume that the masks for the x87 and the SSE unit are
230 * the same.
231 */
232 __fnstcw(&__control);
233 return (~__control & FE_ALL_EXCEPT);
234 }
236 #endif /* __BSD_VISIBLE */
238 __END_DECLS
240 #endif /* !_FENV_H_ */