]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/platform-bionic.git/blob - libm/src/s_log1pf.c
Initial Contribution
[android-sdk/platform-bionic.git] / libm / src / s_log1pf.c
1 /* s_log1pf.c -- float version of s_log1p.c.
2  * Conversion to float by Ian Lance Taylor, Cygnus Support, ian@cygnus.com.
3  */
5 /*
6  * ====================================================
7  * Copyright (C) 1993 by Sun Microsystems, Inc. All rights reserved.
8  *
9  * Developed at SunPro, a Sun Microsystems, Inc. business.
10  * Permission to use, copy, modify, and distribute this
11  * software is freely granted, provided that this notice
12  * is preserved.
13  * ====================================================
14  */
16 #ifndef lint
17 static char rcsid[] = "$FreeBSD: src/lib/msun/src/s_log1pf.c,v 1.9 2005/12/04 12:30:44 bde Exp $";
18 #endif
20 #include "math.h"
21 #include "math_private.h"
23 static const float
24 ln2_hi =   6.9313812256e-01,    /* 0x3f317180 */
25 ln2_lo =   9.0580006145e-06,    /* 0x3717f7d1 */
26 two25 =    3.355443200e+07,     /* 0x4c000000 */
27 Lp1 = 6.6666668653e-01, /* 3F2AAAAB */
28 Lp2 = 4.0000000596e-01, /* 3ECCCCCD */
29 Lp3 = 2.8571429849e-01, /* 3E924925 */
30 Lp4 = 2.2222198546e-01, /* 3E638E29 */
31 Lp5 = 1.8183572590e-01, /* 3E3A3325 */
32 Lp6 = 1.5313838422e-01, /* 3E1CD04F */
33 Lp7 = 1.4798198640e-01; /* 3E178897 */
35 static const float zero = 0.0;
37 float
38 log1pf(float x)
39 {
40         float hfsq,f,c,s,z,R,u;
41         int32_t k,hx,hu,ax;
43         GET_FLOAT_WORD(hx,x);
44         ax = hx&0x7fffffff;
46         k = 1;
47         if (hx < 0x3ed413d0) {                  /* 1+x < sqrt(2)+  */
48             if(ax>=0x3f800000) {                /* x <= -1.0 */
49                 if(x==(float)-1.0) return -two25/zero; /* log1p(-1)=+inf */
50                 else return (x-x)/(x-x);        /* log1p(x<-1)=NaN */
51             }
52             if(ax<0x31000000) {                 /* |x| < 2**-29 */
53                 if(two25+x>zero                 /* raise inexact */
54                     &&ax<0x24800000)            /* |x| < 2**-54 */
55                     return x;
56                 else
57                     return x - x*x*(float)0.5;
58             }
59             if(hx>0||hx<=((int32_t)0xbe95f619)) {
60                 k=0;f=x;hu=1;}          /* sqrt(2)/2- <= 1+x < sqrt(2)+ */
61         }
62         if (hx >= 0x7f800000) return x+x;
63         if(k!=0) {
64             if(hx<0x5a000000) {
65                 *(volatile float *)&u = (float)1.0+x;
66                 GET_FLOAT_WORD(hu,u);
67                 k  = (hu>>23)-127;
68                 /* correction term */
69                 c  = (k>0)? (float)1.0-(u-x):x-(u-(float)1.0);
70                 c /= u;
71             } else {
72                 u  = x;
73                 GET_FLOAT_WORD(hu,u);
74                 k  = (hu>>23)-127;
75                 c  = 0;
76             }
77             hu &= 0x007fffff;
78             /*
79              * The approximation to sqrt(2) used in thresholds is not
80              * critical.  However, the ones used above must give less
81              * strict bounds than the one here so that the k==0 case is
82              * never reached from here, since here we have committed to
83              * using the correction term but don't use it if k==0.
84              */
85             if(hu<0x3504f4) {                   /* u < sqrt(2) */
86                 SET_FLOAT_WORD(u,hu|0x3f800000);/* normalize u */
87             } else {
88                 k += 1;
89                 SET_FLOAT_WORD(u,hu|0x3f000000);        /* normalize u/2 */
90                 hu = (0x00800000-hu)>>2;
91             }
92             f = u-(float)1.0;
93         }
94         hfsq=(float)0.5*f*f;
95         if(hu==0) {     /* |f| < 2**-20 */
96             if(f==zero) if(k==0) return zero;
97                         else {c += k*ln2_lo; return k*ln2_hi+c;}
98             R = hfsq*((float)1.0-(float)0.66666666666666666*f);
99             if(k==0) return f-R; else
100                      return k*ln2_hi-((R-(k*ln2_lo+c))-f);
101         }
102         s = f/((float)2.0+f);
103         z = s*s;
104         R = z*(Lp1+z*(Lp2+z*(Lp3+z*(Lp4+z*(Lp5+z*(Lp6+z*Lp7))))));
105         if(k==0) return f-(hfsq-s*(hfsq+R)); else
106                  return k*ln2_hi-((hfsq-(s*(hfsq+R)+(k*ln2_lo+c)))-f);