]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/platform-bionic.git/blob - libthread_db/libthread_db.c
Upgrade to tzdata2013i.
[android-sdk/platform-bionic.git] / libthread_db / libthread_db.c
1 /*
2  * Copyright 2006 The Android Open Source Project
3  */
5 #include <dirent.h>
6 #include <sys/ptrace.h>
7 #include <stdint.h>
8 #include <thread_db.h>
9 #include <stdlib.h>
10 #include <stdio.h>
12 extern int ps_pglobal_lookup (void *, const char *obj, const char *name, void **sym_addr);
13 extern pid_t ps_getpid(struct ps_prochandle *ph);
15 /*
16  * This is the list of "special" symbols we care about whose addresses are
17  * cached by gdbserver from the host at init time.
18  */
19 enum {
20     SYM_TD_CREATE,
21     SYM_THREAD_LIST,
22     NUM_SYMS
23 };
25 static char const * gSymbols[] = {
26     [SYM_TD_CREATE] = "_thread_created_hook",
27     NULL
28 };
31 char const **
32 td_symbol_list(void)
33 {
34     return gSymbols;
35 }
38 td_err_e
39 td_ta_new(struct ps_prochandle * proc_handle, td_thragent_t ** agent_out)
40 {
41     td_thragent_t * agent;
43     agent = (td_thragent_t *)malloc(sizeof(td_thragent_t));
44     if (!agent) {
45         return TD_MALLOC;
46     }
48     agent->pid = ps_getpid(proc_handle);
49     agent->ph = proc_handle;
50     *agent_out = agent;
52     return TD_OK;
53 }
56 td_err_e
57 td_ta_delete(td_thragent_t * ta)
58 {
59     free(ta);
60     // FIXME: anything else to do?
61     return TD_OK;
62 }
65 /* NOTE: not used by gdb 7.0 */
67 td_err_e
68 td_ta_set_event(td_thragent_t const * agent, td_thr_events_t * events)
69 {
70     return TD_OK;
71 }
74 /* NOTE: not used by gdb 7.0 */
75 static td_thrhandle_t gEventMsgHandle;
77 /* NOTE: not used by gdb 7.0 */
79 static int
80 _event_getmsg_helper(td_thrhandle_t const * handle, void * bkpt_addr)
81 {
82     void * pc;
84 #ifdef __i386__
85     /* Get the eip from offset 12*4 = 48 as defined in the struct
86      * user_regs_struct in user_32.h
87      */
88     pc = (void *)ptrace(PTRACE_PEEKUSR, handle->tid, (void *)48 /* eip */, NULL);
89     /* FIXME - pc is a non-decremented breakpoint address, hence the
90      * addition of 1 on test.  This seems to work for the thread hook
91      * function in libc.so but should be properly fixed.
92      */
93     if (pc == ((int)bkpt_addr + 1)) {
94         /* The hook function takes the id of the new thread as it's first
95          * param, so grab it from ecx at offset 4 in struct user_regs_struct
96          * (using fastcall convention for x86)
97          */
98         gEventMsgHandle.pid = ptrace(PTRACE_PEEKUSR, handle->tid, (void *)4 /* ecx */, NULL);
99         gEventMsgHandle.tid = gEventMsgHandle.pid;
100         return 0x42;
101     }
102 #elif defined(__arm__)
103     pc = (void *)ptrace(PTRACE_PEEKUSR, handle->tid, (void *)60 /* r15/pc */, NULL);
105     if (pc == bkpt_addr) {
106         // The hook function takes the id of the new thread as it's first param,
107         // so grab it from r0.
108         gEventMsgHandle.pid = ptrace(PTRACE_PEEKUSR, handle->tid, (void *)0 /* r0 */, NULL);
109         gEventMsgHandle.tid = gEventMsgHandle.pid;
110         return 0x42;
111     }
112 #elif defined(__mips__)
113     pc = (void *)ptrace(PTRACE_PEEKUSR, handle->tid, (void *)(64*4) /* pc */, NULL);
114     if (pc == bkpt_addr) {
115         // The hook function takes the id of the new thread as it's first param,
116         // so grab it from a0
117         gEventMsgHandle.pid = ptrace(PTRACE_PEEKUSR, handle->tid, (void *)(4*4) /* a0 */, NULL);
118         gEventMsgHandle.tid = gEventMsgHandle.pid;
119         return 0x42;
120     }
121 #endif
122     return 0;
125 /* NOTE: not used by gdb 7.0 */
127 td_err_e
128 td_ta_event_getmsg(td_thragent_t const * agent, td_event_msg_t * event)
130     td_err_e err;
131     void * bkpt_addr;
133     err = ps_pglobal_lookup(NULL, NULL, gSymbols[SYM_TD_CREATE], &bkpt_addr);
134     if (err) {
135         return err;
136     }
138     err = td_ta_thr_iter(agent, _event_getmsg_helper, bkpt_addr, 0, 0, NULL, 0);
139     if (err != 0x42) {
140         return TD_NOMSG;
141     }
143     event->event = TD_CREATE;
144     event->th_p = &gEventMsgHandle; // Nasty hack, but it's the only way!
146     return TD_OK;
150 td_err_e
151 td_ta_map_lwp2thr(td_thragent_t const * agent, lwpid_t lwpid,
152                   td_thrhandle_t *th)
154     th->pid = ps_getpid(agent->ph);
155     th->tid = lwpid;
156     return TD_OK;
160 td_err_e
161 td_thr_get_info(td_thrhandle_t const * handle, td_thrinfo_t * info)
163     info->ti_tid = handle->tid;
164     info->ti_lid = handle->tid;
165     info->ti_state = TD_THR_SLEEP; /* XXX this needs to be read from /proc/<pid>/task/<tid>.
166                                       This is only used to see if the thread is a zombie or not */
167     return TD_OK;
171 /* NOTE: not used by gdb 7.0 */
173 td_err_e
174 td_thr_event_enable(td_thrhandle_t const * handle, td_event_e event)
176     // I don't think we need to do anything here...
177     return TD_OK;
181 /* NOTE: not used by gdb 7.0 */
183 td_err_e
184 td_ta_event_addr(td_thragent_t const * agent, td_event_e event, td_notify_t * notify_out)
186     int32_t err;
188     /*
189      * This is nasty, ps_pglobal_lookup is implemented in gdbserver and looks up
190      * the symbol from it's cache, which is populated at start time with the
191      * symbols returned from td_symbol_list via calls back to the host.
192      */
194     switch (event) {
195         case TD_CREATE:
196             err = ps_pglobal_lookup(NULL, NULL, gSymbols[SYM_TD_CREATE], &notify_out->u.bptaddr);
197             if (err) {
198                 return TD_NOEVENT;
199             }
200             return TD_OK;
201     }
202     return TD_NOEVENT;
206 td_err_e
207 td_ta_clear_event(const td_thragent_t * ta_arg, td_thr_events_t * event)
209     /* Given that gdb 7.0 doesn't use thread events,
210        there's nothing we need to do here.  */
211     return TD_OK;
215 td_err_e
216 td_ta_thr_iter(td_thragent_t const * agent, td_thr_iter_f * func, void * cookie,
217                td_thr_state_e state, int32_t prio, sigset_t * sigmask, uint32_t user_flags)
219     td_err_e err = TD_OK;
220     char path[32];
221     DIR * dir;
222     struct dirent * entry;
223     td_thrhandle_t handle;
225     snprintf(path, sizeof(path), "/proc/%d/task/", agent->pid);
226     dir = opendir(path);
227     if (!dir) {
228         return TD_NOEVENT;
229     }
231     handle.pid = agent->pid;
232     while ((entry = readdir(dir)) != NULL) {
233         if (strcmp(entry->d_name, ".") == 0 || strcmp(entry->d_name, "..") == 0) {
234             continue;
235         }
236         handle.tid = atoi(entry->d_name);
237         if (func(&handle, cookie) != 0) {
238             err = TD_DBERR;
239             break;
240         }
241     }
243     closedir(dir);
245     return err;
248 td_err_e
249 td_thr_tls_get_addr(const td_thrhandle_t * th,
250                     psaddr_t map_address, size_t offset, psaddr_t * address)
252     return TD_NOAPLIC; // FIXME: TODO