]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/platform-bionic.git/blob - linker/dlfcn.cpp
am 1737b159: Merge "Load libraries in breadth-first order"
[android-sdk/platform-bionic.git] / linker / dlfcn.cpp
1 /*
2  * Copyright (C) 2007 The Android Open Source Project
3  *
4  * Licensed under the Apache License, Version 2.0 (the "License");
5  * you may not use this file except in compliance with the License.
6  * You may obtain a copy of the License at
7  *
8  *      http://www.apache.org/licenses/LICENSE-2.0
9  *
10  * Unless required by applicable law or agreed to in writing, software
11  * distributed under the License is distributed on an "AS IS" BASIS,
12  * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13  * See the License for the specific language governing permissions and
14  * limitations under the License.
15  */
17 #include "linker.h"
19 #include <dlfcn.h>
20 #include <pthread.h>
21 #include <stdio.h>
22 #include <stdlib.h>
23 #include <android/dlext.h>
25 #include <bionic/pthread_internal.h>
26 #include "private/bionic_tls.h"
27 #include "private/ScopedPthreadMutexLocker.h"
28 #include "private/ThreadLocalBuffer.h"
30 /* This file hijacks the symbols stubbed out in libdl.so. */
32 static pthread_mutex_t g_dl_mutex = PTHREAD_RECURSIVE_MUTEX_INITIALIZER;
34 static const char* __bionic_set_dlerror(char* new_value) {
35   char** dlerror_slot = &reinterpret_cast<char**>(__get_tls())[TLS_SLOT_DLERROR];
37   const char* old_value = *dlerror_slot;
38   *dlerror_slot = new_value;
39   return old_value;
40 }
42 static void __bionic_format_dlerror(const char* msg, const char* detail) {
43   char* buffer = __get_thread()->dlerror_buffer;
44   strlcpy(buffer, msg, __BIONIC_DLERROR_BUFFER_SIZE);
45   if (detail != nullptr) {
46     strlcat(buffer, ": ", __BIONIC_DLERROR_BUFFER_SIZE);
47     strlcat(buffer, detail, __BIONIC_DLERROR_BUFFER_SIZE);
48   }
50   __bionic_set_dlerror(buffer);
51 }
53 const char* dlerror() {
54   const char* old_value = __bionic_set_dlerror(nullptr);
55   return old_value;
56 }
58 void android_get_LD_LIBRARY_PATH(char* buffer, size_t buffer_size) {
59   ScopedPthreadMutexLocker locker(&g_dl_mutex);
60   do_android_get_LD_LIBRARY_PATH(buffer, buffer_size);
61 }
63 void android_update_LD_LIBRARY_PATH(const char* ld_library_path) {
64   ScopedPthreadMutexLocker locker(&g_dl_mutex);
65   do_android_update_LD_LIBRARY_PATH(ld_library_path);
66 }
68 static void* dlopen_ext(const char* filename, int flags, const android_dlextinfo* extinfo) {
69   ScopedPthreadMutexLocker locker(&g_dl_mutex);
70   soinfo* result = do_dlopen(filename, flags, extinfo);
71   if (result == nullptr) {
72     __bionic_format_dlerror("dlopen failed", linker_get_error_buffer());
73     return nullptr;
74   }
75   return result;
76 }
78 void* android_dlopen_ext(const char* filename, int flags, const android_dlextinfo* extinfo) {
79   return dlopen_ext(filename, flags, extinfo);
80 }
82 void* dlopen(const char* filename, int flags) {
83   return dlopen_ext(filename, flags, nullptr);
84 }
86 void* dlsym(void* handle, const char* symbol) {
87   ScopedPthreadMutexLocker locker(&g_dl_mutex);
89 #if !defined(__LP64__)
90   if (handle == nullptr) {
91     __bionic_format_dlerror("dlsym library handle is null", nullptr);
92     return nullptr;
93   }
94 #endif
96   if (symbol == nullptr) {
97     __bionic_format_dlerror("dlsym symbol name is null", nullptr);
98     return nullptr;
99   }
101   soinfo* found = nullptr;
102   ElfW(Sym)* sym = nullptr;
103   if (handle == RTLD_DEFAULT) {
104     sym = dlsym_linear_lookup(symbol, &found, nullptr);
105   } else if (handle == RTLD_NEXT) {
106     void* caller_addr = __builtin_return_address(0);
107     soinfo* si = find_containing_library(caller_addr);
109     sym = nullptr;
110     if (si && si->next) {
111       sym = dlsym_linear_lookup(symbol, &found, si->next);
112     }
113   } else {
114     sym = dlsym_handle_lookup(reinterpret_cast<soinfo*>(handle), &found, symbol);
115   }
117   if (sym != nullptr) {
118     unsigned bind = ELF_ST_BIND(sym->st_info);
120     if ((bind == STB_GLOBAL || bind == STB_WEAK) && sym->st_shndx != 0) {
121       return reinterpret_cast<void*>(sym->st_value + found->load_bias);
122     }
124     __bionic_format_dlerror("symbol found but not global", symbol);
125     return nullptr;
126   } else {
127     __bionic_format_dlerror("undefined symbol", symbol);
128     return nullptr;
129   }
132 int dladdr(const void* addr, Dl_info* info) {
133   ScopedPthreadMutexLocker locker(&g_dl_mutex);
135   // Determine if this address can be found in any library currently mapped.
136   soinfo* si = find_containing_library(addr);
137   if (si == nullptr) {
138     return 0;
139   }
141   memset(info, 0, sizeof(Dl_info));
143   info->dli_fname = si->name;
144   // Address at which the shared object is loaded.
145   info->dli_fbase = reinterpret_cast<void*>(si->base);
147   // Determine if any symbol in the library contains the specified address.
148   ElfW(Sym)* sym = dladdr_find_symbol(si, addr);
149   if (sym != nullptr) {
150     info->dli_sname = si->strtab + sym->st_name;
151     info->dli_saddr = reinterpret_cast<void*>(si->load_bias + sym->st_value);
152   }
154   return 1;
157 int dlclose(void* handle) {
158   ScopedPthreadMutexLocker locker(&g_dl_mutex);
159   do_dlclose(reinterpret_cast<soinfo*>(handle));
160   // dlclose has no defined errors.
161   return 0;
164 // name_offset: starting index of the name in libdl_info.strtab
165 #define ELF32_SYM_INITIALIZER(name_offset, value, shndx) \
166     { name_offset, \
167       reinterpret_cast<Elf32_Addr>(value), \
168       /* st_size */ 0, \
169       (shndx == 0) ? 0 : (STB_GLOBAL << 4), \
170       /* st_other */ 0, \
171       shndx, \
172     }
174 #define ELF64_SYM_INITIALIZER(name_offset, value, shndx) \
175     { name_offset, \
176       (shndx == 0) ? 0 : (STB_GLOBAL << 4), \
177       /* st_other */ 0, \
178       shndx, \
179       reinterpret_cast<Elf64_Addr>(value), \
180       /* st_size */ 0, \
181     }
183 #if defined(__arm__)
184   // 0000000 00011111 111112 22222222 2333333 3333444444444455555555556666666 6667777777777888888888899999 9999900000000001 1111111112222222222 333333333344444444445
185   // 0123456 78901234 567890 12345678 9012345 6789012345678901234567890123456 7890123456789012345678901234 5678901234567890 1234567890123456789 012345678901234567890
186 #  define ANDROID_LIBDL_STRTAB \
187     "dlopen\0dlclose\0dlsym\0dlerror\0dladdr\0android_update_LD_LIBRARY_PATH\0android_get_LD_LIBRARY_PATH\0dl_iterate_phdr\0android_dlopen_ext\0dl_unwind_find_exidx\0"
188 #elif defined(__aarch64__) || defined(__i386__) || defined(__mips__) || defined(__x86_64__)
189   // 0000000 00011111 111112 22222222 2333333 3333444444444455555555556666666 6667777777777888888888899999 9999900000000001 1111111112222222222
190   // 0123456 78901234 567890 12345678 9012345 6789012345678901234567890123456 7890123456789012345678901234 5678901234567890 1234567890123456789
191 #  define ANDROID_LIBDL_STRTAB \
192     "dlopen\0dlclose\0dlsym\0dlerror\0dladdr\0android_update_LD_LIBRARY_PATH\0android_get_LD_LIBRARY_PATH\0dl_iterate_phdr\0android_dlopen_ext\0"
193 #else
194 #  error Unsupported architecture. Only arm, arm64, mips, mips64, x86 and x86_64 are presently supported.
195 #endif
197 static ElfW(Sym) g_libdl_symtab[] = {
198   // Total length of libdl_info.strtab, including trailing 0.
199   // This is actually the STH_UNDEF entry. Technically, it's
200   // supposed to have st_name == 0, but instead, it points to an index
201   // in the strtab with a \0 to make iterating through the symtab easier.
202   ELFW(SYM_INITIALIZER)(sizeof(ANDROID_LIBDL_STRTAB) - 1, nullptr, 0),
203   ELFW(SYM_INITIALIZER)(  0, &dlopen, 1),
204   ELFW(SYM_INITIALIZER)(  7, &dlclose, 1),
205   ELFW(SYM_INITIALIZER)( 15, &dlsym, 1),
206   ELFW(SYM_INITIALIZER)( 21, &dlerror, 1),
207   ELFW(SYM_INITIALIZER)( 29, &dladdr, 1),
208   ELFW(SYM_INITIALIZER)( 36, &android_update_LD_LIBRARY_PATH, 1),
209   ELFW(SYM_INITIALIZER)( 67, &android_get_LD_LIBRARY_PATH, 1),
210   ELFW(SYM_INITIALIZER)( 95, &dl_iterate_phdr, 1),
211   ELFW(SYM_INITIALIZER)(111, &android_dlopen_ext, 1),
212 #if defined(__arm__)
213   ELFW(SYM_INITIALIZER)(130, &dl_unwind_find_exidx, 1),
214 #endif
215 };
217 // Fake out a hash table with a single bucket.
218 //
219 // A search of the hash table will look through g_libdl_symtab starting with index 1, then
220 // use g_libdl_chains to find the next index to look at. g_libdl_chains should be set up to
221 // walk through every element in g_libdl_symtab, and then end with 0 (sentinel value).
222 //
223 // That is, g_libdl_chains should look like { 0, 2, 3, ... N, 0 } where N is the number
224 // of actual symbols, or nelems(g_libdl_symtab)-1 (since the first element of g_libdl_symtab is not
225 // a real symbol). (See soinfo_elf_lookup().)
226 //
227 // Note that adding any new symbols here requires stubbing them out in libdl.
228 static unsigned g_libdl_buckets[1] = { 1 };
229 #if defined(__arm__)
230 static unsigned g_libdl_chains[] = { 0, 2, 3, 4, 5, 6, 7, 8, 9, 10, 0 };
231 #else
232 static unsigned g_libdl_chains[] = { 0, 2, 3, 4, 5, 6, 7, 8, 9, 0 };
233 #endif
235 static soinfo __libdl_info("libdl.so", nullptr);
237 // This is used by the dynamic linker. Every process gets these symbols for free.
238 soinfo* get_libdl_info() {
239   if ((__libdl_info.flags & FLAG_LINKED) == 0) {
240     __libdl_info.flags |= FLAG_LINKED;
241     __libdl_info.strtab = ANDROID_LIBDL_STRTAB;
242     __libdl_info.symtab = g_libdl_symtab;
243     __libdl_info.nbucket = sizeof(g_libdl_buckets)/sizeof(unsigned);
244     __libdl_info.nchain = sizeof(g_libdl_chains)/sizeof(unsigned);
245     __libdl_info.bucket = g_libdl_buckets;
246     __libdl_info.chain = g_libdl_chains;
247     __libdl_info.has_DT_SYMBOLIC = true;
248     __libdl_info.ref_count = 1;
249   }
251   return &__libdl_info;