1 /*
2 * Copyright (C) 2013 The Android Open Source Project
3 *
4 * Licensed under the Apache License, Version 2.0 (the "License");
5 * you may not use this file except in compliance with the License.
6 * You may obtain a copy of the License at
7 *
8 * http://www.apache.org/licenses/LICENSE-2.0
9 *
10 * Unless required by applicable law or agreed to in writing, software
11 * distributed under the License is distributed on an "AS IS" BASIS,
12 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13 * See the License for the specific language governing permissions and
14 * limitations under the License.
15 */
17 #include <stdlib.h>
18 #include <string.h>
19 #include <sys/mman.h>
21 #include <gtest/gtest.h>
22 #include "buffer_tests.h"
24 // For the comparison buffer tests, the maximum length to test for the
25 // miscompare checks.
26 #define MISCMP_MAX_LENGTH 512
28 #define FENCEPOST_LENGTH 8
30 static int g_single_aligns[][2] = {
31 // Both buffers at same alignment.
32 { 1, 0 },
33 { 2, 0 },
34 { 4, 0 },
35 { 8, 0 },
36 { 16, 0 },
37 { 32, 0 },
38 { 64, 0 },
39 { 128, 0 },
41 // General unaligned cases.
42 { 4, 1 },
43 { 4, 2 },
44 { 4, 3 },
46 { 8, 1 },
47 { 8, 2 },
48 { 8, 3 },
49 { 8, 4 },
50 { 8, 5 },
51 { 8, 6 },
52 { 8, 7 },
54 { 128, 1 },
55 { 128, 4 },
56 { 128, 8 },
57 { 128, 12 },
58 { 128, 16 },
59 };
61 static const size_t g_single_aligns_len = sizeof(g_single_aligns)/sizeof(int[2]);
63 // Set of multiple buffer alignment combinations to be used for string/memory
64 // testing routines.
65 static int g_double_aligns[][4] = {
66 // Both buffers at same alignment.
67 { 1, 0, 1, 0 },
68 { 2, 0, 2, 0 },
69 { 4, 0, 4, 0 },
70 { 8, 0, 8, 0 },
71 { 16, 0, 16, 0 },
72 { 32, 0, 32, 0 },
73 { 64, 0, 64, 0 },
74 { 128, 0, 128, 0 },
76 // Different word alignments between buffers.
77 { 8, 0, 4, 0 },
78 { 4, 0, 8, 0 },
79 { 16, 0, 4, 0 },
80 { 4, 0, 16, 0 },
82 // General unaligned cases.
83 { 4, 0, 4, 1 },
84 { 4, 0, 4, 2 },
85 { 4, 0, 4, 3 },
87 { 4, 1, 4, 0 },
88 { 4, 1, 4, 1 },
89 { 4, 1, 4, 2 },
90 { 4, 1, 4, 3 },
92 { 4, 2, 4, 0 },
93 { 4, 2, 4, 1 },
94 { 4, 2, 4, 2 },
95 { 4, 2, 4, 3 },
97 { 4, 3, 4, 0 },
98 { 4, 3, 4, 1 },
99 { 4, 3, 4, 2 },
100 { 4, 3, 4, 3 },
102 { 8, 0, 8, 1 },
103 { 8, 0, 8, 2 },
104 { 8, 0, 8, 3 },
105 { 8, 0, 8, 4 },
106 { 8, 0, 8, 5 },
107 { 8, 0, 8, 6 },
108 { 8, 0, 8, 7 },
110 { 8, 1, 8, 0 },
111 { 8, 1, 8, 1 },
112 { 8, 1, 8, 2 },
113 { 8, 1, 8, 3 },
114 { 8, 1, 8, 4 },
115 { 8, 1, 8, 5 },
116 { 8, 1, 8, 6 },
117 { 8, 1, 8, 7 },
119 { 8, 2, 8, 0 },
120 { 8, 2, 8, 1 },
121 { 8, 2, 8, 2 },
122 { 8, 2, 8, 3 },
123 { 8, 2, 8, 4 },
124 { 8, 2, 8, 5 },
125 { 8, 2, 8, 6 },
126 { 8, 2, 8, 7 },
128 { 8, 3, 8, 0 },
129 { 8, 3, 8, 1 },
130 { 8, 3, 8, 2 },
131 { 8, 3, 8, 3 },
132 { 8, 3, 8, 4 },
133 { 8, 3, 8, 5 },
134 { 8, 3, 8, 6 },
135 { 8, 3, 8, 7 },
137 { 8, 4, 8, 0 },
138 { 8, 4, 8, 1 },
139 { 8, 4, 8, 2 },
140 { 8, 4, 8, 3 },
141 { 8, 4, 8, 4 },
142 { 8, 4, 8, 5 },
143 { 8, 4, 8, 6 },
144 { 8, 4, 8, 7 },
146 { 8, 5, 8, 0 },
147 { 8, 5, 8, 1 },
148 { 8, 5, 8, 2 },
149 { 8, 5, 8, 3 },
150 { 8, 5, 8, 4 },
151 { 8, 5, 8, 5 },
152 { 8, 5, 8, 6 },
153 { 8, 5, 8, 7 },
155 { 8, 6, 8, 0 },
156 { 8, 6, 8, 1 },
157 { 8, 6, 8, 2 },
158 { 8, 6, 8, 3 },
159 { 8, 6, 8, 4 },
160 { 8, 6, 8, 5 },
161 { 8, 6, 8, 6 },
162 { 8, 6, 8, 7 },
164 { 8, 7, 8, 0 },
165 { 8, 7, 8, 1 },
166 { 8, 7, 8, 2 },
167 { 8, 7, 8, 3 },
168 { 8, 7, 8, 4 },
169 { 8, 7, 8, 5 },
170 { 8, 7, 8, 6 },
171 { 8, 7, 8, 7 },
173 { 128, 1, 128, 4 },
174 { 128, 1, 128, 8 },
175 { 128, 1, 128, 12 },
176 { 128, 1, 128, 16 },
177 { 128, 4, 128, 1 },
178 { 128, 8, 128, 1 },
179 { 128, 12, 128, 1 },
180 { 128, 16, 128, 1 },
181 };
183 static const size_t g_double_aligns_len = sizeof(g_double_aligns)/sizeof(int[4]);
185 static size_t SetIncrement(size_t len) {
186 if (len >= 4096) {
187 return 1024;
188 } else if (len >= 1024) {
189 return 256;
190 }
191 return 1;
192 }
194 // Return a pointer into the current buffer with the specified alignment.
195 static void *GetAlignedPtr(void *orig_ptr, int alignment, int or_mask) {
196 uint64_t ptr = reinterpret_cast<uint64_t>(orig_ptr);
197 if (alignment > 0) {
198 // When setting the alignment, set it to exactly the alignment chosen.
199 // The pointer returned will be guaranteed not to be aligned to anything
200 // more than that.
201 ptr += alignment - (ptr & (alignment - 1));
202 ptr |= alignment | or_mask;
203 }
205 return reinterpret_cast<void*>(ptr);
206 }
208 static void SetFencepost(uint8_t *buffer) {
209 for (int i = 0; i < FENCEPOST_LENGTH; i += 2) {
210 buffer[i] = 0xde;
211 buffer[i+1] = 0xad;
212 }
213 }
215 static void VerifyFencepost(uint8_t *buffer) {
216 for (int i = 0; i < FENCEPOST_LENGTH; i += 2) {
217 if (buffer[i] != 0xde || buffer[i+1] != 0xad) {
218 uint8_t expected_value;
219 if (buffer[i] == 0xde) {
220 i++;
221 expected_value = 0xad;
222 } else {
223 expected_value = 0xde;
224 }
225 ASSERT_EQ(expected_value, buffer[i]);
226 }
227 }
228 }
230 void RunSingleBufferAlignTest(
231 size_t max_test_size, void (*test_func)(uint8_t*, size_t),
232 size_t (*set_incr)(size_t)) {
233 if (!set_incr) {
234 set_incr = SetIncrement;
235 }
237 // Allocate one large buffer with lots of extra space so that we can
238 // guarantee that the all possible alignments will fit.
239 uint8_t *buf = new uint8_t[3*max_test_size];
241 uint8_t *buf_align;
242 for (size_t i = 0; i < g_single_aligns_len; i++) {
243 size_t incr = 1;
244 for (size_t len = 0; len <= max_test_size; len += incr) {
245 incr = set_incr(len);
247 buf_align = reinterpret_cast<uint8_t*>(GetAlignedPtr(
248 buf+FENCEPOST_LENGTH, g_single_aligns[i][0], g_single_aligns[i][1]));
250 SetFencepost(&buf_align[-FENCEPOST_LENGTH]);
251 SetFencepost(&buf_align[len]);
253 test_func(buf_align, len);
255 VerifyFencepost(&buf_align[-FENCEPOST_LENGTH]);
256 VerifyFencepost(&buf_align[len]);
257 }
258 }
259 delete buf;
260 }
262 void RunSrcDstBufferAlignTest(
263 size_t max_test_size, void (*test_func)(uint8_t*, uint8_t*, size_t),
264 size_t (*set_incr)(size_t)) {
265 if (!set_incr) {
266 set_incr = SetIncrement;
267 }
269 // Allocate two large buffers for all of the testing.
270 uint8_t* src = new uint8_t[3*max_test_size];
271 uint8_t* dst = new uint8_t[3*max_test_size];
273 uint8_t* src_align;
274 uint8_t* dst_align;
275 for (size_t i = 0; i < g_double_aligns_len; i++) {
276 size_t incr = 1;
277 for (size_t len = 0; len <= max_test_size; len += incr) {
278 incr = set_incr(len);
280 src_align =
281 reinterpret_cast<uint8_t*>(GetAlignedPtr(
282 src+FENCEPOST_LENGTH, g_double_aligns[i][0], g_double_aligns[i][1]));
283 dst_align =
284 reinterpret_cast<uint8_t*>(GetAlignedPtr(
285 dst+FENCEPOST_LENGTH, g_double_aligns[i][2], g_double_aligns[i][3]));
286 SetFencepost(&dst_align[-FENCEPOST_LENGTH]);
287 SetFencepost(&dst_align[len]);
289 test_func(src_align, dst_align, len);
291 VerifyFencepost(&dst_align[-FENCEPOST_LENGTH]);
292 VerifyFencepost(&dst_align[len]);
293 }
294 }
295 delete src;
296 delete dst;
297 }
299 void RunCmpBufferAlignTest(
300 size_t max_test_size, void (*test_cmp_func)(uint8_t*, uint8_t*, size_t),
301 void (*test_miscmp_func)(uint8_t*, uint8_t*, size_t, size_t),
302 size_t (*set_incr)(size_t)) {
303 if (!set_incr) {
304 set_incr = SetIncrement;
305 }
307 // Allocate two large buffers for all of the testing.
308 uint8_t* buf1 = new uint8_t[3*max_test_size];
309 uint8_t* buf2 = new uint8_t[3*max_test_size];
311 uint8_t* buf1_align;
312 uint8_t* buf2_align;
313 for (size_t i = 0; i < g_double_aligns_len; i++) {
314 size_t incr = 1;
315 for (size_t len = 0; len <= max_test_size; len += incr) {
316 incr = set_incr(len);
318 buf1_align =
319 reinterpret_cast<uint8_t*>(GetAlignedPtr(
320 buf1, g_double_aligns[i][0], g_double_aligns[i][1]));
321 buf2_align =
322 reinterpret_cast<uint8_t*>(GetAlignedPtr(
323 buf2, g_double_aligns[i][2], g_double_aligns[i][3]));
325 // Check by putting all zeroes after both buffers.
326 memset(buf1_align+len, 0, 32);
327 memset(buf2_align+len, 0, 32);
328 test_cmp_func(buf1_align, buf2_align, len);
330 // Check by putting different values after both buffers.
331 for (size_t j = 0; j < 32; j++) {
332 buf1_align[len+j] = j;
333 buf2_align[len+j] = j+1;
334 }
335 test_cmp_func(buf1_align, buf2_align, len);
337 if (len > 0) {
338 // Change the lengths of the buffers and verify that there are
339 // miscompares.
340 for (size_t len2 = len+1; len2 < len+32; len2++) {
341 test_miscmp_func(buf1_align, buf2_align, len, len2);
342 test_miscmp_func(buf1_align, buf2_align, len2, len);
343 }
344 }
345 }
346 }
347 delete buf1;
348 delete buf2;
349 }
351 void RunSingleBufferOverreadTest(void (*test_func)(uint8_t*, size_t)) {
352 // In order to verify that functions are not reading past the end of the
353 // src, create data that ends exactly at an unreadable memory boundary.
354 size_t pagesize = static_cast<size_t>(sysconf(_SC_PAGE_SIZE));
355 uint8_t* memory;
356 ASSERT_TRUE(posix_memalign(reinterpret_cast<void**>(&memory), pagesize,
357 2*pagesize) == 0);
358 memset(memory, 0x23, 2*pagesize);
360 // Make the second page unreadable and unwritable.
361 ASSERT_TRUE(mprotect(&memory[pagesize], pagesize, PROT_NONE) == 0);
363 for (size_t i = 0; i < pagesize; i++) {
364 uint8_t* buf = &memory[pagesize-i];
366 test_func(buf, i);
367 }
368 ASSERT_TRUE(mprotect(&memory[pagesize], pagesize, PROT_READ | PROT_WRITE) == 0);
369 free(memory);
370 }
372 void RunSrcDstBufferOverreadTest(void (*test_func)(uint8_t*, uint8_t*, size_t)) {
373 // In order to verify that functions are not reading past the end of the
374 // src, create data that ends exactly at an unreadable memory boundary.
375 size_t pagesize = static_cast<size_t>(sysconf(_SC_PAGE_SIZE));
376 uint8_t* memory;
377 ASSERT_TRUE(posix_memalign(reinterpret_cast<void**>(&memory), pagesize,
378 2*pagesize) == 0);
379 memset(memory, 0x23, 2*pagesize);
381 // Make the second page unreadable and unwritable.
382 ASSERT_TRUE(mprotect(&memory[pagesize], pagesize, PROT_NONE) == 0);
384 uint8_t* dst = new uint8_t[pagesize];
385 for (size_t i = 0; i < pagesize; i++) {
386 uint8_t* src = &memory[pagesize-i];
388 test_func(src, dst, i);
389 }
390 ASSERT_TRUE(mprotect(&memory[pagesize], pagesize, PROT_READ | PROT_WRITE) == 0);
391 free(memory);
392 delete dst;
393 }
395 void RunCmpBufferOverreadTest(
396 void (*test_cmp_func)(uint8_t*, uint8_t*, size_t),
397 void (*test_miscmp_func)(uint8_t*, uint8_t*, size_t, size_t)) {
398 // In order to verify that functions are not reading past the end of either
399 // of the bufs, create both buffers that end exactly at an unreadable memory
400 // boundary.
401 size_t pagesize = static_cast<size_t>(sysconf(_SC_PAGE_SIZE));
402 uint8_t* memory1;
403 ASSERT_TRUE(posix_memalign(reinterpret_cast<void**>(&memory1), pagesize,
404 2*pagesize) == 0);
405 memset(memory1, 0x23, 2*pagesize);
407 // Make the second page unreadable and unwritable.
408 ASSERT_TRUE(mprotect(&memory1[pagesize], pagesize, PROT_NONE) == 0);
410 uint8_t* memory2;
411 ASSERT_TRUE(posix_memalign(reinterpret_cast<void**>(&memory2), pagesize,
412 2*pagesize) == 0);
413 memset(memory2, 0x23, 2*pagesize);
415 // Make the second page unreadable and unwritable.
416 ASSERT_TRUE(mprotect(&memory2[pagesize], pagesize, PROT_NONE) == 0);
418 for (size_t i = 0; i < pagesize; i++) {
419 uint8_t* buf1 = &memory1[pagesize-i];
420 uint8_t* buf2 = &memory2[pagesize-i];
422 test_cmp_func(buf1, buf2, i);
423 }
425 // Don't cycle through pagesize, MISCMP_MAX_LENGTH bytes should be good.
426 size_t miscmp_len;
427 if (pagesize > MISCMP_MAX_LENGTH) {
428 miscmp_len = MISCMP_MAX_LENGTH;
429 } else {
430 miscmp_len = pagesize;
431 }
432 for (size_t i = 1; i < miscmp_len; i++) {
433 uint8_t* buf1 = &memory1[pagesize-i];
434 for (size_t j = 1; j < miscmp_len; j++) {
435 if (j == i)
436 continue;
438 uint8_t* buf2 = &memory2[pagesize-j];
440 test_miscmp_func(buf1, buf2, i, j);
441 }
442 }
444 ASSERT_TRUE(mprotect(&memory1[pagesize], pagesize, PROT_READ | PROT_WRITE) == 0);
445 ASSERT_TRUE(mprotect(&memory2[pagesize], pagesize, PROT_READ | PROT_WRITE) == 0);
446 free(memory1);
447 free(memory2);
448 }