/* * Copyright (C) 2008 The Android Open Source Project * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in * the documentation and/or other materials provided with the * distribution. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS * FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE * COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, * INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, * BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS * OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED * AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT * OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF * SUCH DAMAGE. */ #include "libc_init_common.h" #include #include #include #include #include #include #include #include #include #include "private/bionic_auxv.h" #include "private/bionic_ssp.h" #include "private/bionic_tls.h" #include "private/KernelArgumentBlock.h" #include "pthread_internal.h" extern "C" abort_msg_t** __abort_message_ptr; extern "C" int __system_properties_init(void); extern "C" int __set_tls(void* ptr); extern "C" int __set_tid_address(int* tid_address); __LIBC_HIDDEN__ void __libc_init_vdso(); // Not public, but well-known in the BSDs. const char* __progname; // Declared in . char** environ; // Declared in "private/bionic_ssp.h". uintptr_t __stack_chk_guard = 0; /* Init TLS for the initial thread. Called by the linker _before_ libc is mapped * in memory. Beware: all writes to libc globals from this function will * apply to linker-private copies and will not be visible from libc later on. * * Note: this function creates a pthread_internal_t for the initial thread and * stores the pointer in TLS, but does not add it to pthread's thread list. This * has to be done later from libc itself (see __libc_init_common). * * This function also stores a pointer to the kernel argument block in a TLS slot to be * picked up by the libc constructor. */ void __libc_init_tls(KernelArgumentBlock& args) { __libc_auxv = args.auxv; static void* tls[BIONIC_TLS_SLOTS]; static pthread_internal_t main_thread; main_thread.tls = tls; // Tell the kernel to clear our tid field when we exit, so we're like any other pthread. // As a side-effect, this tells us our pid (which is the same as the main thread's tid). main_thread.tid = __set_tid_address(&main_thread.tid); main_thread.set_cached_pid(main_thread.tid); // We don't want to free the main thread's stack even when the main thread exits // because things like environment variables with global scope live on it. // We also can't free the pthread_internal_t itself, since that lives on the main // thread's stack rather than on the heap. pthread_attr_init(&main_thread.attr); main_thread.attr.flags = PTHREAD_ATTR_FLAG_USER_ALLOCATED_STACK | PTHREAD_ATTR_FLAG_MAIN_THREAD; main_thread.attr.guard_size = 0; // The main thread has no guard page. main_thread.attr.stack_size = 0; // User code should never see this; we'll compute it when asked. // TODO: the main thread's sched_policy and sched_priority need to be queried. __init_thread(&main_thread, false); __init_tls(&main_thread); __set_tls(main_thread.tls); tls[TLS_SLOT_BIONIC_PREINIT] = &args; __init_alternate_signal_stack(&main_thread); } void __libc_init_common(KernelArgumentBlock& args) { // Initialize various globals. environ = args.envp; errno = 0; __libc_auxv = args.auxv; __progname = args.argv[0] ? args.argv[0] : ""; __abort_message_ptr = args.abort_message_ptr; // AT_RANDOM is a pointer to 16 bytes of randomness on the stack. __stack_chk_guard = *reinterpret_cast(getauxval(AT_RANDOM)); // Get the main thread from TLS and add it to the thread list. pthread_internal_t* main_thread = __get_thread(); _pthread_internal_add(main_thread); __system_properties_init(); // Requires 'environ'. __libc_init_vdso(); } /* This function will be called during normal program termination * to run the destructors that are listed in the .fini_array section * of the executable, if any. * * 'fini_array' points to a list of function addresses. The first * entry in the list has value -1, the last one has value 0. */ void __libc_fini(void* array) { void** fini_array = reinterpret_cast(array); const size_t minus1 = ~(size_t)0; /* ensure proper sign extension */ /* Sanity check - first entry must be -1 */ if (array == NULL || (size_t)fini_array[0] != minus1) { return; } /* skip over it */ fini_array += 1; /* Count the number of destructors. */ int count = 0; while (fini_array[count] != NULL) { ++count; } /* Now call each destructor in reverse order. */ while (count > 0) { void (*func)() = (void (*)()) fini_array[--count]; /* Sanity check, any -1 in the list is ignored */ if ((size_t)func == minus1) { continue; } func(); } #ifndef LIBC_STATIC { extern void __libc_postfini(void) __attribute__((weak)); if (__libc_postfini) { __libc_postfini(); } } #endif }