/* * Copyright (C) 2009 The Android Open Source Project * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in * the documentation and/or other materials provided with the * distribution. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS * FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE * COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, * INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, * BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS * OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED * AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT * OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF * SUCH DAMAGE. */ // Contains definition of structures, global variables, and implementation of // routines that are used by malloc leak detection code and other components in // the system. The trick is that some components expect these data and // routines to be defined / implemented in libc.so, regardless whether or not // malloc leak detection code is going to run. To make things even more tricky, // malloc leak detection code, implemented in libc_malloc_debug.so also // requires access to these variables and routines (to fill allocation entry // hash table, for example). So, all relevant variables and routines are // defined / implemented here and exported to all, leak detection code and // other components via dynamic (libc.so), or static (libc.a) linking. #include "malloc_debug_common.h" #include #include #include #include "private/ScopedPthreadMutexLocker.h" #if defined(USE_JEMALLOC) #include "jemalloc.h" #define Malloc(function) je_ ## function #elif defined(USE_DLMALLOC) #include "dlmalloc.h" #define Malloc(function) dl ## function #else #error "Either one of USE_DLMALLOC or USE_JEMALLOC must be defined." #endif // In a VM process, this is set to 1 after fork()ing out of zygote. int gMallocLeakZygoteChild = 0; static HashTable g_hash_table; // Support for malloc debugging. // Table for dispatching malloc calls, initialized with default dispatchers. static const MallocDebug __libc_malloc_default_dispatch __attribute__((aligned(32))) = { Malloc(calloc), Malloc(free), Malloc(mallinfo), Malloc(malloc), Malloc(malloc_usable_size), Malloc(memalign), Malloc(posix_memalign), #if defined(HAVE_DEPRECATED_MALLOC_FUNCS) Malloc(pvalloc), #endif Malloc(realloc), #if defined(HAVE_DEPRECATED_MALLOC_FUNCS) Malloc(valloc), #endif }; // Selector of dispatch table to use for dispatching malloc calls. static const MallocDebug* __libc_malloc_dispatch = &__libc_malloc_default_dispatch; // Handle to shared library where actual memory allocation is implemented. // This library is loaded and memory allocation calls are redirected there // when libc.debug.malloc environment variable contains value other than // zero: // 1 - For memory leak detections. // 5 - For filling allocated / freed memory with patterns defined by // CHK_SENTINEL_VALUE, and CHK_FILL_FREE macros. // 10 - For adding pre-, and post- allocation stubs in order to detect // buffer overruns. // Note that emulator's memory allocation instrumentation is not controlled by // libc.debug.malloc value, but rather by emulator, started with -memcheck // option. Note also, that if emulator has started with -memcheck option, // emulator's instrumented memory allocation will take over value saved in // libc.debug.malloc. In other words, if emulator has started with -memcheck // option, libc.debug.malloc value is ignored. // Actual functionality for debug levels 1-10 is implemented in // libc_malloc_debug_leak.so, while functionality for emulator's instrumented // allocations is implemented in libc_malloc_debug_qemu.so and can be run inside // the emulator only. #if !defined(LIBC_STATIC) static void* libc_malloc_impl_handle = NULL; #endif // The value of libc.debug.malloc. #if !defined(LIBC_STATIC) static int g_malloc_debug_level = 0; #endif // ============================================================================= // output functions // ============================================================================= static int hash_entry_compare(const void* arg1, const void* arg2) { int result; const HashEntry* e1 = *static_cast(arg1); const HashEntry* e2 = *static_cast(arg2); // if one or both arg pointers are null, deal gracefully if (e1 == NULL) { result = (e2 == NULL) ? 0 : 1; } else if (e2 == NULL) { result = -1; } else { size_t nbAlloc1 = e1->allocations; size_t nbAlloc2 = e2->allocations; size_t size1 = e1->size & ~SIZE_FLAG_MASK; size_t size2 = e2->size & ~SIZE_FLAG_MASK; size_t alloc1 = nbAlloc1 * size1; size_t alloc2 = nbAlloc2 * size2; // sort in descending order by: // 1) total size // 2) number of allocations // // This is used for sorting, not determination of equality, so we don't // need to compare the bit flags. if (alloc1 > alloc2) { result = -1; } else if (alloc1 < alloc2) { result = 1; } else { if (nbAlloc1 > nbAlloc2) { result = -1; } else if (nbAlloc1 < nbAlloc2) { result = 1; } else { result = 0; } } } return result; } // Retrieve native heap information. // // "*info" is set to a buffer we allocate // "*overallSize" is set to the size of the "info" buffer // "*infoSize" is set to the size of a single entry // "*totalMemory" is set to the sum of all allocations we're tracking; does // not include heap overhead // "*backtraceSize" is set to the maximum number of entries in the back trace // ============================================================================= // Exported for use by ddms. // ============================================================================= extern "C" void get_malloc_leak_info(uint8_t** info, size_t* overallSize, size_t* infoSize, size_t* totalMemory, size_t* backtraceSize) { // Don't do anything if we have invalid arguments. if (info == NULL || overallSize == NULL || infoSize == NULL || totalMemory == NULL || backtraceSize == NULL) { return; } *totalMemory = 0; ScopedPthreadMutexLocker locker(&g_hash_table.lock); if (g_hash_table.count == 0) { *info = NULL; *overallSize = 0; *infoSize = 0; *backtraceSize = 0; return; } HashEntry** list = static_cast(Malloc(malloc)(sizeof(void*) * g_hash_table.count)); // Get the entries into an array to be sorted. size_t index = 0; for (size_t i = 0 ; i < HASHTABLE_SIZE ; ++i) { HashEntry* entry = g_hash_table.slots[i]; while (entry != NULL) { list[index] = entry; *totalMemory = *totalMemory + ((entry->size & ~SIZE_FLAG_MASK) * entry->allocations); index++; entry = entry->next; } } // XXX: the protocol doesn't allow variable size for the stack trace (yet) *infoSize = (sizeof(size_t) * 2) + (sizeof(uintptr_t) * BACKTRACE_SIZE); *overallSize = *infoSize * g_hash_table.count; *backtraceSize = BACKTRACE_SIZE; // now get a byte array big enough for this *info = static_cast(Malloc(malloc)(*overallSize)); if (*info == NULL) { *overallSize = 0; Malloc(free)(list); return; } qsort(list, g_hash_table.count, sizeof(void*), hash_entry_compare); uint8_t* head = *info; const size_t count = g_hash_table.count; for (size_t i = 0 ; i < count ; ++i) { HashEntry* entry = list[i]; size_t entrySize = (sizeof(size_t) * 2) + (sizeof(uintptr_t) * entry->numEntries); if (entrySize < *infoSize) { // We're writing less than a full entry, clear out the rest. memset(head + entrySize, 0, *infoSize - entrySize); } else { // Make sure the amount we're copying doesn't exceed the limit. entrySize = *infoSize; } memcpy(head, &(entry->size), entrySize); head += *infoSize; } Malloc(free)(list); } extern "C" void free_malloc_leak_info(uint8_t* info) { Malloc(free)(info); } // ============================================================================= // Allocation functions // ============================================================================= extern "C" void* calloc(size_t n_elements, size_t elem_size) { return __libc_malloc_dispatch->calloc(n_elements, elem_size); } extern "C" void free(void* mem) { __libc_malloc_dispatch->free(mem); } extern "C" struct mallinfo mallinfo() { return __libc_malloc_dispatch->mallinfo(); } extern "C" void* malloc(size_t bytes) { return __libc_malloc_dispatch->malloc(bytes); } extern "C" size_t malloc_usable_size(const void* mem) { return __libc_malloc_dispatch->malloc_usable_size(mem); } extern "C" void* memalign(size_t alignment, size_t bytes) { return __libc_malloc_dispatch->memalign(alignment, bytes); } extern "C" int posix_memalign(void** memptr, size_t alignment, size_t size) { return __libc_malloc_dispatch->posix_memalign(memptr, alignment, size); } #if defined(HAVE_DEPRECATED_MALLOC_FUNCS) extern "C" void* pvalloc(size_t bytes) { return __libc_malloc_dispatch->pvalloc(bytes); } #endif extern "C" void* realloc(void* oldMem, size_t bytes) { return __libc_malloc_dispatch->realloc(oldMem, bytes); } #if defined(HAVE_DEPRECATED_MALLOC_FUNCS) extern "C" void* valloc(size_t bytes) { return __libc_malloc_dispatch->valloc(bytes); } #endif // We implement malloc debugging only in libc.so, so the code below // must be excluded if we compile this file for static libc.a #ifndef LIBC_STATIC #include #include #include #include "private/libc_logging.h" template static void InitMallocFunction(void* malloc_impl_handler, FunctionType* func, const char* prefix, const char* suffix) { char symbol[128]; snprintf(symbol, sizeof(symbol), "%s_%s", prefix, suffix); *func = reinterpret_cast(dlsym(malloc_impl_handler, symbol)); if (*func == NULL) { error_log("%s: dlsym(\"%s\") failed", getprogname(), symbol); } } static void InitMalloc(void* malloc_impl_handler, MallocDebug* table, const char* prefix) { __libc_format_log(ANDROID_LOG_INFO, "libc", "%s: using libc.debug.malloc %d (%s)\n", getprogname(), g_malloc_debug_level, prefix); InitMallocFunction(malloc_impl_handler, &table->calloc, prefix, "calloc"); InitMallocFunction(malloc_impl_handler, &table->free, prefix, "free"); InitMallocFunction(malloc_impl_handler, &table->mallinfo, prefix, "mallinfo"); InitMallocFunction(malloc_impl_handler, &table->malloc, prefix, "malloc"); InitMallocFunction(malloc_impl_handler, &table->malloc_usable_size, prefix, "malloc_usable_size"); InitMallocFunction(malloc_impl_handler, &table->memalign, prefix, "memalign"); InitMallocFunction(malloc_impl_handler, &table->posix_memalign, prefix, "posix_memalign"); #if defined(HAVE_DEPRECATED_MALLOC_FUNCS) InitMallocFunction(malloc_impl_handler, &table->pvalloc, prefix, "pvalloc"); #endif InitMallocFunction(malloc_impl_handler, &table->realloc, prefix, "realloc"); #if defined(HAVE_DEPRECATED_MALLOC_FUNCS) InitMallocFunction(malloc_impl_handler, &table->valloc, prefix, "valloc"); #endif } // Initializes memory allocation framework once per process. static void malloc_init_impl() { const char* so_name = NULL; MallocDebugInit malloc_debug_initialize = NULL; unsigned int qemu_running = 0; unsigned int memcheck_enabled = 0; char env[PROP_VALUE_MAX]; char memcheck_tracing[PROP_VALUE_MAX]; char debug_program[PROP_VALUE_MAX]; // Get custom malloc debug level. Note that emulator started with // memory checking option will have priority over debug level set in // libc.debug.malloc system property. if (__system_property_get("ro.kernel.qemu", env) && atoi(env)) { qemu_running = 1; if (__system_property_get("ro.kernel.memcheck", memcheck_tracing)) { if (memcheck_tracing[0] != '0') { // Emulator has started with memory tracing enabled. Enforce it. g_malloc_debug_level = 20; memcheck_enabled = 1; } } } // If debug level has not been set by memcheck option in the emulator, // lets grab it from libc.debug.malloc system property. if (g_malloc_debug_level == 0 && __system_property_get("libc.debug.malloc", env)) { g_malloc_debug_level = atoi(env); } // Debug level 0 means that we should use default allocation routines. if (g_malloc_debug_level == 0) { return; } // If libc.debug.malloc.program is set and is not a substring of progname, // then exit. if (__system_property_get("libc.debug.malloc.program", debug_program)) { if (!strstr(getprogname(), debug_program)) { return; } } // mksh is way too leaky. http://b/7291287. if (g_malloc_debug_level >= 10) { if (strcmp(getprogname(), "sh") == 0 || strcmp(getprogname(), "/system/bin/sh") == 0) { return; } } // Choose the appropriate .so for the requested debug level. switch (g_malloc_debug_level) { case 1: case 5: case 10: so_name = "libc_malloc_debug_leak.so"; break; case 20: // Quick check: debug level 20 can only be handled in emulator. if (!qemu_running) { error_log("%s: Debug level %d can only be set in emulator\n", getprogname(), g_malloc_debug_level); return; } // Make sure that memory checking has been enabled in emulator. if (!memcheck_enabled) { error_log("%s: Memory checking is not enabled in the emulator\n", getprogname()); return; } so_name = "libc_malloc_debug_qemu.so"; break; default: error_log("%s: Debug level %d is unknown\n", getprogname(), g_malloc_debug_level); return; } // Load .so that implements the required malloc debugging functionality. void* malloc_impl_handle = dlopen(so_name, RTLD_LAZY); if (malloc_impl_handle == NULL) { error_log("%s: Missing module %s required for malloc debug level %d: %s", getprogname(), so_name, g_malloc_debug_level, dlerror()); return; } // Initialize malloc debugging in the loaded module. malloc_debug_initialize = reinterpret_cast(dlsym(malloc_impl_handle, "malloc_debug_initialize")); if (malloc_debug_initialize == NULL) { error_log("%s: Initialization routine is not found in %s\n", getprogname(), so_name); dlclose(malloc_impl_handle); return; } if (!malloc_debug_initialize(&g_hash_table, &__libc_malloc_default_dispatch)) { dlclose(malloc_impl_handle); return; } if (g_malloc_debug_level == 20) { // For memory checker we need to do extra initialization. typedef int (*MemCheckInit)(int, const char*); MemCheckInit memcheck_initialize = reinterpret_cast(dlsym(malloc_impl_handle, "memcheck_initialize")); if (memcheck_initialize == NULL) { error_log("%s: memcheck_initialize routine is not found in %s\n", getprogname(), so_name); dlclose(malloc_impl_handle); return; } if (memcheck_initialize(MALLOC_ALIGNMENT, memcheck_tracing)) { dlclose(malloc_impl_handle); return; } } // No need to init the dispatch table because we can only get // here if debug level is 1, 5, 10, or 20. static MallocDebug malloc_dispatch_table __attribute__((aligned(32))); switch (g_malloc_debug_level) { case 1: InitMalloc(malloc_impl_handle, &malloc_dispatch_table, "leak"); break; case 5: InitMalloc(malloc_impl_handle, &malloc_dispatch_table, "fill"); break; case 10: InitMalloc(malloc_impl_handle, &malloc_dispatch_table, "chk"); break; case 20: InitMalloc(malloc_impl_handle, &malloc_dispatch_table, "qemu_instrumented"); break; default: break; } // Make sure dispatch table is initialized if ((malloc_dispatch_table.calloc == NULL) || (malloc_dispatch_table.free == NULL) || (malloc_dispatch_table.mallinfo == NULL) || (malloc_dispatch_table.malloc == NULL) || (malloc_dispatch_table.malloc_usable_size == NULL) || (malloc_dispatch_table.memalign == NULL) || (malloc_dispatch_table.posix_memalign == NULL) || #if defined(HAVE_DEPRECATED_MALLOC_FUNCS) (malloc_dispatch_table.pvalloc == NULL) || #endif (malloc_dispatch_table.realloc == NULL) #if defined(HAVE_DEPRECATED_MALLOC_FUNCS) || (malloc_dispatch_table.valloc == NULL) #endif ) { error_log("%s: some symbols for libc.debug.malloc level %d were not found (see above)", getprogname(), g_malloc_debug_level); dlclose(malloc_impl_handle); } else { __libc_malloc_dispatch = &malloc_dispatch_table; libc_malloc_impl_handle = malloc_impl_handle; } } static void malloc_fini_impl() { // Our BSD stdio implementation doesn't close the standard streams, it only flushes them. // And it doesn't do that until its atexit handler is run, and we run first! // It's great that other unclosed FILE*s show up as malloc leaks, but we need to manually // clean up the standard streams ourselves. fclose(stdin); fclose(stdout); fclose(stderr); if (libc_malloc_impl_handle != NULL) { MallocDebugFini malloc_debug_finalize = reinterpret_cast(dlsym(libc_malloc_impl_handle, "malloc_debug_finalize")); if (malloc_debug_finalize != NULL) { malloc_debug_finalize(g_malloc_debug_level); } } } #endif // !LIBC_STATIC // Initializes memory allocation framework. // This routine is called from __libc_init routines implemented // in libc_init_static.c and libc_init_dynamic.c files. extern "C" __LIBC_HIDDEN__ void malloc_debug_init() { #if !defined(LIBC_STATIC) static pthread_once_t malloc_init_once_ctl = PTHREAD_ONCE_INIT; if (pthread_once(&malloc_init_once_ctl, malloc_init_impl)) { error_log("Unable to initialize malloc_debug component."); } #endif // !LIBC_STATIC } extern "C" __LIBC_HIDDEN__ void malloc_debug_fini() { #if !defined(LIBC_STATIC) static pthread_once_t malloc_fini_once_ctl = PTHREAD_ONCE_INIT; if (pthread_once(&malloc_fini_once_ctl, malloc_fini_impl)) { error_log("Unable to finalize malloc_debug component."); } #endif // !LIBC_STATIC }