/* * Copyright (C) 2008 The Android Open Source Project * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in * the documentation and/or other materials provided with the * distribution. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS * FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE * COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, * INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, * BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS * OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED * AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT * OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF * SUCH DAMAGE. */ #include #include #include #include #include "pthread_internal.h" #include "private/bionic_macros.h" #include "private/bionic_ssp.h" #include "private/bionic_tls.h" #include "private/libc_logging.h" #include "private/ErrnoRestorer.h" #include "private/ScopedPthreadMutexLocker.h" // Used by gdb to track thread creation. See libthread_db. #ifdef __i386__ extern "C" __attribute__((noinline)) __attribute__((fastcall)) void _thread_created_hook(pid_t) {} #else extern "C" __attribute__((noinline)) void _thread_created_hook(pid_t) {} #endif // x86 uses segment descriptors rather than a direct pointer to TLS. #if __i386__ #include extern "C" __LIBC_HIDDEN__ void __init_user_desc(struct user_desc*, int, void*); #endif static pthread_mutex_t g_pthread_stack_creation_lock = PTHREAD_MUTEX_INITIALIZER; static pthread_mutex_t g_debugger_notification_lock = PTHREAD_MUTEX_INITIALIZER; extern "C" int __isthreaded; // This code is used both by each new pthread and the code that initializes the main thread. void __init_tls(pthread_internal_t* thread) { // Zero-initialize all the slots after TLS_SLOT_SELF and TLS_SLOT_THREAD_ID. for (size_t i = TLS_SLOT_ERRNO; i < BIONIC_TLS_SLOTS; ++i) { thread->tls[i] = NULL; } // Slot 0 must point to itself. The x86 Linux kernel reads the TLS from %fs:0. thread->tls[TLS_SLOT_SELF] = thread->tls; thread->tls[TLS_SLOT_THREAD_ID] = thread; // GCC looks in the TLS for the stack guard on x86, so copy it there from our global. thread->tls[TLS_SLOT_STACK_GUARD] = (void*) __stack_chk_guard; } void __init_alternate_signal_stack(pthread_internal_t* thread) { // Create and set an alternate signal stack. stack_t ss; ss.ss_sp = mmap(NULL, SIGSTKSZ, PROT_READ|PROT_WRITE, MAP_PRIVATE|MAP_ANONYMOUS, 0, 0); if (ss.ss_sp != MAP_FAILED) { ss.ss_size = SIGSTKSZ; ss.ss_flags = 0; sigaltstack(&ss, NULL); thread->alternate_signal_stack = ss.ss_sp; } } int __init_thread(pthread_internal_t* thread, bool add_to_thread_list) { int error = 0; // Set the scheduling policy/priority of the thread. if (thread->attr.sched_policy != SCHED_NORMAL) { sched_param param; param.sched_priority = thread->attr.sched_priority; if (sched_setscheduler(thread->tid, thread->attr.sched_policy, ¶m) == -1) { #if __LP64__ // For backwards compatibility reasons, we only report failures on 64-bit devices. error = errno; #endif __libc_format_log(ANDROID_LOG_WARN, "libc", "pthread_create sched_setscheduler call failed: %s", strerror(errno)); } } thread->cleanup_stack = NULL; if (add_to_thread_list) { _pthread_internal_add(thread); } return error; } static void* __create_thread_stack(pthread_internal_t* thread) { ScopedPthreadMutexLocker lock(&g_pthread_stack_creation_lock); // Create a new private anonymous map. int prot = PROT_READ | PROT_WRITE; int flags = MAP_PRIVATE | MAP_ANONYMOUS | MAP_NORESERVE; void* stack = mmap(NULL, thread->attr.stack_size, prot, flags, -1, 0); if (stack == MAP_FAILED) { __libc_format_log(ANDROID_LOG_WARN, "libc", "pthread_create failed: couldn't allocate %zd-byte stack: %s", thread->attr.stack_size, strerror(errno)); return NULL; } // Set the guard region at the end of the stack to PROT_NONE. if (mprotect(stack, thread->attr.guard_size, PROT_NONE) == -1) { __libc_format_log(ANDROID_LOG_WARN, "libc", "pthread_create failed: couldn't mprotect PROT_NONE %zd-byte stack guard region: %s", thread->attr.guard_size, strerror(errno)); munmap(stack, thread->attr.stack_size); return NULL; } return stack; } static int __pthread_start(void* arg) { pthread_internal_t* thread = reinterpret_cast(arg); // Wait for our creating thread to release us. This lets it have time to // notify gdb about this thread before we start doing anything. // This also provides the memory barrier needed to ensure that all memory // accesses previously made by the creating thread are visible to us. pthread_mutex_lock(&thread->startup_handshake_mutex); pthread_mutex_destroy(&thread->startup_handshake_mutex); __init_alternate_signal_stack(thread); void* result = thread->start_routine(thread->start_routine_arg); pthread_exit(result); return 0; } // A dummy start routine for pthread_create failures where we've created a thread but aren't // going to run user code on it. We swap out the user's start routine for this and take advantage // of the regular thread teardown to free up resources. static void* __do_nothing(void*) { return NULL; } int pthread_create(pthread_t* thread_out, pthread_attr_t const* attr, void* (*start_routine)(void*), void* arg) { ErrnoRestorer errno_restorer; // Inform the rest of the C library that at least one thread was created. __isthreaded = 1; pthread_internal_t* thread = reinterpret_cast(calloc(sizeof(*thread), 1)); if (thread == NULL) { __libc_format_log(ANDROID_LOG_WARN, "libc", "pthread_create failed: couldn't allocate thread"); return EAGAIN; } if (attr == NULL) { pthread_attr_init(&thread->attr); } else { thread->attr = *attr; attr = NULL; // Prevent misuse below. } // Make sure the stack size and guard size are multiples of PAGE_SIZE. thread->attr.stack_size = BIONIC_ALIGN(thread->attr.stack_size, PAGE_SIZE); thread->attr.guard_size = BIONIC_ALIGN(thread->attr.guard_size, PAGE_SIZE); if (thread->attr.stack_base == NULL) { // The caller didn't provide a stack, so allocate one. thread->attr.stack_base = __create_thread_stack(thread); if (thread->attr.stack_base == NULL) { free(thread); return EAGAIN; } } else { // The caller did provide a stack, so remember we're not supposed to free it. thread->attr.flags |= PTHREAD_ATTR_FLAG_USER_ALLOCATED_STACK; } // Make room for the TLS area. // The child stack is the same address, just growing in the opposite direction. // At offsets >= 0, we have the TLS slots. // At offsets < 0, we have the child stack. thread->tls = reinterpret_cast(reinterpret_cast(thread->attr.stack_base) + thread->attr.stack_size - BIONIC_TLS_SLOTS * sizeof(void*)); void* child_stack = thread->tls; __init_tls(thread); // Create a mutex for the thread in TLS to wait on once it starts so we can keep // it from doing anything until after we notify the debugger about it // // This also provides the memory barrier we need to ensure that all // memory accesses previously performed by this thread are visible to // the new thread. pthread_mutex_init(&thread->startup_handshake_mutex, NULL); pthread_mutex_lock(&thread->startup_handshake_mutex); thread->start_routine = start_routine; thread->start_routine_arg = arg; thread->set_cached_pid(getpid()); int flags = CLONE_VM | CLONE_FS | CLONE_FILES | CLONE_SIGHAND | CLONE_THREAD | CLONE_SYSVSEM | CLONE_SETTLS | CLONE_PARENT_SETTID | CLONE_CHILD_CLEARTID; void* tls = thread->tls; #if defined(__i386__) // On x86 (but not x86-64), CLONE_SETTLS takes a pointer to a struct user_desc rather than // a pointer to the TLS itself. user_desc tls_descriptor; __init_user_desc(&tls_descriptor, false, tls); tls = &tls_descriptor; #endif int rc = clone(__pthread_start, child_stack, flags, thread, &(thread->tid), tls, &(thread->tid)); if (rc == -1) { int clone_errno = errno; // We don't have to unlock the mutex at all because clone(2) failed so there's no child waiting to // be unblocked, but we're about to unmap the memory the mutex is stored in, so this serves as a // reminder that you can't rewrite this function to use a ScopedPthreadMutexLocker. pthread_mutex_unlock(&thread->startup_handshake_mutex); if ((thread->attr.flags & PTHREAD_ATTR_FLAG_USER_ALLOCATED_STACK) == 0) { munmap(thread->attr.stack_base, thread->attr.stack_size); } free(thread); __libc_format_log(ANDROID_LOG_WARN, "libc", "pthread_create failed: clone failed: %s", strerror(errno)); return clone_errno; } int init_errno = __init_thread(thread, true); if (init_errno != 0) { // Mark the thread detached and replace its start_routine with a no-op. // Letting the thread run is the easiest way to clean up its resources. thread->attr.flags |= PTHREAD_ATTR_FLAG_DETACHED; thread->start_routine = __do_nothing; pthread_mutex_unlock(&thread->startup_handshake_mutex); return init_errno; } // Notify any debuggers about the new thread. { ScopedPthreadMutexLocker debugger_locker(&g_debugger_notification_lock); _thread_created_hook(thread->tid); } // Publish the pthread_t and unlock the mutex to let the new thread start running. *thread_out = reinterpret_cast(thread); pthread_mutex_unlock(&thread->startup_handshake_mutex); return 0; }