/* * Copyright (C) 2011 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #ifndef BIONIC_ATOMIC_X86_H #define BIONIC_ATOMIC_X86_H /* Define a full memory barrier, this is only needed if we build the * platform for a multi-core device. */ #if defined(ANDROID_SMP) && ANDROID_SMP == 1 __ATOMIC_INLINE__ void __bionic_memory_barrier() { __asm__ __volatile__ ( "mfence" : : : "memory" ); } #else __ATOMIC_INLINE__ void __bionic_memory_barrier() { /* A simple compiler barrier */ __asm__ __volatile__ ( "" : : : "memory" ); } #endif /* Compare-and-swap, without any explicit barriers. Note that this function * returns 0 on success, and 1 on failure. The opposite convention is typically * used on other platforms. */ __ATOMIC_INLINE__ int __bionic_cmpxchg(int32_t old_value, int32_t new_value, volatile int32_t* ptr) { int32_t prev; __asm__ __volatile__ ("lock; cmpxchgl %1, %2" : "=a" (prev) : "q" (new_value), "m" (*ptr), "0" (old_value) : "memory"); return prev != old_value; } /* Swap, without any explicit barriers */ __ATOMIC_INLINE__ int32_t __bionic_swap(int32_t new_value, volatile int32_t *ptr) { __asm__ __volatile__ ("xchgl %1, %0" : "=r" (new_value) : "m" (*ptr), "0" (new_value) : "memory"); return new_value; } /* Atomic increment, without explicit barriers */ __ATOMIC_INLINE__ int32_t __bionic_atomic_inc(volatile int32_t *ptr) { int increment = 1; __asm__ __volatile__ ("lock; xaddl %0, %1" : "+r" (increment), "+m" (*ptr) : : "memory"); /* increment now holds the old value of *ptr */ return increment; } /* Atomic decrement, without explicit barriers */ __ATOMIC_INLINE__ int32_t __bionic_atomic_dec(volatile int32_t *ptr) { int increment = -1; __asm__ __volatile__ ("lock; xaddl %0, %1" : "+r" (increment), "+m" (*ptr) : : "memory"); /* increment now holds the old value of *ptr */ return increment; } #endif /* BIONIC_ATOMIC_X86_H */