#!/usr/bin/python import glob import os import re import subprocess import sys only_unwanted = False if len(sys.argv) > 1: if sys.argv[1] in ('-u', '--unwanted'): only_unwanted = True toolchain = os.environ['ANDROID_TOOLCHAIN'] arch = re.sub(r'.*/linux-x86/([^/]+)/.*', r'\1', toolchain) if arch == 'aarch64': arch = 'arm64' def GetSymbolsFromSo(so_file): # Example readelf output: # 264: 0001623c 4 FUNC GLOBAL DEFAULT 8 cabsf # 266: 00016244 4 FUNC GLOBAL DEFAULT 8 dremf # 267: 00019018 4 OBJECT GLOBAL DEFAULT 11 __fe_dfl_env # 268: 00000000 0 FUNC GLOBAL DEFAULT UND __aeabi_dcmplt r = re.compile(r' +\d+: [0-9a-f]+ +\d+ (I?FUNC|OBJECT) +\S+ +\S+ +\d+ (\S+)') symbols = set() for line in subprocess.check_output(['readelf', '--dyn-syms', '-W', so_file]).split('\n'): if ' HIDDEN ' in line or ' UND ' in line: continue m = r.match(line) if m: symbol = m.group(2) symbol = re.sub('@.*', '', symbol) symbols.add(symbol) return symbols def GetSymbolsFromAndroidSo(*files): symbols = set() for f in files: symbols = symbols | GetSymbolsFromSo('%s/system/lib64/%s' % (os.environ['ANDROID_PRODUCT_OUT'], f)) return symbols def GetSymbolsFromSystemSo(*files): symbols = set() for f in files: f = glob.glob('/lib/x86_64-linux-gnu/%s' % f)[-1] symbols = symbols | GetSymbolsFromSo(f) return symbols def MangleGlibcNameToBionic(name): if name in glibc_to_bionic_names: return glibc_to_bionic_names[name] return name def GetNdkIgnored(): global arch symbols = set() files = glob.glob('%s/ndk/build/tools/unwanted-symbols/%s/*' % (os.getenv('ANDROID_BUILD_TOP'), arch)) for f in files: symbols |= set(open(f, 'r').read().splitlines()) return symbols glibc_to_bionic_names = { '__res_init': 'res_init', '__res_mkquery': 'res_mkquery', '__res_query': 'res_query', '__res_search': 'res_search', } glibc = GetSymbolsFromSystemSo('libc.so.*', 'librt.so.*', 'libpthread.so.*', 'libresolv.so.*', 'libm.so.*') bionic = GetSymbolsFromAndroidSo('libc.so', 'libm.so') ndk_ignored = GetNdkIgnored() glibc = map(MangleGlibcNameToBionic, glibc) # bionic includes various BSD symbols to ease porting other BSD-licensed code. bsd_stuff = set([ 'basename_r', 'dirname_r', 'fgetln', 'fpurge', 'funopen', 'gamma_r', 'gammaf_r', 'getprogname', 'setprogname', 'strlcat', 'strlcpy', 'sys_signame', 'wcslcat', 'wcslcpy' ]) # Some symbols are part of the FORTIFY implementation. FORTIFY_stuff = set([ '__FD_CLR_chk', '__FD_ISSET_chk', '__FD_SET_chk', '__stack_chk_guard', '__stpncpy_chk2', '__strchr_chk', '__strlcat_chk', '__strlcpy_chk', '__strlen_chk', '__strncpy_chk2', '__strrchr_chk', '__umask_chk' ]) # Some symbols are used to implement public macros. macro_stuff = set([ '__assert2', '__errno', '__fe_dfl_env', '__get_h_errno', '__fpclassifyd', '__isfinite', '__isfinitef', '__isfinitel', '__isnormal', '__isnormalf', '__isnormall', '__sF', '__pthread_cleanup_pop', '__pthread_cleanup_push', ]) # bionic exposes various Linux features that glibc doesn't. linux_stuff = set([ 'getauxval', 'gettid', 'tgkill' ]) # Some standard stuff isn't yet in the versions of glibc we're using. std_stuff = set([ 'at_quick_exit', 'c16rtomb', 'c32rtomb', 'mbrtoc16', 'mbrtoc32', ]) # These have mangled names in glibc, with a macro taking the "obvious" name. weird_stuff = set([ 'fstat', 'fstat64', 'fstatat', 'fstatat64', 'isfinite', 'isfinitef', 'isfinitel', 'isnormal', 'isnormalf', 'isnormall', 'lstat', 'lstat64', 'mknod', 'mknodat', 'stat', 'stat64', 'optreset', 'sigsetjmp', ]) # These exist in glibc, but under slightly different names (generally one extra # or one fewer _). TODO: check against glibc names. libresolv_stuff = set([ '__res_send_setqhook', '__res_send_setrhook', '_resolv_flush_cache_for_net', '_resolv_set_nameservers_for_net', 'dn_expand', 'nsdispatch', ]) # Implementation details we know we export (and can't get away from). known = set([ '_ctype_', '__libc_init', ]) if not only_unwanted: print 'glibc:' for symbol in sorted(glibc): print symbol print print 'bionic:' for symbol in sorted(bionic): print symbol print print 'in bionic but not glibc:' allowed_stuff = (bsd_stuff | FORTIFY_stuff | linux_stuff | macro_stuff | std_stuff | weird_stuff | libresolv_stuff | known) for symbol in sorted((bionic - allowed_stuff).difference(glibc)): if symbol in ndk_ignored: symbol += '*' print symbol sys.exit(0)