/* * Copyright 2006 The Android Open Source Project */ #include #include #include #include #include #include extern int ps_pglobal_lookup (void *, const char *obj, const char *name, void **sym_addr); extern pid_t ps_getpid(struct ps_prochandle *ph); /* * This is the list of "special" symbols we care about whose addresses are * cached by gdbserver from the host at init time. */ enum { SYM_TD_CREATE, SYM_THREAD_LIST, NUM_SYMS }; static char const * gSymbols[] = { [SYM_TD_CREATE] = "_thread_created_hook", NULL }; char const ** td_symbol_list(void) { return gSymbols; } td_err_e td_ta_new(struct ps_prochandle * proc_handle, td_thragent_t ** agent_out) { td_thragent_t * agent; agent = (td_thragent_t *)malloc(sizeof(td_thragent_t)); if (!agent) { return TD_MALLOC; } agent->pid = ps_getpid(proc_handle); agent->ph = proc_handle; *agent_out = agent; return TD_OK; } td_err_e td_ta_delete(td_thragent_t * ta) { free(ta); // FIXME: anything else to do? return TD_OK; } /* NOTE: not used by gdb 7.0 */ td_err_e td_ta_set_event(td_thragent_t const * agent, td_thr_events_t * events) { return TD_OK; } /* NOTE: not used by gdb 7.0 */ static td_thrhandle_t gEventMsgHandle; /* NOTE: not used by gdb 7.0 */ static int _event_getmsg_helper(td_thrhandle_t const * handle, void * bkpt_addr) { void * pc; pc = (void *)ptrace(PTRACE_PEEKUSR, handle->tid, (void *)60 /* r15/pc */, NULL); if (pc == bkpt_addr) { // The hook function takes the id of the new thread as it's first param, // so grab it from r0. gEventMsgHandle.pid = ptrace(PTRACE_PEEKUSR, handle->tid, (void *)0 /* r0 */, NULL); gEventMsgHandle.tid = gEventMsgHandle.pid; return 0x42; } return 0; } /* NOTE: not used by gdb 7.0 */ td_err_e td_ta_event_getmsg(td_thragent_t const * agent, td_event_msg_t * event) { td_err_e err; void * bkpt_addr; err = ps_pglobal_lookup(NULL, NULL, gSymbols[SYM_TD_CREATE], &bkpt_addr); if (err) { return err; } err = td_ta_thr_iter(agent, _event_getmsg_helper, bkpt_addr, 0, 0, NULL, 0); if (err != 0x42) { return TD_NOMSG; } event->event = TD_CREATE; event->th_p = &gEventMsgHandle; // Nasty hack, but it's the only way! return TD_OK; } td_err_e td_ta_map_lwp2thr(td_thragent_t const * agent, lwpid_t lwpid, td_thrhandle_t *th) { th->pid = ps_getpid(agent->ph); th->tid = lwpid; return TD_OK; } td_err_e td_thr_get_info(td_thrhandle_t const * handle, td_thrinfo_t * info) { info->ti_tid = handle->tid; info->ti_lid = handle->tid; // Our pthreads uses kernel ids for tids info->ti_state = TD_THR_SLEEP; /* XXX this needs to be read from /proc//task/. This is only used to see if the thread is a zombie or not */ return TD_OK; } /* NOTE: not used by gdb 7.0 */ td_err_e td_thr_event_enable(td_thrhandle_t const * handle, td_event_e event) { // I don't think we need to do anything here... return TD_OK; } /* NOTE: not used by gdb 7.0 */ td_err_e td_ta_event_addr(td_thragent_t const * agent, td_event_e event, td_notify_t * notify_out) { int32_t err; /* * This is nasty, ps_pglobal_lookup is implemented in gdbserver and looks up * the symbol from it's cache, which is populated at start time with the * symbols returned from td_symbol_list via calls back to the host. */ switch (event) { case TD_CREATE: err = ps_pglobal_lookup(NULL, NULL, gSymbols[SYM_TD_CREATE], ¬ify_out->u.bptaddr); if (err) { return TD_NOEVENT; } return TD_OK; } return TD_NOEVENT; } td_err_e td_ta_clear_event(const td_thragent_t * ta_arg, td_thr_events_t * event) { /* Given that gdb 7.0 doesn't use thread events, there's nothing we need to do here. */ return TD_OK; } td_err_e td_ta_thr_iter(td_thragent_t const * agent, td_thr_iter_f * func, void * cookie, td_thr_state_e state, int32_t prio, sigset_t * sigmask, uint32_t user_flags) { td_err_e err = TD_OK; char path[32]; DIR * dir; struct dirent * entry; td_thrhandle_t handle; snprintf(path, sizeof(path), "/proc/%d/task/", agent->pid); dir = opendir(path); if (!dir) { return TD_NOEVENT; } handle.pid = agent->pid; while ((entry = readdir(dir)) != NULL) { if (strcmp(entry->d_name, ".") == 0 || strcmp(entry->d_name, "..") == 0) { continue; } handle.tid = atoi(entry->d_name); if (func(&handle, cookie) != 0) { err = TD_DBERR; break; } } closedir(dir); return err; } td_err_e td_thr_tls_get_addr(const td_thrhandle_t * th, psaddr_t map_address, size_t offset, psaddr_t * address) { return TD_NOAPLIC; // FIXME: TODO }