/* * Copyright (C) 2013 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #include #include #include #include #include "buffer_tests.h" // For the comparison buffer tests, the maximum length to test for the // miscompare checks. #define MISCMP_MAX_LENGTH 512 #define FENCEPOST_LENGTH 8 static int g_single_aligns[][2] = { // Both buffers at same alignment. { 1, 0 }, { 2, 0 }, { 4, 0 }, { 8, 0 }, { 16, 0 }, { 32, 0 }, { 64, 0 }, { 128, 0 }, // General unaligned cases. { 4, 1 }, { 4, 2 }, { 4, 3 }, { 8, 1 }, { 8, 2 }, { 8, 3 }, { 8, 4 }, { 8, 5 }, { 8, 6 }, { 8, 7 }, { 128, 1 }, { 128, 4 }, { 128, 8 }, { 128, 12 }, { 128, 16 }, }; static const size_t g_single_aligns_len = sizeof(g_single_aligns)/sizeof(int[2]); // Set of multiple buffer alignment combinations to be used for string/memory // testing routines. static int g_double_aligns[][4] = { // Both buffers at same alignment. { 1, 0, 1, 0 }, { 2, 0, 2, 0 }, { 4, 0, 4, 0 }, { 8, 0, 8, 0 }, { 16, 0, 16, 0 }, { 32, 0, 32, 0 }, { 64, 0, 64, 0 }, { 128, 0, 128, 0 }, // Different word alignments between buffers. { 8, 0, 4, 0 }, { 4, 0, 8, 0 }, { 16, 0, 4, 0 }, { 4, 0, 16, 0 }, // General unaligned cases. { 4, 0, 4, 1 }, { 4, 0, 4, 2 }, { 4, 0, 4, 3 }, { 4, 1, 4, 0 }, { 4, 1, 4, 1 }, { 4, 1, 4, 2 }, { 4, 1, 4, 3 }, { 4, 2, 4, 0 }, { 4, 2, 4, 1 }, { 4, 2, 4, 2 }, { 4, 2, 4, 3 }, { 4, 3, 4, 0 }, { 4, 3, 4, 1 }, { 4, 3, 4, 2 }, { 4, 3, 4, 3 }, { 8, 0, 8, 1 }, { 8, 0, 8, 2 }, { 8, 0, 8, 3 }, { 8, 0, 8, 4 }, { 8, 0, 8, 5 }, { 8, 0, 8, 6 }, { 8, 0, 8, 7 }, { 8, 1, 8, 0 }, { 8, 1, 8, 1 }, { 8, 1, 8, 2 }, { 8, 1, 8, 3 }, { 8, 1, 8, 4 }, { 8, 1, 8, 5 }, { 8, 1, 8, 6 }, { 8, 1, 8, 7 }, { 8, 2, 8, 0 }, { 8, 2, 8, 1 }, { 8, 2, 8, 2 }, { 8, 2, 8, 3 }, { 8, 2, 8, 4 }, { 8, 2, 8, 5 }, { 8, 2, 8, 6 }, { 8, 2, 8, 7 }, { 8, 3, 8, 0 }, { 8, 3, 8, 1 }, { 8, 3, 8, 2 }, { 8, 3, 8, 3 }, { 8, 3, 8, 4 }, { 8, 3, 8, 5 }, { 8, 3, 8, 6 }, { 8, 3, 8, 7 }, { 8, 4, 8, 0 }, { 8, 4, 8, 1 }, { 8, 4, 8, 2 }, { 8, 4, 8, 3 }, { 8, 4, 8, 4 }, { 8, 4, 8, 5 }, { 8, 4, 8, 6 }, { 8, 4, 8, 7 }, { 8, 5, 8, 0 }, { 8, 5, 8, 1 }, { 8, 5, 8, 2 }, { 8, 5, 8, 3 }, { 8, 5, 8, 4 }, { 8, 5, 8, 5 }, { 8, 5, 8, 6 }, { 8, 5, 8, 7 }, { 8, 6, 8, 0 }, { 8, 6, 8, 1 }, { 8, 6, 8, 2 }, { 8, 6, 8, 3 }, { 8, 6, 8, 4 }, { 8, 6, 8, 5 }, { 8, 6, 8, 6 }, { 8, 6, 8, 7 }, { 8, 7, 8, 0 }, { 8, 7, 8, 1 }, { 8, 7, 8, 2 }, { 8, 7, 8, 3 }, { 8, 7, 8, 4 }, { 8, 7, 8, 5 }, { 8, 7, 8, 6 }, { 8, 7, 8, 7 }, { 128, 1, 128, 4 }, { 128, 1, 128, 8 }, { 128, 1, 128, 12 }, { 128, 1, 128, 16 }, { 128, 4, 128, 1 }, { 128, 8, 128, 1 }, { 128, 12, 128, 1 }, { 128, 16, 128, 1 }, }; static const size_t g_double_aligns_len = sizeof(g_double_aligns)/sizeof(int[4]); static size_t SetIncrement(size_t len) { if (len >= 4096) { return 1024; } else if (len >= 1024) { return 256; } return 1; } // Return a pointer into the current buffer with the specified alignment. static void *GetAlignedPtr(void *orig_ptr, int alignment, int or_mask) { uint64_t ptr = reinterpret_cast(orig_ptr); if (alignment > 0) { // When setting the alignment, set it to exactly the alignment chosen. // The pointer returned will be guaranteed not to be aligned to anything // more than that. ptr += alignment - (ptr & (alignment - 1)); ptr |= alignment | or_mask; } return reinterpret_cast(ptr); } static void SetFencepost(uint8_t *buffer) { for (int i = 0; i < FENCEPOST_LENGTH; i += 2) { buffer[i] = 0xde; buffer[i+1] = 0xad; } } static void VerifyFencepost(uint8_t *buffer) { for (int i = 0; i < FENCEPOST_LENGTH; i += 2) { if (buffer[i] != 0xde || buffer[i+1] != 0xad) { uint8_t expected_value; if (buffer[i] == 0xde) { i++; expected_value = 0xad; } else { expected_value = 0xde; } ASSERT_EQ(expected_value, buffer[i]); } } } void RunSingleBufferAlignTest( size_t max_test_size, void (*test_func)(uint8_t*, size_t), size_t (*set_incr)(size_t)) { if (!set_incr) { set_incr = SetIncrement; } // Allocate one large buffer with lots of extra space so that we can // guarantee that the all possible alignments will fit. uint8_t *buf = new uint8_t[3*max_test_size]; uint8_t *buf_align; for (size_t i = 0; i < g_single_aligns_len; i++) { size_t incr = 1; for (size_t len = 0; len <= max_test_size; len += incr) { incr = set_incr(len); buf_align = reinterpret_cast(GetAlignedPtr( buf+FENCEPOST_LENGTH, g_single_aligns[i][0], g_single_aligns[i][1])); SetFencepost(&buf_align[-FENCEPOST_LENGTH]); SetFencepost(&buf_align[len]); test_func(buf_align, len); VerifyFencepost(&buf_align[-FENCEPOST_LENGTH]); VerifyFencepost(&buf_align[len]); } } delete buf; } void RunSrcDstBufferAlignTest( size_t max_test_size, void (*test_func)(uint8_t*, uint8_t*, size_t), size_t (*set_incr)(size_t)) { if (!set_incr) { set_incr = SetIncrement; } // Allocate two large buffers for all of the testing. uint8_t* src = new uint8_t[3*max_test_size]; uint8_t* dst = new uint8_t[3*max_test_size]; uint8_t* src_align; uint8_t* dst_align; for (size_t i = 0; i < g_double_aligns_len; i++) { size_t incr = 1; for (size_t len = 0; len <= max_test_size; len += incr) { incr = set_incr(len); src_align = reinterpret_cast(GetAlignedPtr( src+FENCEPOST_LENGTH, g_double_aligns[i][0], g_double_aligns[i][1])); dst_align = reinterpret_cast(GetAlignedPtr( dst+FENCEPOST_LENGTH, g_double_aligns[i][2], g_double_aligns[i][3])); SetFencepost(&dst_align[-FENCEPOST_LENGTH]); SetFencepost(&dst_align[len]); test_func(src_align, dst_align, len); VerifyFencepost(&dst_align[-FENCEPOST_LENGTH]); VerifyFencepost(&dst_align[len]); } } delete src; delete dst; } void RunCmpBufferAlignTest( size_t max_test_size, void (*test_cmp_func)(uint8_t*, uint8_t*, size_t), void (*test_miscmp_func)(uint8_t*, uint8_t*, size_t, size_t), size_t (*set_incr)(size_t)) { if (!set_incr) { set_incr = SetIncrement; } // Allocate two large buffers for all of the testing. uint8_t* buf1 = new uint8_t[3*max_test_size]; uint8_t* buf2 = new uint8_t[3*max_test_size]; uint8_t* buf1_align; uint8_t* buf2_align; for (size_t i = 0; i < g_double_aligns_len; i++) { size_t incr = 1; for (size_t len = 0; len <= max_test_size; len += incr) { incr = set_incr(len); buf1_align = reinterpret_cast(GetAlignedPtr( buf1, g_double_aligns[i][0], g_double_aligns[i][1])); buf2_align = reinterpret_cast(GetAlignedPtr( buf2, g_double_aligns[i][2], g_double_aligns[i][3])); // Check by putting all zeroes after both buffers. memset(buf1_align+len, 0, 32); memset(buf2_align+len, 0, 32); test_cmp_func(buf1_align, buf2_align, len); // Check by putting different values after both buffers. for (size_t j = 0; j < 32; j++) { buf1_align[len+j] = j; buf2_align[len+j] = j+1; } test_cmp_func(buf1_align, buf2_align, len); if (len > 0) { // Change the lengths of the buffers and verify that there are // miscompares. for (size_t len2 = len+1; len2 < len+32; len2++) { test_miscmp_func(buf1_align, buf2_align, len, len2); test_miscmp_func(buf1_align, buf2_align, len2, len); } } } } delete buf1; delete buf2; } void RunSingleBufferOverreadTest(void (*test_func)(uint8_t*, size_t)) { // In order to verify that functions are not reading past the end of the // src, create data that ends exactly at an unreadable memory boundary. size_t pagesize = static_cast(sysconf(_SC_PAGE_SIZE)); uint8_t* memory; ASSERT_TRUE(posix_memalign(reinterpret_cast(&memory), pagesize, 2*pagesize) == 0); memset(memory, 0x23, 2*pagesize); // Make the second page unreadable and unwritable. ASSERT_TRUE(mprotect(&memory[pagesize], pagesize, PROT_NONE) == 0); for (size_t i = 0; i < pagesize; i++) { uint8_t* buf = &memory[pagesize-i]; test_func(buf, i); } ASSERT_TRUE(mprotect(&memory[pagesize], pagesize, PROT_READ | PROT_WRITE) == 0); free(memory); } void RunSrcDstBufferOverreadTest(void (*test_func)(uint8_t*, uint8_t*, size_t)) { // In order to verify that functions are not reading past the end of the // src, create data that ends exactly at an unreadable memory boundary. size_t pagesize = static_cast(sysconf(_SC_PAGE_SIZE)); uint8_t* memory; ASSERT_TRUE(posix_memalign(reinterpret_cast(&memory), pagesize, 2*pagesize) == 0); memset(memory, 0x23, 2*pagesize); // Make the second page unreadable and unwritable. ASSERT_TRUE(mprotect(&memory[pagesize], pagesize, PROT_NONE) == 0); uint8_t* dst = new uint8_t[pagesize]; for (size_t i = 0; i < pagesize; i++) { uint8_t* src = &memory[pagesize-i]; test_func(src, dst, i); } ASSERT_TRUE(mprotect(&memory[pagesize], pagesize, PROT_READ | PROT_WRITE) == 0); free(memory); delete dst; } void RunCmpBufferOverreadTest( void (*test_cmp_func)(uint8_t*, uint8_t*, size_t), void (*test_miscmp_func)(uint8_t*, uint8_t*, size_t, size_t)) { // In order to verify that functions are not reading past the end of either // of the bufs, create both buffers that end exactly at an unreadable memory // boundary. size_t pagesize = static_cast(sysconf(_SC_PAGE_SIZE)); uint8_t* memory1; ASSERT_TRUE(posix_memalign(reinterpret_cast(&memory1), pagesize, 2*pagesize) == 0); memset(memory1, 0x23, 2*pagesize); // Make the second page unreadable and unwritable. ASSERT_TRUE(mprotect(&memory1[pagesize], pagesize, PROT_NONE) == 0); uint8_t* memory2; ASSERT_TRUE(posix_memalign(reinterpret_cast(&memory2), pagesize, 2*pagesize) == 0); memset(memory2, 0x23, 2*pagesize); // Make the second page unreadable and unwritable. ASSERT_TRUE(mprotect(&memory2[pagesize], pagesize, PROT_NONE) == 0); for (size_t i = 0; i < pagesize; i++) { uint8_t* buf1 = &memory1[pagesize-i]; uint8_t* buf2 = &memory2[pagesize-i]; test_cmp_func(buf1, buf2, i); } // Don't cycle through pagesize, MISCMP_MAX_LENGTH bytes should be good. size_t miscmp_len; if (pagesize > MISCMP_MAX_LENGTH) { miscmp_len = MISCMP_MAX_LENGTH; } else { miscmp_len = pagesize; } for (size_t i = 1; i < miscmp_len; i++) { uint8_t* buf1 = &memory1[pagesize-i]; for (size_t j = 1; j < miscmp_len; j++) { if (j == i) continue; uint8_t* buf2 = &memory2[pagesize-j]; test_miscmp_func(buf1, buf2, i, j); } } ASSERT_TRUE(mprotect(&memory1[pagesize], pagesize, PROT_READ | PROT_WRITE) == 0); ASSERT_TRUE(mprotect(&memory2[pagesize], pagesize, PROT_READ | PROT_WRITE) == 0); free(memory1); free(memory2); }