/* * Copyright (C) 2012 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ /* * Contributed by: Intel Corporation */ #include #include "BionicDeathTest.h" #include #include #include #include #include #include #if defined(__GLIBC__) // glibc doesn't expose gettid(2). pid_t gettid() { return syscall(__NR_gettid); } #endif // __GLIBC__ // For x86, bionic and glibc have per-thread stack guard values (all identical). #if defined(__i386__) static uint32_t GetGuardFromTls() { uint32_t guard; asm ("mov %%gs:0x14, %0": "=d" (guard)); return guard; } struct stack_protector_checker { std::set tids; std::set guards; void Check() { pid_t tid = gettid(); uint32_t guard = GetGuardFromTls(); printf("[thread %d] %%gs:0x14 = 0x%08x\n", tid, guard); // Duplicate tid. gettid(2) bug? Seeing this would be very upsetting. ASSERT_TRUE(tids.find(tid) == tids.end()); // Uninitialized guard. Our bug. Note this is potentially flaky; we _could_ get // four random zero bytes, but it should be vanishingly unlikely. ASSERT_NE(guard, 0U); tids.insert(tid); guards.insert(guard); } }; static void* ThreadGuardHelper(void* arg) { stack_protector_checker* checker = reinterpret_cast(arg); checker->Check(); return NULL; } #endif // __i386__ TEST(stack_protector, same_guard_per_thread) { #if defined(__i386__) stack_protector_checker checker; size_t thread_count = 10; for (size_t i = 0; i < thread_count; ++i) { pthread_t t; ASSERT_EQ(0, pthread_create(&t, NULL, ThreadGuardHelper, &checker)); void* result; ASSERT_EQ(0, pthread_join(t, &result)); ASSERT_EQ(NULL, result); } ASSERT_EQ(thread_count, checker.tids.size()); // bionic and glibc use the same guard for every thread. ASSERT_EQ(1U, checker.guards.size()); #else // __i386__ GTEST_LOG_(INFO) << "This test does nothing.\n"; #endif // __i386__ } // For ARM and MIPS, glibc has a global stack check guard value. #if defined(__BIONIC__) || defined(__arm__) || defined(__mips__) #define TEST_STACK_CHK_GUARD // Bionic has the global for x86 too, to support binaries that can run on // Android releases that didn't implement the TLS guard value. extern "C" uintptr_t __stack_chk_guard; /* * When this function returns, the stack canary will be inconsistent * with the previous value, which will generate a call to __stack_chk_fail(), * eventually resulting in a SIGABRT. * * This must be marked with "__attribute__ ((noinline))", to ensure the * compiler generates the proper stack guards around this function. */ __attribute__ ((noinline)) static void do_modify_stack_chk_guard() { __stack_chk_guard = 0x12345678; } #endif TEST(stack_protector, global_guard) { #if defined(TEST_STACK_CHK_GUARD) ASSERT_NE(0, gettid()); ASSERT_NE(0U, __stack_chk_guard); #else // TEST_STACK_CHK_GUARD GTEST_LOG_(INFO) << "This test does nothing.\n"; #endif // TEST_STACK_CHK_GUARD } class stack_protector_DeathTest : public BionicDeathTest {}; TEST_F(stack_protector_DeathTest, modify_stack_protector) { #if defined(TEST_STACK_CHK_GUARD) ASSERT_EXIT(do_modify_stack_chk_guard(), testing::KilledBySignal(SIGABRT), ""); #else // TEST_STACK_CHK_GUARD GTEST_LOG_(INFO) << "This test does nothing.\n"; #endif // TEST_STACK_CHK_GUARD }