diff --git a/libc/Android.mk b/libc/Android.mk
index 5718d185f72d698adf0490dec05fd7d2dffc70c2..d8cc721ca4a90078d31c96c477a0a5896c4687f2 100644 (file)
--- a/libc/Android.mk
+++ b/libc/Android.mk
unistd/initgroups.c \
unistd/isatty.c \
unistd/issetugid.c \
+ unistd/killpg.c \
unistd/lseek64.c \
unistd/mmap.c \
unistd/nice.c \
unistd/sbrk.c \
unistd/send.c \
unistd/setegid.c \
+ unistd/setuid.c \
unistd/seteuid.c \
+ unistd/setreuid.c \
+ unistd/setresuid.c \
unistd/setpgrp.c \
unistd/sigblock.c \
unistd/siginterrupt.c \
unistd/siglist.c \
unistd/signal.c \
+ unistd/signame.c \
unistd/sigsetmask.c \
unistd/sigsuspend.c \
unistd/sigwait.c \
stdlib/tolower_.c \
stdlib/toupper_.c \
stdlib/wchar.c \
- string/bcopy.c \
string/index.c \
string/memccpy.c \
string/memchr.c \
string/memmem.c \
- string/memmove.c.arm \
string/memrchr.c \
string/memswap.c \
string/strcasecmp.c \
string/strcasestr.c \
string/strcat.c \
string/strchr.c \
- string/strcmp.c \
string/strcoll.c \
string/strcpy.c \
string/strcspn.c \
string/strlcat.c \
string/strlcpy.c \
string/strncat.c \
- string/strncmp.c \
string/strncpy.c \
string/strndup.c \
string/strnlen.c \
bionic/__errno.c \
bionic/__set_errno.c \
bionic/_rand48.c \
+ bionic/cpuacct.c \
bionic/arc4random.c \
bionic/basename.c \
bionic/basename_r.c \
+ bionic/clearenv.c \
bionic/dirname.c \
bionic/dirname_r.c \
bionic/drand48.c \
bionic/erand48.c \
+ bionic/err.c \
+ bionic/fdprintf.c \
bionic/fork.c \
+ bionic/fts.c \
bionic/if_nametoindex.c \
bionic/if_indextoname.c \
bionic/ioctl.c \
netbsd/resolv/res_mkquery.c \
netbsd/resolv/res_query.c \
netbsd/resolv/res_send.c \
- netbsd/resolv/res_state.c.arm \
+ netbsd/resolv/res_state.c \
netbsd/resolv/res_cache.c \
netbsd/net/nsdispatch.c \
netbsd/net/getaddrinfo.c \
netbsd/nameser/ns_ttl.c \
netbsd/nameser/ns_netint.c \
netbsd/nameser/ns_print.c \
- netbsd/nameser/ns_samedomain.c
+ netbsd/nameser/ns_samedomain.c \
+ regex/regcomp.c \
+ regex/regerror.c \
+ regex/regexec.c \
+ regex/regfree.c \
# Architecture specific source files go here
# =========================================================
ifeq ($(TARGET_ARCH),arm)
libc_common_src_files += \
bionic/eabi.c \
+ bionic/bionic_clone.c \
arch-arm/bionic/__get_pc.S \
arch-arm/bionic/__get_sp.S \
arch-arm/bionic/_exit_with_stack_teardown.S \
arch-arm/bionic/sigsetjmp.S \
arch-arm/bionic/strlen.c.arm \
arch-arm/bionic/syscall.S \
+ string/memmove.c.arm \
+ string/bcopy.c \
+ string/strcmp.c \
+ string/strncmp.c \
unistd/socketcalls.c
# These files need to be arm so that gdbserver
arch-x86/bionic/setjmp.S \
arch-x86/bionic/_setjmp.S \
arch-x86/bionic/vfork.S \
- arch-x86/string/bzero.S \
- arch-x86/string/memset.S \
- arch-x86/string/memcmp.S \
- arch-x86/string/memcpy.S \
+ arch-x86/bionic/syscall.S \
+ arch-x86/string/bcopy_wrapper.S \
+ arch-x86/string/memcpy_wrapper.S \
+ arch-x86/string/memmove_wrapper.S \
+ arch-x86/string/bzero_wrapper.S \
+ arch-x86/string/memcmp_wrapper.S \
+ arch-x86/string/memset_wrapper.S \
+ arch-x86/string/strcmp_wrapper.S \
+ arch-x86/string/strncmp_wrapper.S \
arch-x86/string/strlen.S \
bionic/pthread.c \
bionic/pthread-timers.c \
arch-x86/bionic/dl_iterate_phdr_static.c
libc_arch_dynamic_src_files :=
-endif # x86
+else # !x86
+
+ifeq ($(TARGET_ARCH),sh)
+libc_common_src_files += \
+ arch-sh/bionic/__get_pc.S \
+ arch-sh/bionic/__get_sp.S \
+ arch-sh/bionic/_exit_with_stack_teardown.S \
+ arch-sh/bionic/_setjmp.S \
+ arch-sh/bionic/atomics_sh.c \
+ arch-sh/bionic/atomic_cmpxchg.S \
+ arch-sh/bionic/clone.S \
+ arch-sh/bionic/pipe.S \
+ arch-sh/bionic/memcpy.S \
+ arch-sh/bionic/memset.S \
+ arch-sh/bionic/bzero.S \
+ arch-sh/bionic/setjmp.S \
+ arch-sh/bionic/sigsetjmp.S \
+ arch-sh/bionic/syscall.S \
+ arch-sh/bionic/memmove.S \
+ arch-sh/bionic/__set_tls.c \
+ arch-sh/bionic/__get_tls.c \
+ arch-sh/bionic/ffs.S \
+ string/bcopy.c \
+ string/strcmp.c \
+ string/strncmp.c \
+ string/memcmp.c \
+ string/strlen.c \
+ bionic/eabi.c \
+ bionic/pthread.c \
+ bionic/pthread-timers.c \
+ bionic/ptrace.c \
+ unistd/socketcalls.c
+endif # sh
+
+endif # !x86
endif # !arm
# Define some common cflags
-DNEED_PSELECT=1 \
-DINET6 \
-I$(LOCAL_PATH)/private \
- -DUSE_DL_PREFIX
+ -DUSE_DL_PREFIX \
+ -DPOSIX_MISTAKE
+
+# these macro definitions are required to implement the
+# 'timezone' and 'daylight' global variables, as well as
+# properly update the 'tm_gmtoff' field in 'struct tm'.
+#
+libc_common_cflags += \
+ -DTM_GMTOFF=tm_gmtoff \
+ -DUSG_COMPAT=1
ifeq ($(strip $(DEBUG_BIONIC_LIBC)),true)
libc_common_cflags += -DDEBUG
else # !arm
ifeq ($(TARGET_ARCH),x86)
libc_crt_target_cflags := -m32
+
+ # Enable recent IA friendly memory routines (such as for Atom)
+ # These will not work on the earlier x86 machines
+ libc_common_cflags += -mtune=i686 -DUSE_SSSE3 -DUSE_SSE2
endif # x86
endif # !arm
LOCAL_SRC_FILES := \
$(libc_arch_static_src_files) \
bionic/dlmalloc.c \
+ bionic/malloc_debug_common.c \
bionic/libc_init_static.c
-LOCAL_CFLAGS := $(libc_common_cflags)
-
-ifeq ($(WITH_MALLOC_CHECK_LIBC_A),true)
- LOCAL_CFLAGS += -DMALLOC_LEAK_CHECK
- LOCAL_SRC_FILES += bionic/malloc_leak.c.arm
-endif
-
+LOCAL_CFLAGS := $(libc_common_cflags) \
+ -DLIBC_STATIC
LOCAL_C_INCLUDES := $(libc_common_c_includes)
-
LOCAL_MODULE := libc
LOCAL_WHOLE_STATIC_LIBRARIES := libc_common
LOCAL_SYSTEM_SHARED_LIBRARIES :=
LOCAL_SRC_FILES := \
$(libc_arch_dynamic_src_files) \
bionic/dlmalloc.c \
- bionic/malloc_leak.c.arm \
+ bionic/malloc_debug_common.c \
bionic/libc_init_dynamic.c
LOCAL_MODULE:= libc
include $(BUILD_SHARED_LIBRARY)
+# For all builds, except for the -user build we will enable memory
+# allocation checking (including memory leaks, buffer overwrites, etc.)
+# Note that all these checks are also controlled by env. settings
+# that can enable, or disable specific checks. Note also that some of
+# the checks are available only in emulator and are implemeted in
+# libc_malloc_qemu_instrumented.so.
+ifneq ($(TARGET_BUILD_VARIANT),user)
+
# ========================================================
-# libc_debug.so
+# libc_malloc_debug_leak.so
# ========================================================
include $(CLEAR_VARS)
LOCAL_C_INCLUDES := $(libc_common_c_includes)
LOCAL_SRC_FILES := \
- $(libc_arch_dynamic_src_files) \
- bionic/dlmalloc.c \
- bionic/malloc_leak.c.arm \
- bionic/libc_init_dynamic.c
+ bionic/malloc_debug_leak.c
-LOCAL_MODULE:= libc_debug
+LOCAL_MODULE:= libc_malloc_debug_leak
-# WARNING: The only library libc.so should depend on is libdl.so! If you add other libraries,
-# make sure to add -Wl,--exclude-libs=libgcc.a to the LOCAL_LDFLAGS for those libraries. This
-# ensures that symbols that are pulled into those new libraries from libgcc.a are not declared
-# external; if that were the case, then libc would not pull those symbols from libgcc.a as it
-# should, instead relying on the external symbols from the dependent libraries. That would
-# create an "cloaked" dependency on libgcc.a in libc though the libraries, which is not what
-# you wanted!
+LOCAL_SHARED_LIBRARIES := libc
+LOCAL_WHOLE_STATIC_LIBRARIES := libc_common
+LOCAL_SYSTEM_SHARED_LIBRARIES :=
+# Don't prelink
+LOCAL_PRELINK_MODULE := false
+# Don't install on release build
+LOCAL_MODULE_TAGS := eng debug
-LOCAL_SHARED_LIBRARIES := libdl
+include $(BUILD_SHARED_LIBRARY)
+
+
+# ========================================================
+# libc_malloc_debug_qemu.so
+# ========================================================
+include $(CLEAR_VARS)
+
+LOCAL_CFLAGS := \
+ $(libc_common_cflags) \
+ -DMALLOC_QEMU_INSTRUMENT
+
+LOCAL_C_INCLUDES := $(libc_common_c_includes)
+
+LOCAL_SRC_FILES := \
+ bionic/malloc_debug_qemu.c
+
+LOCAL_MODULE:= libc_malloc_debug_qemu
+
+LOCAL_SHARED_LIBRARIES := libc
LOCAL_WHOLE_STATIC_LIBRARIES := libc_common
LOCAL_SYSTEM_SHARED_LIBRARIES :=
# Don't prelink
LOCAL_PRELINK_MODULE := false
# Don't install on release build
-LOCAL_MODULE_TAGS := eng
+LOCAL_MODULE_TAGS := eng debug
include $(BUILD_SHARED_LIBRARY)
+endif #!user
+
+
# ========================================================
include $(call all-makefiles-under,$(LOCAL_PATH))