index 26927623393b031e0c40632a0d6a10cb64bf0ec7..e04cf8e7f8246682ee406e61117a77a1447d1998 100644 (file)
#include "pthread_internal.h"
-extern "C" void _exit_with_stack_teardown(void*, size_t);
-extern "C" void __exit(int);
+extern "C" __noreturn void _exit_with_stack_teardown(void*, size_t);
+extern "C" __noreturn void __exit(int);
extern "C" int __set_tid_address(int*);
/* CAVEAT: our implementation of pthread_cleanup_push/pop doesn't support C++ exceptions
// Keep track of what we need to know about the stack before we lose the pthread_internal_t.
void* stack_base = thread->attr.stack_base;
size_t stack_size = thread->attr.stack_size;
- bool user_allocated_stack = ((thread->attr.flags & PTHREAD_ATTR_FLAG_USER_ALLOCATED_STACK) != 0);
+ bool free_stack = false;
- pthread_mutex_lock(&gThreadListLock);
+ pthread_mutex_lock(&g_thread_list_lock);
if ((thread->attr.flags & PTHREAD_ATTR_FLAG_DETACHED) != 0) {
// The thread is detached, so we can free the pthread_internal_t.
// First make sure that the kernel does not try to clear the tid field
// because we'll have freed the memory before the thread actually exits.
__set_tid_address(NULL);
- _pthread_internal_remove_locked(thread);
- } else {
- // Make sure that the pthread_internal_t doesn't have stale pointers to a stack that
- // will be unmapped after the exit call below.
- if (!user_allocated_stack) {
- thread->attr.stack_base = NULL;
- thread->attr.stack_size = 0;
- thread->tls = NULL;
+
+ // pthread_internal_t is freed below with stack, not here.
+ _pthread_internal_remove_locked(thread, false);
+ if (!thread->user_allocated_stack()) {
+ free_stack = true;
}
- // pthread_join is responsible for destroying the pthread_internal_t for non-detached threads.
- // The kernel will futex_wake on the pthread_internal_t::tid field to wake pthread_join.
}
- pthread_mutex_unlock(&gThreadListLock);
+ pthread_mutex_unlock(&g_thread_list_lock);
- if (user_allocated_stack) {
- // Cleaning up this thread's stack is the creator's responsibility, not ours.
- __exit(0);
- } else {
+ // Detached threads exit with stack teardown, and everything deallocated here.
+ // Threads that can be joined exit but leave their stacks for the pthread_join caller to clean up.
+ if (free_stack) {
// We need to munmap the stack we're running on before calling exit.
// That's not something we can do in C.
sigprocmask(SIG_SETMASK, &mask, NULL);
_exit_with_stack_teardown(stack_base, stack_size);
+ } else {
+ __exit(0);
}
-
- // NOTREACHED, but we told the compiler this function is noreturn, and it doesn't believe us.
- abort();
}