index 41f46368c4e15a2e35691efe74ec0349d0f236ca..95097b7ea0b54f7ef89bdd3b697513fec9615bdf 100644 (file)
#include <pthread.h>
+#include "private/bionic_tls.h"
+
+/* Has the thread been detached by a pthread_join or pthread_detach call? */
+#define PTHREAD_ATTR_FLAG_DETACHED 0x00000001
+
+/* Was the thread's stack allocated by the user rather than by us? */
+#define PTHREAD_ATTR_FLAG_USER_ALLOCATED_STACK 0x00000002
+
+/* Has the thread been joined by another thread? */
+#define PTHREAD_ATTR_FLAG_JOINED 0x00000004
+
+/* Is this the main thread? */
+#define PTHREAD_ATTR_FLAG_MAIN_THREAD 0x80000000
+
struct pthread_internal_t {
struct pthread_internal_t* next;
struct pthread_internal_t* prev;
pid_t tid;
- void** tls;
+ private:
+ pid_t cached_pid_;
+
+ public:
+ pid_t invalidate_cached_pid() {
+ pid_t old_value;
+ get_cached_pid(&old_value);
+ set_cached_pid(0);
+ return old_value;
+ }
+
+ void set_cached_pid(pid_t value) {
+ cached_pid_ = value;
+ }
+
+ bool get_cached_pid(pid_t* cached_pid) {
+ *cached_pid = cached_pid_;
+ return (*cached_pid != 0);
+ }
+
+ bool user_allocated_stack() {
+ return (attr.flags & PTHREAD_ATTR_FLAG_USER_ALLOCATED_STACK) != 0;
+ }
pthread_attr_t attr;
void* alternate_signal_stack;
+ pthread_mutex_t startup_handshake_mutex;
+
+ void* tls[BIONIC_TLS_SLOTS];
+
/*
* The dynamic linker implements dlerror(3), which makes it hard for us to implement this
* per-thread buffer by simply using malloc(3) and free(3).
*/
#define __BIONIC_DLERROR_BUFFER_SIZE 512
char dlerror_buffer[__BIONIC_DLERROR_BUFFER_SIZE];
-};
+} __attribute__((aligned(16))); // Align it as thread stack top below it should be aligned.
__LIBC_HIDDEN__ int __init_thread(pthread_internal_t* thread, bool add_to_thread_list);
__LIBC_HIDDEN__ void __init_tls(pthread_internal_t* thread);
__LIBC_HIDDEN__ void __init_alternate_signal_stack(pthread_internal_t*);
__LIBC_HIDDEN__ void _pthread_internal_add(pthread_internal_t* thread);
-__LIBC_HIDDEN__ pthread_internal_t* __get_thread(void);
-
-__LIBC_HIDDEN__ void pthread_key_clean_all(void);
-__LIBC_HIDDEN__ void _pthread_internal_remove_locked(pthread_internal_t* thread);
-
-/* Has the thread been detached by a pthread_join or pthread_detach call? */
-#define PTHREAD_ATTR_FLAG_DETACHED 0x00000001
-
-/* Was the thread's stack allocated by the user rather than by us? */
-#define PTHREAD_ATTR_FLAG_USER_ALLOCATED_STACK 0x00000002
-/* Has the thread been joined by another thread? */
-#define PTHREAD_ATTR_FLAG_JOINED 0x00000004
+/* Various third-party apps contain a backport of our pthread_rwlock implementation that uses this. */
+extern "C" __LIBC64_HIDDEN__ pthread_internal_t* __get_thread(void);
-/* Is this the main thread? */
-#define PTHREAD_ATTR_FLAG_MAIN_THREAD 0x80000000
+__LIBC_HIDDEN__ void pthread_key_clean_all(void);
+__LIBC_HIDDEN__ void _pthread_internal_remove_locked(pthread_internal_t* thread, bool free_thread);
/*
- * Traditionally we give threads a 1MiB stack. When we started
+ * Traditionally we gave threads a 1MiB stack. When we started
* allocating per-thread alternate signal stacks to ease debugging of
* stack overflows, we subtracted the same amount we were using there
* from the default thread stack size. This should keep memory usage
@@ -86,10 +116,8 @@ __LIBC_HIDDEN__ void _pthread_internal_remove_locked(pthread_internal_t* thread)
*/
#define PTHREAD_STACK_SIZE_DEFAULT ((1 * 1024 * 1024) - SIGSTKSZ)
-__LIBC_HIDDEN__ extern pthread_internal_t* gThreadList;
-__LIBC_HIDDEN__ extern pthread_mutex_t gThreadListLock;
-
-__LIBC_HIDDEN__ int __timespec_from_absolute(timespec*, const timespec*, clockid_t);
+__LIBC_HIDDEN__ extern pthread_internal_t* g_thread_list;
+__LIBC_HIDDEN__ extern pthread_mutex_t g_thread_list_lock;
/* Needed by fork. */
__LIBC_HIDDEN__ extern void __bionic_atfork_run_prepare();