index 79d8bcad86425b18dc8d662b33b8d3d33e771b3e..21d59fa57a87789eab19625a28eac5ab90390b8c 100644 (file)
--- a/libc/include/sys/cdefs.h
+++ b/libc/include/sys/cdefs.h
#ifndef __has_builtin
#define __has_builtin(x) 0
#endif
+#ifndef __has_attribute
+#define __has_attribute(x) 0
+#endif
/*
* or later, for e.g. features that appeared in a particular version
* of GNU C. Usage:
*
- * #if __GNUC_PREREQ__(major, minor)
+ * #if __GNUC_PREREQ(major, minor)
* ...cool feature...
* #else
* ...delete feature...
* #endif
*/
#ifdef __GNUC__
-#define __GNUC_PREREQ__(x, y) \
+#define __GNUC_PREREQ(x, y) \
((__GNUC__ == (x) && __GNUC_MINOR__ >= (y)) || \
(__GNUC__ > (x)))
#else
-#define __GNUC_PREREQ__(x, y) 0
+#define __GNUC_PREREQ(x, y) 0
#endif
-#include <sys/cdefs_elf.h>
+#define __strong_alias(alias, sym) \
+ __asm__(".global " #alias "\n" \
+ #alias " = " #sym);
#if defined(__cplusplus)
#define __BEGIN_DECLS extern "C" {
* GCC2 provides __extension__ to suppress warnings for various GNU C
* language extensions under "-ansi -pedantic".
*/
-#if !__GNUC_PREREQ__(2, 0)
+#if !__GNUC_PREREQ(2, 0)
#define __extension__ /* delete __extension__ if non-gcc or gcc1 */
#endif
* these work for GNU C++ (modulo a slight glitch in the C++ grammar
* in the distribution version of 2.5.5).
*/
-#if !__GNUC_PREREQ__(2, 5)
+#if !__GNUC_PREREQ(2, 5)
#define __attribute__(x) /* delete __attribute__ if non-gcc or gcc1 */
#if defined(__GNUC__) && !defined(__STRICT_ANSI__)
#define __dead __volatile
#define __pure
#endif
-#if __GNUC_PREREQ__(2, 7)
+#if __GNUC_PREREQ(2, 7)
#define __unused __attribute__((__unused__))
#else
#define __unused /* delete */
#define __pure2 __attribute__((__const__)) /* Android-added: used by FreeBSD libm */
-#if __GNUC_PREREQ__(3, 1)
+#if __GNUC_PREREQ(3, 1)
#define __used __attribute__((__used__))
#else
#define __used /* delete */
#endif
-#if __GNUC_PREREQ__(2, 7)
+#if __GNUC_PREREQ(2, 7)
#define __packed __attribute__((__packed__))
#define __aligned(x) __attribute__((__aligned__(x)))
#define __section(x) __attribute__((__section__(x)))
#define __section(x) error: no __section for this compiler
#endif
-#if !__GNUC_PREREQ__(2, 8)
+#if !__GNUC_PREREQ(2, 8)
#define __extension__
#endif
-#if __GNUC_PREREQ__(2, 8)
+#if __GNUC_PREREQ(2, 8)
#define __statement(x) __extension__(x)
#elif defined(lint)
#define __statement(x) (0)
#if defined(__STDC__VERSION__) && __STDC_VERSION__ >= 199901L
#define __restrict restrict
#else
-#if !__GNUC_PREREQ__(2, 92)
+#if !__GNUC_PREREQ(2, 92)
#define __restrict /* delete __restrict when not supported */
#endif
#endif
* in GCC 2.95.
*/
#if !defined(__STDC_VERSION__) || !(__STDC_VERSION__ >= 199901L)
-#if __GNUC_PREREQ__(2, 6)
+#if __GNUC_PREREQ(2, 6)
#define __func__ __PRETTY_FUNCTION__
-#elif __GNUC_PREREQ__(2, 4)
+#elif __GNUC_PREREQ(2, 4)
#define __func__ __FUNCTION__
#else
#define __func__ ""
#endif
#endif /* !(__STDC_VERSION__ >= 199901L) */
-#if defined(_KERNEL)
-#if defined(NO_KERNEL_RCSIDS)
-#undef __KERNEL_RCSID
-#define __KERNEL_RCSID(_n, _s) /* nothing */
-#endif /* NO_KERNEL_RCSIDS */
-#endif /* _KERNEL */
-
/*
* A barrier to stop the optimizer from moving code or assume live
* register values. This is gcc specific, the version is more or less
* arbitrary, might work with older compilers.
*/
-#if __GNUC_PREREQ__(2, 95)
+#if __GNUC_PREREQ(2, 95)
#define __insn_barrier() __asm __volatile("":::"memory")
#else
#define __insn_barrier() /* */
* basic block reordering that this affects can often generate
* larger code.
*/
-#if __GNUC_PREREQ__(2, 96)
+#if __GNUC_PREREQ(2, 96)
#define __predict_true(exp) __builtin_expect((exp) != 0, 1)
#define __predict_false(exp) __builtin_expect((exp) != 0, 0)
#else
#define __predict_false(exp) (exp)
#endif
-#if __GNUC_PREREQ__(2, 96)
+#if __GNUC_PREREQ(2, 96)
#define __noreturn __attribute__((__noreturn__))
#define __mallocfunc __attribute__((malloc))
#define __purefunc __attribute__((pure))
#define __purefunc
#endif
-#if __GNUC_PREREQ__(3, 1)
+#if __GNUC_PREREQ(3, 1)
#define __always_inline __attribute__((__always_inline__))
#else
#define __always_inline
#endif
-#if __GNUC_PREREQ__(3, 4)
+#if __GNUC_PREREQ(3, 4)
#define __wur __attribute__((__warn_unused_result__))
#else
#define __wur
#endif
-#if __GNUC_PREREQ__(4, 3)
+#if __GNUC_PREREQ(4, 3)
#define __errordecl(name, msg) extern void name(void) __attribute__((__error__(msg)))
#define __warnattr(msg) __attribute__((__warning__(msg)))
#else
* do it in <sys/cdefs.h> instead because that's where our existing
* _POSIX_C_SOURCE tests were, and we're already confident that <sys/cdefs.h>
* is included everywhere it should be.
+ *
+ * The _GNU_SOURCE test needs to come before any _BSD_SOURCE or _POSIX* tests
+ * because _GNU_SOURCE implies everything else.
*/
-#if defined(_BSD_SOURCE)
-# define __USE_BSD 1
-#endif
-
#if defined(_GNU_SOURCE)
# define __USE_GNU 1
+# undef _POSIX_SOURCE
+# define _POSIX_SOURCE 1
+# undef _POSIX_C_SOURCE
+# define _POSIX_C_SOURCE 200809L
+# undef _BSD_SOURCE
+# define _BSD_SOURCE 1
+#endif
+
+#if defined(_BSD_SOURCE)
+# define __USE_BSD 1
#endif
/*-
#endif
#define __bos0(s) __builtin_object_size((s), 0)
+#if __GNUC_PREREQ(4,3) || __has_attribute(__artificial__)
+#define __BIONIC_FORTIFY_INLINE extern __inline__ __always_inline __attribute__((gnu_inline)) __attribute__((__artificial__))
+#else
#define __BIONIC_FORTIFY_INLINE extern __inline__ __always_inline __attribute__((gnu_inline))
#endif
+#endif
#define __BIONIC_FORTIFY_UNKNOWN_SIZE ((size_t) -1)
/* Used to tag non-static symbols that are private and never exposed by the shared library. */