diff --git a/linker/dlfcn.cpp b/linker/dlfcn.cpp
index 5d6db8e29f601f610f6e6b32dcd654f877d071f7..7ef94c059e438f59d4c69f9be26a8e2a084ffcca 100644 (file)
--- a/linker/dlfcn.cpp
+++ b/linker/dlfcn.cpp
/* This file hijacks the symbols stubbed out in libdl.so. */
-static pthread_mutex_t g_dl_mutex = PTHREAD_RECURSIVE_MUTEX_INITIALIZER;
+static pthread_mutex_t g_dl_mutex = PTHREAD_RECURSIVE_MUTEX_INITIALIZER_NP;
static const char* __bionic_set_dlerror(char* new_value) {
char** dlerror_slot = &reinterpret_cast<char**>(__get_tls())[TLS_SLOT_DLERROR];
static void __bionic_format_dlerror(const char* msg, const char* detail) {
char* buffer = __get_thread()->dlerror_buffer;
strlcpy(buffer, msg, __BIONIC_DLERROR_BUFFER_SIZE);
- if (detail != NULL) {
+ if (detail != nullptr) {
strlcat(buffer, ": ", __BIONIC_DLERROR_BUFFER_SIZE);
strlcat(buffer, detail, __BIONIC_DLERROR_BUFFER_SIZE);
}
}
const char* dlerror() {
- const char* old_value = __bionic_set_dlerror(NULL);
+ const char* old_value = __bionic_set_dlerror(nullptr);
return old_value;
}
static void* dlopen_ext(const char* filename, int flags, const android_dlextinfo* extinfo) {
ScopedPthreadMutexLocker locker(&g_dl_mutex);
soinfo* result = do_dlopen(filename, flags, extinfo);
- if (result == NULL) {
+ if (result == nullptr) {
__bionic_format_dlerror("dlopen failed", linker_get_error_buffer());
- return NULL;
+ return nullptr;
}
return result;
}
@@ -80,33 +80,33 @@ void* android_dlopen_ext(const char* filename, int flags, const android_dlextinf
}
void* dlopen(const char* filename, int flags) {
- return dlopen_ext(filename, flags, NULL);
+ return dlopen_ext(filename, flags, nullptr);
}
void* dlsym(void* handle, const char* symbol) {
ScopedPthreadMutexLocker locker(&g_dl_mutex);
#if !defined(__LP64__)
- if (handle == NULL) {
- __bionic_format_dlerror("dlsym library handle is null", NULL);
- return NULL;
+ if (handle == nullptr) {
+ __bionic_format_dlerror("dlsym library handle is null", nullptr);
+ return nullptr;
}
#endif
- if (symbol == NULL) {
- __bionic_format_dlerror("dlsym symbol name is null", NULL);
- return NULL;
+ if (symbol == nullptr) {
+ __bionic_format_dlerror("dlsym symbol name is null", nullptr);
+ return nullptr;
}
- soinfo* found = NULL;
- ElfW(Sym)* sym = NULL;
+ soinfo* found = nullptr;
+ ElfW(Sym)* sym = nullptr;
if (handle == RTLD_DEFAULT) {
- sym = dlsym_linear_lookup(symbol, &found, NULL);
+ sym = dlsym_linear_lookup(symbol, &found, nullptr);
} else if (handle == RTLD_NEXT) {
void* caller_addr = __builtin_return_address(0);
soinfo* si = find_containing_library(caller_addr);
- sym = NULL;
+ sym = nullptr;
if (si && si->next) {
sym = dlsym_linear_lookup(symbol, &found, si->next);
}
sym = dlsym_handle_lookup(reinterpret_cast<soinfo*>(handle), &found, symbol);
}
- if (sym != NULL) {
+ if (sym != nullptr) {
unsigned bind = ELF_ST_BIND(sym->st_info);
if ((bind == STB_GLOBAL || bind == STB_WEAK) && sym->st_shndx != 0) {
- return reinterpret_cast<void*>(sym->st_value + found->load_bias);
+ return reinterpret_cast<void*>(found->resolve_symbol_address(sym));
}
__bionic_format_dlerror("symbol found but not global", symbol);
- return NULL;
+ return nullptr;
} else {
__bionic_format_dlerror("undefined symbol", symbol);
- return NULL;
+ return nullptr;
}
}
// Determine if this address can be found in any library currently mapped.
soinfo* si = find_containing_library(addr);
- if (si == NULL) {
+ if (si == nullptr) {
return 0;
}
info->dli_fbase = reinterpret_cast<void*>(si->base);
// Determine if any symbol in the library contains the specified address.
- ElfW(Sym)* sym = dladdr_find_symbol(si, addr);
- if (sym != NULL) {
- info->dli_sname = si->strtab + sym->st_name;
- info->dli_saddr = reinterpret_cast<void*>(si->load_bias + sym->st_value);
+ ElfW(Sym)* sym = si->find_symbol_by_address(addr);
+ if (sym != nullptr) {
+ info->dli_sname = si->get_string(sym->st_name);
+ info->dli_saddr = reinterpret_cast<void*>(si->resolve_symbol_address(sym));
}
return 1;
// name_offset: starting index of the name in libdl_info.strtab
#define ELF32_SYM_INITIALIZER(name_offset, value, shndx) \
{ name_offset, \
- reinterpret_cast<Elf32_Addr>(reinterpret_cast<void*>(value)), \
+ reinterpret_cast<Elf32_Addr>(value), \
/* st_size */ 0, \
(shndx == 0) ? 0 : (STB_GLOBAL << 4), \
/* st_other */ 0, \
(shndx == 0) ? 0 : (STB_GLOBAL << 4), \
/* st_other */ 0, \
shndx, \
- reinterpret_cast<Elf64_Addr>(reinterpret_cast<void*>(value)), \
+ reinterpret_cast<Elf64_Addr>(value), \
/* st_size */ 0, \
}
// This is actually the STH_UNDEF entry. Technically, it's
// supposed to have st_name == 0, but instead, it points to an index
// in the strtab with a \0 to make iterating through the symtab easier.
- ELFW(SYM_INITIALIZER)(sizeof(ANDROID_LIBDL_STRTAB) - 1, NULL, 0),
+ ELFW(SYM_INITIALIZER)(sizeof(ANDROID_LIBDL_STRTAB) - 1, nullptr, 0),
ELFW(SYM_INITIALIZER)( 0, &dlopen, 1),
ELFW(SYM_INITIALIZER)( 7, &dlclose, 1),
ELFW(SYM_INITIALIZER)( 15, &dlsym, 1),
static unsigned g_libdl_chains[] = { 0, 2, 3, 4, 5, 6, 7, 8, 9, 0 };
#endif
-// Defined as global because we do not yet have access
-// to synchronization functions __cxa_guard_* needed
-// to define statics inside functions.
-static soinfo __libdl_info;
+static soinfo __libdl_info("libdl.so", nullptr, 0, RTLD_GLOBAL);
// This is used by the dynamic linker. Every process gets these symbols for free.
soinfo* get_libdl_info() {
- if (__libdl_info.name[0] == '\0') {
- // initialize
- strncpy(__libdl_info.name, "libdl.so", sizeof(__libdl_info.name));
- __libdl_info.flags = FLAG_LINKED | FLAG_NEW_SOINFO;
- __libdl_info.strtab = ANDROID_LIBDL_STRTAB;
- __libdl_info.symtab = g_libdl_symtab;
- __libdl_info.nbucket = sizeof(g_libdl_buckets)/sizeof(unsigned);
- __libdl_info.nchain = sizeof(g_libdl_chains)/sizeof(unsigned);
- __libdl_info.bucket = g_libdl_buckets;
- __libdl_info.chain = g_libdl_chains;
- __libdl_info.has_DT_SYMBOLIC = true;
+ if ((__libdl_info.flags_ & FLAG_LINKED) == 0) {
+ __libdl_info.flags_ |= FLAG_LINKED;
+ __libdl_info.strtab_ = ANDROID_LIBDL_STRTAB;
+ __libdl_info.symtab_ = g_libdl_symtab;
+ __libdl_info.nbucket_ = sizeof(g_libdl_buckets)/sizeof(unsigned);
+ __libdl_info.nchain_ = sizeof(g_libdl_chains)/sizeof(unsigned);
+ __libdl_info.bucket_ = g_libdl_buckets;
+ __libdl_info.chain_ = g_libdl_chains;
+ __libdl_info.ref_count_ = 1;
+ __libdl_info.strtab_size_ = sizeof(ANDROID_LIBDL_STRTAB);
+ __libdl_info.local_group_root_ = &__libdl_info;
}
return &__libdl_info;