diff --git a/linker/linker.cpp b/linker/linker.cpp
index 09ffa23993a81a545a73d727e68b611fadd00578..34099316fe163eda504e9cd52cb7581012bcdb6c 100644 (file)
--- a/linker/linker.cpp
+++ b/linker/linker.cpp
#include <stdlib.h>
#include <string.h>
#include <sys/mman.h>
+#include <sys/param.h>
#include <unistd.h>
#include <new>
// Copy the necessary fields into the debug structure.
link_map* map = &(info->link_map_head);
map->l_addr = info->load_bias;
- map->l_name = reinterpret_cast<char*>(info->name);
+ map->l_name = info->name;
map->l_ld = info->dynamic;
// Stick the new library at the end of the list.
}
static void notify_gdb_of_load(soinfo* info) {
- if (info->flags & FLAG_EXE) {
+ if (info->is_main_executable()) {
// GDB already knows about the main executable
return;
}
}
static void notify_gdb_of_unload(soinfo* info) {
- if (info->flags & FLAG_EXE) {
+ if (info->is_main_executable()) {
// GDB already knows about the main executable
return;
}
g_soinfo_links_allocator.protect_all(protection);
}
-static soinfo* soinfo_alloc(const char* name, struct stat* file_stat, int rtld_flags) {
+static soinfo* soinfo_alloc(const char* name, struct stat* file_stat, off64_t file_offset, uint32_t rtld_flags) {
if (strlen(name) >= SOINFO_NAME_LEN) {
DL_ERR("library name \"%s\" too long", name);
return nullptr;
}
- soinfo* si = new (g_soinfo_allocator.alloc()) soinfo(name, file_stat, rtld_flags);
+ soinfo* si = new (g_soinfo_allocator.alloc()) soinfo(name, file_stat, file_offset, rtld_flags);
sonext->next = si;
sonext = si;
}
prev = trav;
}
+
if (trav == nullptr) {
// si was not in solist
- DL_ERR("name \"%s\" is not in solist!", si->name);
+ DL_ERR("name \"%s\"@%p is not in solist!", si->name, si);
return;
}
g_soinfo_allocator.free(si);
}
-
static void parse_path(const char* path, const char* delimiters,
const char** array, char* buf, size_t buf_size, size_t max_count) {
if (path == nullptr) {
@@ -415,123 +416,180 @@ int dl_iterate_phdr(int (*cb)(dl_phdr_info* info, size_t size, void* data), void
return rv;
}
-static ElfW(Sym)* soinfo_elf_lookup(soinfo* si, unsigned hash, const char* name) {
- ElfW(Sym)* symtab = si->symtab;
- const char* strtab = si->strtab;
+ElfW(Sym)* soinfo::find_symbol_by_name(SymbolName& symbol_name) {
+ return is_gnu_hash() ? gnu_lookup(symbol_name) : elf_lookup(symbol_name);
+}
- TRACE_TYPE(LOOKUP, "SEARCH %s in %s@%p %x %zd",
- name, si->name, reinterpret_cast<void*>(si->base), hash, hash % si->nbucket);
+static bool is_symbol_global_and_defined(const soinfo* si, const ElfW(Sym)* s) {
+ if (ELF_ST_BIND(s->st_info) == STB_GLOBAL ||
+ ELF_ST_BIND(s->st_info) == STB_WEAK) {
+ return s->st_shndx != SHN_UNDEF;
+ } else if (ELF_ST_BIND(s->st_info) != STB_LOCAL) {
+ DL_WARN("unexpected ST_BIND value: %d for '%s' in '%s'",
+ ELF_ST_BIND(s->st_info), si->get_string(s->st_name), si->name);
+ }
- for (unsigned n = si->bucket[hash % si->nbucket]; n != 0; n = si->chain[n]) {
- ElfW(Sym)* s = symtab + n;
- if (strcmp(strtab + s->st_name, name)) continue;
+ return false;
+}
- // only concern ourselves with global and weak symbol definitions
- switch (ELF_ST_BIND(s->st_info)) {
- case STB_GLOBAL:
- case STB_WEAK:
- if (s->st_shndx == SHN_UNDEF) {
- continue;
- }
+ElfW(Sym)* soinfo::gnu_lookup(SymbolName& symbol_name) {
+ uint32_t hash = symbol_name.gnu_hash();
+ uint32_t h2 = hash >> gnu_shift2_;
- TRACE_TYPE(LOOKUP, "FOUND %s in %s (%p) %zd",
- name, si->name, reinterpret_cast<void*>(s->st_value),
- static_cast<size_t>(s->st_size));
- return s;
- case STB_LOCAL:
- continue;
- default:
- __libc_fatal("ERROR: Unexpected ST_BIND value: %d for '%s' in '%s'",
- ELF_ST_BIND(s->st_info), name, si->name);
+ uint32_t bloom_mask_bits = sizeof(ElfW(Addr))*8;
+ uint32_t word_num = (hash / bloom_mask_bits) & gnu_maskwords_;
+ ElfW(Addr) bloom_word = gnu_bloom_filter_[word_num];
+
+ // test against bloom filter
+ if ((1 & (bloom_word >> (hash % bloom_mask_bits)) & (bloom_word >> (h2 % bloom_mask_bits))) == 0) {
+ return nullptr;
+ }
+
+ // bloom test says "probably yes"...
+ uint32_t n = bucket_[hash % nbucket_];
+
+ if (n == 0) {
+ return nullptr;
+ }
+
+ do {
+ ElfW(Sym)* s = symtab_ + n;
+ if (((chain_[n] ^ hash) >> 1) == 0 &&
+ strcmp(get_string(s->st_name), symbol_name.get_name()) == 0 &&
+ is_symbol_global_and_defined(this, s)) {
+ return s;
+ }
+ } while ((chain_[n++] & 1) == 0);
+
+ return nullptr;
+}
+
+ElfW(Sym)* soinfo::elf_lookup(SymbolName& symbol_name) {
+ uint32_t hash = symbol_name.elf_hash();
+
+ TRACE_TYPE(LOOKUP, "SEARCH %s in %s@%p h=%x(elf) %zd",
+ symbol_name.get_name(), name, reinterpret_cast<void*>(base), hash, hash % nbucket_);
+
+ for (uint32_t n = bucket_[hash % nbucket_]; n != 0; n = chain_[n]) {
+ ElfW(Sym)* s = symtab_ + n;
+ if (strcmp(get_string(s->st_name), symbol_name.get_name()) == 0 && is_symbol_global_and_defined(this, s)) {
+ TRACE_TYPE(LOOKUP, "FOUND %s in %s (%p) %zd",
+ symbol_name.get_name(), name, reinterpret_cast<void*>(s->st_value),
+ static_cast<size_t>(s->st_size));
+ return s;
}
}
TRACE_TYPE(LOOKUP, "NOT FOUND %s in %s@%p %x %zd",
- name, si->name, reinterpret_cast<void*>(si->base), hash, hash % si->nbucket);
-
+ symbol_name.get_name(), name, reinterpret_cast<void*>(base), hash, hash % nbucket_);
return nullptr;
}
-soinfo::soinfo(const char* name, const struct stat* file_stat, int rtld_flags) {
+soinfo::soinfo(const char* name, const struct stat* file_stat, off64_t file_offset, int rtld_flags) {
memset(this, 0, sizeof(*this));
strlcpy(this->name, name, sizeof(this->name));
- flags = FLAG_NEW_SOINFO;
- version = SOINFO_VERSION;
+ flags_ = FLAG_NEW_SOINFO;
+ version_ = SOINFO_VERSION;
if (file_stat != nullptr) {
- set_st_dev(file_stat->st_dev);
- set_st_ino(file_stat->st_ino);
+ this->st_dev_ = file_stat->st_dev;
+ this->st_ino_ = file_stat->st_ino;
+ this->file_offset_ = file_offset;
}
- this->rtld_flags = rtld_flags;
+ this->rtld_flags_ = rtld_flags;
}
-static unsigned elfhash(const char* _name) {
- const unsigned char* name = reinterpret_cast<const unsigned char*>(_name);
- unsigned h = 0, g;
- while (*name) {
- h = (h << 4) + *name++;
- g = h & 0xf0000000;
- h ^= g;
- h ^= g >> 24;
+uint32_t SymbolName::elf_hash() {
+ if (!has_elf_hash_) {
+ const unsigned char* name = reinterpret_cast<const unsigned char*>(name_);
+ uint32_t h = 0, g;
+
+ while (*name) {
+ h = (h << 4) + *name++;
+ g = h & 0xf0000000;
+ h ^= g;
+ h ^= g >> 24;
+ }
+
+ elf_hash_ = h;
+ has_elf_hash_ = true;
}
- return h;
+
+ return elf_hash_;
}
-static ElfW(Sym)* soinfo_do_lookup(soinfo* si, const char* name, soinfo** lsi) {
- unsigned elf_hash = elfhash(name);
- ElfW(Sym)* s = nullptr;
+uint32_t SymbolName::gnu_hash() {
+ if (!has_gnu_hash_) {
+ uint32_t h = 5381;
+ const unsigned char* name = reinterpret_cast<const unsigned char*>(name_);
+ while (*name != 0) {
+ h += (h << 5) + *name++; // h*33 + c = h + h * 32 + c = h + h << 5 + c
+ }
- if (somain != nullptr) {
- DEBUG("%s: looking up %s in executable %s",
- si->name, name, somain->name);
+ gnu_hash_ = h;
+ has_gnu_hash_ = true;
+ }
- // 1. Look for it in the main executable
- s = soinfo_elf_lookup(somain, elf_hash, name);
- if (s != nullptr) {
- *lsi = somain;
- }
+ return gnu_hash_;
+}
- // 2. Look for it in the ld_preloads
- if (s == nullptr) {
- for (int i = 0; g_ld_preloads[i] != NULL; i++) {
- s = soinfo_elf_lookup(g_ld_preloads[i], elf_hash, name);
- if (s != nullptr) {
- *lsi = g_ld_preloads[i];
- break;
- }
- }
- }
+static ElfW(Sym)* soinfo_do_lookup(soinfo* si_from, const char* name, soinfo** si_found_in,
+ const soinfo::soinfo_list_t& global_group, const soinfo::soinfo_list_t& local_group) {
+ SymbolName symbol_name(name);
+ ElfW(Sym)* s = nullptr;
- /* Look for symbols in the local scope (the object who is
- * searching). This happens with C++ templates on x86 for some
- * reason.
- *
- * Notes on weak symbols:
- * The ELF specs are ambiguous about treatment of weak definitions in
- * dynamic linking. Some systems return the first definition found
- * and some the first non-weak definition. This is system dependent.
- * Here we return the first definition found for simplicity. */
+ /* "This element's presence in a shared object library alters the dynamic linker's
+ * symbol resolution algorithm for references within the library. Instead of starting
+ * a symbol search with the executable file, the dynamic linker starts from the shared
+ * object itself. If the shared object fails to supply the referenced symbol, the
+ * dynamic linker then searches the executable file and other shared objects as usual."
+ *
+ * http://www.sco.com/developers/gabi/2012-12-31/ch5.dynamic.html
+ *
+ * Note that this is unlikely since static linker avoids generating
+ * relocations for -Bsymbolic linked dynamic executables.
+ */
+ if (si_from->has_DT_SYMBOLIC) {
+ DEBUG("%s: looking up %s in local scope (DT_SYMBOLIC)", si_from->name, name);
+ s = si_from->find_symbol_by_name(symbol_name);
+ if (s != nullptr) {
+ *si_found_in = si_from;
+ }
+ }
- if (s == nullptr) {
- s = soinfo_elf_lookup(si, elf_hash, name);
+ // 1. Look for it in global_group
+ if (s == nullptr) {
+ global_group.visit([&](soinfo* global_si) {
+ DEBUG("%s: looking up %s in %s (from global group)", si_from->name, name, global_si->name);
+ s = global_si->find_symbol_by_name(symbol_name);
if (s != nullptr) {
- *lsi = si;
+ *si_found_in = global_si;
+ return false;
}
- }
+
+ return true;
+ });
}
+ // 2. Look for it in the local group
if (s == nullptr) {
- si->get_children().visit([&](soinfo* child) {
- DEBUG("%s: looking up %s in %s", si->name, name, child->name);
- s = soinfo_elf_lookup(child, elf_hash, name);
+ local_group.visit([&](soinfo* local_si) {
+ if (local_si == si_from && si_from->has_DT_SYMBOLIC) {
+ // we already did this - skip
+ return true;
+ }
+
+ DEBUG("%s: looking up %s in %s (from local group)", si_from->name, name, local_si->name);
+ s = local_si->find_symbol_by_name(symbol_name);
if (s != nullptr) {
- *lsi = child;
+ *si_found_in = local_si;
return false;
}
+
return true;
});
}
@@ -539,9 +597,9 @@ static ElfW(Sym)* soinfo_do_lookup(soinfo* si, const char* name, soinfo** lsi) {
if (s != nullptr) {
TRACE_TYPE(LOOKUP, "si %s sym %s s->st_value = %p, "
"found in %s, base = %p, load bias = %p",
- si->name, name, reinterpret_cast<void*>(s->st_value),
- (*lsi)->name, reinterpret_cast<void*>((*lsi)->base),
- reinterpret_cast<void*>((*lsi)->load_bias));
+ si_from->name, name, reinterpret_cast<void*>(s->st_value),
+ (*si_found_in)->name, reinterpret_cast<void*>((*si_found_in)->base),
+ reinterpret_cast<void*>((*si_found_in)->load_bias));
}
return s;
typedef linked_list_t<LoadTask> LoadTaskList;
-// This is used by dlsym(3). It performs symbol lookup only within the
-// specified soinfo object and its dependencies in breadth first order.
-ElfW(Sym)* dlsym_handle_lookup(soinfo* si, soinfo** found, const char* name) {
+// This function walks down the tree of soinfo dependencies
+// in breadth-first order and
+// * calls action(soinfo* si) for each node, and
+// * terminates walk if action returns false.
+//
+// walk_dependencies_tree returns false if walk was terminated
+// by the action and true otherwise.
+template<typename F>
+static bool walk_dependencies_tree(soinfo* root_soinfos[], size_t root_soinfos_size, F action) {
SoinfoLinkedList visit_list;
SoinfoLinkedList visited;
- visit_list.push_back(si);
- soinfo* current_soinfo;
- while ((current_soinfo = visit_list.pop_front()) != nullptr) {
- if (visited.contains(current_soinfo)) {
+ for (size_t i = 0; i < root_soinfos_size; ++i) {
+ visit_list.push_back(root_soinfos[i]);
+ }
+
+ soinfo* si;
+ while ((si = visit_list.pop_front()) != nullptr) {
+ if (visited.contains(si)) {
continue;
}
- ElfW(Sym)* result = soinfo_elf_lookup(current_soinfo, elfhash(name), name);
-
- if (result != nullptr) {
- *found = current_soinfo;
- return result;
+ if (!action(si)) {
+ return false;
}
- visited.push_back(current_soinfo);
- current_soinfo->get_children().for_each([&](soinfo* child) {
+ visited.push_back(si);
+
+ si->get_children().for_each([&](soinfo* child) {
visit_list.push_back(child);
});
}
- return nullptr;
+ return true;
+}
+
+
+// This is used by dlsym(3). It performs symbol lookup only within the
+// specified soinfo object and its dependencies in breadth first order.
+ElfW(Sym)* dlsym_handle_lookup(soinfo* si, soinfo** found, const char* name) {
+ ElfW(Sym)* result = nullptr;
+ SymbolName symbol_name(name);
+
+
+ walk_dependencies_tree(&si, 1, [&](soinfo* current_soinfo) {
+ result = current_soinfo->find_symbol_by_name(symbol_name);
+ if (result != nullptr) {
+ *found = current_soinfo;
+ return false;
+ }
+
+ return true;
+ });
+
+ return result;
}
/* This is used by dlsym(3) to performs a global symbol lookup. If the
specified soinfo (for RTLD_NEXT).
*/
ElfW(Sym)* dlsym_linear_lookup(const char* name, soinfo** found, soinfo* start) {
- unsigned elf_hash = elfhash(name);
+ SymbolName symbol_name(name);
if (start == nullptr) {
start = solist;
continue;
}
- s = soinfo_elf_lookup(si, elf_hash, name);
+ s = si->find_symbol_by_name(symbol_name);
if (s != nullptr) {
*found = si;
break;
return nullptr;
}
-ElfW(Sym)* dladdr_find_symbol(soinfo* si, const void* addr) {
- ElfW(Addr) soaddr = reinterpret_cast<ElfW(Addr)>(addr) - si->base;
+ElfW(Sym)* soinfo::find_symbol_by_address(const void* addr) {
+ return is_gnu_hash() ? gnu_addr_lookup(addr) : elf_addr_lookup(addr);
+}
+
+static bool symbol_matches_soaddr(const ElfW(Sym)* sym, ElfW(Addr) soaddr) {
+ return sym->st_shndx != SHN_UNDEF &&
+ soaddr >= sym->st_value &&
+ soaddr < sym->st_value + sym->st_size;
+}
+
+ElfW(Sym)* soinfo::gnu_addr_lookup(const void* addr) {
+ ElfW(Addr) soaddr = reinterpret_cast<ElfW(Addr)>(addr) - base;
+
+ for (size_t i = 0; i < nbucket_; ++i) {
+ uint32_t n = bucket_[i];
+
+ if (n == 0) {
+ continue;
+ }
+
+ do {
+ ElfW(Sym)* sym = symtab_ + n;
+ if (symbol_matches_soaddr(sym, soaddr)) {
+ return sym;
+ }
+ } while ((chain_[n++] & 1) == 0);
+ }
+
+ return nullptr;
+}
+
+ElfW(Sym)* soinfo::elf_addr_lookup(const void* addr) {
+ ElfW(Addr) soaddr = reinterpret_cast<ElfW(Addr)>(addr) - base;
// Search the library's symbol table for any defined symbol which
// contains this address.
- for (size_t i = 0; i < si->nchain; ++i) {
- ElfW(Sym)* sym = &si->symtab[i];
- if (sym->st_shndx != SHN_UNDEF &&
- soaddr >= sym->st_value &&
- soaddr < sym->st_value + sym->st_size) {
+ for (size_t i = 0; i < nchain_; ++i) {
+ ElfW(Sym)* sym = symtab_ + i;
+ if (symbol_matches_soaddr(sym, soaddr)) {
return sym;
}
}
static void for_each_dt_needed(const soinfo* si, F action) {
for (ElfW(Dyn)* d = si->dynamic; d->d_tag != DT_NULL; ++d) {
if (d->d_tag == DT_NEEDED) {
- action(si->strtab + d->d_un.d_val);
+ action(si->get_string(d->d_un.d_val));
}
}
}
static soinfo* load_library(LoadTaskList& load_tasks, const char* name, int rtld_flags, const android_dlextinfo* extinfo) {
int fd = -1;
+ off64_t file_offset = 0;
ScopedFd file_guard(-1);
if (extinfo != nullptr && (extinfo->flags & ANDROID_DLEXT_USE_LIBRARY_FD) != 0) {
fd = extinfo->library_fd;
+ if ((extinfo->flags & ANDROID_DLEXT_USE_LIBRARY_FD_OFFSET) != 0) {
+ file_offset = extinfo->library_fd_offset;
+ }
} else {
// Open the file.
fd = open_library(name);
@@ -776,9 +895,22 @@ static soinfo* load_library(LoadTaskList& load_tasks, const char* name, int rtld
file_guard.reset(fd);
}
+ if ((file_offset % PAGE_SIZE) != 0) {
+ DL_ERR("file offset for the library \"%s\" is not page-aligned: %" PRId64, name, file_offset);
+ return nullptr;
+ }
+ if (file_offset < 0) {
+ DL_ERR("file offset for the library \"%s\" is negative: %" PRId64, name, file_offset);
+ return nullptr;
+ }
+
struct stat file_stat;
if (TEMP_FAILURE_RETRY(fstat(fd, &file_stat)) != 0) {
- DL_ERR("unable to stat file for the library %s: %s", name, strerror(errno));
+ DL_ERR("unable to stat file for the library \"%s\": %s", name, strerror(errno));
+ return nullptr;
+ }
+ if (file_offset >= file_stat.st_size) {
+ DL_ERR("file offset for the library \"%s\" >= file size: %" PRId64 " >= %" PRId64, name, file_offset, file_stat.st_size);
return nullptr;
}
@@ -788,7 +920,8 @@ static soinfo* load_library(LoadTaskList& load_tasks, const char* name, int rtld
if (si->get_st_dev() != 0 &&
si->get_st_ino() != 0 &&
si->get_st_dev() == file_stat.st_dev &&
- si->get_st_ino() == file_stat.st_ino) {
+ si->get_st_ino() == file_stat.st_ino &&
+ si->get_file_offset() == file_offset) {
TRACE("library \"%s\" is already loaded under different name/path \"%s\" - will return existing soinfo", name, si->name);
return si;
}
@@ -800,12 +933,12 @@ static soinfo* load_library(LoadTaskList& load_tasks, const char* name, int rtld
}
// Read the ELF header and load the segments.
- ElfReader elf_reader(name, fd);
+ ElfReader elf_reader(name, fd, file_offset);
if (!elf_reader.Load(extinfo)) {
return nullptr;
}
- soinfo* si = soinfo_alloc(SEARCH_NAME(name), &file_stat, rtld_flags);
+ soinfo* si = soinfo_alloc(SEARCH_NAME(name), &file_stat, file_offset, rtld_flags);
if (si == nullptr) {
return nullptr;
}
@@ -815,7 +948,7 @@ static soinfo* load_library(LoadTaskList& load_tasks, const char* name, int rtld
si->phnum = elf_reader.phdr_count();
si->phdr = elf_reader.loaded_phdr();
- if (!si->PrelinkImage()) {
+ if (!si->prelink_image()) {
soinfo_free(si);
return nullptr;
}
@@ -853,34 +986,51 @@ static soinfo* find_library_internal(LoadTaskList& load_tasks, const char* name,
static void soinfo_unload(soinfo* si);
-static bool is_recursive(soinfo* si, soinfo* parent) {
- if (parent == nullptr) {
- return false;
- }
-
- if (si == parent) {
- DL_ERR("recursive link to \"%s\"", si->name);
- return true;
+// TODO: this is slightly unusual way to construct
+// the global group for relocation. Not every RTLD_GLOBAL
+// library is included in this group for backwards-compatibility
+// reasons.
+//
+// This group consists of the main executable, LD_PRELOADs
+// and libraries with the DF_1_GLOBAL flag set.
+static soinfo::soinfo_list_t make_global_group() {
+ soinfo::soinfo_list_t global_group;
+ for (soinfo* si = somain; si != nullptr; si = si->next) {
+ if ((si->get_dt_flags_1() & DF_1_GLOBAL) != 0) {
+ global_group.push_back(si);
+ }
}
- return !parent->get_parents().visit([&](soinfo* grandparent) {
- return !is_recursive(si, grandparent);
- });
+ return global_group;
}
-static bool find_libraries(const char* const library_names[], size_t library_names_size, soinfo* soinfos[],
- soinfo* ld_preloads[], size_t ld_preloads_size, int rtld_flags, const android_dlextinfo* extinfo) {
+static bool find_libraries(soinfo* start_with, const char* const library_names[], size_t library_names_count, soinfo* soinfos[],
+ soinfo* ld_preloads[], size_t ld_preloads_count, int rtld_flags, const android_dlextinfo* extinfo) {
// Step 0: prepare.
LoadTaskList load_tasks;
- for (size_t i = 0; i < library_names_size; ++i) {
+ for (size_t i = 0; i < library_names_count; ++i) {
const char* name = library_names[i];
- load_tasks.push_back(LoadTask::create(name, nullptr));
+ load_tasks.push_back(LoadTask::create(name, start_with));
+ }
+
+ // Construct global_group.
+ soinfo::soinfo_list_t global_group = make_global_group();
+
+ // If soinfos array is null allocate one on stack.
+ // The array is needed in case of failure; for example
+ // when library_names[] = {libone.so, libtwo.so} and libone.so
+ // is loaded correctly but libtwo.so failed for some reason.
+ // In this case libone.so should be unloaded on return.
+ // See also implementation of failure_guard below.
+
+ if (soinfos == nullptr) {
+ size_t soinfos_size = sizeof(soinfo*)*library_names_count;
+ soinfos = reinterpret_cast<soinfo**>(alloca(soinfos_size));
+ memset(soinfos, 0, soinfos_size);
}
- // Libraries added to this list in reverse order so that we can
- // start linking from bottom-up - see step 2.
- SoinfoLinkedList found_libs;
- size_t soinfos_size = 0;
+ // list of libraries to link - see step 2.
+ size_t soinfos_count = 0;
auto failure_guard = make_scope_guard([&]() {
// Housekeeping
@@ -888,7 +1038,7 @@ static bool find_libraries(const char* const library_names[], size_t library_nam
LoadTask::deleter(t);
});
- for (size_t i = 0; i<soinfos_size; ++i) {
+ for (size_t i = 0; i<soinfos_count; ++i) {
soinfo_unload(soinfos[i]);
}
});
@@ -902,90 +1052,164 @@ static bool find_libraries(const char* const library_names[], size_t library_nam
soinfo* needed_by = task->get_needed_by();
- if (is_recursive(si, needed_by)) {
- return false;
- }
-
- si->ref_count++;
if (needed_by != nullptr) {
needed_by->add_child(si);
}
- found_libs.push_front(si);
- // When ld_preloads is not null first
- // ld_preloads_size libs are in fact ld_preloads.
- if (ld_preloads != nullptr && soinfos_size < ld_preloads_size) {
- ld_preloads[soinfos_size] = si;
+ if (si->is_linked()) {
+ si->increment_ref_count();
+ }
+
+ // When ld_preloads is not null, the first
+ // ld_preloads_count libs are in fact ld_preloads.
+ if (ld_preloads != nullptr && soinfos_count < ld_preloads_count) {
+ // Add LD_PRELOADed libraries to the global group for future runs.
+ // There is no need to explicitly add them to the global group
+ // for this run because they are going to appear in the local
+ // group in the correct order.
+ si->set_dt_flags_1(si->get_dt_flags_1() | DF_1_GLOBAL);
+ ld_preloads[soinfos_count] = si;
}
- if (soinfos_size<library_names_size) {
- soinfos[soinfos_size++] = si;
+ if (soinfos_count < library_names_count) {
+ soinfos[soinfos_count++] = si;
}
}
// Step 2: link libraries.
- soinfo* si;
- while ((si = found_libs.pop_front()) != nullptr) {
- if ((si->flags & FLAG_LINKED) == 0) {
- if (!si->LinkImage(extinfo)) {
+ soinfo::soinfo_list_t local_group;
+ walk_dependencies_tree(
+ start_with == nullptr ? soinfos : &start_with,
+ start_with == nullptr ? soinfos_count : 1,
+ [&] (soinfo* si) {
+ local_group.push_back(si);
+ return true;
+ });
+
+ // We need to increment ref_count in case
+ // the root of the local group was not linked.
+ bool was_local_group_root_linked = local_group.front()->is_linked();
+
+ bool linked = local_group.visit([&](soinfo* si) {
+ if (!si->is_linked()) {
+ if (!si->link_image(global_group, local_group, extinfo)) {
return false;
}
- si->flags |= FLAG_LINKED;
+ si->set_linked();
}
+
+ return true;
+ });
+
+ if (linked) {
+ failure_guard.disable();
}
- // All is well - found_libs and load_tasks are empty at this point
- // and all libs are successfully linked.
- failure_guard.disable();
- return true;
+ if (!was_local_group_root_linked) {
+ local_group.front()->increment_ref_count();
+ }
+
+ return linked;
}
static soinfo* find_library(const char* name, int rtld_flags, const android_dlextinfo* extinfo) {
- if (name == nullptr) {
- somain->ref_count++;
- return somain;
- }
-
soinfo* si;
- if (!find_libraries(&name, 1, &si, nullptr, 0, rtld_flags, extinfo)) {
+ if (name == nullptr) {
+ si = somain;
+ } else if (!find_libraries(nullptr, &name, 1, &si, nullptr, 0, rtld_flags, extinfo)) {
return nullptr;
}
return si;
}
-static void soinfo_unload(soinfo* si) {
- if (si->ref_count == 1) {
- TRACE("unloading '%s'", si->name);
- si->CallDestructors();
+static void soinfo_unload(soinfo* root) {
+ // Note that the library can be loaded but not linked;
+ // in which case there is no root but we still need
+ // to walk the tree and unload soinfos involved.
+ //
+ // This happens on unsuccessful dlopen, when one of
+ // the DT_NEEDED libraries could not be linked/found.
+ if (root->is_linked()) {
+ root = root->get_local_group_root();
+ }
+
+ if (!root->can_unload()) {
+ TRACE("not unloading '%s' - the binary is flagged with NODELETE", root->name);
+ return;
+ }
+
+ size_t ref_count = root->is_linked() ? root->decrement_ref_count() : 0;
+
+ if (ref_count == 0) {
+ soinfo::soinfo_list_t local_unload_list;
+ soinfo::soinfo_list_t external_unload_list;
+ soinfo::soinfo_list_t depth_first_list;
+ depth_first_list.push_back(root);
+ soinfo* si = nullptr;
- if (si->has_min_version(0)) {
- soinfo* child = nullptr;
- while ((child = si->get_children().pop_front()) != nullptr) {
- TRACE("%s needs to unload %s", si->name, child->name);
- soinfo_unload(child);
+ while ((si = depth_first_list.pop_front()) != nullptr) {
+ if (local_unload_list.contains(si)) {
+ continue;
}
- } else {
- for_each_dt_needed(si, [&] (const char* library_name) {
- TRACE("deprecated (old format of soinfo): %s needs to unload %s", si->name, library_name);
- soinfo* needed = find_library(library_name, RTLD_NOLOAD, nullptr);
- if (needed != nullptr) {
- soinfo_unload(needed);
- } else {
- // Not found: for example if symlink was deleted between dlopen and dlclose
- // Since we cannot really handle errors at this point - print and continue.
- PRINT("warning: couldn't find %s needed by %s on unload.", library_name, si->name);
+
+ local_unload_list.push_back(si);
+
+ if (si->has_min_version(0)) {
+ soinfo* child = nullptr;
+ while ((child = si->get_children().pop_front()) != nullptr) {
+ TRACE("%s@%p needs to unload %s@%p", si->name, si, child->name, child);
+ if (local_unload_list.contains(child)) {
+ continue;
+ } else if (child->is_linked() && child->get_local_group_root() != root) {
+ external_unload_list.push_back(child);
+ } else {
+ depth_first_list.push_front(child);
+ }
}
- });
+ } else {
+#ifdef __LP64__
+ __libc_fatal("soinfo for \"%s\"@%p has no version", si->name, si);
+#else
+ PRINT("warning: soinfo for \"%s\"@%p has no version", si->name, si);
+ for_each_dt_needed(si, [&] (const char* library_name) {
+ TRACE("deprecated (old format of soinfo): %s needs to unload %s", si->name, library_name);
+ soinfo* needed = find_library(library_name, RTLD_NOLOAD, nullptr);
+ if (needed != nullptr) {
+ // Not found: for example if symlink was deleted between dlopen and dlclose
+ // Since we cannot really handle errors at this point - print and continue.
+ PRINT("warning: couldn't find %s needed by %s on unload.", library_name, si->name);
+ return;
+ } else if (local_unload_list.contains(needed)) {
+ // already visited
+ return;
+ } else if (needed->is_linked() && needed->get_local_group_root() != root) {
+ // external group
+ external_unload_list.push_back(needed);
+ } else {
+ // local group
+ depth_first_list.push_front(needed);
+ }
+ });
+#endif
+ }
}
- notify_gdb_of_unload(si);
- si->ref_count = 0;
- soinfo_free(si);
+ local_unload_list.for_each([](soinfo* si) {
+ si->call_destructors();
+ });
+
+ while ((si = local_unload_list.pop_front()) != nullptr) {
+ notify_gdb_of_unload(si);
+ soinfo_free(si);
+ }
+
+ while ((si = external_unload_list.pop_front()) != nullptr) {
+ soinfo_unload(si);
+ }
} else {
- si->ref_count--;
- TRACE("not unloading '%s', decrementing ref_count to %zd", si->name, si->ref_count);
+ TRACE("not unloading '%s' group, decrementing ref_count to %zd", root->name, ref_count);
}
}
}
soinfo* do_dlopen(const char* name, int flags, const android_dlextinfo* extinfo) {
- if ((flags & ~(RTLD_NOW|RTLD_LAZY|RTLD_LOCAL|RTLD_GLOBAL|RTLD_NOLOAD)) != 0) {
+ if ((flags & ~(RTLD_NOW|RTLD_LAZY|RTLD_LOCAL|RTLD_GLOBAL|RTLD_NODELETE|RTLD_NOLOAD)) != 0) {
DL_ERR("invalid flags to dlopen: %x", flags);
return nullptr;
}
- if (extinfo != nullptr && ((extinfo->flags & ~(ANDROID_DLEXT_VALID_FLAG_BITS)) != 0)) {
- DL_ERR("invalid extended flags to android_dlopen_ext: %" PRIx64, extinfo->flags);
- return nullptr;
+ if (extinfo != nullptr) {
+ if ((extinfo->flags & ~(ANDROID_DLEXT_VALID_FLAG_BITS)) != 0) {
+ DL_ERR("invalid extended flags to android_dlopen_ext: 0x%" PRIx64, extinfo->flags);
+ return nullptr;
+ }
+ if ((extinfo->flags & ANDROID_DLEXT_USE_LIBRARY_FD) == 0 &&
+ (extinfo->flags & ANDROID_DLEXT_USE_LIBRARY_FD_OFFSET) != 0) {
+ DL_ERR("invalid extended flag combination (ANDROID_DLEXT_USE_LIBRARY_FD_OFFSET without ANDROID_DLEXT_USE_LIBRARY_FD): 0x%" PRIx64, extinfo->flags);
+ return nullptr;
+ }
}
protect_data(PROT_READ | PROT_WRITE);
soinfo* si = find_library(name, flags, extinfo);
if (si != nullptr) {
- si->CallConstructors();
+ si->call_constructors();
}
protect_data(PROT_READ);
return si;
}
#if defined(USE_RELA)
-int soinfo::Relocate(ElfW(Rela)* rela, unsigned count) {
+int soinfo::relocate(ElfW(Rela)* rela, unsigned count, const soinfo_list_t& global_group, const soinfo_list_t& local_group) {
for (size_t idx = 0; idx < count; ++idx, ++rela) {
unsigned type = ELFW(R_TYPE)(rela->r_info);
unsigned sym = ELFW(R_SYM)(rela->r_info);
soinfo* lsi = nullptr;
if (sym != 0) {
- sym_name = reinterpret_cast<const char*>(strtab + symtab[sym].st_name);
- s = soinfo_do_lookup(this, sym_name, &lsi);
+ sym_name = get_string(symtab_[sym].st_name);
+ s = soinfo_do_lookup(this, sym_name, &lsi, global_group,local_group);
if (s == nullptr) {
// We only allow an undefined symbol if this is a weak reference...
- s = &symtab[sym];
+ s = &symtab_[sym];
if (ELF_ST_BIND(s->st_info) != STB_WEAK) {
DL_ERR("cannot locate symbol \"%s\" referenced by \"%s\"...", sym_name, name);
return -1;
}
#else // REL, not RELA.
-int soinfo::Relocate(ElfW(Rel)* rel, unsigned count) {
+int soinfo::relocate(ElfW(Rel)* rel, unsigned count, const soinfo_list_t& global_group, const soinfo_list_t& local_group) {
for (size_t idx = 0; idx < count; ++idx, ++rel) {
unsigned type = ELFW(R_TYPE)(rel->r_info);
// TODO: don't use unsigned for 'sym'. Use uint32_t or ElfW(Addr) instead.
soinfo* lsi = nullptr;
if (sym != 0) {
- sym_name = reinterpret_cast<const char*>(strtab + symtab[sym].st_name);
- s = soinfo_do_lookup(this, sym_name, &lsi);
+ sym_name = get_string(symtab_[sym].st_name);
+ s = soinfo_do_lookup(this, sym_name, &lsi, global_group, local_group);
if (s == nullptr) {
// We only allow an undefined symbol if this is a weak reference...
- s = &symtab[sym];
+ s = &symtab_[sym];
if (ELF_ST_BIND(s->st_info) != STB_WEAK) {
DL_ERR("cannot locate symbol \"%s\" referenced by \"%s\"...", sym_name, name);
return -1;
#endif
#if defined(__mips__)
-static bool mips_relocate_got(soinfo* si) {
- ElfW(Addr)** got = si->plt_got;
+bool soinfo::mips_relocate_got(const soinfo_list_t& global_group, const soinfo_list_t& local_group) {
+ ElfW(Addr)** got = plt_got_;
if (got == nullptr) {
return true;
}
- unsigned local_gotno = si->mips_local_gotno;
- unsigned gotsym = si->mips_gotsym;
- unsigned symtabno = si->mips_symtabno;
- ElfW(Sym)* symtab = si->symtab;
// got[0] is the address of the lazy resolver function.
// got[1] may be used for a GNU extension.
// Set it to a recognizable address in case someone calls it (should be _rtld_bind_start).
// FIXME: maybe this should be in a separate routine?
- if ((si->flags & FLAG_LINKER) == 0) {
+ if ((flags_ & FLAG_LINKER) == 0) {
size_t g = 0;
got[g++] = reinterpret_cast<ElfW(Addr)*>(0xdeadbeef);
if (reinterpret_cast<intptr_t>(got[g]) < 0) {
got[g++] = reinterpret_cast<ElfW(Addr)*>(0xdeadfeed);
}
// Relocate the local GOT entries.
- for (; g < local_gotno; g++) {
- got[g] = reinterpret_cast<ElfW(Addr)*>(reinterpret_cast<uintptr_t>(got[g]) + si->load_bias);
+ for (; g < mips_local_gotno_; g++) {
+ got[g] = reinterpret_cast<ElfW(Addr)*>(reinterpret_cast<uintptr_t>(got[g]) + load_bias);
}
}
// Now for the global GOT entries...
- ElfW(Sym)* sym = symtab + gotsym;
- got = si->plt_got + local_gotno;
- for (size_t g = gotsym; g < symtabno; g++, sym++, got++) {
+ ElfW(Sym)* sym = symtab_ + mips_gotsym_;
+ got = plt_got_ + mips_local_gotno_;
+ for (size_t g = mips_gotsym_; g < mips_symtabno_; g++, sym++, got++) {
// This is an undefined reference... try to locate it.
- const char* sym_name = si->strtab + sym->st_name;
+ const char* sym_name = get_string(sym->st_name);
soinfo* lsi = nullptr;
- ElfW(Sym)* s = soinfo_do_lookup(si, sym_name, &lsi);
+ ElfW(Sym)* s = soinfo_do_lookup(this, sym_name, &lsi, global_group, local_group);
if (s == nullptr) {
// We only allow an undefined symbol if this is a weak reference.
- s = &symtab[g];
+ s = &symtab_[g];
if (ELF_ST_BIND(s->st_info) != STB_WEAK) {
DL_ERR("cannot locate \"%s\"...", sym_name);
return false;
}
#endif
-void soinfo::CallArray(const char* array_name __unused, linker_function_t* functions, size_t count, bool reverse) {
+void soinfo::call_array(const char* array_name __unused, linker_function_t* functions, size_t count, bool reverse) {
if (functions == nullptr) {
return;
}
@@ -1595,13 +1822,13 @@ void soinfo::CallArray(const char* array_name __unused, linker_function_t* funct
for (int i = begin; i != end; i += step) {
TRACE("[ %s[%d] == %p ]", array_name, i, functions[i]);
- CallFunction("function", functions[i]);
+ call_function("function", functions[i]);
}
TRACE("[ Done calling %s for '%s' ]", array_name, name);
}
-void soinfo::CallFunction(const char* function_name __unused, linker_function_t function) {
+void soinfo::call_function(const char* function_name __unused, linker_function_t function) {
if (function == nullptr || reinterpret_cast<uintptr_t>(function) == static_cast<uintptr_t>(-1)) {
return;
}
@@ -1615,13 +1842,13 @@ void soinfo::CallFunction(const char* function_name __unused, linker_function_t
protect_data(PROT_READ | PROT_WRITE);
}
-void soinfo::CallPreInitConstructors() {
+void soinfo::call_pre_init_constructors() {
// DT_PREINIT_ARRAY functions are called before any other constructors for executables,
// but ignored in a shared library.
- CallArray("DT_PREINIT_ARRAY", preinit_array, preinit_array_count, false);
+ call_array("DT_PREINIT_ARRAY", preinit_array_, preinit_array_count_, false);
}
-void soinfo::CallConstructors() {
+void soinfo::call_constructors() {
if (constructors_called) {
return;
}
// out above, the libc constructor will be called again (recursively!).
constructors_called = true;
- if ((flags & FLAG_EXE) == 0 && preinit_array != nullptr) {
+ if (!is_main_executable() && preinit_array_ != nullptr) {
// The GNU dynamic linker silently ignores these, but we warn the developer.
PRINT("\"%s\": ignoring %zd-entry DT_PREINIT_ARRAY in shared library!",
- name, preinit_array_count);
+ name, preinit_array_count_);
}
get_children().for_each([] (soinfo* si) {
- si->CallConstructors();
+ si->call_constructors();
});
TRACE("\"%s\": calling constructors", name);
// DT_INIT should be called before DT_INIT_ARRAY if both are present.
- CallFunction("DT_INIT", init_func);
- CallArray("DT_INIT_ARRAY", init_array, init_array_count, false);
+ call_function("DT_INIT", init_func_);
+ call_array("DT_INIT_ARRAY", init_array_, init_array_count_, false);
}
-void soinfo::CallDestructors() {
+void soinfo::call_destructors() {
if (!constructors_called) {
return;
}
TRACE("\"%s\": calling destructors", name);
// DT_FINI_ARRAY must be parsed in reverse order.
- CallArray("DT_FINI_ARRAY", fini_array, fini_array_count, true);
+ call_array("DT_FINI_ARRAY", fini_array_, fini_array_count_, true);
// DT_FINI should be called after DT_FINI_ARRAY if both are present.
- CallFunction("DT_FINI", fini_func);
+ call_function("DT_FINI", fini_func_);
// This is needed on second call to dlopen
// after library has been unloaded with RTLD_NODELETE
void soinfo::add_child(soinfo* child) {
if (has_min_version(0)) {
- child->parents.push_back(this);
- this->children.push_back(child);
+ child->parents_.push_back(this);
+ this->children_.push_back(child);
}
}
}
// 1. Untie connected soinfos from 'this'.
- children.for_each([&] (soinfo* child) {
- child->parents.remove_if([&] (const soinfo* parent) {
+ children_.for_each([&] (soinfo* child) {
+ child->parents_.remove_if([&] (const soinfo* parent) {
return parent == this;
});
});
- parents.for_each([&] (soinfo* parent) {
- parent->children.remove_if([&] (const soinfo* child) {
+ parents_.for_each([&] (soinfo* parent) {
+ parent->children_.remove_if([&] (const soinfo* child) {
return child == this;
});
});
// 2. Once everything untied - clear local lists.
- parents.clear();
- children.clear();
+ parents_.clear();
+ children_.clear();
}
-void soinfo::set_st_dev(dev_t dev) {
+dev_t soinfo::get_st_dev() const {
if (has_min_version(0)) {
- st_dev = dev;
+ return st_dev_;
}
-}
-void soinfo::set_st_ino(ino_t ino) {
+ return 0;
+};
+
+ino_t soinfo::get_st_ino() const {
if (has_min_version(0)) {
- st_ino = ino;
+ return st_ino_;
}
+
+ return 0;
}
-dev_t soinfo::get_st_dev() {
- if (has_min_version(0)) {
- return st_dev;
+off64_t soinfo::get_file_offset() const {
+ if (has_min_version(1)) {
+ return file_offset_;
}
return 0;
-};
+}
-ino_t soinfo::get_st_ino() {
- if (has_min_version(0)) {
- return st_ino;
+uint32_t soinfo::get_rtld_flags() const {
+ if (has_min_version(1)) {
+ return rtld_flags_;
}
return 0;
}
-int soinfo::get_rtld_flags() {
+uint32_t soinfo::get_dt_flags_1() const {
if (has_min_version(1)) {
- return rtld_flags;
+ return dt_flags_1_;
}
return 0;
}
+void soinfo::set_dt_flags_1(uint32_t dt_flags_1) {
+ if (has_min_version(1)) {
+ if ((dt_flags_1 & DF_1_GLOBAL) != 0) {
+ rtld_flags_ |= RTLD_GLOBAL;
+ }
+
+ if ((dt_flags_1 & DF_1_NODELETE) != 0) {
+ rtld_flags_ |= RTLD_NODELETE;
+ }
+
+ dt_flags_1_ = dt_flags_1;
+ }
+}
// This is a return on get_children()/get_parents() if
// 'this->flags' does not have FLAG_NEW_SOINFO set.
soinfo::soinfo_list_t& soinfo::get_children() {
if (has_min_version(0)) {
- return this->children;
+ return children_;
}
return g_empty_list;
}
soinfo::soinfo_list_t& soinfo::get_parents() {
- if ((this->flags & FLAG_NEW_SOINFO) == 0) {
- return g_empty_list;
+ if (has_min_version(0)) {
+ return parents_;
}
- return this->parents;
+ return g_empty_list;
}
ElfW(Addr) soinfo::resolve_symbol_address(ElfW(Sym)* s) {
return static_cast<ElfW(Addr)>(s->st_value + load_bias);
}
+const char* soinfo::get_string(ElfW(Word) index) const {
+ if (has_min_version(1) && (index >= strtab_size_)) {
+ __libc_fatal("%s: strtab out of bounds error; STRSZ=%zd, name=%d", name, strtab_size_, index);
+ }
+
+ return strtab_ + index;
+}
+
+bool soinfo::is_gnu_hash() const {
+ return (flags_ & FLAG_GNU_HASH) != 0;
+}
+
+bool soinfo::can_unload() const {
+ return (get_rtld_flags() & (RTLD_NODELETE | RTLD_GLOBAL)) == 0;
+}
+
+bool soinfo::is_linked() const {
+ return (flags_ & FLAG_LINKED) != 0;
+}
+
+bool soinfo::is_main_executable() const {
+ return (flags_ & FLAG_EXE) != 0;
+}
+
+void soinfo::set_linked() {
+ flags_ |= FLAG_LINKED;
+}
+
+void soinfo::set_linker_flag() {
+ flags_ |= FLAG_LINKER;
+}
+
+void soinfo::set_main_executable() {
+ flags_ |= FLAG_EXE;
+}
+
+void soinfo::increment_ref_count() {
+ local_group_root_->ref_count_++;
+}
+
+size_t soinfo::decrement_ref_count() {
+ return --local_group_root_->ref_count_;
+}
+
+soinfo* soinfo::get_local_group_root() const {
+ return local_group_root_;
+}
+
/* Force any of the closed stdin, stdout and stderr to be associated with
/dev/null. */
static int nullify_closed_stdio() {
return return_value;
}
-bool soinfo::PrelinkImage() {
+bool soinfo::prelink_image() {
/* Extract dynamic section */
ElfW(Word) dynamic_flags = 0;
phdr_table_get_dynamic_section(phdr, phnum, load_bias, &dynamic, &dynamic_flags);
/* We can't log anything until the linker is relocated */
- bool relocating_linker = (flags & FLAG_LINKER) != 0;
+ bool relocating_linker = (flags_ & FLAG_LINKER) != 0;
if (!relocating_linker) {
INFO("[ linking %s ]", name);
- DEBUG("si->base = %p si->flags = 0x%08x", reinterpret_cast<void*>(base), flags);
+ DEBUG("si->base = %p si->flags = 0x%08x", reinterpret_cast<void*>(base), flags_);
}
if (dynamic == nullptr) {
// TODO: glibc dynamic linker uses this name for
// initial library lookup; consider doing the same here.
break;
+
case DT_HASH:
- nbucket = reinterpret_cast<uint32_t*>(load_bias + d->d_un.d_ptr)[0];
- nchain = reinterpret_cast<uint32_t*>(load_bias + d->d_un.d_ptr)[1];
- bucket = reinterpret_cast<uint32_t*>(load_bias + d->d_un.d_ptr + 8);
- chain = reinterpret_cast<uint32_t*>(load_bias + d->d_un.d_ptr + 8 + nbucket * 4);
+ if (nbucket_ != 0) {
+ // in case of --hash-style=both, we prefer gnu
+ break;
+ }
+
+ nbucket_ = reinterpret_cast<uint32_t*>(load_bias + d->d_un.d_ptr)[0];
+ nchain_ = reinterpret_cast<uint32_t*>(load_bias + d->d_un.d_ptr)[1];
+ bucket_ = reinterpret_cast<uint32_t*>(load_bias + d->d_un.d_ptr + 8);
+ chain_ = reinterpret_cast<uint32_t*>(load_bias + d->d_un.d_ptr + 8 + nbucket_ * 4);
+ break;
+
+ case DT_GNU_HASH:
+ if (nbucket_ != 0) {
+ // in case of --hash-style=both, we prefer gnu
+ nchain_ = 0;
+ }
+
+ nbucket_ = reinterpret_cast<uint32_t*>(load_bias + d->d_un.d_ptr)[0];
+ // skip symndx
+ gnu_maskwords_ = reinterpret_cast<uint32_t*>(load_bias + d->d_un.d_ptr)[2];
+ gnu_shift2_ = reinterpret_cast<uint32_t*>(load_bias + d->d_un.d_ptr)[3];
+
+ gnu_bloom_filter_ = reinterpret_cast<ElfW(Addr)*>(load_bias + d->d_un.d_ptr + 16);
+ bucket_ = reinterpret_cast<uint32_t*>(gnu_bloom_filter_ + gnu_maskwords_);
+ // amend chain for symndx = header[1]
+ chain_ = bucket_ + nbucket_ - reinterpret_cast<uint32_t*>(load_bias + d->d_un.d_ptr)[1];
+
+ if (!powerof2(gnu_maskwords_)) {
+ DL_ERR("invalid maskwords for gnu_hash = 0x%x, in \"%s\" expecting power to two", gnu_maskwords_, name);
+ return false;
+ }
+ --gnu_maskwords_;
+
+ flags_ |= FLAG_GNU_HASH;
break;
+
case DT_STRTAB:
- strtab = reinterpret_cast<const char*>(load_bias + d->d_un.d_ptr);
+ strtab_ = reinterpret_cast<const char*>(load_bias + d->d_un.d_ptr);
break;
+
+ case DT_STRSZ:
+ strtab_size_ = d->d_un.d_val;
+ break;
+
case DT_SYMTAB:
- symtab = reinterpret_cast<ElfW(Sym)*>(load_bias + d->d_un.d_ptr);
+ symtab_ = reinterpret_cast<ElfW(Sym)*>(load_bias + d->d_un.d_ptr);
break;
+
case DT_SYMENT:
if (d->d_un.d_val != sizeof(ElfW(Sym))) {
- DL_ERR("invalid DT_SYMENT: %zd", static_cast<size_t>(d->d_un.d_val));
+ DL_ERR("invalid DT_SYMENT: %zd in \"%s\"", static_cast<size_t>(d->d_un.d_val), name);
return false;
}
break;
-#if !defined(__LP64__)
+
case DT_PLTREL:
+#if defined(USE_RELA)
+ if (d->d_un.d_val != DT_RELA) {
+ DL_ERR("unsupported DT_PLTREL in \"%s\"; expected DT_RELA", name);
+ return false;
+ }
+#else
if (d->d_un.d_val != DT_REL) {
- DL_ERR("unsupported DT_RELA in \"%s\"", name);
+ DL_ERR("unsupported DT_PLTREL in \"%s\"; expected DT_REL", name);
return false;
}
- break;
#endif
+ break;
+
case DT_JMPREL:
#if defined(USE_RELA)
- plt_rela = reinterpret_cast<ElfW(Rela)*>(load_bias + d->d_un.d_ptr);
+ plt_rela_ = reinterpret_cast<ElfW(Rela)*>(load_bias + d->d_un.d_ptr);
#else
- plt_rel = reinterpret_cast<ElfW(Rel)*>(load_bias + d->d_un.d_ptr);
+ plt_rel_ = reinterpret_cast<ElfW(Rel)*>(load_bias + d->d_un.d_ptr);
#endif
break;
+
case DT_PLTRELSZ:
#if defined(USE_RELA)
- plt_rela_count = d->d_un.d_val / sizeof(ElfW(Rela));
+ plt_rela_count_ = d->d_un.d_val / sizeof(ElfW(Rela));
#else
- plt_rel_count = d->d_un.d_val / sizeof(ElfW(Rel));
+ plt_rel_count_ = d->d_un.d_val / sizeof(ElfW(Rel));
#endif
break;
+
case DT_PLTGOT:
#if defined(__mips__)
// Used by mips and mips64.
- plt_got = reinterpret_cast<ElfW(Addr)**>(load_bias + d->d_un.d_ptr);
+ plt_got_ = reinterpret_cast<ElfW(Addr)**>(load_bias + d->d_un.d_ptr);
#endif
// Ignore for other platforms... (because RTLD_LAZY is not supported)
break;
+
case DT_DEBUG:
// Set the DT_DEBUG entry to the address of _r_debug for GDB
// if the dynamic table is writable
#endif
#if defined(USE_RELA)
case DT_RELA:
- rela = reinterpret_cast<ElfW(Rela)*>(load_bias + d->d_un.d_ptr);
+ rela_ = reinterpret_cast<ElfW(Rela)*>(load_bias + d->d_un.d_ptr);
break;
+
case DT_RELASZ:
- rela_count = d->d_un.d_val / sizeof(ElfW(Rela));
+ rela_count_ = d->d_un.d_val / sizeof(ElfW(Rela));
break;
+
case DT_RELAENT:
if (d->d_un.d_val != sizeof(ElfW(Rela))) {
DL_ERR("invalid DT_RELAENT: %zd", static_cast<size_t>(d->d_un.d_val));
return false;
}
break;
+
+ // ignored (see DT_RELCOUNT comments for details)
case DT_RELACOUNT:
- // ignored (see DT_RELCOUNT comments for details)
break;
+
case DT_REL:
DL_ERR("unsupported DT_REL in \"%s\"", name);
return false;
+
case DT_RELSZ:
DL_ERR("unsupported DT_RELSZ in \"%s\"", name);
return false;
#else
case DT_REL:
- rel = reinterpret_cast<ElfW(Rel)*>(load_bias + d->d_un.d_ptr);
+ rel_ = reinterpret_cast<ElfW(Rel)*>(load_bias + d->d_un.d_ptr);
break;
+
case DT_RELSZ:
- rel_count = d->d_un.d_val / sizeof(ElfW(Rel));
+ rel_count_ = d->d_un.d_val / sizeof(ElfW(Rel));
break;
+
case DT_RELENT:
if (d->d_un.d_val != sizeof(ElfW(Rel))) {
DL_ERR("invalid DT_RELENT: %zd", static_cast<size_t>(d->d_un.d_val));
return false;
}
break;
+
+ // "Indicates that all RELATIVE relocations have been concatenated together,
+ // and specifies the RELATIVE relocation count."
+ //
+ // TODO: Spec also mentions that this can be used to optimize relocation process;
+ // Not currently used by bionic linker - ignored.
case DT_RELCOUNT:
- // "Indicates that all RELATIVE relocations have been concatenated together,
- // and specifies the RELATIVE relocation count."
- //
- // TODO: Spec also mentions that this can be used to optimize relocation process;
- // Not currently used by bionic linker - ignored.
break;
case DT_RELA:
DL_ERR("unsupported DT_RELA in \"%s\"", name);
return false;
#endif
case DT_INIT:
- init_func = reinterpret_cast<linker_function_t>(load_bias + d->d_un.d_ptr);
- DEBUG("%s constructors (DT_INIT) found at %p", name, init_func);
+ init_func_ = reinterpret_cast<linker_function_t>(load_bias + d->d_un.d_ptr);
+ DEBUG("%s constructors (DT_INIT) found at %p", name, init_func_);
break;
+
case DT_FINI:
- fini_func = reinterpret_cast<linker_function_t>(load_bias + d->d_un.d_ptr);
- DEBUG("%s destructors (DT_FINI) found at %p", name, fini_func);
+ fini_func_ = reinterpret_cast<linker_function_t>(load_bias + d->d_un.d_ptr);
+ DEBUG("%s destructors (DT_FINI) found at %p", name, fini_func_);
break;
+
case DT_INIT_ARRAY:
- init_array = reinterpret_cast<linker_function_t*>(load_bias + d->d_un.d_ptr);
- DEBUG("%s constructors (DT_INIT_ARRAY) found at %p", name, init_array);
+ init_array_ = reinterpret_cast<linker_function_t*>(load_bias + d->d_un.d_ptr);
+ DEBUG("%s constructors (DT_INIT_ARRAY) found at %p", name, init_array_);
break;
+
case DT_INIT_ARRAYSZ:
- init_array_count = ((unsigned)d->d_un.d_val) / sizeof(ElfW(Addr));
+ init_array_count_ = ((unsigned)d->d_un.d_val) / sizeof(ElfW(Addr));
break;
+
case DT_FINI_ARRAY:
- fini_array = reinterpret_cast<linker_function_t*>(load_bias + d->d_un.d_ptr);
- DEBUG("%s destructors (DT_FINI_ARRAY) found at %p", name, fini_array);
+ fini_array_ = reinterpret_cast<linker_function_t*>(load_bias + d->d_un.d_ptr);
+ DEBUG("%s destructors (DT_FINI_ARRAY) found at %p", name, fini_array_);
break;
+
case DT_FINI_ARRAYSZ:
- fini_array_count = ((unsigned)d->d_un.d_val) / sizeof(ElfW(Addr));
+ fini_array_count_ = ((unsigned)d->d_un.d_val) / sizeof(ElfW(Addr));
break;
+
case DT_PREINIT_ARRAY:
- preinit_array = reinterpret_cast<linker_function_t*>(load_bias + d->d_un.d_ptr);
- DEBUG("%s constructors (DT_PREINIT_ARRAY) found at %p", name, preinit_array);
+ preinit_array_ = reinterpret_cast<linker_function_t*>(load_bias + d->d_un.d_ptr);
+ DEBUG("%s constructors (DT_PREINIT_ARRAY) found at %p", name, preinit_array_);
break;
+
case DT_PREINIT_ARRAYSZ:
- preinit_array_count = ((unsigned)d->d_un.d_val) / sizeof(ElfW(Addr));
+ preinit_array_count_ = ((unsigned)d->d_un.d_val) / sizeof(ElfW(Addr));
break;
+
case DT_TEXTREL:
#if defined(__LP64__)
DL_ERR("text relocations (DT_TEXTREL) found in 64-bit ELF file \"%s\"", name);
has_text_relocations = true;
break;
#endif
+
case DT_SYMBOLIC:
- // ignored
+ has_DT_SYMBOLIC = true;
break;
+
case DT_NEEDED:
++needed_count;
break;
+
case DT_FLAGS:
if (d->d_un.d_val & DF_TEXTREL) {
#if defined(__LP64__)
has_text_relocations = true;
#endif
}
+ if (d->d_un.d_val & DF_SYMBOLIC) {
+ has_DT_SYMBOLIC = true;
+ }
break;
-#if defined(__mips__)
- case DT_STRSZ:
+
+ case DT_FLAGS_1:
+ set_dt_flags_1(d->d_un.d_val);
+
+ if ((d->d_un.d_val & ~SUPPORTED_DT_FLAGS_1) != 0) {
+ DL_WARN("Unsupported flags DT_FLAGS_1=%p", reinterpret_cast<void*>(d->d_un.d_val));
+ }
break;
+#if defined(__mips__)
case DT_MIPS_RLD_MAP:
// Set the DT_MIPS_RLD_MAP entry to the address of _r_debug for GDB.
{
*dp = &_r_debug;
}
break;
+
case DT_MIPS_RLD_VERSION:
case DT_MIPS_FLAGS:
case DT_MIPS_BASE_ADDRESS:
break;
case DT_MIPS_SYMTABNO:
- mips_symtabno = d->d_un.d_val;
+ mips_symtabno_ = d->d_un.d_val;
break;
case DT_MIPS_LOCAL_GOTNO:
- mips_local_gotno = d->d_un.d_val;
+ mips_local_gotno_ = d->d_un.d_val;
break;
case DT_MIPS_GOTSYM:
- mips_gotsym = d->d_un.d_val;
+ mips_gotsym_ = d->d_un.d_val;
break;
#endif
+ // Ignored: "Its use has been superseded by the DF_BIND_NOW flag"
+ case DT_BIND_NOW:
+ break;
+
+ // Ignore: bionic does not support symbol versioning...
+ case DT_VERSYM:
+ case DT_VERDEF:
+ case DT_VERDEFNUM:
+ case DT_VERNEED:
+ case DT_VERNEEDNUM:
+ break;
default:
if (!relocating_linker) {
- DEBUG("%s: unused DT entry: type %p arg %p", name,
+ DL_WARN("%s: unused DT entry: type %p arg %p", name,
reinterpret_cast<void*>(d->d_tag), reinterpret_cast<void*>(d->d_un.d_val));
}
break;
}
DEBUG("si->base = %p, si->strtab = %p, si->symtab = %p",
- reinterpret_cast<void*>(base), strtab, symtab);
+ reinterpret_cast<void*>(base), strtab_, symtab_);
// Sanity checks.
if (relocating_linker && needed_count != 0) {
DL_ERR("linker cannot have DT_NEEDED dependencies on other libraries");
return false;
}
- if (nbucket == 0) {
- DL_ERR("empty/missing DT_HASH in \"%s\" (built with --hash-style=gnu?)", name);
+ if (nbucket_ == 0) {
+ DL_ERR("empty/missing DT_HASH/DT_GNU_HASH in \"%s\" (new hash type from the future?)", name);
return false;
}
- if (strtab == 0) {
+ if (strtab_ == 0) {
DL_ERR("empty/missing DT_STRTAB in \"%s\"", name);
return false;
}
- if (symtab == 0) {
+ if (symtab_ == 0) {
DL_ERR("empty/missing DT_SYMTAB in \"%s\"", name);
return false;
}
return true;
}
-bool soinfo::LinkImage(const android_dlextinfo* extinfo) {
+bool soinfo::link_image(const soinfo_list_t& global_group, const soinfo_list_t& local_group, const android_dlextinfo* extinfo) {
+
+ local_group_root_ = local_group.front();
+ if (local_group_root_ == nullptr) {
+ local_group_root_ = this;
+ }
#if !defined(__LP64__)
if (has_text_relocations) {
#endif
#if defined(USE_RELA)
- if (rela != nullptr) {
+ if (rela_ != nullptr) {
DEBUG("[ relocating %s ]", name);
- if (Relocate(rela, rela_count)) {
+ if (relocate(rela_, rela_count_, global_group, local_group)) {
return false;
}
}
- if (plt_rela != nullptr) {
+ if (plt_rela_ != nullptr) {
DEBUG("[ relocating %s plt ]", name);
- if (Relocate(plt_rela, plt_rela_count)) {
+ if (relocate(plt_rela_, plt_rela_count_, global_group, local_group)) {
return false;
}
}
#else
- if (rel != nullptr) {
+ if (rel_ != nullptr) {
DEBUG("[ relocating %s ]", name);
- if (Relocate(rel, rel_count)) {
+ if (relocate(rel_, rel_count_, global_group, local_group)) {
return false;
}
}
- if (plt_rel != nullptr) {
+ if (plt_rel_ != nullptr) {
DEBUG("[ relocating %s plt ]", name);
- if (Relocate(plt_rel, plt_rel_count)) {
+ if (relocate(plt_rel_, plt_rel_count_, global_group, local_group)) {
return false;
}
}
#endif
#if defined(__mips__)
- if (!mips_relocate_got(this)) {
+ if (!mips_relocate_got(global_group, local_group)) {
return false;
}
#endif
return;
}
- soinfo* si = soinfo_alloc("[vdso]", nullptr, 0);
+ soinfo* si = soinfo_alloc("[vdso]", nullptr, 0, 0);
si->phdr = reinterpret_cast<ElfW(Phdr)*>(reinterpret_cast<char*>(ehdr_vdso) + ehdr_vdso->e_phoff);
si->phnum = ehdr_vdso->e_phnum;
si->size = phdr_table_get_load_size(si->phdr, si->phnum);
si->load_bias = get_elf_exec_load_bias(ehdr_vdso);
- si->PrelinkImage();
- si->LinkImage(nullptr);
+ si->prelink_image();
+ si->link_image(g_empty_list, soinfo::soinfo_list_t::make_list(si), nullptr);
#endif
}
#else
#define LINKER_PATH "/system/bin/linker"
#endif
-static soinfo linker_soinfo_for_gdb(LINKER_PATH, nullptr, 0);
+static soinfo linker_soinfo_for_gdb(LINKER_PATH, nullptr, 0, 0);
/* gdb expects the linker to be in the debug shared object list.
* Without this, gdb has trouble locating the linker's ".text"
@@ -2273,13 +2658,13 @@ static ElfW(Addr) __linker_init_post_relocation(KernelArgumentBlock& args, ElfW(
INFO("[ android linker & debugger ]");
- soinfo* si = soinfo_alloc(args.argv[0], nullptr, RTLD_GLOBAL);
+ soinfo* si = soinfo_alloc(args.argv[0], nullptr, 0, RTLD_GLOBAL);
if (si == nullptr) {
exit(EXIT_FAILURE);
}
/* bootstrap the link map, the main exe always needs to be first */
- si->flags |= FLAG_EXE;
+ si->set_main_executable();
link_map* map = &(si->link_map_head);
map->l_addr = 0;
@@ -2312,7 +2697,6 @@ static ElfW(Addr) __linker_init_post_relocation(KernelArgumentBlock& args, ElfW(
}
}
si->dynamic = nullptr;
- si->ref_count = 1;
ElfW(Ehdr)* elf_hdr = reinterpret_cast<ElfW(Ehdr)*>(si->base);
if (elf_hdr->e_type != ET_DYN) {
@@ -2326,7 +2710,10 @@ static ElfW(Addr) __linker_init_post_relocation(KernelArgumentBlock& args, ElfW(
somain = si;
- si->PrelinkImage();
+ si->prelink_image();
+
+ // add somain to global group
+ si->set_dt_flags_1(si->get_dt_flags_1() | DF_1_GLOBAL);
// Load ld_preloads and dependencies.
StringLinkedList needed_library_name_list;
@@ -2343,36 +2730,32 @@ static ElfW(Addr) __linker_init_post_relocation(KernelArgumentBlock& args, ElfW(
});
const char* needed_library_names[needed_libraries_count];
- soinfo* needed_library_si[needed_libraries_count];
memset(needed_library_names, 0, sizeof(needed_library_names));
needed_library_name_list.copy_to_array(needed_library_names, needed_libraries_count);
- if (needed_libraries_count > 0 && !find_libraries(needed_library_names, needed_libraries_count, needed_library_si, g_ld_preloads, ld_preloads_count, RTLD_GLOBAL, nullptr)) {
- __libc_format_fd(2, "CANNOT LINK EXECUTABLE DEPENDENCIES: %s\n", linker_get_error_buffer());
- exit(EXIT_FAILURE);
- }
-
- for (size_t i = 0; i<needed_libraries_count; ++i) {
- si->add_child(needed_library_si[i]);
- }
-
- if (!si->LinkImage(nullptr)) {
+ if (needed_libraries_count > 0 && !find_libraries(si, needed_library_names, needed_libraries_count, nullptr, g_ld_preloads, ld_preloads_count, RTLD_GLOBAL, nullptr)) {
__libc_format_fd(2, "CANNOT LINK EXECUTABLE: %s\n", linker_get_error_buffer());
exit(EXIT_FAILURE);
+ } else if (needed_libraries_count == 0) {
+ if (!si->link_image(g_empty_list, soinfo::soinfo_list_t::make_list(si), nullptr)) {
+ __libc_format_fd(2, "CANNOT LINK EXECUTABLE: %s\n", linker_get_error_buffer());
+ exit(EXIT_FAILURE);
+ }
+ si->increment_ref_count();
}
add_vdso(args);
- si->CallPreInitConstructors();
+ si->call_pre_init_constructors();
- /* After the PrelinkImage, the si->load_bias is initialized.
+ /* After the prelink_image, the si->load_bias is initialized.
* For so lib, the map->l_addr will be updated in notify_gdb_of_load.
* We need to update this value for so exe here. So Unwind_Backtrace
* for some arch like x86 could work correctly within so exe.
*/
map->l_addr = si->load_bias;
- si->CallConstructors();
+ si->call_constructors();
#if TIMING
gettimeofday(&t1, nullptr);
ElfW(Ehdr)* elf_hdr = reinterpret_cast<ElfW(Ehdr)*>(linker_addr);
ElfW(Phdr)* phdr = reinterpret_cast<ElfW(Phdr)*>(linker_addr + elf_hdr->e_phoff);
- soinfo linker_so("[dynamic linker]", nullptr, 0);
+ soinfo linker_so("[dynamic linker]", nullptr, 0, 0);
// If the linker is not acting as PT_INTERP entry_point is equal to
// _start. Which means that the linker is running as an executable and
linker_so.dynamic = nullptr;
linker_so.phdr = phdr;
linker_so.phnum = elf_hdr->e_phnum;
- linker_so.flags |= FLAG_LINKER;
-
- if (!(linker_so.PrelinkImage() && linker_so.LinkImage(nullptr))) {
+ linker_so.set_linker_flag();
+
+ // This might not be obvious... The reasons why we pass g_empty_list
+ // in place of local_group here are (1) we do not really need it, because
+ // linker is built with DT_SYMBOLIC and therefore relocates its symbols against
+ // itself without having to look into local_group and (2) allocators
+ // are not yet initialized, and therefore we cannot use linked_list.push_*
+ // functions at this point.
+ if (!(linker_so.prelink_image() && linker_so.link_image(g_empty_list, g_empty_list, nullptr))) {
// It would be nice to print an error message, but if the linker
// can't link itself, there's no guarantee that we'll be able to
// call write() (because it involves a GOT reference). We may as
__libc_init_tls(args);
// Initialize the linker's own global variables
- linker_so.CallConstructors();
+ linker_so.call_constructors();
// Initialize static variables. Note that in order to
// get correct libdl_info we need to call constructors