diff --git a/linker/linker.cpp b/linker/linker.cpp
index 9f458b444fda6e0763f5bb268ad070dadbb2b7c3..45889485f982a895af9195b59181b9dd3b0d6609 100644 (file)
--- a/linker/linker.cpp
+++ b/linker/linker.cpp
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
-#include <sys/atomics.h>
#include <sys/mman.h>
#include <sys/stat.h>
#include <unistd.h>
*
* open issues / todo:
*
+ * - are we doing everything we should for ARM_COPY relocations?
* - cleaner error reporting
* - after linking, set as much stuff as possible to READONLY
* and NOEXEC
}
// ...but nvidia binary blobs (at least) rely on this behavior, so fall through for now.
#if defined(__LP64__)
- // TODO: uncomment this after bug b/7465467 is fixed.
- // return -1;
+ return -1;
#endif
}
}
}
-soinfo* do_dlopen(const char* name, int flags, soinfo* caller, const android_dlextinfo* extinfo) {
+soinfo* do_dlopen(const char* name, int flags, const android_dlextinfo* extinfo) {
if ((flags & ~(RTLD_NOW|RTLD_LAZY|RTLD_LOCAL|RTLD_GLOBAL|RTLD_NOLOAD)) != 0) {
DL_ERR("invalid flags to dlopen: %x", flags);
return NULL;
@@ -841,9 +840,6 @@ soinfo* do_dlopen(const char* name, int flags, soinfo* caller, const android_dle
soinfo* si = find_library(name, flags, extinfo);
if (si != NULL) {
si->CallConstructors();
- if (caller != NULL) {
- caller->add_child(si);
- }
}
protect_data(PROT_READ);
return si;
@@ -1041,17 +1037,52 @@ static int soinfo_relocate(soinfo* si, ElfW(Rela)* rela, unsigned count, soinfo*
break;
case R_AARCH64_COPY:
- /*
- * ET_EXEC is not supported so this should not happen.
- *
- * http://infocenter.arm.com/help/topic/com.arm.doc.ihi0044d/IHI0044D_aaelf.pdf
- *
- * Section 4.7.1.10 "Dynamic relocations"
- * R_AARCH64_COPY may only appear in executable objects where e_type is
- * set to ET_EXEC.
- */
- DL_ERR("%s R_AARCH64_COPY relocations are not supported", si->name);
- return -1;
+ if ((si->flags & FLAG_EXE) == 0) {
+ /*
+ * http://infocenter.arm.com/help/topic/com.arm.doc.ihi0044d/IHI0044D_aaelf.pdf
+ *
+ * Section 4.7.1.10 "Dynamic relocations"
+ * R_AARCH64_COPY may only appear in executable objects where e_type is
+ * set to ET_EXEC.
+ *
+ * FLAG_EXE is set for both ET_DYN and ET_EXEC executables.
+ * We should explicitly disallow ET_DYN executables from having
+ * R_AARCH64_COPY relocations.
+ */
+ DL_ERR("%s R_AARCH64_COPY relocations only supported for ET_EXEC", si->name);
+ return -1;
+ }
+ count_relocation(kRelocCopy);
+ MARK(rela->r_offset);
+ TRACE_TYPE(RELO, "RELO COPY %16llx <- %lld @ %16llx %s\n",
+ reloc,
+ s->st_size,
+ (sym_addr + rela->r_addend),
+ sym_name);
+ if (reloc == (sym_addr + rela->r_addend)) {
+ ElfW(Sym)* src = soinfo_do_lookup(NULL, sym_name, &lsi, needed);
+
+ if (src == NULL) {
+ DL_ERR("%s R_AARCH64_COPY relocation source cannot be resolved", si->name);
+ return -1;
+ }
+ if (lsi->has_DT_SYMBOLIC) {
+ DL_ERR("%s invalid R_AARCH64_COPY relocation against DT_SYMBOLIC shared "
+ "library %s (built with -Bsymbolic?)", si->name, lsi->name);
+ return -1;
+ }
+ if (s->st_size < src->st_size) {
+ DL_ERR("%s R_AARCH64_COPY relocation size mismatch (%lld < %lld)",
+ si->name, s->st_size, src->st_size);
+ return -1;
+ }
+ memcpy(reinterpret_cast<void*>(reloc),
+ reinterpret_cast<void*>(src->st_value + lsi->load_bias), src->st_size);
+ } else {
+ DL_ERR("%s R_AARCH64_COPY relocation target cannot be resolved", si->name);
+ return -1;
+ }
+ break;
case R_AARCH64_TLS_TPREL64:
TRACE_TYPE(RELO, "RELO TLS_TPREL64 *** %16llx <- %16llx - %16llx\n",
reloc, (sym_addr + rela->r_addend), rela->r_offset);
@@ -1229,17 +1260,48 @@ static int soinfo_relocate(soinfo* si, ElfW(Rel)* rel, unsigned count, soinfo* n
*reinterpret_cast<ElfW(Addr)*>(reloc) += sym_addr - rel->r_offset;
break;
case R_ARM_COPY:
- /*
- * ET_EXEC is not supported so this should not happen.
- *
- * http://infocenter.arm.com/help/topic/com.arm.doc.ihi0044d/IHI0044D_aaelf.pdf
- *
- * Section 4.7.1.10 "Dynamic relocations"
- * R_ARM_COPY may only appear in executable objects where e_type is
- * set to ET_EXEC.
- */
- DL_ERR("%s R_ARM_COPY relocations are not supported", si->name);
- return -1;
+ if ((si->flags & FLAG_EXE) == 0) {
+ /*
+ * http://infocenter.arm.com/help/topic/com.arm.doc.ihi0044d/IHI0044D_aaelf.pdf
+ *
+ * Section 4.7.1.10 "Dynamic relocations"
+ * R_ARM_COPY may only appear in executable objects where e_type is
+ * set to ET_EXEC.
+ *
+ * TODO: FLAG_EXE is set for both ET_DYN and ET_EXEC executables.
+ * We should explicitly disallow ET_DYN executables from having
+ * R_ARM_COPY relocations.
+ */
+ DL_ERR("%s R_ARM_COPY relocations only supported for ET_EXEC", si->name);
+ return -1;
+ }
+ count_relocation(kRelocCopy);
+ MARK(rel->r_offset);
+ TRACE_TYPE(RELO, "RELO %08x <- %d @ %08x %s", reloc, s->st_size, sym_addr, sym_name);
+ if (reloc == sym_addr) {
+ ElfW(Sym)* src = soinfo_do_lookup(NULL, sym_name, &lsi, needed);
+
+ if (src == NULL) {
+ DL_ERR("%s R_ARM_COPY relocation source cannot be resolved", si->name);
+ return -1;
+ }
+ if (lsi->has_DT_SYMBOLIC) {
+ DL_ERR("%s invalid R_ARM_COPY relocation against DT_SYMBOLIC shared "
+ "library %s (built with -Bsymbolic?)", si->name, lsi->name);
+ return -1;
+ }
+ if (s->st_size < src->st_size) {
+ DL_ERR("%s R_ARM_COPY relocation size mismatch (%d < %d)",
+ si->name, s->st_size, src->st_size);
+ return -1;
+ }
+ memcpy(reinterpret_cast<void*>(reloc),
+ reinterpret_cast<void*>(src->st_value + lsi->load_bias), src->st_size);
+ } else {
+ DL_ERR("%s R_ARM_COPY relocation target cannot be resolved", si->name);
+ return -1;
+ }
+ break;
#elif defined(__i386__)
case R_386_JMP_SLOT:
count_relocation(kRelocAbsolute);
@@ -1867,10 +1929,8 @@ static bool soinfo_link_image(soinfo* si, const android_dlextinfo* extinfo) {
if (si->has_text_relocations) {
// Make segments writable to allow text relocations to work properly. We will later call
// phdr_table_protect_segments() after all of them are applied and all constructors are run.
-#if !defined(__i386__) // The platform itself has too many text relocations on x86.
DL_WARN("%s has text relocations. This is wasting memory and prevents "
"security hardening. Please fix.", si->name);
-#endif
if (phdr_table_unprotect_segments(si->phdr, si->phnum, si->load_bias) < 0) {
DL_ERR("can't unprotect loadable segments for \"%s\": %s",
si->name, strerror(errno));
@@ -2109,11 +2169,13 @@ static ElfW(Addr) __linker_init_post_relocation(KernelArgumentBlock& args, ElfW(
si->dynamic = NULL;
si->ref_count = 1;
+#if defined(__LP64__)
ElfW(Ehdr)* elf_hdr = reinterpret_cast<ElfW(Ehdr)*>(si->base);
if (elf_hdr->e_type != ET_DYN) {
__libc_format_fd(2, "error: only position independent executables (PIE) are supported.\n");
exit(EXIT_FAILURE);
}
+#endif
// Use LD_LIBRARY_PATH and LD_PRELOAD (but only if we aren't setuid/setgid).
parse_LD_LIBRARY_PATH(ldpath_env);