diff --git a/linker/linker.h b/linker/linker.h
index 21ecb225aae3f92669b4452ec91120b042b26a1c..f7aa11c70747c586bc2cb10631745792625493c3 100644 (file)
--- a/linker/linker.h
+++ b/linker/linker.h
#endif
soinfo* next;
- uint32_t flags;
-
private:
- const char* strtab;
- ElfW(Sym)* symtab;
+ uint32_t flags_;
- size_t nbucket;
- size_t nchain;
- uint32_t* bucket;
- uint32_t* chain;
+ const char* strtab_;
+ ElfW(Sym)* symtab_;
+
+ size_t nbucket_;
+ size_t nchain_;
+ uint32_t* bucket_;
+ uint32_t* chain_;
- public:
#if defined(__mips__) || !defined(__LP64__)
// This is only used by mips and mips64, but needs to be here for
// all 32-bit architectures to preserve binary compatibility.
- ElfW(Addr)** plt_got;
+ ElfW(Addr)** plt_got_;
#endif
#if defined(USE_RELA)
- ElfW(Rela)* plt_rela;
- size_t plt_rela_count;
+ ElfW(Rela)* plt_rela_;
+ size_t plt_rela_count_;
- ElfW(Rela)* rela;
- size_t rela_count;
+ ElfW(Rela)* rela_;
+ size_t rela_count_;
#else
- ElfW(Rel)* plt_rel;
- size_t plt_rel_count;
+ ElfW(Rel)* plt_rel_;
+ size_t plt_rel_count_;
- ElfW(Rel)* rel;
- size_t rel_count;
+ ElfW(Rel)* rel_;
+ size_t rel_count_;
#endif
- linker_function_t* preinit_array;
- size_t preinit_array_count;
+ linker_function_t* preinit_array_;
+ size_t preinit_array_count_;
- linker_function_t* init_array;
- size_t init_array_count;
- linker_function_t* fini_array;
- size_t fini_array_count;
+ linker_function_t* init_array_;
+ size_t init_array_count_;
+ linker_function_t* fini_array_;
+ size_t fini_array_count_;
- linker_function_t init_func;
- linker_function_t fini_func;
+ linker_function_t init_func_;
+ linker_function_t fini_func_;
#if defined(__arm__)
+ public:
// ARM EABI section used for stack unwinding.
uint32_t* ARM_exidx;
size_t ARM_exidx_count;
-#elif defined(__mips__)
private:
- uint32_t mips_symtabno;
- uint32_t mips_local_gotno;
- uint32_t mips_gotsym;
+#elif defined(__mips__)
+ uint32_t mips_symtabno_;
+ uint32_t mips_local_gotno_;
+ uint32_t mips_gotsym_;
bool mips_relocate_got(const soinfo_list_t& global_group, const soinfo_list_t& local_group);
- public:
#endif
-
- size_t ref_count;
+ size_t ref_count_;
+ public:
link_map link_map_head;
bool constructors_called;
#endif
bool has_DT_SYMBOLIC;
+ public:
soinfo(const char* name, const struct stat* file_stat, off64_t file_offset, int rtld_flags);
- void CallConstructors();
- void CallDestructors();
- void CallPreInitConstructors();
- bool PrelinkImage();
- bool LinkImage(const soinfo_list_t& global_group, const soinfo_list_t& local_group, const android_dlextinfo* extinfo);
+ void call_constructors();
+ void call_destructors();
+ void call_pre_init_constructors();
+ bool prelink_image();
+ bool link_image(const soinfo_list_t& global_group, const soinfo_list_t& local_group, const android_dlextinfo* extinfo);
void add_child(soinfo* child);
void remove_all_links();
bool is_gnu_hash() const;
bool inline has_min_version(uint32_t min_version) const {
- return (flags & FLAG_NEW_SOINFO) != 0 && version >= min_version;
+ return (flags_ & FLAG_NEW_SOINFO) != 0 && version_ >= min_version;
}
+ bool is_linked() const;
+ bool is_main_executable() const;
+
+ void set_linked();
+ void set_linker_flag();
+ void set_main_executable();
+
+ void increment_ref_count();
+ size_t decrement_ref_count();
+
+ soinfo* get_local_group_root() const;
+
private:
ElfW(Sym)* elf_lookup(SymbolName& symbol_name);
ElfW(Sym)* elf_addr_lookup(const void* addr);
ElfW(Sym)* gnu_lookup(SymbolName& symbol_name);
ElfW(Sym)* gnu_addr_lookup(const void* addr);
- void CallArray(const char* array_name, linker_function_t* functions, size_t count, bool reverse);
- void CallFunction(const char* function_name, linker_function_t function);
+ void call_array(const char* array_name, linker_function_t* functions, size_t count, bool reverse);
+ void call_function(const char* function_name, linker_function_t function);
#if defined(USE_RELA)
- int Relocate(ElfW(Rela)* rela, unsigned count, const soinfo_list_t& global_group, const soinfo_list_t& local_group);
+ int relocate(ElfW(Rela)* rela, unsigned count, const soinfo_list_t& global_group, const soinfo_list_t& local_group);
#else
- int Relocate(ElfW(Rel)* rel, unsigned count, const soinfo_list_t& global_group, const soinfo_list_t& local_group);
+ int relocate(ElfW(Rel)* rel, unsigned count, const soinfo_list_t& global_group, const soinfo_list_t& local_group);
#endif
private:
// This part of the structure is only available
// when FLAG_NEW_SOINFO is set in this->flags.
- uint32_t version;
+ uint32_t version_;
// version >= 0
- dev_t st_dev;
- ino_t st_ino;
+ dev_t st_dev_;
+ ino_t st_ino_;
// dependency graph
- soinfo_list_t children;
- soinfo_list_t parents;
+ soinfo_list_t children_;
+ soinfo_list_t parents_;
// version >= 1
- off64_t file_offset;
- uint32_t rtld_flags;
- uint32_t dt_flags_1;
- size_t strtab_size;
+ off64_t file_offset_;
+ uint32_t rtld_flags_;
+ uint32_t dt_flags_1_;
+ size_t strtab_size_;
// version >= 2
- uint32_t gnu_maskwords;
- uint32_t gnu_shift2;
+ uint32_t gnu_maskwords_;
+ uint32_t gnu_shift2_;
+ ElfW(Addr)* gnu_bloom_filter_;
- ElfW(Addr)* gnu_bloom_filter;
+ soinfo* local_group_root_;
friend soinfo* get_libdl_info();
};