diff --git a/linker/linker.h b/linker/linker.h
index 28969332d51ad732939d9289a9c30fad65406846..f7aa11c70747c586bc2cb10631745792625493c3 100644 (file)
--- a/linker/linker.h
+++ b/linker/linker.h
#define FLAG_LINKED 0x00000001
#define FLAG_EXE 0x00000004 // The main executable
#define FLAG_LINKER 0x00000010 // The linker itself
+#define FLAG_GNU_HASH 0x00000040 // uses gnu hash
#define FLAG_NEW_SOINFO 0x40000000 // new soinfo format
+#define SUPPORTED_DT_FLAGS_1 (DF_1_NOW | DF_1_GLOBAL | DF_1_NODELETE)
+
#define SOINFO_VERSION 1
#define SOINFO_NAME_LEN 128
struct soinfo;
class SoinfoListAllocator {
-public:
+ public:
static LinkedListEntry<soinfo>* alloc();
static void free(LinkedListEntry<soinfo>* entry);
-private:
+
+ private:
// unconstructable
DISALLOW_IMPLICIT_CONSTRUCTORS(SoinfoListAllocator);
};
+class SymbolName {
+ public:
+ explicit SymbolName(const char* name)
+ : name_(name), has_elf_hash_(false), has_gnu_hash_(false),
+ elf_hash_(0), gnu_hash_(0) { }
+
+ const char* get_name() {
+ return name_;
+ }
+
+ uint32_t elf_hash();
+ uint32_t gnu_hash();
+
+ private:
+ const char* name_;
+ bool has_elf_hash_;
+ bool has_gnu_hash_;
+ uint32_t elf_hash_;
+ uint32_t gnu_hash_;
+
+ DISALLOW_IMPLICIT_CONSTRUCTORS(SymbolName);
+};
+
struct soinfo {
public:
typedef LinkedList<soinfo, SoinfoListAllocator> soinfo_list_t;
#endif
soinfo* next;
- unsigned flags;
+ private:
+ uint32_t flags_;
- const char* strtab;
- ElfW(Sym)* symtab;
+ const char* strtab_;
+ ElfW(Sym)* symtab_;
- size_t nbucket;
- size_t nchain;
- unsigned* bucket;
- unsigned* chain;
+ size_t nbucket_;
+ size_t nchain_;
+ uint32_t* bucket_;
+ uint32_t* chain_;
#if defined(__mips__) || !defined(__LP64__)
// This is only used by mips and mips64, but needs to be here for
// all 32-bit architectures to preserve binary compatibility.
- ElfW(Addr)** plt_got;
+ ElfW(Addr)** plt_got_;
#endif
#if defined(USE_RELA)
- ElfW(Rela)* plt_rela;
- size_t plt_rela_count;
+ ElfW(Rela)* plt_rela_;
+ size_t plt_rela_count_;
- ElfW(Rela)* rela;
- size_t rela_count;
+ ElfW(Rela)* rela_;
+ size_t rela_count_;
#else
- ElfW(Rel)* plt_rel;
- size_t plt_rel_count;
+ ElfW(Rel)* plt_rel_;
+ size_t plt_rel_count_;
- ElfW(Rel)* rel;
- size_t rel_count;
+ ElfW(Rel)* rel_;
+ size_t rel_count_;
#endif
- linker_function_t* preinit_array;
- size_t preinit_array_count;
+ linker_function_t* preinit_array_;
+ size_t preinit_array_count_;
- linker_function_t* init_array;
- size_t init_array_count;
- linker_function_t* fini_array;
- size_t fini_array_count;
+ linker_function_t* init_array_;
+ size_t init_array_count_;
+ linker_function_t* fini_array_;
+ size_t fini_array_count_;
- linker_function_t init_func;
- linker_function_t fini_func;
+ linker_function_t init_func_;
+ linker_function_t fini_func_;
#if defined(__arm__)
+ public:
// ARM EABI section used for stack unwinding.
- unsigned* ARM_exidx;
+ uint32_t* ARM_exidx;
size_t ARM_exidx_count;
+ private:
#elif defined(__mips__)
- unsigned mips_symtabno;
- unsigned mips_local_gotno;
- unsigned mips_gotsym;
-#endif
+ uint32_t mips_symtabno_;
+ uint32_t mips_local_gotno_;
+ uint32_t mips_gotsym_;
+ bool mips_relocate_got(const soinfo_list_t& global_group, const soinfo_list_t& local_group);
- size_t ref_count;
+#endif
+ size_t ref_count_;
+ public:
link_map link_map_head;
bool constructors_called;
#endif
bool has_DT_SYMBOLIC;
- soinfo(const char* name, const struct stat* file_stat, int rtld_flags);
+ public:
+ soinfo(const char* name, const struct stat* file_stat, off64_t file_offset, int rtld_flags);
- void CallConstructors();
- void CallDestructors();
- void CallPreInitConstructors();
- bool PrelinkImage();
- bool LinkImage(const android_dlextinfo* extinfo);
+ void call_constructors();
+ void call_destructors();
+ void call_pre_init_constructors();
+ bool prelink_image();
+ bool link_image(const soinfo_list_t& global_group, const soinfo_list_t& local_group, const android_dlextinfo* extinfo);
void add_child(soinfo* child);
void remove_all_links();
- void set_st_dev(dev_t st_dev);
- void set_st_ino(ino_t st_ino);
- ino_t get_st_ino();
- dev_t get_st_dev();
+ ino_t get_st_ino() const;
+ dev_t get_st_dev() const;
+ off64_t get_file_offset() const;
- int get_rtld_flags();
+ uint32_t get_rtld_flags() const;
+ uint32_t get_dt_flags_1() const;
+ void set_dt_flags_1(uint32_t dt_flags_1);
soinfo_list_t& get_children();
soinfo_list_t& get_parents();
+ ElfW(Sym)* find_symbol_by_name(SymbolName& symbol_name);
+ ElfW(Sym)* find_symbol_by_address(const void* addr);
ElfW(Addr) resolve_symbol_address(ElfW(Sym)* s);
- bool inline has_min_version(uint32_t min_version) {
- return (flags & FLAG_NEW_SOINFO) != 0 && version >= min_version;
+ const char* get_string(ElfW(Word) index) const;
+ bool can_unload() const;
+ bool is_gnu_hash() const;
+
+ bool inline has_min_version(uint32_t min_version) const {
+ return (flags_ & FLAG_NEW_SOINFO) != 0 && version_ >= min_version;
}
+
+ bool is_linked() const;
+ bool is_main_executable() const;
+
+ void set_linked();
+ void set_linker_flag();
+ void set_main_executable();
+
+ void increment_ref_count();
+ size_t decrement_ref_count();
+
+ soinfo* get_local_group_root() const;
+
private:
- void CallArray(const char* array_name, linker_function_t* functions, size_t count, bool reverse);
- void CallFunction(const char* function_name, linker_function_t function);
+ ElfW(Sym)* elf_lookup(SymbolName& symbol_name);
+ ElfW(Sym)* elf_addr_lookup(const void* addr);
+ ElfW(Sym)* gnu_lookup(SymbolName& symbol_name);
+ ElfW(Sym)* gnu_addr_lookup(const void* addr);
+
+ void call_array(const char* array_name, linker_function_t* functions, size_t count, bool reverse);
+ void call_function(const char* function_name, linker_function_t function);
#if defined(USE_RELA)
- int Relocate(ElfW(Rela)* rela, unsigned count);
+ int relocate(ElfW(Rela)* rela, unsigned count, const soinfo_list_t& global_group, const soinfo_list_t& local_group);
#else
- int Relocate(ElfW(Rel)* rel, unsigned count);
+ int relocate(ElfW(Rel)* rel, unsigned count, const soinfo_list_t& global_group, const soinfo_list_t& local_group);
#endif
private:
// This part of the structure is only available
// when FLAG_NEW_SOINFO is set in this->flags.
- uint32_t version;
+ uint32_t version_;
// version >= 0
- dev_t st_dev;
- ino_t st_ino;
+ dev_t st_dev_;
+ ino_t st_ino_;
// dependency graph
- soinfo_list_t children;
- soinfo_list_t parents;
+ soinfo_list_t children_;
+ soinfo_list_t parents_;
// version >= 1
- int rtld_flags;
+ off64_t file_offset_;
+ uint32_t rtld_flags_;
+ uint32_t dt_flags_1_;
+ size_t strtab_size_;
+
+ // version >= 2
+ uint32_t gnu_maskwords_;
+ uint32_t gnu_shift2_;
+ ElfW(Addr)* gnu_bloom_filter_;
+
+ soinfo* local_group_root_;
+
+ friend soinfo* get_libdl_info();
};
-extern soinfo* get_libdl_info();
+soinfo* get_libdl_info();
void do_android_get_LD_LIBRARY_PATH(char*, size_t);
void do_android_update_LD_LIBRARY_PATH(const char* ld_library_path);
ElfW(Sym)* dlsym_linear_lookup(const char* name, soinfo** found, soinfo* start);
soinfo* find_containing_library(const void* addr);
-ElfW(Sym)* dladdr_find_symbol(soinfo* si, const void* addr);
ElfW(Sym)* dlsym_handle_lookup(soinfo* si, soinfo** found, const char* name);
void debuggerd_init();