diff --git a/linker/linker.h b/linker/linker.h
index d28f70e148e3ee2084cf7ae2fb60955096dba357..f7aa11c70747c586bc2cb10631745792625493c3 100644 (file)
--- a/linker/linker.h
+++ b/linker/linker.h
#endif
soinfo* next;
- uint32_t flags;
-
private:
+ uint32_t flags_;
+
const char* strtab_;
ElfW(Sym)* symtab_;
linker_function_t init_func_;
linker_function_t fini_func_;
- public:
#if defined(__arm__)
+ public:
// ARM EABI section used for stack unwinding.
uint32_t* ARM_exidx;
size_t ARM_exidx_count;
-#elif defined(__mips__)
private:
+#elif defined(__mips__)
uint32_t mips_symtabno_;
uint32_t mips_local_gotno_;
uint32_t mips_gotsym_;
bool mips_relocate_got(const soinfo_list_t& global_group, const soinfo_list_t& local_group);
#endif
-
+ size_t ref_count_;
public:
- size_t ref_count;
link_map link_map_head;
bool constructors_called;
bool is_gnu_hash() const;
bool inline has_min_version(uint32_t min_version) const {
- return (flags & FLAG_NEW_SOINFO) != 0 && version_ >= min_version;
+ return (flags_ & FLAG_NEW_SOINFO) != 0 && version_ >= min_version;
}
+ bool is_linked() const;
+ bool is_main_executable() const;
+
+ void set_linked();
+ void set_linker_flag();
+ void set_main_executable();
+
+ void increment_ref_count();
+ size_t decrement_ref_count();
+
+ soinfo* get_local_group_root() const;
+
private:
ElfW(Sym)* elf_lookup(SymbolName& symbol_name);
ElfW(Sym)* elf_addr_lookup(const void* addr);
// version >= 2
uint32_t gnu_maskwords_;
uint32_t gnu_shift2_;
-
ElfW(Addr)* gnu_bloom_filter_;
+ soinfo* local_group_root_;
+
friend soinfo* get_libdl_info();
};