]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/platform-bionic.git/blobdiff - linker/linker.h
Support gethostbyname_r_ERANGE.
[android-sdk/platform-bionic.git] / linker / linker.h
index f6e3a48bad839ca11f2fe4f1de4d24d3503a8bfb..f7aa11c70747c586bc2cb10631745792625493c3 100644 (file)
 #define FLAG_LINKED     0x00000001
 #define FLAG_EXE        0x00000004 // The main executable
 #define FLAG_LINKER     0x00000010 // The linker itself
+#define FLAG_GNU_HASH   0x00000040 // uses gnu hash
 #define FLAG_NEW_SOINFO 0x40000000 // new soinfo format
 
+#define SUPPORTED_DT_FLAGS_1 (DF_1_NOW | DF_1_GLOBAL | DF_1_NODELETE)
+
 #define SOINFO_VERSION 1
 
 #define SOINFO_NAME_LEN 128
@@ -103,14 +106,38 @@ typedef void (*linker_function_t)();
 struct soinfo;
 
 class SoinfoListAllocator {
-public:
+ public:
   static LinkedListEntry<soinfo>* alloc();
   static void free(LinkedListEntry<soinfo>* entry);
-private:
+
+ private:
   // unconstructable
   DISALLOW_IMPLICIT_CONSTRUCTORS(SoinfoListAllocator);
 };
 
+class SymbolName {
+ public:
+  explicit SymbolName(const char* name)
+      : name_(name), has_elf_hash_(false), has_gnu_hash_(false),
+        elf_hash_(0), gnu_hash_(0) { }
+
+  const char* get_name() {
+    return name_;
+  }
+
+  uint32_t elf_hash();
+  uint32_t gnu_hash();
+
+ private:
+  const char* name_;
+  bool has_elf_hash_;
+  bool has_gnu_hash_;
+  uint32_t elf_hash_;
+  uint32_t gnu_hash_;
+
+  DISALLOW_IMPLICIT_CONSTRUCTORS(SymbolName);
+};
+
 struct soinfo {
  public:
   typedef LinkedList<soinfo, SoinfoListAllocator> soinfo_list_t;
@@ -134,60 +161,63 @@ struct soinfo {
 #endif
 
   soinfo* next;
-  unsigned flags;
-
  private:
-  const char* strtab;
- public:
-  ElfW(Sym)* symtab;
+  uint32_t flags_;
 
-  size_t nbucket;
-  size_t nchain;
-  unsigned* bucket;
-  unsigned* chain;
+  const char* strtab_;
+  ElfW(Sym)* symtab_;
+
+  size_t nbucket_;
+  size_t nchain_;
+  uint32_t* bucket_;
+  uint32_t* chain_;
 
 #if defined(__mips__) || !defined(__LP64__)
   // This is only used by mips and mips64, but needs to be here for
   // all 32-bit architectures to preserve binary compatibility.
-  ElfW(Addr)** plt_got;
+  ElfW(Addr)** plt_got_;
 #endif
 
 #if defined(USE_RELA)
-  ElfW(Rela)* plt_rela;
-  size_t plt_rela_count;
+  ElfW(Rela)* plt_rela_;
+  size_t plt_rela_count_;
 
-  ElfW(Rela)* rela;
-  size_t rela_count;
+  ElfW(Rela)* rela_;
+  size_t rela_count_;
 #else
-  ElfW(Rel)* plt_rel;
-  size_t plt_rel_count;
+  ElfW(Rel)* plt_rel_;
+  size_t plt_rel_count_;
 
-  ElfW(Rel)* rel;
-  size_t rel_count;
+  ElfW(Rel)* rel_;
+  size_t rel_count_;
 #endif
 
-  linker_function_t* preinit_array;
-  size_t preinit_array_count;
+  linker_function_t* preinit_array_;
+  size_t preinit_array_count_;
 
-  linker_function_t* init_array;
-  size_t init_array_count;
-  linker_function_t* fini_array;
-  size_t fini_array_count;
+  linker_function_t* init_array_;
+  size_t init_array_count_;
+  linker_function_t* fini_array_;
+  size_t fini_array_count_;
 
-  linker_function_t init_func;
-  linker_function_t fini_func;
+  linker_function_t init_func_;
+  linker_function_t fini_func_;
 
 #if defined(__arm__)
+ public:
   // ARM EABI section used for stack unwinding.
-  unsigned* ARM_exidx;
+  uint32_t* ARM_exidx;
   size_t ARM_exidx_count;
+ private:
 #elif defined(__mips__)
-  unsigned mips_symtabno;
-  unsigned mips_local_gotno;
-  unsigned mips_gotsym;
-#endif
+  uint32_t mips_symtabno_;
+  uint32_t mips_local_gotno_;
+  uint32_t mips_gotsym_;
+  bool mips_relocate_got(const soinfo_list_t& global_group, const soinfo_list_t& local_group);
 
-  size_t ref_count;
+#endif
+  size_t ref_count_;
+ public:
   link_map link_map_head;
 
   bool constructors_called;
@@ -201,64 +231,97 @@ struct soinfo {
 #endif
   bool has_DT_SYMBOLIC;
 
-  soinfo(const char* name, const struct stat* file_stat, int rtld_flags);
+ public:
+  soinfo(const char* name, const struct stat* file_stat, off64_t file_offset, int rtld_flags);
 
-  void CallConstructors();
-  void CallDestructors();
-  void CallPreInitConstructors();
-  bool PrelinkImage();
-  bool LinkImage(const android_dlextinfo* extinfo);
+  void call_constructors();
+  void call_destructors();
+  void call_pre_init_constructors();
+  bool prelink_image();
+  bool link_image(const soinfo_list_t& global_group, const soinfo_list_t& local_group, const android_dlextinfo* extinfo);
 
   void add_child(soinfo* child);
   void remove_all_links();
 
-  void set_st_dev(dev_t st_dev);
-  void set_st_ino(ino_t st_ino);
-  ino_t get_st_ino();
-  dev_t get_st_dev();
+  ino_t get_st_ino() const;
+  dev_t get_st_dev() const;
+  off64_t get_file_offset() const;
 
-  int get_rtld_flags();
+  uint32_t get_rtld_flags() const;
+  uint32_t get_dt_flags_1() const;
+  void set_dt_flags_1(uint32_t dt_flags_1);
 
   soinfo_list_t& get_children();
   soinfo_list_t& get_parents();
 
+  ElfW(Sym)* find_symbol_by_name(SymbolName& symbol_name);
+  ElfW(Sym)* find_symbol_by_address(const void* addr);
   ElfW(Addr) resolve_symbol_address(ElfW(Sym)* s);
 
   const char* get_string(ElfW(Word) index) const;
+  bool can_unload() const;
+  bool is_gnu_hash() const;
 
   bool inline has_min_version(uint32_t min_version) const {
-    return (flags & FLAG_NEW_SOINFO) != 0 && version >= min_version;
+    return (flags_ & FLAG_NEW_SOINFO) != 0 && version_ >= min_version;
   }
+
+  bool is_linked() const;
+  bool is_main_executable() const;
+
+  void set_linked();
+  void set_linker_flag();
+  void set_main_executable();
+
+  void increment_ref_count();
+  size_t decrement_ref_count();
+
+  soinfo* get_local_group_root() const;
+
  private:
-  void CallArray(const char* array_name, linker_function_t* functions, size_t count, bool reverse);
-  void CallFunction(const char* function_name, linker_function_t function);
+  ElfW(Sym)* elf_lookup(SymbolName& symbol_name);
+  ElfW(Sym)* elf_addr_lookup(const void* addr);
+  ElfW(Sym)* gnu_lookup(SymbolName& symbol_name);
+  ElfW(Sym)* gnu_addr_lookup(const void* addr);
+
+  void call_array(const char* array_name, linker_function_t* functions, size_t count, bool reverse);
+  void call_function(const char* function_name, linker_function_t function);
 #if defined(USE_RELA)
-  int Relocate(ElfW(Rela)* rela, unsigned count);
+  int relocate(ElfW(Rela)* rela, unsigned count, const soinfo_list_t& global_group, const soinfo_list_t& local_group);
 #else
-  int Relocate(ElfW(Rel)* rel, unsigned count);
+  int relocate(ElfW(Rel)* rel, unsigned count, const soinfo_list_t& global_group, const soinfo_list_t& local_group);
 #endif
 
  private:
   // This part of the structure is only available
   // when FLAG_NEW_SOINFO is set in this->flags.
-  uint32_t version;
+  uint32_t version_;
 
   // version >= 0
-  dev_t st_dev;
-  ino_t st_ino;
+  dev_t st_dev_;
+  ino_t st_ino_;
 
   // dependency graph
-  soinfo_list_t children;
-  soinfo_list_t parents;
+  soinfo_list_t children_;
+  soinfo_list_t parents_;
 
   // version >= 1
-  int rtld_flags;
-  size_t strtab_size;
+  off64_t file_offset_;
+  uint32_t rtld_flags_;
+  uint32_t dt_flags_1_;
+  size_t strtab_size_;
+
+  // version >= 2
+  uint32_t gnu_maskwords_;
+  uint32_t gnu_shift2_;
+  ElfW(Addr)* gnu_bloom_filter_;
+
+  soinfo* local_group_root_;
 
   friend soinfo* get_libdl_info();
 };
 
-extern soinfo* get_libdl_info();
+soinfo* get_libdl_info();
 
 void do_android_get_LD_LIBRARY_PATH(char*, size_t);
 void do_android_update_LD_LIBRARY_PATH(const char* ld_library_path);
@@ -268,7 +331,6 @@ void do_dlclose(soinfo* si);
 ElfW(Sym)* dlsym_linear_lookup(const char* name, soinfo** found, soinfo* start);
 soinfo* find_containing_library(const void* addr);
 
-ElfW(Sym)* dladdr_find_symbol(soinfo* si, const void* addr);
 ElfW(Sym)* dlsym_handle_lookup(soinfo* si, soinfo** found, const char* name);
 
 void debuggerd_init();