]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/platform-bionic.git/blobdiff - linker/linker_phdr.cpp
Support gethostbyname_r_ERANGE.
[android-sdk/platform-bionic.git] / linker / linker_phdr.cpp
index 44c8e9e705d6abc85905bc8f97b812f81db5d8dd..ffd4de28a8e670043c382e289b82a8abbec77a56 100644 (file)
@@ -29,7 +29,6 @@
 #include "linker_phdr.h"
 
 #include <errno.h>
-#include <machine/exec.h>
 #include <sys/mman.h>
 #include <sys/types.h>
 #include <sys/stat.h>
 #include "linker.h"
 #include "linker_debug.h"
 
+static int GetTargetElfMachine() {
+#if defined(__arm__)
+  return EM_ARM;
+#elif defined(__aarch64__)
+  return EM_AARCH64;
+#elif defined(__i386__)
+  return EM_386;
+#elif defined(__mips__)
+  return EM_MIPS;
+#elif defined(__x86_64__)
+  return EM_X86_64;
+#endif
+}
+
 /**
   TECHNICAL NOTE ON ELF LOADING.
 
                                       MAYBE_MAP_FLAG((x), PF_R, PROT_READ) | \
                                       MAYBE_MAP_FLAG((x), PF_W, PROT_WRITE))
 
-ElfReader::ElfReader(const char* name, int fd)
-    : name_(name), fd_(fd),
+ElfReader::ElfReader(const char* name, int fd, off64_t file_offset)
+    : name_(name), fd_(fd), file_offset_(file_offset),
       phdr_num_(0), phdr_mmap_(nullptr), phdr_table_(nullptr), phdr_size_(0),
       load_start_(nullptr), load_size_(0), load_bias_(0),
       loaded_phdr_(nullptr) {
@@ -142,11 +155,12 @@ bool ElfReader::Load(const android_dlextinfo* extinfo) {
 }
 
 bool ElfReader::ReadElfHeader() {
-  ssize_t rc = TEMP_FAILURE_RETRY(read(fd_, &header_, sizeof(header_)));
+  ssize_t rc = TEMP_FAILURE_RETRY(pread64(fd_, &header_, sizeof(header_), file_offset_));
   if (rc < 0) {
     DL_ERR("can't read file \"%s\": %s", name_, strerror(errno));
     return false;
   }
+
   if (rc != sizeof(header_)) {
     DL_ERR("\"%s\" is too small to be an ELF executable: only found %zd bytes", name_,
            static_cast<size_t>(rc));
@@ -199,7 +213,7 @@ bool ElfReader::VerifyElfHeader() {
     return false;
   }
 
-  if (header_.e_machine != ELF_TARG_MACH) {
+  if (header_.e_machine != GetTargetElfMachine()) {
     DL_ERR("\"%s\" has unexpected e_machine: %d", name_, header_.e_machine);
     return false;
   }
@@ -225,7 +239,7 @@ bool ElfReader::ReadProgramHeader() {
 
   phdr_size_ = page_max - page_min;
 
-  void* mmap_result = mmap(nullptr, phdr_size_, PROT_READ, MAP_PRIVATE, fd_, page_min);
+  void* mmap_result = mmap64(nullptr, phdr_size_, PROT_READ, MAP_PRIVATE, fd_, file_offset_ + page_min);
   if (mmap_result == MAP_FAILED) {
     DL_ERR("\"%s\" phdr mmap failed: %s", name_, strerror(errno));
     return false;
@@ -356,12 +370,12 @@ bool ElfReader::LoadSegments() {
     ElfW(Addr) file_length = file_end - file_page_start;
 
     if (file_length != 0) {
-      void* seg_addr = mmap(reinterpret_cast<void*>(seg_page_start),
+      void* seg_addr = mmap64(reinterpret_cast<void*>(seg_page_start),
                             file_length,
                             PFLAGS_TO_PROT(phdr->p_flags),
                             MAP_FIXED|MAP_PRIVATE,
                             fd_,
-                            file_page_start);
+                            file_offset_ + file_page_start);
       if (seg_addr == MAP_FAILED) {
         DL_ERR("couldn't map \"%s\" segment %zd: %s", name_, i, strerror(errno));
         return false;
@@ -721,9 +735,9 @@ void phdr_table_get_dynamic_section(const ElfW(Phdr)* phdr_table, size_t phdr_co
   }
 }
 
-// Returns the address of the program header table as it appears in the loaded
-// segments in memory. This is in contrast with 'phdr_table_' which
-// is temporary and will be released before the library is relocated.
+// Sets loaded_phdr_ to the address of the program header table as it appears
+// in the loaded segments in memory. This is in contrast with phdr_table_,
+// which is temporary and will be released before the library is relocated.
 bool ElfReader::FindPhdr() {
   const ElfW(Phdr)* phdr_limit = phdr_table_ + phdr_num_;